# oakctl tool

`oakctl` is a command-line tool for OAK cameras. It can create, deploy, and manage apps on OAK4 devices and self-hosted systems
running `oak-agent`. It also provides [RVC2 device
management](https://docs.luxonis.com/software-v3/depthai/depthai-components/bootloader.md) through `oakctl rvc2`.

Note that oak-agent is pre-installed on OAK4 devices (it's baked into the [Luxonis
OS](https://docs.luxonis.com/software-v3/sw-stack/luxonis-os.md)), so you can start using `oakctl` right away.

## Installation

#### Linux/MacOS

On 64bit system, run:

```bash
bash -c "$(curl -fsSL https://oakctl-releases.luxonis.com/oakctl-installer.sh)"
```

#### Windows

Download and install using the [Windows
Installer](https://oakctl-releases.luxonis.com/data/latest/windows_x86_64/oakctl-installer.exe).

## Update

You can update the `oakctl` tool later like this:

```bash
oakctl self-update
```

> **Problems updating on Windows**
> If you have problems updating the oakctl version on Windows, download the installer from [here](https://oakctl-releases.luxonis.com/data/latest/windows_x86_64/oakctl.msi).

## USB Internet Sharing

> **Version note**
> `oakctl v0.22.0` and `Luxonis OS 1.32.0` or newer is required for USB Internet sharing.

If your OAK4 is connected over USB and needs access to the internet, you can share your host computer's internet connection to the
device with `oakctl usbd`. This is useful for workflows such as `oakctl app run`, `oakctl app build`, working with hub, updating
the device OS, and any other operation which requires an internet connection.

When enabled, the `oakctl-usbd` background service watches for supported OAK USB Ethernet interfaces and configures the host-side
networking automatically, including interface addressing, IP forwarding, and NAT. On Linux, it also installs a udev rule so
`NetworkManager` and `systemd-networkd` do not take control of the OAK4 USB Ethernet interface.

`oakctl usbd` is opt-in and disabled by default.

### Enable `oakctl usbd`

```bash
oakctl usbd enable
```

This installs the service if needed, enables it, and starts it. The command requires elevated privileges, so `oakctl` may prompt
for administrator or root access.

> **Windows limitation**
> On Windows, `oakctl-usbd` can share the internet with only one OAK4 device at a time. When multiple devices are connected, use `oakctl usbd status` to see which device is selected and `oakctl usbd share-to <device>` to select a different one. `<device>` can be a device serial number or a USB location such as `usb:0-1.4`. Use `oakctl usbd share-to auto` to restore automatic selection.

You can check whether the service is enabled and see the sharing state of connected devices:

```bash
oakctl usbd status
```

### Disable `oakctl usbd`

```bash
oakctl usbd disable
```

This stops the service and disables it.

## Usage

### Connect to a device

If only one device is available within the network, you can connect to it with the following command:

```bash
oakctl connect
```

If you have multiple devices or the device is not in the same network as your PC, you can specify the device's IPv4 address to
connect to it:

```bash
oakctl connect 10.0.1.24
```

Optionally, you can store your device's password using `--with-password` flag. This will prevent you from entering the password
every time the session expires.

A connection to a device can be inspected using `oakctl device connection get`, or cleared with `oakctl device connection unset`.

### Find devices

`oakctl` allows you to interact with your devices that have oak-agent installed. You can list all available devices (found on your
network) with the following command:

```bash
oakctl list
+---+---------------+---------------+------------+----------------+---------------+-------+
| # | Serial Number | Device        | Connection | OS             | Agent Version | Setup |
+=========================================================================================+
| 1 | 1623452492    | Luxonis, Inc. | 10.0.1.24  | OS RVC4 1.18.0 | 0.13.7        | OK    |
|   |               |  OAK4-D R7    |            |                |               |       |
+---+---------------+---------------+------------+----------------+---------------+-------+
```

When oakctl asks you to choose between several devices, the highlighted device's status LED turns white so you can tell which
camera is which. To stop others on the network from lighting the LED, add `dl=n` to the agent configuration during
[setup](https://docs.luxonis.com/hardware/platform/deploy/oak4-deployment-guide/oak4-advanced.md), for example `oakctl device
setup apply --agent-config "dl=n"`.

### App Development

You can run the app with the command below:

```bash
oakctl app run /app/path/to/source
```

By default, `oakctl app run` uses `oakapp.toml` from the provided app directory. Use `--oakapp-file` to select an alternative
config file (for example `oakapp.dev.toml` or `oakapp.prod.toml`), as long as that file is inside the same app directory tree.

#### Optional flags:

| Flag | Description |
| --- | --- |
| `-b, --detach` | Run the app in detached mode. You can stop it with `oakctl app stop <APP_ID>`. |
| `-d, --device [<DEVICE>]` | Specify device using IP, `IP:PORT`, index, or Serial Number from `oakctl list`. |
| `-i, --invalidate` | Invalidate cache and force rebuild. |
| `-e, --env <KEY=VALUE>` | Export runtime environment variable to the app (can be provided multiple times). |
| `--env-file <FILE>` | Export runtime environment variables from a `.env` file. |
| `--oakapp-file [<PATH>]` | Use an alternative `oakapp.toml` file (for example dev/prod variants) from inside the provided app
directory tree. |
| `--preserve-line-endings` | Disable automatic CRLF to LF conversion before uploading files to device. |

#### Exit code

Unless run with `--detach`, `oakctl app run` exits with the app's exit code. If the app is killed by a signal, the exit code is
`128 + signal` (for example `137` for `SIGKILL`). Stopping the app yourself, for example with Ctrl+C, exits successfully
regardless of the app's exit code.

#### Example apps

We prepared [example apps](https://github.com/luxonis/oak-examples/tree/main/neural-networks) that you can run on your OAK4
device. Below we'll use [Human pose
detection](https://github.com/luxonis/oak-examples/tree/main/neural-networks/pose-estimation/human-pose) example, which also
contains the [`oakapp.toml`](https://docs.luxonis.com/software-v3/oak-apps/configuration.md):

```bash
git clone https://github.com/luxonis/oak-examples.git
cd oak-examples
# Run an app
oakctl app run ./neural-networks/pose-estimation/human-pose # or some other example
```

#### Environment variables

You can pass environment variables to the app using `-e, --env` flag or `--env-file` flag. These variables will be available in
the app's runtime environment and can be used to configure the app without changing the code.

```bash
oakctl app run ./app/path --env KEY1=VALUE1 --env KEY2=VALUE2
```

Some apps may require specific environment variables to be set for them at build time (for example API keys, model download links,
etc.). In that case, you can set those variables in the `oakapp.toml` file using `build_env` field or pass them during build with
`--build-arg` flag:

```bash
oakctl app build ./app/path --build-arg KEY1=VALUE1 --build-arg KEY2=VALUE
```

Some environment variables are set in each app by default:

| Variable | Description |
| --- | --- |
| `OAKAGENT_APP_ID` | Unique app ID. |
| `OAKAGENT_CONTAINER_ID` | Container ID (may differ from App ID if the app was updated). |
| `OAKAGENT_APP_IDENTIFIER` | App identifier from `oakapp.toml`. |
| `OAKAGENT_APP_VERSION` | App version from `oakapp.toml`. |
| `DEPTHAI_CACHE_DIR` | Path to the DepthAI cache directory; prefer to not modify manually. |
| `DEPTHAI_ZOO_MODELS_PATH` | Path to DepthAI Zoo models directory; set based on `depthai_models` field in `oakapp.toml`; prefer
to not modify manually. |
| `DEPTHAI_ZOO_CACHE_PATH` | Path to DepthAI Zoo cache directory; used for caching downloaded models; prefer to not modify
manually. |
| `DEPTHAI_ZOO_INTERNET_CHECK` | Enable internet connectivity check for model downloads; set based on `depthai_models` field in
`oakapp.toml`; prefer to not modify manually. |
| `DEPTHAI_DEVICE_NAME_LIST` | Set to `127.0.0.1` on all RVC4 devices to make sure that standalone apps use only the device they
are running on, even if there are multiple devices on the same network. |
| `OAKAPP_STATIC_FRONTEND_PATH` | Path to static frontend files for the app. |
| `OAKAPP_STATIC_FRONTEND_PORT` | Port for serving static frontend files. It is set from range 9000-9128 to avoid conflicts with
the ports used by the agent or other apps. |
| `OAKAGENT_STORAGE_APP` | App-specific persistent storage path. |
| `OAKAGENT_STORAGE_SHARED` | Shared storage path accessible across apps with the same identifier. |
| `OAKAGENT_STORAGE_GLOBAL` | Global storage path on the device. |
| `OAK_WEBRTC_TURN_CREDENTIALS_URL` | TURN credentials endpoint derived from the device's Hub signaling URL. |
| `OAKAGENT_PRIVATE_HTTP_PWD` | Dynamic password to access the [oak-agent
API](https://docs.luxonis.com/software-v3/oak-apps/oak-agent-api.md). |

> **Persistent Storage**
> Persistent storage paths are used to store data that should persist across app restarts and updates. These paths are mounted into the app's container. You can choose the target directory name for the storage in the container with `oakapp.toml` configuration (`storage_dir_name`).

 * `OAKAGENT_STORAGE_APP` is a storage path that is unique to each app and is not shared with other apps. It is useful for storing
   app-specific data that should not be accessible by other apps.
 * `OAKAGENT_STORAGE_SHARED` is a storage path that is shared between all apps with the same identifier. It is useful for storing
   data that should be accessible by different installations of the same app.
 * `OAKAGENT_STORAGE_GLOBAL` is a global storage path that is not tied to any specific app. It is useful for storing data that
   should be accessible regardless of which apps are installed or running.

### Inspect a Running App

`oakctl inspect` connects to the [DepthAI
`RemoteConnection`](https://docs.luxonis.com/software-v3/depthai/tools/oak-visualizer.md) exposed by a running app. It provides a
quick way to understand a live pipeline, examine its topics, and capture data.

| Command | Description |
| --- | --- |
| `oakctl inspect topics` | List advertised topics as JSON. |
| `oakctl inspect pipeline` | Print the complete pipeline graph as JSON. |
| `oakctl inspect frames <topic> --count <count> --out <dir>` | Save decoded image frames as PNG files. |
| `oakctl inspect dump <topic> --count <count>` | Stream decoded topic messages as JSONL. Use `--seconds <duration>` instead of
`--count` to capture for a fixed time. |
| `oakctl inspect snapshot --out <dir>` | Capture the first sample received from every advertised topic. |

Use `-d <device>` to inspect an app on an OAK device:

```bash
oakctl inspect topics -d 1
```

Without `-d` or `--url`, `oakctl inspect` connects to `ws://127.0.0.1:8765`. A topic is advertised only after the app publishes
its first message on that topic. Discovery waits for up to 10 seconds by default; change this with `--timeout <duration>`.

### App Management

You can install multiple apps on the device. If you are developing an app, you can share compiled apps with others within the
team.

Be sure you run only one DepthAI app at a time.

Most of the app management commands have optional flags `-d, --device <DEVICE>` to specify the device to run the command on (IP
address or index from the `oakctl list`).

#### List installed apps

If you setup the device and adopted in the Hub, you probably have one app installed (`com.luxonis.default`).

```bash
$ oakctl app list
+---+--------+---------------------------+---------+----------------+-------------------+
| E | App Id | Identifier                | Status  | Health         | Frontend URL      |
+=======================================================================================+
| * | f8da5  | com.luxonis.default:1.3.8 | running | not configured | 10.0.1.24:9000    |
+---+--------+---------------------------+---------+----------------+-------------------+
```

First column (`E`) has asterisk if the app is enabled.

Any app can be in one of the following states: `installing`, `building`, `ready`, `starting`, `running`, `stopping`, `stopped`,
`deleting`, `deleted`, `unknown`.

`Ready` means the app is installed and ready to run, but it was not started since the agent was started, while `stopped` means the
app is installed but not running, it was stopped by the user.

> **Note**
> App IDs are truncated in the list for better readability. If there are multiple apps with the same prefix, the truncation length increases until all app IDs are unique. You can also use the `--long` flag to show full app IDs in the list. All app control commands accept both full and truncated App IDs as long as they are unique.

#### App control flow

The basic commands to control the app are `start`, `stop`, and `uninstall`. First, let's start the app:

```bash
$ oakctl app start 612a745c-8d68-4264-a3d6-d06d14275ef5
Starting app 612a745c-8d68-4264-a3d6-d06d14275ef5 ...
  App has been started!
```

You can also use a unique App ID prefix:

```bash
$ oakctl app start 612a745c
```

Now, let's read app logs - this command will read the app's logs and print them to the console as they are received:

```bash
$ oakctl app logs <app-id>
Reading logs ...
  Press Ctrl+C to stop reading logs.
  App output:
    [2025-02-12T14:37:54Z] Hello cli 1 / Wed Feb 12 14:37:54 UTC 2025
```

Optionally, you can specify the number of previous lines to read with the `-n` flag:

```bash
oakctl app logs <app-id> -n 10
```

If you only want historical logs without attaching to live output, use:

```bash
oakctl app logs <app-id> --no-follow
```

Now you can stop the app:

```bash
$ oakctl app stop 612a745c-8d68-4264-a3d6-d06d14275ef5
Stopping app 612a745c-8d68-4264-a3d6-d06d14275ef5 ...
  App has been stopped!
```

And here is how you can delete the app:

```bash
$ oakctl app uninstall 612a745c-8d68-4264-a3d6-d06d14275ef5
Deleting app 612a745c-8d68-4264-a3d6-d06d14275ef5 ...
  App has been deleted!
```

Any app can be enabled or disabled. If the app is enabled, it will start automatically when the device is booted.

```bash
oakctl app enable <app-id>
```

You can also disable the app with the `disable` command:

```bash
oakctl app disable <app-id>
```

Note that some app commands such as `start`, `restart`, `stop`, `uninstall`, `enable`, and `disable` support a flag `--all` (or
`-a` for short) instead of a specific app ID to perform their action on all apps installed on the device.

To interactively attach to the already running App on the device use the `exec` command:

```bash
oakctl app exec <app-id> -i /bin/bash
```

This will open an interactive bash shell inside the app's container, allowing you to inspect files, processes, and environment
variables.

> **Note**
> Be careful when modifying files or saving data inside the container, as changes can be lost when the container is stopped or removed. Better approach is to mount a persistent folder from the host device into the container using mounts (see [`oakapp.toml` configuration](https://docs.luxonis.com/software-v3/oak-apps/configuration.md)) or persistent storage that is managed by the OAK agent (see `OAKAGENT_STORAGE_APP`, `OAKAGENT_STORAGE_SHARED`, `OAKAGENT_STORAGE_GLOBAL` environment variables).

#### Install an app

App can be found in Hub in section [OAK4 Apps](https://hub.luxonis.com/control/apps/team-apps?tab=oak4). There are apps that are
shared with the team and apps that are shared with your team or public apps. By default, a newly installed app stops all others
and is enabled and running. You can modify this behavior by using `--enable=false` or `--keep-others` flags.

App installation is done by following command:

```bash
$ oakctl app install com-example-emotion_recognition_1-0-1.oakapp
Sending data to agent ...
  Data sent successfully!

✔ Oakapp package built successfully.                                                                                                         
Installed app has ID: ddb8a884-d9e1-4779-a88b-c30d5d1e265f

Start the app:  oakctl app start ddb8a884-d9e1-4779-a88b-c30d5d1e265f
```

App can be installed from a source directory, an `*.oakapp` file, from Hub (by identifier) or from URL.

To build an app from its source directory on the device and install it in one step, pass the directory:

```bash
# Build and install from a source directory
oakctl app install .

# Use a different app configuration within the source directory
oakctl app install . --oakapp-file configs/oakapp.toml
```

If you want to install app from Hub, do this:

```bash
# Install app by identifier
oakctl app install -i com.example.app
```

There is also an option to install app by URL if the app is somewhere on the internet:

```bash
# Install app by URL
oakctl app install -u https://example.com/app.oakapp
```

#### Update an app

App updates can be performed using the `oakctl app install` command. By default, `oakctl app install` attempts to update an
existing app with the same identifier. Use the `--force-new` flag to install a new instance instead of updating (this is useful
for self-hosted oak-agent; Luxonis OS does not allow multiple DepthAI apps at the same time).

If multiple apps share the same identifier, specify which one to update using the `--update <APP_ID>` flag. Use the short app ID
or full UUID from `oakctl app list`:

```bash
oakctl app install ./my-app.oakapp --update <APP_ID>
```

The update process follows these steps:

 1. The new app version is downloaded from the Hub, URL, or local `*.oakapp` file (depending on the source: `-i`, `-u`, or file
    path). The current version remains running during this step.
 2. Once the new version is downloaded and validated, the current version stops and the new version starts. Any previous rollback
    version is then removed.

For more control, you can perform updates manually:

`oakctl app install --manual-update` downloads and prepares the new version without stopping the current one. Verify readiness
with `oakctl app list`.

`oakctl app update <APP_ID> --commit` stops the current version and starts the new one.

`oakctl app update <APP_ID> --rollback` reverts to the previous version if issues occur.

`oakctl app update <APP_ID> --finalize` removes the old version kept for rollback once you confirm the new version is stable.

#### Build And Publish App

You can build your own app. The process will produce `*.oakapp` file that can be installed on other devices:

```bash
oakctl app build ./folder/app/src
```

By default, `oakctl app build` uses `oakapp.toml` from the provided app directory. Use `--oakapp-file` to select an alternative
config file (for example `oakapp.dev.toml` or `oakapp.prod.toml`), as long as that file is inside the same app directory tree.

Optional flags:

 * `-d, --device [<DEVICE>]` - specify device using IP, `IP:PORT`, index, or Serial Number from `oakctl list`
 * `-k, --keep` - keep the container after the build (useful if you want to `oakctl app start` it right after the build)
 * `-p, --publish` - publish the app to the Hub after the build (the app will show up in the Hub's [OAK4
   Apps](https://hub.luxonis.com/control/apps/team-apps?tab=oak4)).
 * `-O, --optimized` - build the app in optimized mode (smaller size, longer build time)
 * `-U, --update-description` - update the app description on the Hub if the app is published
 * `-N, --no-download` - do not download the `*.oakapp` file to host after build
 * `-o, --output [<PATH>]` - path to the directory where the built `*.oakapp` file should be downloaded
 * `--oakapp-file [<PATH>]` - use an alternative `oakapp.toml` file from inside the provided app directory tree
 * `--preserve-line-endings` - disable automatic CRLF to LF conversion before uploading files to device

If you publish the app, you need to specify the app's identifier and unique version in `oakapp.toml` file.

Build packages left on the device, including builds made with `--no-download`, are removed after 24 hours.

### App health

App health is reported separately from the app's lifecycle status. Apps report health through watchdogs: each watchdog monitors
progress using periodic pings and triggers a configured action if its timeout expires without a ping.

| Health | Meaning |
| --- | --- |
| Not configured | The app has no active watchdogs. |
| Healthy | The app has active watchdogs, and all are healthy. |
| Degraded | One or more watchdogs are degraded. The health state's `reasons` lists the descriptions of the degraded watchdogs. |

A watchdog with the `degrade` action marks the app as degraded when it becomes unhealthy. A watchdog with the `restart_app` action
restarts the app instead.

When an app stops or restarts, all of its watchdogs are stopped and deleted. Each app must therefore create the watchdogs it needs
dynamically at startup and/or during runtime. Send pings after meaningful progress, such as processing a frame or completing a
work cycle. See the [oak-agent API reference](https://docs.luxonis.com/software-v3/oak-apps/oak-agent-api.md) for all watchdog
operations.

View app lifecycle status and health, including degradation reasons when applicable:

```bash
oakctl app status
```

Show all registered watchdogs:

```bash
oakctl app status --watchdogs
```

Show historical app health events, such as watchdog creation, health changes, and restarts triggered by a watchdog:

```bash
oakctl app status --history
```

Optionally, pass `N` to specify the number of events to show. For example, to show 10 events:

```bash
oakctl app status --history 10
```

### Hub connection

For some operations, you need to connect the device to the Hub. You can do this with the following command:

```bash
oakctl hub login
```

After you log in, you can check the status of the connection with the following command:

```bash
oakctl hub status
```

To change the active team, run `oakctl hub login` again and select the team in the web login flow. `oakctl hub switch-team` is an
alias to `oakctl hub login`.

Logout using:

```bash
oakctl hub logout
```

Once you're logged in, you can publish built `*.oakapp` packages:

```bash
oakctl hub publish <oakapp-file>
```

You can also run local scripts that require the Hub token for model downloads, etc.:

```bash
oakctl hub run-script <script-file>
```

### Device Management

#### Device Info

Device info command will show you the device's information, such as OS version, agent version, architecture, serial number, and
model.

```bash
$ oakctl device info
Device Info:
  OS:                   Luxonis OS RVC4 1.4.0
  Agent Version:        2.0.11 (rvc4)
  Architecture:         linux/arm64
  Serial Number:        2713799968
  Model:                Luxonis, Inc. KalamaP OAK4-D R1
```

Use `--check_internet` flag to check internet connectivity as well.

#### Device Statistics

Use `oakctl device stats` to monitor resource usage while developing, deploying, or troubleshooting an app:

```bash
oakctl device stats
```

The report brings CPU usage, DSP utilization, SoC temperature, memory, power, filesystem usage, and network activity into one
view. The power section shows the available input and reserved output power of each port (USB PD, PoE, M8), with voltage and
current. When the device is connected over USB, the report also shows the negotiated USB link speed, for example `super-speed`
(`usb_link_speed` in JSON output). Use `--watch [<interval>]` for continuous monitoring, `--all` to include every filesystem in
the default output, or `--format json` for machine-readable output. Running `--watch` without an interval refreshes every two
seconds. Some metrics, such as power and DSP data, may not be available on every platform.

#### Aux Connector

On devices with an M8 or M16 aux connector, `oakctl device aux` shows what each pin of the connector carries and switches pins
between their functions, such as GPIO, UART, I2C or FSYNC.

Show the connector type, each pin's available functions and default, and the switches the board offers:

```bash
oakctl device aux info
```

Show each pin's current function and direction, and who holds it (a process on the device or a kernel driver):

```bash
oakctl device aux status
```

Change a pin's function with `set <PIN> <FUNCTION>`. Pin labels and functions come from `info`:

```bash
# Make pin 1 a GPIO
oakctl device aux set 1 gpio

# Make pins 1 and 6 a UART
oakctl device aux set 1 uart
```

UART and I2C use a pair of pins. If `set` moves a pin into or out of a pair, its partner moves too, and the output lists every pin
that changed. The change lasts until the next change or reboot. `set` doesn't lock the pin; it fails if the pin is busy, for
example because a program or kernel driver holds it or something is plugged in, and the error says why.

On boards that can route USB2 to the connector, switch the route between the USB-C port and the connector:

```bash
oakctl device aux usb set connector
oakctl device aux usb set usb-c
```

`usb set <ROUTE>` is short for `switch set usb <ROUTE>`.

A pin set to `gpio` is a line of the `aux-connector` gpiochip, named `aux-<PIN>`. Control it on the device with libgpiod, for
example:

```bash
gpioset $(gpiofind aux-1)=1
```

While a program holds the line, the pin's function can't be changed.

Use `-f json` in scripts: each command prints one JSON document. If the agent refuses a request, oakctl prints an `error` document
with a `kind` (`busy`, `invalid`, `unavailable` or `failed`) and exits with code 1. A `busy` error also names the holder.

#### Device Diagnostics

Collect a diagnostics bundle for troubleshooting:

```bash
oakctl device diagnostics
```

This saves the bundle locally as `oak-diagnostics-<timestamp>.tar.gz` in the current directory without uploading it. Existing
files are not overwritten.

> **Diagnostics contain unredacted data**
> Bundles may contain sensitive logs and configuration, along with device identity.

Use `-d <DEVICE>` to select a device and `-o bundle.tar.gz` to choose the output path.

To collect and upload directly from the device to Luxonis support:

```bash
oakctl device diagnostics -d <DEVICE> --upload
```

Add `-o bundle.tar.gz` to also download a local copy after a successful upload. If the device has no internet access, upload
through your computer instead:

```bash
oakctl device diagnostics -d <DEVICE> --upload --via-host -o bundle.tar.gz
```

`--via-host` requires `--upload` and retains the completed local bundle if uploading fails. Successful uploads print a diagnostics
ID to share with Luxonis support. Uploads do not retry or switch routes automatically. If an upload is interrupted before an ID is
returned, contact support before retrying because the bundle may already have been stored.

#### Device Update

Device can be updated with the following command - possible values for `CHANNEL` are `stable` and `beta`:

```bash
oakctl device update --channel=[CHANNEL]
```

This command will check the latest available version and update the device if the version is different.

You can select the specific version to update to using `--select` flag:

```bash
oakctl device update --select --channel=[CHANNEL]
```

To update to an exact version without prompting, use `--version`. Add `--channel` for versions outside `stable`; a version that
isn't available fails.

```bash
oakctl device update --version 1.45.0 --yes
```

Alternatively, you can directly provide an update URL or a path to a local file using either `--url` or `--path` flags:

```bash
oakctl device update --url=[URL]
oakctl device update --path=[PATH]
```

To download an OTA update package to the host without installing it on the device, specify a destination directory:

```bash
oakctl device update --download <DIR>
```

If the device has no internet connection, oakctl automatically downloads the update on your computer and transfers it to the
device. Your computer needs internet access and a connection to the device. Use `--local` to force this path even when the device
has internet access:

```bash
oakctl device update --local
```

To show the latest OS update status recorded on the device, run:

```bash
oakctl device update --status
```

The status command does not start an update and is not supported on self-hosted agent.

#### Device Reboot

You can reboot the device using `oakctl`:

```bash
oakctl device reboot
```

This command will reboot the device and wait for it to come back online.

#### Device Unlock (SSH)

Devices have SSH access disabled by default. You can enable it using the following command:

```bash
oakctl device unlock
```

This command will prompt you to set a password.

Use `-y` and `--password` to enable root SSH password login without prompts:

```bash
oakctl device unlock -d <DEVICE> -y --password '<new-root-password>'
```

Empty passwords are accepted.

Run `oakctl device unlock` again to change the root password or reapply SSH password login. On a device that is already unlocked,
oakctl asks for confirmation first; `-y` skips it.

#### Device Flash

You can flash the device (USB only) with a new Luxonis OS image using the following command:

```bash
oakctl device reflash [<path-to-tar.xz>]
```

Path to the `*.tar.xz` image is optional; if not specified, the latest stable image will be downloaded and flashed. For detailed
flashing and OS update instructions see [updating OS page](https://docs.luxonis.com/software-v3/sw-stack/luxonis-os.md).

Add `-y` (or `--yes`) to skip interactive confirmation in an automated flashing workflow. Select the intended device with `-d
<DEVICE>`.

To flash an exact OS version, use `--version`; add `--channel` for versions outside `stable`:

```bash
oakctl device reflash --version 1.45.0 --yes
```

To download the full OS image without flashing the device, run:

```bash
oakctl device reflash --download <DIR>
```

Combine it with `--version` to download a specific version.

### Access the device over USB with ADB

`oakctl` includes a bundled ADB tool. Use `oakctl adb` on your host computer to access an OAK4 connected over USB. See [OAK4
Advanced](https://docs.luxonis.com/hardware/platform/deploy/oak4-deployment-guide/oak4-advanced.md) for USB connection and power
requirements.

| Command | Description |
| --- | --- |
| `oakctl adb devices` | List connected ADB devices and their serial numbers. |
| `oakctl adb shell` | Open an interactive shell; run `exit` to return to the host. |
| `oakctl adb shell cat /etc/os-release` | Run a single command on the camera. |
| `oakctl adb push ./file.txt /data/` | Transfer `./file.txt` from the host to `/data/file.txt` on the device. |
| `oakctl adb pull /data/file.txt ./` | Transfer `/data/file.txt` from the device to the host at `./file.txt`. |

The shell runs in the camera's OS. To open a shell inside an app container, use `oakctl app exec <app-id> -i /bin/bash` instead.

With multiple ADB devices connected, use the serial from `oakctl adb devices`:

```bash
oakctl adb -s <ADB_SERIAL> shell
```

ADB uses `-s` for this selection; the usual oakctl `-d` device selector and saved `oakctl connect` connection do not select the
ADB device.

For operations requiring root permissions, run `oakctl adb root` (or `oakctl adb -s <ADB_SERIAL> root`). This restarts the
camera's ADB daemon; wait for it to reconnect before retrying.

Use `oakctl adb --help` for wrapper usage and `oakctl adb help` for the bundled ADB command reference.

## oak-agent

`oak-agent` is a service that runs on the OAK4 device and manages the containers. It's responsible for:

 * managing apps, running containers;
 * communicating with the `oakctl` tool;
 * communicating with the Hub (cloud platform).

### Containers

`oak-agent` uses `runc` as a lightweight container runtime, which is also what Docker/Podman uses. We opted-in for `runc` because
it's lightweight and gives us full control over the container lifecycle.

## Release Notes for oakctl and oak-agent

### oakctl v0.32.0 (November 12, 2026)

#### Added

 * `oakctl device aux` to configure and query the M8/M16 aux connector.
 * `oakctl app install <source-directory>` builds and installs an app from source.
 * `oakctl app status <app-id>` shows app status and health. Use `--watchdogs` to list the app's watchdogs, `--history [NUMBER]`
   to show recent watchdog events, and `-f json` for JSON output.
 * `oakctl device stats` shows input and output power contracts (USB PD, PoE, M8) and the negotiated USB link speed. The speed is
   also available as `usb_link_speed` in its JSON output and as `usb.usb_link_speed` in `oakctl list -f json`.
 * `oakctl device reflash --cdt <BOARD>` also flashes the board's CDT (Configuration Data Table) from the OS build.
 * `oakctl device reflash` reuses the last extracted OS when the same archive or URL is flashed again, for example when flashing
   many devices in a row.
 * `--version <VERSION>` for `oakctl device update` and `oakctl device reflash` to pick an exact OS version from the selected
   channel.
 * `--yes` for `oakctl device reboot`, `oakctl viewer` and `oakctl registry login` to skip confirmations.
 * oakctl can run without a terminal: commands that need input fail with a hint instead of waiting for it.

#### Changed

 * When oakctl asks you to choose a device, you can move through the list with the Up/Down arrow keys. When possible, the
   highlighted device's status LED turns white so you can tell which camera is which.
 * `oakctl list` shows the device's product name instead of the DTS model when available.
 * `oakctl app list` includes a Health column and a `health` field in JSON output. Agents without healthcheck support report `not
   configured`.
 * `oakctl device unlock` can be repeated to change the root password and reapply SSH password login settings. Already unlocked
   devices show a warning instead of failing with "Device is already unlocked".
 * `oakctl device update --yes` now also confirms a full reflash, which erases device data, on devices too old for OTA updates.
 * App installation checks the device's free storage before uploading the package, so oversized apps fail early instead of filling
   the device.

#### Fixed

 * USB internet sharing on Windows is more reliable: oakctl retries ICS failures, checks the sharing setup before using it, and
   clears stale ICS settings left on unplugged OAK adapters, which left the device without internet after a host reboot.
 * On Linux, `oakctl usbd enable`, installation and self-update check that `cdc_ncm` can be loaded before setting up USB internet
   sharing.
 * On Windows, oakctl commands no longer fail with "Access is denied" when several oakctl processes run at once.
 * `oakctl device reflash` failed with `unable to open <BOARD>_CDT.bin` on build folders modified to flash a CDT. oakctl now
   flashes a CDT only when `--cdt` is given.
 * Stopping an app with Ctrl+C no longer cuts off its shutdown logs in `oakctl app run`, attached `oakctl app logs` and Hub live
   logs.
 * `oakctl app run` no longer reports `App output stream ended` when the app exits normally. It exits with the app's exit code, or
   `128 + signal` if the app was killed by a signal.
 * On Windows, oakctl honors `RUST_LOG` for diagnostic logging, as on Linux and macOS.
 * Updated dependencies to address security advisories.

### agent v0.29.0 (November 12, 2026)

#### Added

 * [App healthchecks](https://docs.luxonis.com/software-v3/oak-apps/oak-agent-api.md) with watchdogs. Missed heartbeats can mark
   an app as degraded or restart it automatically; watchdog events are kept for inspection through `oakctl app status`.
 * [Hub connectivity checks](https://docs.luxonis.com/software-v3/oak-apps/oak-agent-api.md) for apps through the oak-agent API
   (`GET /v1/network/health`). They probe Hub services, Events API access, and app and OS downloads.
 * App installation checks the device's free storage before downloading or writing a package, so oversized apps fail early instead
   of filling the device. Hub installs are rejected before the download. Newly built `.oakapp` packages record their uncompressed
   size for this check.
 * Support for `oakctl device aux`, installing apps from source, power contracts and USB link speed in `oakctl device stats`, and
   the product name in `oakctl list`.
 * Clients can light the status LED white to identify a device while it shows its idle color. Setup can disable this with `dl=n`
   in the agent setup configuration.

#### Fixed

 * Apps that mount `devtmpfs` over `/dev` in `additional_mounts` start again; since agent v0.28.0 they failed with `error setting
   up /dev symlinks`. New apps should still use a bind mount; see [Device access in the app
   configuration](https://docs.luxonis.com/software-v3/oak-apps/configuration.md).
 * USB internet sharing (`oakctl usbd`) sometimes didn't work after the device booted with USB connected, until the cable was
   replugged. The usbd log showed `USB bootstrap API did not become available within 30 seconds`.
 * Stopping an app during a build interrupts the build and cleans up its containers instead of waiting for the build to finish,
   including with `oakctl app stop --all`.
 * Fixed app updates occasionally deleting the newly installed version.
 * An interrupted base image download no longer makes later retries fail with `File exists`.
 * Apps are no longer reported as ready when packaging fails, and leftover installation files are cleaned up.
 * Closed the remaining causes of apps failing with `stat /bin/sh: no such file or directory` after an agent crash.
 * `oakctl app stop` and `restart` no longer fail with a runc error when the app exits on its own right at its `stop_grace_period`
   deadline.
 * Changing the app version in `oakapp.toml` is now reflected across `oakctl app run` invocations.
 * Shutdown logs of an app stopped with Ctrl+C are kept until the app has stopped, including during a force kill.
 * Self-hosted oak-agent: devices plugged in after the agent starts are visible to the agent and to apps that mount `/dev`. Re-run
   the installation script to apply this to existing installations.
 * Updated dependencies to address security advisories.

### oakctl v0.31.1 (October 21, 2026)

#### Fixed

 * Fixed permission errors when updating from older oakctl versions on Linux and macOS by preserving executable permissions on the
   bundled RVC2 helper.
 * USB internet sharing on Linux now detects conflicting nftables table ownership before enabling the service and explains how to
   resolve it, including firewalld's `NftablesTableOwner` setting.
 * Fixed firewall backend detection when iptables compatibility warnings appear on stderr.
 * Updated ZIP and TLS dependencies to address security advisories.

#### Changed

 * Clarified that `oakctl app install --update` accepts the short app ID or full UUID from `oakctl app list`, and added an update
   example to command help.

### oakctl v0.31.0 (October 14, 2026)

#### Added

 * [RVC2 device management](https://docs.luxonis.com/software-v3/depthai/depthai-components/bootloader.md) through `oakctl rvc2`:
   discovery, device information, USB and network configuration, bootloader updates, factory reset, standalone application
   removal, and USB ROM recovery.
 * `oakctl device diagnostics` to save a diagnostics bundle locally or upload it to Luxonis support with `--upload`. Use
   `--via-host` with `--upload` when the device has no internet connection, and `-o` to save a local copy. Bundles contain
   unredacted logs and configuration; uploads return an ID to share with support.
 * Linux ARMv7 (32-bit, armhf) builds through the shell installer. These builds have second-tier support: they are not tested, and
   `oakctl adb` and `oakctl device reflash` are unavailable.
 * `oakctl update` as an alias for `oakctl self-update`.
 * Available teams and `-f json` output in `oakctl hub status`.
 * DSP utilization in `oakctl device stats` on supported devices.
 * `-y` and `--password` for non-interactive `oakctl device unlock`, including support for empty passwords.
 * `-y` for non-interactive `oakctl device reflash`.
 * `--enable-usbd` and `--skip-usbd` for the installer and self-update to explicitly enable USB internet sharing or skip service
   setup and updates. Linux also supports `--skip-udev` with `--skip-usbd` to defer USB rule setup.

#### Changed

 * Linux and macOS installations now use `~/.local/bin`, migrate legacy installations, and update shell profiles unless
   `--no-modify-path` is passed. Self-update must run as the owner of the oakctl installation.
 * The installer and self-update ask whether to enable USB internet sharing when no preference has been saved. Non-interactive
   setup requires an explicit `--enable-usbd` or `--skip-usbd` choice when needed.
 * The USB sharing service uses a separate root-owned binary. On Linux, installation and self-update install the rule that
   prevents NetworkManager and systemd-networkd from managing OAK4 USB interfaces; disabling sharing retains the rule.
 * `oakctl device update` automatically downloads an OS update on your computer and transfers it to a device that has no internet
   connection. Use `--local` to force this behavior.
 * `oakctl device list` shows a notice when RVC2 cameras are detected; use `oakctl rvc2 list` to list and select them.
 * `oakctl app config get` and `set` accept `-d` after the subcommand.

#### Fixed

 * `oakctl app logs` returns retained output for stopped or failed apps and reports a clear version requirement for agents without
   retained-log support.
 * Improved device discovery when mDNS retries or address recovery are needed, and fixed panics caused by invalid device
   selectors.
 * Downloads retry transient failures, resume interrupted transfers where supported, and detect stalled or incomplete downloads.
 * Fixed missing JSON transfer progress when sending a local OS update to the device.
 * Fixed Windows installation and self-update in non-interactive sessions and prevented the Windows installer from terminating the
   oakctl process performing an update.
 * Fixed self-update failing in non-interactive sessions when passwordless sudo is configured.

### agent v0.28.0 (October 14, 2026)

#### Added

 * Support for `oakctl device diagnostics` and DSP utilization in `oakctl device stats`.
 * [Device-access rules](https://docs.luxonis.com/software-v3/oak-apps/configuration.md) that select a host device by `path`, with
   `optional = true` to skip a missing path at startup. Numeric rules also accept `major = "*"` and `minor = "*"`.
 * Configurable password login for the WebTerminal through `t=y` in the agent setup configuration. Omitting `t`, or setting `t=n`,
   keeps passwordless terminal access.
 * Automatic cleanup of idle build packages, including `oakctl app build --no-download` output, after 24 hours without a download
   request.

#### Changed

 * Individual device nodes in `required_devices` and `optional_devices` automatically receive `rwm` permissions. Explicit
   `allowed_devices` rules apply afterward and can restrict access; omitted `access` defaults to `rwm`. Rebuild existing app
   packages to include automatic grants. Duplicate device sources or targets are rejected with a descriptive error.
 * Apps receive `OAK_WEBRTC_TURN_CREDENTIALS_URL`, derived from the Hub signaling URL, in place of `OAK_WEBRTC_HUB_API_URL`.
 * Updated the bundled container runtime, `runc`, from `v1.3.1` to `v1.5.1`.

#### Fixed

 * Fixed `oakctl app exec` hanging when a command exits almost immediately under heavy device load, which could also block other
   app commands.
 * Fixed stopping apps during automatic restart and improved app start, stop, restart, and uninstall transitions.
 * The agent waits for containers to stop after `SIGKILL` before deleting them.
 * App builds recover from `Lower layer index out of bounds` failures.
 * Downloads retry transient network failures, resume interrupted transfers where supported, and detect stalled or incomplete
   downloads. Built packages remain available across retries until cleaned up.

#### Known issues

 * Apps that mount `devtmpfs` over `/dev` in `additional_mounts` fail to build or start with `error setting up /dev symlinks`.
   Mount `/dev` as a bind mount instead; see [Device access in the app
   configuration](https://docs.luxonis.com/software-v3/oak-apps/configuration.md).

### oakctl v0.30.1 (September 3, 2026)

#### Added

 * On Windows, added: `oakctl usbd share-to <device|auto>` to be able to control which device the internet is shared to.
 * `oakctl device stats` to show CPU, Memory, Filesystem usage and other useful device data.
 * Added a hint for oakapp.toml parsing errors that likely originated from an ill-positioned `[base_image]` section.
 * `oakctl device update --status` to show the latest OS update status recorded by `agentconfd`.

#### Fixed

 * USB internet sharing on `Windows Home`.
 * Preserve `=` for app config values passed through the `--env` flag.

#### Changed

 * Expanded `oakctl usbd status` to include more details about the `oakctl-usbd` state.

### agent v0.27.1 (September 3, 2026)

#### Added

 * Automatic app restart support through the `restart_policy` field in `oakapp.toml`.
 * Support for `oakctl device stats`.

#### Fixed

 * Fixed a prolonged time-synchronization delay when the internet was unreachable upon device startup.
 * WebRTC stability improvements.
 * Improved internal handling of losing the connection to oakctl during `oakctl app run/build`.
 * "App is in unknown state" after power cycle (`.process.pid file exists`).
 * `static-fe: no such file or directory` error when running `oakctl app run` consecutively.
 * Generic `log detach` error hiding build errors when running `oakctl app run`.
 * `static-fe: no such file or directory` error on `oakctl app run .` after changing the `base_image` in `oakapp.toml`.
 * `app config` getting deleted after `oakctl app install --update`.
 * `oakctl app restart` now changes the app state into `restarting` instead of `stopping` followed by `starting`.

### oakctl v0.29.1 (August 26, 2026)

#### Fixed

 * oakctl Windows installer error: `0x80070666`. The error could occur on some computers due to conflicting `vc_redist` versions.

### oakctl v0.29.0 (August 25, 2026)

#### Added

 * `oakctl inspect` to list DepthAI RemoteConnection topics, print the pipeline graph, and capture frames or snapshots from a
   running DepthAI app.

### oakctl v0.28.0 (August 20, 2026)

#### Added

 * `--download <DIR>` argument to `oakctl device update` and `oakctl device reflash`, which allows you to download the update
   package to your computer without flashing it.

### oakctl v0.27.3 (August 12, 2026)

#### Fixed

 * oakctl self-update: resource is busy error when `oakctl-usbd` is enabled.

### oakctl v0.27.2 (August 11, 2026)

#### Fixed

 * oakctl signature on Windows.

#### Changed

 * Better error message when using the new `base_image` syntax with an old agent.

### oakctl v0.27.1 (August 3, 2026)

#### Fixed

 * `oakctl` panic on initialization.

### oakctl v0.27.0 (July 30, 2026)

#### Added

 * Wi-Fi configuration support in the `oakctl device setup apply` and `oakctl device setup apply-b64` commands.
 * `oakctl registry login` and `oakctl registry logout` for authenticating with container registries. This enables private image
   pulls and helps avoid unauthenticated pull rate limits.
 * The `--all` flag for `oakctl app uninstall`, `start`, `stop`, `restart`, `enable`, and `disable`.
 * `oakctl device sahara enable|disable` to enable or disable Sahara on a device.
 * `oakctl device uart enable|disable` to enable or disable Linux kernel logs and the login shell over UART.
 * License and 3rd party license notices distribution

#### Fixed

 * Fixed `oakctl app prune-storage` for apps that have been updated.
 * Fixed a long delay when starting `oakctl` commands if a default route was configured but the internet was unreachable.
 * Fixed timeouts when running `oakctl app prune-storage`.
 * Fixed `oakctl app exec -i` when an app mounts `/dev`.
 * Improved `oakctl list` output for devices connected over USB that are not reachable over the network.
 * `oakctl device reflash` on Windows 11

### agent v0.25.0 (July 15, 2026)

#### Added

 * New private HTTP API endpoints (`device-reboot`, `app-stop`, `app-restart`).
 * Support for: `oakctl device sahara enable|disable` to enable or disable Sahara on the device.
 * Support for `oakctl device uart enable|disable` to enable or disable the linux kernel logs and login shell on UART.
 * Persistent logs: * Use journald for logging oakapp output.
    * Ability to ingest app logs into hub.
 * License notices.
 * Added `wifi` support for device setup.
 * Support for `--all` flag on `oakctl app` `uninstall`, `start`, `stop`, `restart`, `enable`, `disable`.

#### Fixed

 * Fixed `app prune-storage` timeout

### agent v0.23.0 (June 17, 2026)

#### Changed

 * App shutdown: apps are now stopped gracefully by sending SIGTERM to the app process and waiting for it to exit, instead of
   forcefully killing the container immediately. This allows apps to perform cleanup during shutdown.

#### Fixed

 * Fixed partial device setup state on failure to retrieve Hub service URLs.
 * `oakctl app prune storage` for apps which have been updated.

### agent v0.22.1 (June 2, 2026)

#### Added

 * Deletion of deleted containers to `oakctl app prune-storage`

### oakctl v0.23.0 (May 29, 2026)

#### Added

 * Added analytics to `oakctl`. Analytics can be disabled with the `OAKCTL_ANALYTICS=0` environment variable.

#### Changed

 * Removed the deprecation notice on `oakctl app install --update`.

### oakctl v0.22.0 (May 21, 2026)

#### Added

 * `oakctl app examples list` to show available OAK app examples and `oakctl app examples clone <path>` to download the
   `oak-examples` repository locally.
 * USB internet sharing support via `oakctl usbd`. * Added the `oakctl-usbd` background service to share the host's internet
   connection with OAK devices over USB.
    * Added `oakctl usbd <status|enable|disable>` to manage the `oakctl-usbd` service.

#### Changed

 * Removed deprecation notices from `oakctl list`, `oakctl connect`, `oakctl setup`, `oakctl setup-b64`, and `oakctl start-setup`.
 * Made `oakctl list` and `oakctl connect` visible again in help output.

### agent v0.20.0 (May 7, 2026)

#### Added

 * USB Internet sharing support.

### agent v0.19.1, oakctl v0.20.0 (May 5, 2026)

#### Fixed

 * `oakctl adb` would sometimes exit with code `255` even though the `adb` command succeeded.
 * `oakctl` no longer shows the new-version availability prompt when running `self-update`.

#### Added

 * `oakctl device update --url/--path` to update an RVC device OS from a URL or local file.
 * `oakctl device update --local` to download OS updates locally.
 * `oakctl device connection get|unset` to inspect or clear the current device connection after using `oakctl connect`.

#### Changed

 * `oakctl` CLI consistency: * `oakctl list` was moved to `oakctl device list` (the old command is hidden and shows a deprecation
   notice).
    * `oakctl connect` was moved to `oakctl device connection set` (the old command is hidden and shows a deprecation notice).
    * `oakctl start-setup` was moved to `oakctl device setup start` (the old command is hidden and shows a deprecation notice).
    * `oakctl setup` was moved to `oakctl device setup apply` (the old command is hidden and shows a deprecation notice).
    * `oakctl device flash` was renamed to `oakctl device reflash` (the old command is hidden and shows a deprecation notice).
    * `oakctl app delete` was renamed to `oakctl app uninstall` (the old command is hidden and shows a deprecation notice).
    * `oakctl hub publish` was moved to `oakctl app publish` (the old command is hidden and shows a deprecation notice).
    * `oakctl app config <app_id> set|get` was refactored to `oakctl app config set|get <app_id>`.
    * `oakctl setup-b64` was moved to `oakctl device setup apply-b64` (the old command is hidden and shows a deprecation notice).
 * Expanded `--help` output across all of `oakctl`. Help now includes example commands and short explanations of core concepts.

### agent v0.18.6, oakctl v0.18.6 (April 8, 2026)

#### Added

 * `oakctl app install` now deletes unnecessary files after installation to save storage space.
 * `oakctl app prune-storage` now removes installation and download files too.
 * `oakctl app delete` now also deletes malformed apps.
 * `oakctl device info` now shows: * date
    * network information
    * HTTP API port for downloading built apps
 * `oakctl app run` no longer rebuilds the whole app if a command fails during build steps; it keeps successfully built layers
   instead.
 * New `oakapp.toml` definition: * Added `shell` field to specify the default shell for `RUN` commands, `build_steps`, and
   `entrypoint` (default: `["/bin/sh", "-c"]`).
    * Commands can now be written in shell form (string) or exec form (array of strings).
    * Removed `shlex`-based parsing because it did not support constructs like redirection and pipes.
    * Added optional `arg` section for build-time environment variables and `--build-arg` flag for `oakctl app build` and `oakctl
      app run`.
    * Added optional `additional_build_mounts` section for mounts used only during the build stage.
 * All Hub service endpoints can now be configured by API. * Use `OAKCTL_HUB_API_URL` in `oakctl`.
    * Use `api=` in setup-utility config for `oak-agent`.

#### Changed

 * Renamed the env variable that selects the Hub services environment in `oakctl` from `ENV` to `OAKCTL_ENV`.

### agent v0.18.3, oakctl v0.18.2 (February 17, 2026)

#### Added

 * Image download progress reporting during `oakctl app build` and `oakctl app run` commands.
 * GPU support for self-hosted agent, which allows oak apps to use the host's Nvidia GPU if enabled.
 * `oakctl app [build|run] --oakapp-file [PATH]` arg to specify a custom path to the `oakapp.toml` file.
 * `oakctl app logs --no-follow` arg to avoid attaching to the log stream.
 * Remote command execution from Luxonis Hub.
 * Replaced `--*-b64` arguments of `oakctl setup` with a new subcommand `oakctl setup-b64`.
 * Rejection of relative paths in `oakapp.toml` mount fields: `required_mounts`, `required_devices`, `optional_mounts`,
   `optional_devices`, `additional_mounts`.
 * `oakctl device update` support for self-hosted oak-agent.

#### Fixed

 * `Failed to mount overlayfs` error on `oakctl app build` when trying to use a base image with many layers (around 30).
 * `oakctl adb` on jetson.
 * Added installation of QDL udev rules to `oakctl self-update`. * Fixes some instances of `qdl: Failed to open device` during
   `oakctl device flash`.
 * `/etc/resolv.conf` missing in container on second app run after editing `oakapp.toml`.

### agent v0.17.4, oakctl v0.17.4 (January 15, 2026)

#### Added

 * `oakctl app build --output [PATH]` argument to indicate where to download the `*.oakapp` file after building it.
 * Base64-encoded arguments of `oakctl setup` command to ensure cross-OS-compatible escaping of special characters for the
   Hub-generated setup command.
 * Automated check for new `oakctl` versions once per day.
 * `oakctl app prune-storage` command to remove unnecessary app files.
 * `oakctl app list --long` flag to show full App ID.
 * `oak-agent` tests WebRTC connection.
 * `oakctl device info` and `oakctl list` show adoption status.
 * Welcome ACK factory reset support.
 * `oakctl app install` updates an existing app by default. * Can be modified with `--force-new` flag to install as a new app.
    * Can be modified with `--update` flag to update a specific existing app.
 * `oakctl app install --env / --env-file` to set environment variables during app installation.
 * Multiplatform self-hosted Docker image.

#### Changed

 * `oakctl app list` now shows App IDs truncated to 3 characters by default; truncation increases automatically when there are
   collisions.
 * `oak-agent` saves new app build metadata.
 * Self-hosted WebRTC terminal opens host shell instead of container shell.
 * `oakctl app <ACTION> <app-id>` commands now accept both full and truncated App IDs.

#### Fixed

 * Fixed an issue where OTA update status deserialization failed if multiple messages were received in a single read.
 * `oakctl` on Windows converts CRLF to LF automatically.
 * Self-hosted `oak-agent`/`oakctl` fixes: * fixed `oakctl device info --check_internet`
    * fixed `oakctl device reboot`
    * fixed `oakctl setup` command (failed on some devices like RPi)
    * `adb` binary for ARM devices was missing (mistakenly included x86 binary instead)
 * Fixed app publish upload with `OAKCTL_HUB_TOKEN`.
 * `oakctl` builds for macOS ARM and Windows were not signed.
 * Fixed build cache invalidation for `oak-agent`.
 * Fixed an issue where `oakctl` did not save and/or read `sn-data.json` correctly.

#### Deprecated

 * `OAKCTL_HUB_LOGIN_TOKEN` env renamed to `OAKCTL_HUB_TOKEN`.
 * `oakctl hub switch-team` is now an alias to `oakctl hub login` (team is selected in web login flow).
 * `--enabled` flag renamed from `-e` to `-E`.

### oakctl v0.16.5 (December 15, 2025)

#### Added

 * New flag `--yes` for non-interactive `oakctl device update`.
 * New flag `--check_internet` for `oakctl device update` to check internet connectivity before updating.
 * `oakctl viewer` command to open Viewer is enabled.
 * New flag `--no-download` for `oakctl app build` to skip downloading built `*.oakapp` file to host; useful for tests.
 * New flags `--enable` and `--disable-others` for `oakctl app start`.

#### Changed

 * `oakctl hub login` now uses web-based authentication flow.
 * Minor improvements for integration into Viewer.