Live View and Static Frontend
Open Frontend
To open an application's frontend, navigate to:
Devices → Select a Device → Apps (Tab) → Select a Running Application → Open Frontend.
Devices → Select a Device → Apps (Tab) → Select a Running Application → Open Frontend.
Default Visualizer
This option is available only for applications that include a custom frontend. If no frontend is shipped with the app, the default visualizer will open instead, where live streams and outputs are specified through DepthAI's RemoteConnection component.