CLI
Deprecation Notice
This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.
Command Line
1hubctl [command] [options][command] with one of the available commands described below and [options] with any applicable command-specific options.General commands
version - Prints the version of the Luxonis Hub Agent.An example:Command Line
1$ hubctl version
2Installed agent version: 24.55.1308status - Prints the status of the Luxonis Hub Agent.An example:Command Line
1$ hubctl status
2╔═══════════════════════════════════════════════════════════════╗
3║ ║
4║ Luxonis Hub Agent (24.55.1308 | linux/arm64 | DepthAI 2.21.2) ║
5║ ║
6╚═══════════════════════════════════════════════════════════════╝
7
8Web UI https://localhost:9010
9DepthAI 2.21.2
10
11Connected to cloud? yes (https://hub.luxonis.com)
12Team Luxonis
13Pending detections 0
14
15
16Link to robot in cloud
17https://hub.luxonis.com/robots/00000000-0000-0000-0000-000000000000start - Starts the Luxonis Hub Agent.Requires root privileges
An example:Command Line
1$ sudo hubctl startstop - Stops the Luxonis Hub Agent.Requires root privileges
An example:Command Line
1$ sudo hubctl stoprestart - Restarts the Luxonis Hub Agent.Requires root privileges
An example:Command Line
1$ sudo hubctl restartstartup - Enables or disables automatic launch of the Luxonis Hub Agent on startup.Arguments:enableenables automatic launchdisabledisables automatic launch
Command Line
1$ hubctl startup enablelogs - Displays logs from the Luxonis Hub Agent.Options:-f,--followdo not terminate, keep following the logs (default: false)-a,--allprints all available logs (consider piping toless) (default: false)-l,--last <lines>how many lines (from the end to print) (default: "20")--since <linux date>filter since--until <linux date>filter until--format <json|pretty|plain>choose format of logs (default: "pretty")
Command Line
1$ hubctl logs
263 23:05:28 I user/agent/hub-connection : received see_you
363 23:05:31 I user/agent/apps/logs : uploading app logs to RH | pending -> 0
463 23:05:36 I user/agent/apps/logs : uploading app logs to RH | pending -> 0
563 23:05:41 I user/agent/apps/logs : uploading app logs to RH | pending -> 0upload-support - Uploads a support file to Luxonis. Please provide the hash printed at the end to our support team.An example:Command Line
1$ hubctl upload-support
2File has been uploaded with hash: f0a83c01bc4c7c7f0bd466d6cca2ec9071f8c267e6e65385f744e94f1caa734dreset - Resets the Luxonis Hub Agent to its post-installation state.Requires root privileges
An example:Command Line
1$ sudo hubctl reset --i-understand-consequences --keep-robot-in-cloudCloud commands
cloud connect - Connects the Luxonis Hub Agent to Luxonis Hub.An example:Command Line
1$ hubctl cloud connect
2Already connected to cloud (team Luxonis). Disconnect first to connect again.
3hubctl cloud disconnectcloud disconnect - Disconnects the Luxonis Hub Agent from Luxonis Hub.An example:Command Line
1$ hubctl cloud disconnectcloud force-sync - Forces manual synchronization with Luxonis Hub.An example:Command Line
1$ hubctl cloud force-syncDevices commands
devices - Displays a list of devices connected to the Luxonis Hub Agent.An example:Command Line
1$ hubctl devices
2┌────────────────────┬────────────────────┬───────────────────────┬──────────┬─────────┬──────────────────┬──────┐
3│ serial │ name │ product │ location │ status │ connectionStatus │ app │
4├────────────────────┼────────────────────┼───────────────────────┼──────────┼─────────┼──────────────────┼──────┤
5│ 18443010116C870E00 │ 18443010116C870E00 │ OAK-D-PRO-FF (DM9098) │ USB 2.1 │ success │ ready │ none │
6└────────────────────┴────────────────────┴───────────────────────┴──────────┴─────────┴──────────────────┴──────┘Apps commands
apps list - Displays a list of installed apps.An example:Command Line
1$ hubctl apps list
2┌──────────────────────────────────────┬─────────┬─────────┬──────────────────────────┬────────────┐
3│ id │ type │ status │ started at │ stopped at │
4├──────────────────────────────────────┼─────────┼─────────┼──────────────────────────┼────────────┤
5│ bfeb4f73-f503-458a-8c24-b88258f9523a │ builtin │ Running │ 2024-03-01T08:15:33.282Z │ │
6└──────────────────────────────────────┴─────────┴─────────┴──────────────────────────┴────────────┘