Install Luxonis Hub Agent
Deprecation Notice
This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.
Requirements
| Operating system | |
|---|---|
| Ubuntu (Desktop or Server) | 20.04, 22.04 |
| Raspberry Pi OS | any version |
Only 64-bit operating systems are supported!
To determine whether your system is 32 or 64 bit use the
getconf LONG_BIT command.Raspberry 5 supported operating systems
Since Ubuntu 22.04 LTS is not officially supported on the Raspberry Pi 5, it is necessary to use Raspberry Pi OS with this hardware.
Hardware
| RAM / Memory | |
|---|---|
| Minimum | 2 GB |
| Recommended | 4 - 8 GB |
| Development | 8+ GB |
Expected storage use
| Storage | |
|---|---|
| Agent | 500 MB (2x to enable updates) |
| Average Application (docker image) | 500 MB - 2 GB |
| Average Application (source) | <100 MB |
| Average Application (model) | 5 MB - 500 MB |
| Events (video /images/files) | depends on use case |
Installation of the agent
Uninstallation of the agent
Command Line
1sudo robothub-uninstallRequires root privileges