# OAK vs StereoLabs ZED

Compared to StereoLabs ZED cameras, OAK cameras feature a ton of on-device features (stereo depth estimation/disparity matching,
custom AI models, object tracking, scripting, encoding etc.).

![OAK cameras next to StereoLabs ZED 2i](https://docs.luxonis.com/static/images/hardware/comparison/vs-zed-devices.webp)

## Overview

Here's a quick comparison of on-device capabilities between OAK cameras and ZED cameras. More details can be found at [On-device
feature comparison](#On-device%20feature%20comparison).

| On-device capability | OAK Cameras | ZED cameras |
| --- | --- | --- |
| Camera ISP | ✔️ | ✔️ |
| Stereo matching | ✔️ | - |
| Stereo postprocessing | ✔️ | - |
| AI processing | ✔️ | - |
| CV processing | ✔️ | - |
| Video encoding | ✔️ | - |

Essentially, ZED cameras require a powerful host computer with beefy NVIDIA GPU to process the stereo data and run AI models. OAK
cameras can do all the processing on-device, eliminating the need for a powerful host (see [Host
requirements](#Host%20requirements) for details).

## Depth accuracy comparison

From our own evaluation (details at [Stereo cameras accuracy comparison blog
post](https://discuss.luxonis.com/blog/3734-depth-accuracy-comparison-luxonis-oak-vs-stereolab-zed-vs-intel-realsense)), we found
that among the tested cameras, the OAK-D Long Range delivers the most impressive long-range depth accuracy. Its 15cm baseline
significantly reduces depth errors, making it ideal for applications requiring extended-range perception.

Camera Performance Overview

 * OAK-D Long Range: Excels in long-range performance with a 15cm baseline, ensuring great depth accuracy and minimal errors at
   greater distances.
 * ZED 2i: Performs well at long ranges, benefiting from a 12cm baseline and high 2K resolution.
 * OAK-D Pro: Provides a balanced active stereo depth estimation performance across various distances with its 7.5cm baseline.

![OAK vs ZED 2i depth error chart](https://docs.luxonis.com/static/images/hardware/comparison/oak-vs-zed.webp)

For more details, please visit [Depth Accuracy comparison
docs](https://docs.luxonis.com/hardware/platform/depth/depth-accuracy.md).

## Host requirements

### OAK Cameras

With most processing occurring on the device, OAK cameras can efficiently run on low-powered host computers like the [Raspberry Pi
Zero](https://docs.luxonis.com/hardware/platform/deploy/to-rpi.md).

### ZED Cameras

 * No Onboard Compute: All AI and depth processing are handled by a connected host, which demands considerably more processing
   power.
 * Minimum System Requirements for ZED Series (ZED 2i, etc.): * CPU: Dual-core 2.3GHz or faster
    * RAM: At least 4GB
    * GPU: NVIDIA GPU with Compute Capability > 3.0 (required for real-time depth processing)
 * ZED X Series (ZED X, ZED X Mini) Requirements * Requires NVIDIA Jetson AGX Orin / Orin NX for operation

## Comparison overview

| Specification | [OAK-D Pro](hw-catalog://OAK-D Pro) / [-W](hw-catalog://OAK-D Pro W) | [OAK-D Lite](hw-catalog://OAK-D Lite) |
[OAK ToF](hw-catalog://OAK-D ToF) | [ZED
Mini](https://cdn.sanity.io/files/s18ewfw4/staging/ebcd46896092d1ee6212b7f4d81aaa1c479c2440.pdf/ZED%20Mini%20Datasheet%20v1.1.pdf)
| [ZED
2i](https://cdn.sanity.io/files/s18ewfw4/staging/c059860f8fe49f3856f6b8da770eb13cc543ac2c.pdf/ZED%202i%20Datasheet%20v1.2.pdf) 4mm
/ 2.1mm |
| --- | --- | --- | --- | --- | --- |
| RGB | IMX378 | IMX214 | IMX378 | OV4689 | OV4689 |
| RGB HFOV | 66˚ / 109˚ | 69˚ | 66˚ | 102˚ | 72˚ / 110˚ |
| RGB Shutter | Rolling / Global | Rolling | Rolling | Rolling | Rolling |
| RGB resolution | 12MP | 13MP | 12MP | 4MP | 4MP |
| Depth Type | Active Stereo | Passive Stereo | ToF | Passive Stereo | Passive Stereo |
| Depth sensor | OV9282 | OV7251 | 33D ToF | OV2740 | OV9282 |
| Stereo Shutter | Global | Global | / | Rolling | Rolling |
| Stereo baseline | 7.5cm | 7.5cm | / | 6.3cm | 12cm |
| Depth HFOV | 72˚ / 127˚ | 72˚ | 70˚ | 102˚ | 72˚ / 110˚ |
| Min Depth | 20 cm | 20 cm | 20 cm | 10 cm | 150 cm / 30 cm |
| Depth resolution | 1280x800 | 640x480 | 1280x800 | 1920x1080 | 1920x1080 |
| IR LED | ✔️ | - | ✔️ | - | - |
| ToF | - | - | ✔️ | - | - |
| IMU | ✔️ | - | ✔️ | ✔️ | ✔️ |
| Barometer | - | - | - | - | ✔️ |

## Modular design

Our platform was built from the ground up with the idea of being customizable. All of our products based on
[OAK-SoM](hw-catalog://OAK-SoM (sets)) are open-source so you can easily redesign the board (see [Integrating DepthAI into
products](https://docs.luxonis.com/hardware/platform/deploy/oak2-som-development-guide.md)), for example to change the stereo
baseline distance or use a different image sensor (we support [a bunch of different
sensors](https://docs.luxonis.com/hardware/platform/sensors/sensors.md)).

OAK FFC line is great for prototyping, as it allows users to use different camera sensors/optics and place them at an ideal stereo
baseline distance for their application.

Below is a long-range disparity depth visualized over a color frame. This customer used narrow FOV M12 lenses with wide stereo
baseline distance (25cm) to achieve such results with our platform.

![Long-range disparity depth over color frame](https://user-images.githubusercontent.com/18037362/184261853-7d447b7d-1ff9-4c8d-871c-eb230591eae1.png)

See [stereo depth documentation](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md) on max depth
perception calculations based on camera intrinsics/baseline distance.

## On-device feature comparison

OAK cameras integrate a wide range of advanced processing capabilities directly on-device, eliminating the need for a powerful
external host. In contrast, StereoLabs™ ZED cameras rely entirely on host-based processing. Here's a snapshot of what Luxonis
offers:

 * Custom AI models - You can run any AI/NN model(s) on the device, as long as all layers are supported. You can also choose from
   200+ pretrained NN models from [Open Model Zoo](https://github.com/openvinotoolkit/open_model_zoo) and [DepthAI Model
   Zoo](https://github.com/luxonis/depthai-model-zoo).
 * Object detection - Most popular object detectors have been converted and run on our devices. DepthAI supports onboard decoding
   of Yolo and MobileNet based NN models.
 * Object tracking - [ObjectTracker](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/object_tracker.md) node
   comes with 4 tracker types, and it also supports tracking of objects in 3D space.
 * On-device scripting - [Script](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/script.md) node enables
   users to run custom Python 3.9 scripts that will run on the device, used for managing the flow of the pipeline (business
   logic).
 * Video/Image encoding - [VideoEncoder](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/video_encoder.md)
   node allows encoding into MJPEG, H265, or H264 formats.
 * Image Manipulation - [ImageManip](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/image_manip.md) node
   allows users to resize, warp, crop, flip, and thumbnail image frames and do type conversions (YUV420, NV12, RGB, etc.)
 * Skeleton/Hand Tracking - Detect and track key points of a hand or human pose. Geaxgx's demos: [Hand
   tracker](https://github.com/geaxgx/depthai_hand_tracker), [Blazepose](https://github.com/geaxgx/depthai_blazepose),
   [Movenet](https://github.com/geaxgx/depthai_movenet).
 * 3D Semantic segmentation - Perceive the world with semantically-labeled pixels. [DeeplabV3 demo
   here](https://github.com/luxonis/oak-examples/tree/master/gen2-deeplabv3_depth).
 * 3D Object Pose Estimation - MediaPipe's
   [Objectron](https://github.com/google-ai-edge/mediapipe/blob/master/docs/solutions/objectron.md) has been converted to run on
   OAK cameras. Video [here](https://youtu.be/C3M_JOtmQCk).
 * 3D Edge Detection - [EdgeDetector](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/edge_detector.md) node
   uses Sobel filter to detect edges. With depth information, you can get physical position of these edges.
 * Feature Tracking - [FeatureTracker](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/feature_tracker.md)
   node detects and tracks key points (features).
 * 3D Feature Tracking - With depth information, you can track these features in physical space.
 * OCR - Optical character recognition, [demo here](https://github.com/luxonis/oak-examples/tree/master/gen2-ocr).