# Deploy with Raspberry Pi

Our devices can also be connected to small SBCs like a Raspberry Pi (RPi). To install
[DepthAI](https://github.com/luxonis/depthai-python) on a RPi, you should install
[dependencies](https://docs.luxonis.com/software/depthai/manual-install.md) and then install the [DepthAI
library](https://docs.luxonis.com/software/depthai/manual-install.md) with `pip`.

DepthAI library has prebuilt wheels for RPi on [PyPi](https://pypi.org/project/depthai/).

## Using pre-configured RPi OS image

We provide Raspberry Pi OS images that have DepthAI and all its dependencies pre-installed. [Pre-configured RPi images are
available here](https://drive.google.com/drive/folders/1O50jPpGj_82jkAokdrsG--k9OBQfMXK5?usp=sharing).

 * OAK_CM4_POE - Uses RPi OS (default one), has pre-installed DepthAI. Required hardware: 8 GB uSD card or larger. This image is
   flashed on uSD cards that get sent with [OAK-D CM4](https://shop.luxonis.com/products/oak-d-cm4) and [OAK-D CM4
   PoE](https://shop.luxonis.com/products/oak-d-cm4-poe). To enable 2nd uSD card, see workaround
   [here](#Known%20image%20limitations). We recommend that users use this image for all OAK cameras.
 * KS_Rpi_OS_Full - Uses RPi Full OS, has pre-installed DepthAI and [CEP](https://github.com/cortictechnology/cep). Required
   hardware: 32 GB uSD card or larger, RPi 4 with 4 GB RAM. This image was flashed on uSD cards that were sent to KickStarter
   backers. Only use this image if you want CEP platform!

Steps taken to create these images and changelog can be found
[here](https://docs.google.com/document/d/1c4JhIY2ulcgaaycUBOsAbUI1EJ_7Zx4ux4alaxFc_ts/edit?usp=sharing).

### Flashing uSD card

 1. Download the RPi image from Google Drive (link above). Download [Balena Etcher](https://www.balena.io/etcher) program. You can
    also use RPi Imager, but we have noticed that sometimes there are issues.
 2. Open Balena Etcher. If you have downloaded .AppImage, you might need to right-click on it and click Run to start the program.
 3. Click on the Flash from file and select the .zip image you have previously downloaded.
 4. Select the target uSD card.
 5. Click Flash! and wait until it's finished.
 6. After flashing is complete, safely remove the uSD card, insert it into RPi, and power the RPi

## Powering OAK from RPi

On [RPi documentation](https://www.raspberrypi.com/documentation/computers/raspberry-pi.html#typical-power-requirements), it
states that Raspberry Pi 2 or later models can supply up to 1.2A through a USB port. With simple pipelines, OAK cameras draw less
than 1A, which means that you could power an OAK camera directly from RPi via USB-C cable, except if:

 * Your pipeline is complex - especially video encoding and AI inferencing create power peaks that can lead to brownout.
 * You have additional USB devices connected to a RPi USB port that draw too much current. In total, RPi can supply 1.2A, so if
   all USB devices draw more than 1.2A, brownout will occur.
   > **Bypass current limitation**
   > Check [this guide](https://raspberrypi.stackexchange.com/questions/104038/can-the-pi-4-power-2-external-usb-3-hdds/104044#104044) on how to bypass the current limitation. Note that this will void your warranty.
 * You have the Pro version of the OAK camera that has IR laser dot projector and IR illumination LED, which additionally draw up
   to 0.25A.

We still recommend externally powering your OAK camera either via barrel jack (on older devices), or with a
[Y-adapter](hw-catalog://Y-adapter). The reason is that OAK have current spikes (especially when using Video Encoder and running
AI inference), which can lead to brownout.

## SSH into the RPi

If you are using a pre-configured RPi OS image, SSH server is already enabled, otherwise you need to create file `ssh` inside this
boot volume, so SSH server will be enabled on startup ([tutorial
here](https://linuxize.com/post/how-to-enable-ssh-on-raspberry-pi/)).

If you have RPi with WiFi connectivity, you can set the WiFi SSID/Password by creating (and editing) `wpa_supplicant.conf` inside
the boot volume ([tutorial here](https://raspberrytips.com/raspberry-pi-wifi-setup)).

After connecting RPi via ethernet/WiFi to the same LAN as your computer, you can SSH into the RPi with the command below. If RPi
and computer are not in the same LAN, you will have to specify RPi's IP instead of `luxonis.local` - which is the default name of
your RPi on pre-configured RPi images.

```bash
ssh pi@luxonis.local -X
```

`-X` argument enables X11 forwarding on Linux - so OpenCV's `imshow` images will get forwarded to your computer via SSH. On MacOS,
X11 isn't installed by default, so you have [to download it](https://www.xquartz.org), more information
[here](https://www.raspberrypi.com/documentation/computers/remote-access.html#secure-shell-from-linux-or-mac-os).

When you SSH into the RPi for the first time, it will warn you about authenticity, like the log below.

```bash
The authenticity of host 'raspberrypi.local (192.168.1.222)' can't be established.
ECDSA key fingerprint is SHA256:stb5mbRQeX6veOq8Wzg81rz9IHonxJR2++Q8bDYryTo.
Are you sure you want to continue connecting (yes/no/[fingerprint])?
```

type `yes` to continue.

After this command, you will need to provide the password. The default RPi OS password is `raspberry`. You should change it.

After SSH was successful, let's try running an example app:

```bash
python depthai-python/examples/MobileNet/rgb_mobilenet.py
```

## Known image limitations

 1. On OAK_CM4_PoE, since image V8, second uSD card support is disabled. That's because if uSD card support is enabled (for
    storage purposes), WiFi connectivity is disabled. To enable 2nd uSD card support (and disable WiFi connectivity), you can edit
    `/boot/config.txt` and uncomment the line `dtoverlay=sdhost,poll_once=off` at the end of the file, then reboot the system.

## Flashing an image to the eMMC

[OAK-D CM4](hw-catalog://OAK-D CM4) and [OAK-D CM4 PoE](hw-catalog://OAK-D CM4 PoE) have Raspberry Pi Compute module 4 (CM4)
on-board. Most OAK-D-CM4 batches have CM4 with an eMMC memory on there, and most OAK-D CM4 PoE boards have CM4 Lite, which doesn't
have eMMC memory, but instead boots from the uSD card. It's straight forward how to flash an image to the uSD card, and here we
will go through the process of flashing an image to the eMMC that's on the CM4.

Here's an OAK-D-CM4, which has CM4 with eMMC memory that is indicated by the red arrow. CM4 Lite versions won't have this chip in
that location.

To flash an image to the CM4 eMMC ([official RPi
guide](https://www.raspberrypi.com/documentation/computers/compute-module.html#flashing-the-compute-module-emmc)), first need to
enable USB_BOOT with the header pin. By default, connector is on the 2 header pins that are indicated as `DIS` (disabled), so we
have to move the connector to the `EN` pins (enabled).

After switching the pin connector to `EN`, we can connect a micro-USB cable from our computer to the micro-USB connector that's
also indicated by the red rectangle above. After connecting the micro-USB, you should supply the power via 5V barrel jack.

After connecting both the micro-USB and power, we need to enable RPi USB boot. We have followed the [tutorial
here](https://github.com/raspberrypi/usbboot). After building the program and running it, you should see something similar:

```bash
/Documents/usbboot$ sudo ./rpiboot
RPIBOOT: build-date Apr 21 2022 version 20220315~121405 445356e1
Waiting for BCM2835/6/7/2711...
Loading embedded: bootcode4.bin
Sending bootcode.bin
Successful read 4 bytes
Waiting for BCM2835/6/7/2711...
Loading embedded: bootcode4.bin
Second stage boot server
Loading embedded: start4.elf
File read: start4.elf
Second stage boot server done
```

After the boot is done, you should see the eMMC memory inside [Raspberry Pi Imager](https://www.raspberrypi.com/software) or
[Balena Etcher](https://www.balena.io/etcher) (what we have used, screenshot below), so you can easily flash desired image to the
eMMC. After flashing is complete, make sure to disable the USB boot (by switching the connector again) and restart the device. It
should boot from the newly flashed image!

## Raspberry Pi Zero

[Raspberry Pi Zero](https://www.raspberrypi.com/products/raspberry-pi-zero) is a great single-board computer (SBC) in terms of
price per performance. You can get one for about $5. It has 512MB RAM, 1GHz single-core CPU, and optional on-board Bluetooth and
WiFi connectivity (RPI Zero W, which costs about $10). It consumes about 0.5W.

RPi Zero is sufficient for streaming metadata (NN results), low-resolution encoded videos, or light computing. If you intend to
stream high-res videos, perform heavy computing (e.g. with OpenCV) or post-processing, RPi Zero won't be the best choice for host
computer.

### Connect OAK camera to a RPI Zero

RPI Zero has one micro USB connector for peripherals. You can use your standard USB-C (to USB-A) cable, but you will need OTG
connector/cable to connect an OAK camera to the RPI Zero.

All of the above options work. We are not connected/affiliated with these companies, but here's where we got the left connector
([Aliexpress](https://www.aliexpress.com/item/1005001873492004.html?spm=a2g0o.productlist.0.0.4259778c8zzJWk&algo_pvid=108d8130-3b53-4e3b-98ab-e025d519330d&algo_exp_id=108d8130-3b53-4e3b-98ab-e025d519330d-1&pdp_ext_f=%7B%22sku_id%22%3A%2212000022480660847%22%7D)),
and right connector
([Aliexpress](https://www.aliexpress.com/item/1005001894832301.html?spm=a2g0o.productlist.0.0.4259778c8zzJWk&algo_pvid=108d8130-3b53-4e3b-98ab-e025d519330d&algo_exp_id=108d8130-3b53-4e3b-98ab-e025d519330d-0&pdp_ext_f=%7B%22sku_id%22%3A%2212000018040382364%22%7D)).

From our testing, RPi Zero was able to provide enough power to the OAK-D without an external power supply (either power jack or
[Y-adapter](hw-catalog://Y-adapter)).

## RPi Troubleshooting

### RPi Locking Up / OAK crashing on RPi

The Raspberry Pi has a max limit of 1.2A across all its USB ports, and OAK cameras can take up to 1A (at max power, usually closer
to 500mA).

So if you are seeing lockups, it could be that you are over this 1.2A limit as a result of the total power of the USB devices
drawing from the Pi. Using a powered hub can prevent this, or powering fewer other things off of the Pi over USB.

This may also manifest in OAK randomly crashing on the Pi. This can become particularly often if OAK is configured to do many
things at once. This is becoming increasingly likely as we enable DepthAI to do more and more things at once - and thereby
increase the maximum power that OAK can pull. It is seeming like the peak power (current) spikes from OAK can go over what the Pi
can handle, causing OAK to brown-out and return an error.

So if you are experiencing issues with DepthAI stability on Raspberry, try powering OAK camera via a power-supply and/or a powered
USB hub to see if the error goes away.

### SSH-ing without X11 forwarding

If you SSH into your RPi without `-x` argument and try to display a frame (eg. `cv2.imshow()`), you will likely get an error like
below:

 * `(-2:Unspecified error) Can't initialize GTK backend in function 'cvInitSystem'`
 * `qt.qpa.xcb: could not connect to display. qt.qpa.plugin: Could not load the Qt platform plugin "xcb".`
 * `This application failed to start because no Qt platform plugin could be initialized.`

The solution is to use X11 forwarding when SSHing to the RPi, see [SSH into the RPi](#SSH%20into%20the%20RPi).