# PointCloud

Computes a 3D point cloud from a depth map. Optionally takes an aligned color input to produce colorized point clouds.

> **Note**
> Runs on the host by default. On RVC4 you can offload it to the device with `setRunOnHost(False)`. On RVC2 only host-side processing is supported. Added in DepthAI v3.6.0.

## How to place it

#### Python

```python
import depthai as dai

with dai.Pipeline() as pipeline:
    pointCloud = pipeline.create(dai.node.PointCloud)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto pointCloud = pipeline.create<dai::node::PointCloud>();
```

## Inputs and Outputs

`passthroughDepth` forwards the original depth frame used to compute a given `PointCloudData` output. Useful when input queues are
non-blocking and you need to correlate depth frames with their corresponding point clouds.

## Configuration

All settings can be set via `initialConfig` before pipeline start, or sent at runtime through `inputConfig`. Sending a new config
mid-stream is safe — the node reinitializes automatically when configuration, calibration, or frame transformation changes.

See [PointCloudConfig](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages/pointcloud_config.md) for detailed
descriptions and usage examples.

#### Python

```python
pc = pipeline.create(dai.node.PointCloud)
pc.initialConfig.setOrganized(True)
pc.initialConfig.setLengthUnit(dai.LengthUnit.METER)
pc.initialConfig.setTargetCoordinateSystem(dai.CameraBoardSocket.CAM_A)
pc.setNumFramesPool(8)
```

#### C++

```cpp
auto pc = pipeline.create<dai::node::PointCloud>();
pc->initialConfig->setOrganized(true);
pc->initialConfig->setLengthUnit(dai::LengthUnit::METER);
pc->initialConfig->setTargetCoordinateSystem(dai::CameraBoardSocket::CAM_A);
pc->setNumFramesPool(8);
```

## Coordinate system

By default the node reads `T_frame_to_ref` from the depth frame's `ImgTransformation` extrinsics and applies it, so the output
point cloud is in the reference (origin) camera coordinate system. On top of that, you can apply one of three additional
transformations:

### 1. Camera socket coordinate system

Transform the point cloud into the coordinate system of another camera on the device (e.g. `CameraBoardSocket.CAM_A`). The origin
is at the camera sensor, rotation follows the camera's optical frame. The node uses the device calibration to compute the
extrinsic transformation automatically.

```python
# Point cloud in the coordinate system of the color camera (CAM_A)
pc.initialConfig.setTargetCoordinateSystem(dai.CameraBoardSocket.CAM_A)
```

### 2. Housing coordinate system

Transform the point cloud into a housing coordinate system. This uses the device's housing coordinate definitions to express all
points relative to a physical point on the device enclosure.

```python
# Point cloud in the VESA mount coordinate system
pc.initialConfig.setTargetCoordinateSystem(dai.HousingCoordinateSystem.VESA_A)
```

Available housing coordinate systems:

 * `HousingCoordinateSystem.CAM_A` – `CAM_D` — Origin at the same point as `CameraBoardSocket.CAM_A` – `CAM_D`. The difference is
   rotation: the X-Y plane is parallel to the front glass of the device, whereas camera socket coordinate systems are rotated to
   the camera's optical frame.
 * `HousingCoordinateSystem.FRONT_CAM_A` – `FRONT_CAM_D` — Positioned similarly to `HousingCoordinateSystem.CAM_A` – `CAM_D`, but
   shifted forward to the front side of the front glass.
 * `HousingCoordinateSystem.VESA_A` – `VESA_J` — Device mounting points.
 * `HousingCoordinateSystem.IMU` — IMU sensor origin.

### 3. Custom transformation matrix

Apply an arbitrary 4×4 transformation matrix representing `T_ref_to_custom` — the transform from the reference camera to your
custom coordinate system. The node composes it with the frame extrinsics to get the final applied transform:

```python
# 90° rotation around Z axis
transform = [
    [0.0, -1.0, 0.0, 0.0],
    [1.0,  0.0, 0.0, 0.0],
    [0.0,  0.0, 1.0, 0.0],
    [0.0,  0.0, 0.0, 1.0],
]
pc.initialConfig.setTransformationMatrix(transform)
```

If no coordinate system target is set and the transformation matrix is identity, only the frame extrinsics (`T_frame_to_ref`) are
applied, bringing points into the reference camera frame.

### Interaction between options

The three modes are mutually exclusive. Setting a camera socket or housing coordinate system sets the coordinate system type to
`CAMERA_SOCKET` or `HOUSING` respectively — in those modes the custom transformation matrix from `setTransformationMatrix` is
ignored. The custom matrix is only used when the coordinate system type is `DEFAULT` (i.e. neither `setTargetCoordinateSystem`
overload was called).

All three methods can also be called on the node directly (forwarded to `initialConfig`):

```python
pc.setTargetCoordinateSystem(dai.CameraBoardSocket.CAM_A)
# or
pc.setTargetCoordinateSystem(dai.HousingCoordinateSystem.VESA_A)
```

## Usage

### Point cloud from stereo depth

Generate a basic point cloud from stereo depth.

#### Python

```python
import depthai as dai

pipeline = dai.Pipeline()

left = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B)
right = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_C)
stereo = pipeline.create(dai.node.StereoDepth)
left.requestOutput((640, 400)).link(stereo.left)
right.requestOutput((640, 400)).link(stereo.right)

pc = pipeline.create(dai.node.PointCloud)
pc.initialConfig.setLengthUnit(dai.LengthUnit.METER)
stereo.depth.link(pc.inputDepth)

q = pc.outputPointCloud.createOutputQueue(maxSize=4, blocking=False)

with pipeline:
    pipeline.start()
    while pipeline.isRunning():
        pclData = q.get()
        points = pclData.getPoints()  # np.ndarray (N, 3) float32
        print(f"Points: {len(points)}, Z=[{pclData.getMinZ():.2f}, {pclData.getMaxZ():.2f}]")
```

#### C++

```cpp
#include <iostream>
#include "depthai/depthai.hpp"

int main() {
    dai::Pipeline pipeline;

    auto left = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_B);
    auto right = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_C);
    auto stereo = pipeline.create<dai::node::StereoDepth>();
    left->requestOutput(std::make_pair(640, 400))->link(stereo->left);
    right->requestOutput(std::make_pair(640, 400))->link(stereo->right);

    auto pc = pipeline.create<dai::node::PointCloud>();
    pc->initialConfig->setLengthUnit(dai::LengthUnit::METER);
    stereo->depth.link(pc->inputDepth);

    auto q = pc->outputPointCloud.createOutputQueue(4, false);

    pipeline.start();
    while(pipeline.isRunning()) {
        auto pclData = q->get<dai::PointCloudData>();
        auto points = pclData->getPoints();
        std::cout << "Points: " << points.size()
                  << ", Z=[" << pclData->getMinZ() << ", " << pclData->getMaxZ() << "]" << std::endl;
    }
    pipeline.stop();
    return 0;
}
```

### Colorized point cloud

Link depth and color images aligned to the same coordinate system. Typically the depth is aligned to the color camera.

#### Python

```python
import depthai as dai

pipeline = dai.Pipeline()

left = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B)
right = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_C)
color = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_A)

stereo = pipeline.create(dai.node.StereoDepth)
left.requestFullResolutionOutput().link(stereo.left)
right.requestFullResolutionOutput().link(stereo.right)

colorOut = color.requestOutput((640, 400), type=dai.ImgFrame.Type.RGB888i,
                               resizeMode=dai.ImgResizeMode.CROP, enableUndistortion=True)

pc = pipeline.create(dai.node.PointCloud)
pc.initialConfig.setLengthUnit(dai.LengthUnit.METER)

# Align depth to the color camera
platform = pipeline.getDefaultDevice().getPlatform()
if platform == dai.Platform.RVC4:
    imageAlign = pipeline.create(dai.node.ImageAlign)
    stereo.depth.link(imageAlign.input)
    colorOut.link(imageAlign.inputAlignTo)
    imageAlign.outputAligned.link(pc.inputDepth)
else:
    colorOut.link(stereo.inputAlignTo)
    stereo.depth.link(pc.inputDepth)

colorOut.link(pc.inputColor)

q = pc.outputPointCloud.createOutputQueue(maxSize=4, blocking=False)

with pipeline:
    pipeline.start()
    while pipeline.isRunning():
        pcd = q.get()
        if pcd.isColor():
            xyz, rgba = pcd.getPointsRGB()
            print(f"Points: {len(xyz)}, color=yes, Z=[{pcd.getMinZ():.2f}, {pcd.getMaxZ():.2f}]")
```

#### C++

```cpp
#include <iostream>
#include "depthai/depthai.hpp"

int main() {
    dai::Pipeline pipeline;

    auto left = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_B);
    auto right = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_C);
    auto color = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_A);

    auto stereo = pipeline.create<dai::node::StereoDepth>();
    left->requestFullResolutionOutput()->link(stereo->left);
    right->requestFullResolutionOutput()->link(stereo->right);

    auto colorOut = color->requestOutput(std::make_pair(640, 400), dai::ImgFrame::Type::RGB888i,
                                         dai::ImgResizeMode::CROP, std::nullopt, true);

    auto pc = pipeline.create<dai::node::PointCloud>();
    pc->initialConfig->setLengthUnit(dai::LengthUnit::METER);

    auto platform = pipeline.getDefaultDevice()->getPlatform();
    if(platform == dai::Platform::RVC4) {
        auto imageAlign = pipeline.create<dai::node::ImageAlign>();
        stereo->depth.link(imageAlign->input);
        colorOut->link(imageAlign->inputAlignTo);
        imageAlign->outputAligned.link(pc->inputDepth);
    } else {
        colorOut->link(stereo->inputAlignTo);
        stereo->depth.link(pc->inputDepth);
    }

    colorOut->link(pc->getColorInput());

    auto q = pc->outputPointCloud.createOutputQueue(4, false);

    pipeline.start();
    while(pipeline.isRunning()) {
        auto pcd = q->get<dai::PointCloudData>();
        if(pcd->isColor()) {
            auto points = pcd->getPointsRGB();
            std::cout << "Points: " << points.size() << ", color=yes"
                      << ", Z=[" << pcd->getMinZ() << ", " << pcd->getMaxZ() << "]" << std::endl;
        }
    }
    pipeline.stop();
    return 0;
}
```

## Examples

 * [PointCloud](https://docs.luxonis.com/software-v3/depthai/examples/pointcloud/point_cloud.md) — Minimal colorized point cloud
   example.
 * [PointCloud Visualizer](https://docs.luxonis.com/software-v3/depthai/examples/pointcloud/point_cloud_visualizer.md) — Live 3D
   visualization with Open3D.
 * [PointCloud Showcase](https://docs.luxonis.com/software-v3/depthai/examples/pointcloud/point_cloud_showcase.md) — Demonstrates
   filtered, organized, coordinate transforms, custom matrix, and colorized modes.

## Reference

### dai::node::PointCloud

Kind: class

PointCloud node. Computes point cloud from depth frames.

One depth stream is linked to inputDepth (optionally colorized through getColorInput() ). Additional depth streams can be linked
with getDepthInput(name) ; every stream is deprojected with its own intrinsics, transformed into the common target coordinate
system using its frame extrinsics and the merged result is sent as a single PointCloudData message. Depth streams from several
devices share a coordinate system once the pipeline carries a multi-device calibration ( Pipeline::setMultiDeviceCalibration ). On
the host the streams of a synced group are deprojected concurrently, one thread per stream; useCPUMT additionally splits every
stream over several threads. useGPU computes on the GPU: on an RVC4 device through OpenCL, on the host through Kompute when
compiled in. The compute method is part of the node properties, so it also applies when the node runs on the device. The output
can be expressed in the coordinate system of any camera socket or housing of any device in the pipeline
(setTargetCoordinateSystem). Targets on another device than the one owning the reference camera of a depth frame are resolved
through the multi-device calibration of the pipeline and the calibration of the target device.

#### dai::node::PointCloud::Impl

Kind: class

##### LengthUnit targetLengthUnit

Kind: variable

##### Impl()

Kind: function

##### void setLogger(const std::shared_ptr<::spdlog::logger > & log)

Kind: function

##### void computePointCloudDense(const uint8_t * depthData, std::vector< Point3f > & points)

Kind: function

##### void computePointCloudDenseColored(const uint8_t * depthData, const uint8_t * colorData, std::vector< Point3fRGBA > & points)

Kind: function

##### const Point3f * computeDenseOnGpu(const uint8_t * depthData, const std::shared_ptr< Memory > & depthMemory)

Kind: function

##### const Point3fRGBA * computeDenseColoredOnGpu(const uint8_t * depthData, const std::shared_ptr< Memory > & depthMemory, const uint8_t * colorData, const std::shared_ptr< Memory > & colorMemory)

Kind: function

##### void applyTransformation(std::vector< PointT > & points)

Kind: function

##### std::vector< PointT > filterValidPoints(const std::vector< PointT > & densePoints)

Kind: function

##### void setLengthUnit(dai::LengthUnit lengthUnit)

Kind: function

##### void useCPU()

Kind: function

##### void useCPUMT(uint32_t numThreads)

Kind: function

##### void useGPU(uint32_t device, std::shared_ptr< internal::PointCloudGpuBackend > backend)

Kind: function

Compute through backend when given, otherwise through Kompute on GPU device when compiled in. Throws when neither is available.

##### void setIntrinsics(float fx, float fy, float cx, float cy, unsigned int width, unsigned int height)

Kind: function

##### void setDistortion(CameraModel model, std::vector< float > coefficients)

Kind: function

##### void setExtrinsics(const std::vector< std::vector< float >> & transformMatrix)

Kind: function

##### void clearExtrinsics()

Kind: function

##### bool usesGPU()

Kind: function

#### dai::Backend Backend

Kind: enum

Backend preference for ImageManip on RVC4. CPU: Run ImageManip on the CPU.; HW: Prefer the dedicated hardware image manipulation
backend.; GPU: Prefer the GPU backend.; AUTO: Let the runtime select the backend automatically (GPU with CPU fallback).
Hardware-accelerated backends can cause some unexpected behavior when using multiple ImageManip nodes in series. Currently, the
only operation affected is downscaling.

##### CPU

Kind: enum_value

##### HW

Kind: enum_value

##### GPU

Kind: enum_value

##### AUTO

Kind: enum_value

#### std::shared_ptr< PointCloudConfig > initialConfig

Kind: variable

Initial config to use when computing the point cloud.

#### Input inputConfig

Kind: variable

Input PointCloudConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.

#### Subnode < node::Sync > sync

Kind: variable

Sync subnode for synchronized depth + color input. When only depth is connected, Sync passes through single-item MessageGroups.
When both depth and color are connected, Sync pairs them by timestamp.

#### InputMap & syncInputs

Kind: variable

#### Input & inputDepth

Kind: variable

Input message with depth data used to create the point cloud. Routed through the internal Sync subnode. Equivalent to
getDepthInput("").

#### Output outputPointCloud

Kind: variable

Outputs PointCloudData message

#### Output passthroughDepth

Kind: variable

Passthrough depth from which the point cloud was calculated. Suitable for when input queue is set to non-blocking behavior. With
several depth streams every depth frame of the merged group is passed through, in stream order.

#### PointCloud()

Kind: function

#### PointCloud(std::unique_ptr< Properties > props)

Kind: function

#### ~PointCloud()

Kind: function

#### Input & getColorInput()

Kind: function

Get the optional color input for colorized point clouds. Lazily creates the Sync entry so that depth-only mode works without Sync
waiting for a color frame that never arrives. Link an aligned color image (RGB888i, same dimensions as depth) to this input to
enable colored point cloud output.

#### Input & getDepthInput(const std::string & name)

Kind: function

Get (or create) an additional depth input. Every depth stream linked to this node is synchronized by the internal Sync subnode,
deprojected with its own intrinsics and transformed into the target coordinate system using its frame extrinsics. The clouds of
all streams are merged into one output PointCloudData . All depth frames must therefore share a target coordinate system (
Extrinsics::toDeviceId / Extrinsics::toCameraSocket ); depth from several devices requires a multi-device calibration on the
pipeline. Groups whose streams do not share a coordinate system are dropped with a warning. When the depth streams come from more
than one device and the Sync timestamp source is left at its default, the Sync subnode is moved to the host at build time so that
the streams can be paired with host timestamps. parameters: name: Name of the depth stream. An empty name refers to inputDepth.

#### Input & getColorInput(const std::string & name)

Kind: function

Get (or create) the color input paired with the depth stream name . The output is colorized only when every depth stream has a
matching color frame. parameters: name: Name of the depth stream. An empty name refers to the default color input.

#### std::vector< std::string > getDepthInputNames()

Kind: function

Names of the depth streams of this node (inputDepth and every getDepthInput(name) call), the default (unnamed) stream first.
Streams that are never linked are left out of the synchronization by the Sync subnode.

#### void buildStage1()

Kind: function

Moves the Sync subnode to the host when depth streams come from more than one device.

#### void setNumFramesPool(int numFramesPool)

Kind: function

Specify number of frames in pool. parameters: numFramesPool: How many frames should the pool have

#### void setRunOnHost(bool runOnHost)

Kind: function

Specify whether to run on host or device By default, the node will run on host.

#### PointCloud & setBackend(Backend backend)

Kind: function

Select the compute backend. CPU uses the configured CPU thread count; GPU and AUTO try OpenCL on RVC4 or Kompute on the host and
fall back to CPU when unavailable. CPU is the default. AUTO resolves to GPU with CPU fallback. Dedicated HW acceleration is not
supported. parameters: backend: Backend preference return: This node for chaining parameters: std::invalid_argument: when backend
is HW or an unknown value

#### Backend getBackend()

Kind: function

Get the configured backend (AUTO resolves to GPU); runtime fallback does not change it.

#### PointCloud & setNumThreads(uint32_t numThreads)

Kind: function

Set CPU threads per depth stream. Also selects CPU_MT or CPU when the backend is CPU. GPU fallback remains single-threaded, as
with useGPU() . parameters: numThreads: Thread count; zero is clamped to one. The effective default for CPU is one. return: This
node for chaining

#### uint32_t getNumThreads()

Kind: function

Get the CPU thread count per depth stream; single-threaded CPU reports one.

#### void useCPU()

Kind: function

Use single-threaded CPU for processing (one thread per depth stream on the host). Default.

#### void useCPUMT(uint32_t numThreads)

Kind: function

Use multi-threaded CPU for processing: every depth stream is split over numThreads threads.

#### void useGPU(uint32_t device)

Kind: function

Use GPU for point cloud computation: OpenCL on an RVC4 device, Kompute on the host when compiled in. When no GPU is available at
runtime the node logs a warning and falls back to the CPU. parameters: device: GPU device index (default 0)

#### void setTargetCoordinateSystem(CameraBoardSocket targetCamera)

Kind: function

Set target coordinate system to transform point cloud. The socket is looked up on the device that owns the reference camera of the
depth frame. parameters: targetCamera: Target camera socket

#### void setTargetCoordinateSystem(HousingCoordinateSystem housingCS)

Kind: function

Set target coordinate system to housing coordinate system Point cloud will be transformed to this housing coordinate system of the
device that owns the reference camera of the depth frame. parameters: housingCS: Target housing coordinate system

#### void setTargetCoordinateSystem(const std::string & targetDeviceId, CameraBoardSocket targetCamera)

Kind: function

Set target coordinate system to a camera socket of any device in the pipeline. Depth frames whose reference camera lives on
another device are transformed through the multi-device calibration of the pipeline ( Pipeline::setMultiDeviceCalibration ), which
has to connect the two devices, and the calibration of the target device. Every depth stream is resolved independently, so streams
of several devices can be merged into a cloud expressed in the coordinate system of one of them. Not supported when the node runs
on a device. parameters: targetDeviceId: Device ID of the device owning the target camera socket; targetCamera: Target camera
socket

#### void setTargetCoordinateSystem(const std::string & targetDeviceId, HousingCoordinateSystem housingCS)

Kind: function

Set target coordinate system to a housing coordinate system of any device in the pipeline. See
setTargetCoordinateSystem(targetDeviceId, targetCamera) for how other devices are resolved. parameters: targetDeviceId: Device ID
of the device owning the housing coordinate system; housingCS: Target housing coordinate system

#### void setDeviceCalibration(const std::string & deviceId, const CalibrationHandler & calibration)

Kind: function

Override the calibration used for a device, for recorded/offline streams and tests. The node otherwise reads the calibration of a
device from the pipeline. Only used when the node runs on the host; call it before the pipeline is started. parameters: deviceId:
Device ID the calibration belongs to; calibration: Calibration of that device

#### void setTargetCoordinateSystem(CameraBoardSocket targetCamera, bool useSpecTranslation)

Kind: function

Deprecated: use setTargetCoordinateSystem(targetCamera) instead.

#### void setTargetCoordinateSystem(HousingCoordinateSystem housingCS, bool useSpecTranslation)

Kind: function

Deprecated: use setTargetCoordinateSystem(housingCS) instead.

#### bool runOnHost()

Kind: function

Returns true or false whether the node should be run on host or not.

#### void buildInternal()

Kind: function

Function called from within the create function to build the node. This function is useful for initialization, setting up inputs
and outputs = stuff that cannot be perform in the constuctor.

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.