# SpatialImgDetections

Similar to [ImgDetections](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages/img_detections.md), but this
message includes XYZ coordinates of the detected objects as well.

## Saving and loading

`SpatialImgDetections` messages can be saved to a file with `save()` and read back with `load()`. The saved file is a binary
protobuf envelope.

See [Message `save` and `load` functions](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages.md) for usage.

## Remapping

`SpatialImgDetections` is transformable, which means it can be remapped into another frame's coordinate system. See [`Remapping
transformable messages`](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages.md) for details.

## Examples of functionality

 * [Spatial Detection
   Network](https://docs.luxonis.com/software-v3/depthai/examples/spatial_detection_network/spatial_detection.md)

## Reference

### dai::SpatialImgDetections

Kind: class

SpatialImgDetections message. Carries detection results together with spatial location data

#### ImgDetectionsT < SpatialImgDetection > Base

Kind: typedef

#### LengthUnit unit

Kind: variable

Length unit used by all imgDetections' spatialCoordinates in this list.

#### std::optional< ImgTransformation > transformation

Kind: variable

#### ~SpatialImgDetections()

Kind: function

#### void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)

Kind: function

#### DatatypeEnum getDatatype()

Kind: function

Get the datatype of this specific message.

return: DatatypeEnum

#### SpatialImgDetections transformTo(const ImgTransformation & target)

Kind: function

Returns a new SpatialImgDetections message with the spatial detections transformed into the target image transformation. For each
detection, the bounding box is assumed to lie on a plane parallel to the image plane at depth detection.spatialCoordinates.z (that
is, all four bounding-box corners are projected using the same depth value). The transformed corners are then fit with the
smallest enclosing rotated rectangle to preserve rectangularity. parameters: target: Target image transformation. return:
SpatialImgDetections with transformed detections.

#### DEPTHAI_SERIALIZE(SpatialImgDetections, sequenceNum, ts, tsDevice, tsSystem, detections, transformation, segmentationMaskWidth, segmentationMaskHeight, unit)

Kind: function

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.