# Camera multiple outputs

Example showcases DepthAIv3's functionality to request an output stream directly from the
[Camera](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/camera.md) node, instead of having to create and
configure multiple [ImageManip](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/image_manip.md) nodes.

```python
output1 = camera_node.requestOutput(
    size=(640, 480),
    type=dai.ImgFrame.Type.BGR888p,
    resize_mode=dai.ImgResizeMode.CROP,
    fps=15
)
output2 = cam.requestOutput(
    size=(1000, 500),
    type=dai.ImgFrame.Type.NV12,
    resize_mode=dai.ImgResizeMode.STRETCH,
    fps=20
)
```

Resize mode can be either `CROP`, `STRETCH`, or `LETTERBOX`, which come into play if there's a mismatch between sensor aspect
ratio (AR) and requested aspect ratio. For more information (pros/cons of each) check [Input frame AR
mismatch](https://docs.luxonis.com/software-v3/depthai/tutorials/resolution-techniques.md) documentation.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- XLinkOut (5)
- XLinkOut (3)
- XLinkOut (1)

Pipeline connections:
- Camera(0) -> XLinkOut (5) (0 -> in)
- Camera(0) -> XLinkOut (3) (1 -> in)
- Camera(0) -> XLinkOut (1) (2 -> in)

## Source code

#### Python

```python
#!/usr/bin/env python3

import sys

import cv2
import depthai as dai
import time

# Create pipeline

def exit_usage() -> None:
    print(
        "WRONG USAGE! correct usage example:\n"
        "python camera_multiple_outputs.py 640 480 0 30 CAM_A 300 300 0 30 CAM_A 300 300 1 30 CAM_A \n"
        "where 0 is resize mode: 0 == CROP, 1 == STRETCH, 2 == LETTERBOX\n"
        "and 30 is FPS"
    )
    exit(1)

class FPSCounter:
    def __init__(self):
        self.frameTimes = []

    def tick(self):
        now = time.time()
        self.frameTimes.append(now)
        self.frameTimes = self.frameTimes[-100:]

    def getFps(self):
        if len(self.frameTimes) <= 1:
            return 0
        # Calculate the FPS
        return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])

args = sys.argv[1:]
if len(args) < 5 or len(args) % 5 != 0:
    exit_usage()

with dai.Pipeline() as pipeline:
    cams: dict = {}
    queues = []
    for i in range(0, len(args), 5):
        cap = dai.ImgFrameCapability()
        cap.size.fixed((int(args[i]), int(args[i + 1])))
        cropArg = int(args[i + 2])
        if cropArg == 0:
            cap.resizeMode = dai.ImgResizeMode.CROP
        elif cropArg == 1:
            cap.resizeMode = dai.ImgResizeMode.STRETCH
        elif cropArg == 2:
            cap.resizeMode = dai.ImgResizeMode.LETTERBOX
        else:
            exit_usage()
        cap.fps.fixed(float(args[i + 3]))
        camArg = args[i + 4]
        socket: dai.CameraBoardSocket
        if camArg == "CAM_A":
            socket = dai.CameraBoardSocket.CAM_A
        elif camArg == "CAM_B":
            socket = dai.CameraBoardSocket.CAM_B
        elif camArg == "CAM_C":
            socket = dai.CameraBoardSocket.CAM_C
        elif camArg == "CAM_D":
            socket = dai.CameraBoardSocket.CAM_D
        else:
            exit_usage()
        if socket not in cams:
            cams[socket] = pipeline.create(dai.node.Camera).build(socket)
        queues.append(cams[socket].requestOutput(cap, True).createOutputQueue())

    # Connect to device and start pipeline
    pipeline.start()
    FPSCounters = [FPSCounter() for _ in queues]
    while pipeline.isRunning():
        for index, queue in enumerate(queues):
            videoIn = queue.tryGet()
            if videoIn is not None:
                FPSCounters[index].tick()
                assert isinstance(videoIn, dai.ImgFrame)
                if (videoIn.getSequenceNum() % 60) == 0:
                    print(
                        f"frame {videoIn.getWidth()}x{videoIn.getHeight()} | {videoIn.getSequenceNum()}: exposure={videoIn.getExposureTime()}us, timestamp: {videoIn.getTimestampDevice()}"
                    )
                # Get BGR frame from NV12 encoded video frame to show with opencv
                # Visualizing the frame on slower hosts might have overhead
                cvFrame = videoIn.getCvFrame()
                # Draw FPS
                cv2.putText(cvFrame, f"{FPSCounters[index].getFps():.2f} FPS", (2, 20), cv2.FONT_HERSHEY_SIMPLEX, 0.5, (0, 255, 0))
                cv2.imshow("video " + str(index), cvFrame)

        if cv2.waitKey(1) == ord("q"):
            break
```

#### C++

```cpp
#include <atomic>
#include <chrono>
#include <csignal>
#include <iostream>
#include <map>
#include <memory>
#include <opencv2/opencv.hpp>
#include <vector>

#include "depthai/depthai.hpp"

std::atomic<bool> quitEvent(false);

void signalHandler(int) {
    quitEvent = true;
}

class FPSCounter {
   public:
    void tick() {
        auto now = std::chrono::steady_clock::now();
        frameTimes.push_back(now);
        if(frameTimes.size() > 100) {
            frameTimes.erase(frameTimes.begin());
        }
    }

    float getFps() {
        if(frameTimes.size() <= 1) return 0.0f;
        auto duration = std::chrono::duration_cast<std::chrono::milliseconds>(frameTimes.back() - frameTimes.front()).count();
        return (frameTimes.size() - 1) * 1000.0f / duration;
    }

   private:
    std::vector<std::chrono::steady_clock::time_point> frameTimes;
};

void exitUsage() {
    std::cout << "WRONG USAGE! correct usage example:\n"
              << "./camera_multiple_outputs 640 480 0 30 CAM_A 300 300 0 30 CAM_A 300 300 1 30 CAM_A\n"
              << "where 0 is resize mode: 0 == CROP, 1 == STRETCH, 2 == LETTERBOX\n"
              << "and 30 is FPS" << std::endl;
    exit(1);
}

int main(int argc, char* argv[]) {
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    if(argc < 6 || (argc - 1) % 5 != 0) {
        exitUsage();
    }

    // Create device
    std::shared_ptr<dai::Device> device = std::make_shared<dai::Device>();

    // Create pipeline
    dai::Pipeline pipeline(device);

    // Parse arguments and create cameras
    std::map<dai::CameraBoardSocket, std::shared_ptr<dai::node::Camera>> cams;
    std::vector<std::shared_ptr<dai::MessageQueue>> queues;
    std::vector<FPSCounter> fpsCounters;

    for(int i = 1; i < argc; i += 5) {
        int width = std::stoi(argv[i]);
        int height = std::stoi(argv[i + 1]);
        int resizeMode = std::stoi(argv[i + 2]);
        float fps = std::stof(argv[i + 3]);
        std::string camArg = argv[i + 4];

        // Create capability
        auto cap = std::make_shared<dai::ImgFrameCapability>();
        cap->size.fixed(std::make_pair(width, height));

        // Set resize mode
        switch(resizeMode) {
            case 0:
                cap->resizeMode = dai::ImgResizeMode::CROP;
                break;
            case 1:
                cap->resizeMode = dai::ImgResizeMode::STRETCH;
                break;
            case 2:
                cap->resizeMode = dai::ImgResizeMode::LETTERBOX;
                break;
            default:
                exitUsage();
        }

        cap->fps.fixed(fps);

        // Parse camera socket
        dai::CameraBoardSocket socket;
        if(camArg == "CAM_A")
            socket = dai::CameraBoardSocket::CAM_A;
        else if(camArg == "CAM_B")
            socket = dai::CameraBoardSocket::CAM_B;
        else if(camArg == "CAM_C")
            socket = dai::CameraBoardSocket::CAM_C;
        else if(camArg == "CAM_D")
            socket = dai::CameraBoardSocket::CAM_D;
        else
            exitUsage();

        // Create camera if not exists
        if(cams.find(socket) == cams.end()) {
            cams[socket] = pipeline.create<dai::node::Camera>()->build(socket);
        }

        // Create output queue
        queues.push_back(cams[socket]->requestOutput(*cap, true)->createOutputQueue());
        fpsCounters.push_back(FPSCounter());
    }

    // Start pipeline
    pipeline.start();

    while(pipeline.isRunning() && !quitEvent) {
        for(size_t i = 0; i < queues.size(); i++) {
            auto videoIn = queues[i]->tryGet<dai::ImgFrame>();
            if(videoIn != nullptr) {
                fpsCounters[i].tick();
                if(!(videoIn->getSequenceNum() % 60))
                    std::cout << "frame " << videoIn->getWidth() << "x" << videoIn->getHeight() << " | " << videoIn->getSequenceNum()
                              << ": exposure=" << videoIn->getExposureTime().count()
                              << "us, timestamp: " << videoIn->getTimestampDevice().time_since_epoch().count() << std::endl;

                cv::Mat cvFrame = videoIn->getCvFrame();

                // Draw FPS
                cv::putText(cvFrame,
                            std::to_string(fpsCounters[i].getFps()).substr(0, 4) + " FPS",
                            cv::Point(2, 20),
                            cv::FONT_HERSHEY_SIMPLEX,
                            0.5,
                            cv::Scalar(0, 255, 0));

                cv::imshow("video " + std::to_string(i), cvFrame);
            }
        }

        if(cv::waitKey(1) == 'q') {
            break;
        }
    }

    pipeline.stop();
    pipeline.wait();

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.