# Object Tracker Remap

This example demonstrates running YOLOv6-nano detection with the
[ObjectTracker](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/object_tracker.md) node and remapping
bounding boxes onto a colorized depth frame using transformation metadata, ensuring accurate alignment across streams (RGB ↔
Depth).

## Demo

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- NeuralNetwork (2)
- DetectionParser (3)
- ObjectTracker (4)
- Camera(5)
- StereoDepth (7)
- Camera(6)

Pipeline connections:
- Camera(0) -> NeuralNetwork (2) (0 -> in)
- NeuralNetwork (2) -> DetectionParser (3) (out -> in)
- NeuralNetwork (2) -> ObjectTracker (4) (passthrough -> inputDetectionFrame)
- NeuralNetwork (2) -> ObjectTracker (4) (passthrough -> inputTrackerFrame)
- DetectionParser (3) -> ObjectTracker (4) (out -> inputDetections)
- Camera(5) -> StereoDepth (7) (0 -> left)
- Camera(6) -> StereoDepth (7) (0 -> right)

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai

# Create pipeline
with dai.Pipeline() as pipeline:
    colorSockets = pipeline.getDefaultDevice().getConnectedCameras(dai.CameraSensorType.COLOR)
    colorSocket = colorSockets[0] if colorSockets else dai.CameraBoardSocket.CAM_A
    cameraNode = pipeline.create(dai.node.Camera).build(colorSocket)
    detectionNetwork = pipeline.create(dai.node.DetectionNetwork).build(cameraNode, dai.NNModelDescription("yolov6-nano"))
    objectTracker = pipeline.create(dai.node.ObjectTracker)
    labelMap = detectionNetwork.getClasses()
    depth = pipeline.create(dai.node.Depth).build(dai.node.Depth.Algorithm.AUTO)

    detectionNetwork.out.link(objectTracker.inputDetections)
    detectionNetwork.passthrough.link(objectTracker.inputDetectionFrame)
    detectionNetwork.passthrough.link(objectTracker.inputTrackerFrame)

    qRgb = detectionNetwork.passthrough.createOutputQueue()
    qTrack = objectTracker.out.createOutputQueue()
    qDepth = depth.depth.createOutputQueue()

    pipeline.start()

    def displayFrame(name: str, frame: dai.ImgFrame, tracklets: dai.Tracklets):
        color = (0, 255, 0)
        assert tracklets.getTransformation() is not None
        if(frame.getType() == dai.ImgFrame.Type.RAW16):
            cvFrame = dai.utility.colorizeDepthFrame(frame).getCvFrame()
        else:
            cvFrame = frame.getCvFrame()
        for tracklet in tracklets.tracklets:
            # Get the shape of the frame from which the detections originated for denormalization
            normShape = tracklets.getTransformation().getSize()

            # Create rotated rectangle to remap
            # Here we use an intermediate dai.Rect to create a dai.RotatedRect to simplify construction and denormalization
            rotRect = dai.RotatedRect(tracklet.roi.denormalize(normShape[0], normShape[1]), 0)
            # Remap the detection rectangle to target frame
            remapped = tracklets.getTransformation().remapRectTo(frame.getTransformation(), rotRect)
            # Remapped rectangle could be rotated, so we get the bounding box
            bbox = [int(l) for l in remapped.getOuterRect()]
            cv2.putText(
                cvFrame,
                labelMap[tracklet.label],
                (bbox[0] + 10, bbox[1] + 20),
                cv2.FONT_HERSHEY_TRIPLEX,
                0.5,
                255,
            )
            cv2.putText(
                cvFrame,
                f"{int(tracklet.srcImgDetection.confidence * 100)}%",
                (bbox[0] + 10, bbox[1] + 40),
                cv2.FONT_HERSHEY_TRIPLEX,
                0.5,
                255,
            )
            cv2.rectangle(cvFrame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2)
        # Show the frame
        cv2.imshow(name, cvFrame)

    while pipeline.isRunning():
        inRgb: dai.ImgFrame = qRgb.get()
        inTrack: dai.Tracklets = qTrack.get()
        inDepth: dai.ImgFrame = qDepth.get()
        hasRgb = inRgb is not None
        hasDepth = inDepth is not None
        hasTrack = inTrack is not None
        if hasRgb:
            displayFrame("rgb", inRgb, inTrack)
        if hasDepth:
            displayFrame("depth", inDepth, inTrack)
        if cv2.waitKey(1) == ord("q"):
            pipeline.stop()
            break
```

#### C++

```cpp
#include <iostream>
#include <opencv2/opencv.hpp>
#include <string>
#include <vector>

#include "depthai/depthai.hpp"

// Helper function to display frames with detections
void displayFrame(const std::string& name,
                  std::shared_ptr<dai::ImgFrame> frame,
                  std::shared_ptr<dai::Tracklets> tracklets,
                  const std::vector<std::string>& labelMap) {
    cv::Scalar color(0, 255, 0);
    cv::Mat cvFrame;

    if(frame->getType() == dai::ImgFrame::Type::RAW16) {
        cvFrame = dai::utility::colorizeDepthFrame(*frame).getCvFrame();
    } else {
        cvFrame = frame->getCvFrame();
    }

    if(!tracklets) {
        // std::cout << "No detections or transformation data for " << name << std::endl;
        cv::imshow(name, cvFrame);
        return;
    }

    if(!tracklets->getTransformation().has_value()) {
        return;
    }

    const auto sourceTransform = tracklets->getTransformation().value();
    const auto& targetTransform = frame->transformation;

    for(const auto& tracklet : tracklets->tracklets) {
        auto normShape = sourceTransform.getSize();

        dai::Rect rect = tracklet.roi;
        rect = rect.denormalize(static_cast<float>(normShape.first), static_cast<float>(normShape.second));
        dai::RotatedRect rotRect(rect, 0);

        auto remapped = sourceTransform.remapRectTo(targetTransform, rotRect);
        auto bbox = remapped.getOuterRect();

        cv::putText(cvFrame,
                    labelMap[tracklet.label],
                    cv::Point(static_cast<int>(bbox[0]) + 10, static_cast<int>(bbox[1]) + 20),
                    cv::FONT_HERSHEY_TRIPLEX,
                    0.5,
                    cv::Scalar(255, 255, 255));
        cv::putText(cvFrame,
                    std::to_string(static_cast<int>(tracklet.srcImgDetection.confidence * 100)) + "%",
                    cv::Point(static_cast<int>(bbox[0]) + 10, static_cast<int>(bbox[1]) + 40),
                    cv::FONT_HERSHEY_TRIPLEX,
                    0.5,
                    cv::Scalar(255, 255, 255));
        cv::rectangle(cvFrame,
                      cv::Point(static_cast<int>(bbox[0]), static_cast<int>(bbox[1])),
                      cv::Point(static_cast<int>(bbox[2]), static_cast<int>(bbox[3])),
                      color,
                      2);
    }
    cv::imshow(name, cvFrame);
}

int main() {
    dai::Pipeline pipeline;

    auto colorSockets = pipeline.getDefaultDevice()->getConnectedCameras(dai::CameraSensorType::COLOR);
    auto colorSocket = colorSockets.empty() ? dai::CameraBoardSocket::CAM_A : colorSockets.front();
    auto cameraNode = pipeline.create<dai::node::Camera>();
    cameraNode->build(colorSocket);

    auto detectionNetwork = pipeline.create<dai::node::DetectionNetwork>();
    dai::NNModelDescription modelDescription;
    modelDescription.model = "yolov6-nano";
    detectionNetwork->build(cameraNode, modelDescription);
    auto objectTracker = pipeline.create<dai::node::ObjectTracker>();
    auto labelMap = detectionNetwork->getClasses().value_or(std::vector<std::string>{});

    auto depth = pipeline.create<dai::node::Depth>();
    depth->build(dai::node::Depth::Algorithm::AUTO);

    detectionNetwork->out.link(objectTracker->inputDetections);
    detectionNetwork->passthrough.link(objectTracker->inputDetectionFrame);
    detectionNetwork->passthrough.link(objectTracker->inputTrackerFrame);

    auto qRgb = detectionNetwork->passthrough.createOutputQueue();
    auto qTrack = objectTracker->out.createOutputQueue();
    auto qDepth = depth->depth().createOutputQueue();

    pipeline.start();

    while(pipeline.isRunning()) {
        auto inRgb = qRgb->tryGet<dai::ImgFrame>();
        auto inTrack = qTrack->tryGet<dai::Tracklets>();
        auto inDepth = qDepth->tryGet<dai::ImgFrame>();

        bool hasRgb = inRgb != nullptr;
        bool hasDepth = inDepth != nullptr;
        bool hasTrack = inTrack != nullptr;

        if(hasRgb && hasTrack) {
            displayFrame("rgb", inRgb, inTrack, labelMap);
        }
        if(hasDepth && hasTrack) {
            displayFrame("depth", inDepth, inTrack, labelMap);
        }

        if(cv::waitKey(1) == 'q') {
            pipeline.stop();