# Object Tracker Replay

This example demonstrates running YOLOv6-nano object detection with the
[ObjectTracker](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/object_tracker.md) node on a replayed video
using the ReplayVideo host node (or a live camera when requested).

It displays per-object Track IDs and status;  this demo does not compute XYZ coordinates.

## Demo

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Run

Default (demo clip):

```python
python object_tracker_replay.py
```

Use your own video file:

```python
python object_tracker_replay.py -i /path/to/video.mp4
```

Use the live camera instead of a file:

```python
python object_tracker_replay.py --camera True
```

## Pipeline

Pipeline nodes:
- Camera(0)
- NeuralNetwork (2)
- DetectionParser (3)
- ObjectTracker (4)

Pipeline connections:
- Camera(0) -> NeuralNetwork (2) (0 -> in)
- NeuralNetwork (2) -> DetectionParser (3) (out -> in)
- NeuralNetwork (2) -> ObjectTracker (4) (passthrough -> inputTrackerFrame)
- NeuralNetwork (2) -> ObjectTracker (4) (passthrough -> inputDetectionFrame)
- DetectionParser (3) -> ObjectTracker (4) (out -> inputDetections)

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
import time

from pathlib import Path
from argparse import ArgumentParser

scriptDir = Path(__file__).resolve().parent
examplesRoot = (scriptDir / Path('../')).resolve()  # This resolves the parent directory correctly
models = examplesRoot / 'models'
videoPath = models / 'construction_vest.mp4'

parser = ArgumentParser()
parser.add_argument("-i", "--inputVideo", default=videoPath, help="Input video name")
parser.add_argument("-c", "--camera", type=bool, help="Use camera as input", default=False)
args = parser.parse_args()

# Create pipeline
with dai.Pipeline() as pipeline:
    # Define sources and outputs
    inputSource = None
    if args.camera: 
        camRgb = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_A)
        inputSource = camRgb
    else:
        replay = pipeline.create(dai.node.ReplayVideo)
        replay.setReplayVideoFile(Path(args.inputVideo))
        inputSource = replay

    detectionNetwork = pipeline.create(dai.node.DetectionNetwork).build(inputSource, "yolov6-nano")
    objectTracker = pipeline.create(dai.node.ObjectTracker)

    detectionNetwork.setConfidenceThreshold(0.6)
    detectionNetwork.input.setBlocking(False)
    labelMap = detectionNetwork.getClasses()

    objectTracker.setDetectionLabelsToTrack([0])  # track only person
    # possible tracking types: ZERO_TERM_COLOR_HISTOGRAM, ZERO_TERM_IMAGELESS, SHORT_TERM_IMAGELESS, SHORT_TERM_KCF
    objectTracker.setTrackerType(dai.TrackerType.SHORT_TERM_IMAGELESS)
    # take the smallest ID when new object is tracked, possible options: SMALLEST_ID, UNIQUE_ID
    objectTracker.setTrackerIdAssignmentPolicy(dai.TrackerIdAssignmentPolicy.SMALLEST_ID)

    preview = objectTracker.passthroughTrackerFrame.createOutputQueue()
    tracklets = objectTracker.out.createOutputQueue()

    detectionNetwork.passthrough.link(objectTracker.inputTrackerFrame)

    detectionNetwork.passthrough.link(objectTracker.inputDetectionFrame)
    detectionNetwork.out.link(objectTracker.inputDetections)

    startTime = time.monotonic()
    counter = 0
    fps = 0
    color = (255, 255, 255)
    pipeline.start()
    while(pipeline.isRunning()):
        imgFrame = preview.get()
        track = tracklets.get()
        assert isinstance(imgFrame, dai.ImgFrame), "Expected ImgFrame"
        assert isinstance(track, dai.Tracklets), "Expected Tracklets"

        counter+=1
        current_time = time.monotonic()
        if (current_time - startTime) > 1 :
            fps = counter / (current_time - startTime)
            counter = 0
            startTime = current_time

        frame = imgFrame.getCvFrame()
        trackletsData = track.tracklets
        for t in trackletsData:
            roi = t.roi.denormalize(frame.shape[1], frame.shape[0])
            x1 = int(roi.topLeft().x)
            y1 = int(roi.topLeft().y)
            x2 = int(roi.bottomRight().x)
            y2 = int(roi.bottomRight().y)

            try:
                label = labelMap[t.label]
            except:
                label = t.label

            cv2.putText(frame, str(label), (x1 + 10, y1 + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
            cv2.putText(frame, f"ID: {[t.id]}", (x1 + 10, y1 + 35), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
            cv2.putText(frame, t.status.name, (x1 + 10, y1 + 50), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
            cv2.rectangle(frame, (x1, y1), (x2, y2), color, cv2.FONT_HERSHEY_SIMPLEX)

        cv2.putText(frame, "NN fps: {:.2f}".format(fps), (2, frame.shape[0] - 4), cv2.FONT_HERSHEY_TRIPLEX, 0.4, color)

        cv2.imshow("tracker", frame)

        if cv2.waitKey(1) == ord('q'):
            break
```

#### C++

```cpp
#include <chrono>
#include <depthai/depthai.hpp>
#include <opencv2/opencv.hpp>

#include "depthai/pipeline/datatype/Tracklets.hpp"

int main() {
    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto replay = pipeline.create<dai::node::ReplayVideo>();
    replay->setReplayVideoFile(VIDEO_PATH);

    // Create spatial detection network
    dai::NNModelDescription modelDescription{"yolov6-nano"};
    auto detectionNetwork = pipeline.create<dai::node::DetectionNetwork>()->build(replay, modelDescription);
    detectionNetwork->setConfidenceThreshold(0.6f);
    detectionNetwork->input.setBlocking(false);

    // Create object tracker
    auto objectTracker = pipeline.create<dai::node::ObjectTracker>();
    objectTracker->setDetectionLabelsToTrack({0});  // track only person
    objectTracker->setTrackerType(dai::TrackerType::SHORT_TERM_IMAGELESS);
    objectTracker->setTrackerIdAssignmentPolicy(dai::TrackerIdAssignmentPolicy::SMALLEST_ID);

    // Create output queues
    auto preview = objectTracker->passthroughTrackerFrame.createOutputQueue();
    auto tracklets = objectTracker->out.createOutputQueue();

    // Link nodes
    detectionNetwork->passthrough.link(objectTracker->inputTrackerFrame);

    detectionNetwork->passthrough.link(objectTracker->inputDetectionFrame);
    detectionNetwork->out.link(objectTracker->inputDetections);

    // Start pipeline
    pipeline.start();

    // FPS calculation variables
    auto startTime = std::chrono::steady_clock::now();
    int counter = 0;
    float fps = 0;
    cv::Scalar color(255, 255, 255);

    while(pipeline.isRunning()) {
        auto imgFrame = preview->get<dai::ImgFrame>();
        auto track = tracklets->get<dai::Tracklets>();

        counter++;
        auto currentTime = std::chrono::steady_clock::now();
        auto elapsed = std::chrono::duration_cast<std::chrono::seconds>(currentTime - startTime).count();
        if(elapsed >= 1) {
            fps = counter / static_cast<float>(elapsed);
            counter = 0;
            startTime = currentTime;
        }

        cv::Mat frame = imgFrame->getCvFrame();
        auto trackletsData = track->tracklets;

        for(const auto& t : trackletsData) {
            auto roi = t.roi.denormalize(frame.cols, frame.rows);
            int x1 = static_cast<int>(roi.topLeft().x);
            int y1 = static_cast<int>(roi.topLeft().y);
            int x2 = static_cast<int>(roi.bottomRight().x);
            int y2 = static_cast<int>(roi.bottomRight().y);

            std::string label;
            try {
                label = detectionNetwork->getClasses().value()[t.label];
            } catch(...) {
                label = std::to_string(t.label);
            }

            cv::putText(frame, label, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, color);
            cv::putText(frame, "ID: " + std::to_string(t.id), cv::Point(x1 + 10, y1 + 35), cv::FONT_HERSHEY_TRIPLEX, 0.5, color);
            cv::putText(frame,
                        std::string(t.status == dai::Tracklet::TrackingStatus::LOST ? "LOST" : "TRACKED"),
                        cv::Point(x1 + 10, y1 + 50),
                        cv::FONT_HERSHEY_TRIPLEX,
                        0.5,
                        color);
            cv::rectangle(frame, cv::Point(x1, y1), cv::Point(x2, y2), color, cv::FONT_HERSHEY_SIMPLEX);
        }

        cv::putText(frame, "NN fps: " + std::to_string(fps).substr(0, 4), cv::Point(2, frame.rows - 4), cv::FONT_HERSHEY_TRIPLEX, 0.4, color);

        cv::imshow("tracker", frame);

        if(cv::waitKey(1) == 'q') {