# PointCloud Visualizer

Live 3D visualization of a colorized point cloud using Open3D. Links stereo depth and an aligned RGB camera to the
[PointCloud](https://docs.luxonis.com/software-v3/depthai/depthai-components/host_nodes/pointcloud.md) node and displays the
result in an interactive Open3D window alongside a colorized depth view.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Source code

#### Python

```python
#!/usr/bin/env python3
"""
PointCloud Visualizer

Live 3D visualization of stereo-depth point clouds using Open3D.
Press Q in the Open3D window (or Ctrl-C in the terminal) to quit.
"""

import time

import cv2
import numpy as np

try:
    import open3d as o3d
except ImportError:
    raise SystemExit("Please install open3d: pip install open3d")

import depthai as dai

def main() -> None:
    print("PointCloud Visualizer")
    print("=====================")
    print("Connecting to device...")

    device = dai.Device()
    print(f"Device: {device.getDeviceName()}  (ID: {device.getDeviceId()})\n")

    with dai.Pipeline(device) as pipeline:
        # ── Camera + Depth ─────────────────────────────────────
        colorSockets = device.getConnectedCameras(dai.CameraSensorType.COLOR)
        colorSocket = colorSockets[0] if colorSockets else dai.CameraBoardSocket.CAM_A
        color = pipeline.create(dai.node.Camera).build(colorSocket)
        colorOut = color.requestOutput(
            (640, 400), type=dai.ImgFrame.Type.RGB888i,
            resizeMode=dai.ImgResizeMode.CROP, enableUndistortion=True,
        )

        depth = pipeline.create(dai.node.Depth).build(dai.node.Depth.Algorithm.AUTO, None, (640, 400))
        depth.setAlignTo(colorOut)

        # ── PointCloud node ───────────────────────────────────────────
        pc = pipeline.create(dai.node.PointCloud)
        pc.setRunOnHost(True)
        pc.initialConfig.setLengthUnit(dai.LengthUnit.METER)
        depth.depth.link(pc.inputDepth)
        colorOut.link(pc.inputColor)

        queue = pc.outputPointCloud.createOutputQueue(maxSize=4, blocking=False)
        qDepth = pc.passthroughDepth.createOutputQueue(maxSize=4, blocking=False)

        # ── Open3D setup ──────────────────────────────────────────────
        vis = o3d.visualization.Visualizer()
        vis.create_window("PointCloud Visualizer")
        pcd = o3d.geometry.PointCloud()
        coord = o3d.geometry.TriangleMesh.create_coordinate_frame(size=0.1)
        vis.add_geometry(coord)
        first = True

        # ── Start pipeline & wait for auto-exposure ───────────────────
        pipeline.start()
        print("Waiting for auto-exposure to settle...")
        time.sleep(1)
        queue.tryGetAll()  # drain stale frames
        qDepth.tryGetAll()

        print("Streaming... Press Q in the Open3D window to quit.")

        try:
            while True:
                pclData = queue.tryGet()

                if pclData is not None:
                    if pclData.isColor():
                        points, colors = pclData.getPointsRGB()
                        if len(points) > 0:
                            pcd.points = o3d.utility.Vector3dVector(points.astype(np.float64))
                            pcd.colors = o3d.utility.Vector3dVector(
                                np.delete(colors / 255.0, 3, 1).astype(np.float64)
                            )
                    else:
                        points = pclData.getPoints()
                        if len(points) > 0:
                            pcd.points = o3d.utility.Vector3dVector(points)
                            pcd.colors = o3d.utility.Vector3dVector()

                    if len(pcd.points) > 0:
                        if first:
                            vis.add_geometry(pcd)
                            ctr = vis.get_view_control()
                            ctr.set_front([0, 0, -1])
                            ctr.set_up([0, -1, 0])
                            ctr.set_lookat([0, 0, 1])
                            ctr.set_zoom(0.3)
                            first = False
                        else:
                            vis.update_geometry(pcd)

                # Show colorized depth in an OpenCV window
                depthMsg = qDepth.tryGet()
                if depthMsg is not None:
                    cv2.imshow("Depth", dai.utility.colorizeDepthFrame(depthMsg, 300, 12000, cv2.COLORMAP_HOT, useLog=True).getCvFrame())

                if cv2.waitKey(1) == ord("q"):
                    break
                if not vis.poll_events():
                    break
                vis.update_renderer()

        except KeyboardInterrupt:
            print("\nStopping...")

        vis.destroy_window()
        cv2.destroyAllWindows()

    print("Done.")

if __name__ == "__main__":
    main()
```

#### C++

```cpp
/**
 * PointCloud Visualizer
 *
 * Live 3D visualization of colorized stereo-depth point clouds using the
 * built-in RemoteConnection (foxglove) visualizer.
 *
 * Run the example, then open the visualizer in a browser (default
 * http://localhost:8082) to see the live point cloud.
 * Press 'q' in the viewer or Ctrl-C in the terminal to quit.
 */

#include <csignal>
#include <iostream>

#include "depthai/depthai.hpp"
#include "depthai/remote_connection/RemoteConnection.hpp"

// ---------------------------------------------------------------------------
static volatile std::sig_atomic_t isRunning{1};
void signalHandler(int) {
    isRunning = 0;
}

// ---------------------------------------------------------------------------
int main() {
    std::signal(SIGINT, signalHandler);

    std::cout << "PointCloud Visualizer\n"
              << "=====================\n"
              << "Connecting to device...\n";

    dai::RemoteConnection remoteConnector;
    dai::Pipeline pipeline;

    auto device = pipeline.getDefaultDevice();
    std::cout << "Device: " << device->getDeviceName() << "  (ID: " << device->getDeviceId() << ")\n\n";

    const auto size = std::make_pair(640, 400);

    // ── Cameras ──────────────────────────────────────────────────────
    auto colorSockets = device->getConnectedCameras(dai::CameraSensorType::COLOR);
    auto colorSocket = colorSockets.empty() ? dai::CameraBoardSocket::CAM_A : colorSockets.front();
    auto color = pipeline.create<dai::node::Camera>();
    color->build(colorSocket);

    // ── Align depth to color camera ──────────────────────────────────
    auto colorOut = color->requestOutput(size, dai::ImgFrame::Type::RGB888i, dai::ImgResizeMode::CROP, std::nullopt, true);

    auto depth = pipeline.create<dai::node::Depth>();
    depth->build(dai::node::Depth::Algorithm::AUTO, std::nullopt, std::make_pair(640u, 400u));
    depth->setAlignTo(*colorOut);

    // ── PointCloud node ──────────────────────────────────────────────
    auto pc = pipeline.create<dai::node::PointCloud>();
    pc->setRunOnHost(true);
    depth->depth().link(pc->inputDepth);
    colorOut->link(pc->getColorInput());

    // Publish the point cloud to the remote visualizer
    remoteConnector.addTopic("pcl", pc->outputPointCloud);

    pipeline.start();
    remoteConnector.registerPipeline(pipeline);

    device->setIrLaserDotProjectorIntensity(0.7);

    std::cout << "Pipeline started.\n"
              << "Open the visualizer at http://localhost:8082 to see the point cloud.\n"
              << "Press 'q' in the viewer or Ctrl-C to quit.\n";

    while(isRunning != 0 && pipeline.isRunning()) {
        int key = remoteConnector.waitKey(1);
        if(key == 'q') {
            std::cout << "Got 'q' key from the remote connection.\n";
            break;
        }
    }

    std::cout << "Done.\n";
    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.