# Script Switch All Cameras

Switch between cameras by pressing a key.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- Script (3)
- XLinkOut (7)
- Camera(1)
- Camera(2)
- XLinkIn(6)

Pipeline connections:
- XLinkIn(6) -> Script (3) (out -> control)
- Script (3) -> XLinkOut (7) (out -> in)
- Camera(2) -> Script (3) (0 -> 2)
- Camera(1) -> Script (3) (0 -> 1)
- Camera(0) -> Script (3) (0 -> 0)

## Source code

#### Python

```python
import depthai as dai
import time
import cv2

# Create pipeline
device = dai.Device()
pipeline = dai.Pipeline(device)

cameras = [
    pipeline.create(dai.node.Camera).build(socket)
    for socket in device.getConnectedCameras()
]
inputKeys = []
script = pipeline.create(dai.node.Script)

for i, camera in enumerate(cameras):
    inputName = str(i)
    camera.requestFullResolutionOutput().link(script.inputs[inputName])
    script.inputs[inputName].setBlocking(False)
    script.inputs[inputName].setMaxSize(1)
    inputKeys.append(inputName)

controlQueue = script.inputs["control"].createInputQueue()
preview = script.outputs["out"].createOutputQueue()

inputKeysSize = len(inputKeys)
script.setScript(
    f"""
    inputToStream = 0
    maxID = {inputKeysSize} - 1
    while True:
        controlMessage = node.inputs["control"].tryGet()
        if controlMessage is not None:
            if(inputToStream < maxID):
                inputToStream += 1
            else:
                inputToStream = 0
        frame = node.inputs[str(inputToStream)].get()
        node.outputs["out"].send(frame)
"""
)

pipeline.start()
print("To switch between streams, press 's'")
with pipeline:
    while pipeline.isRunning():
        previewMessage = preview.get()
        assert isinstance(previewMessage, dai.ImgFrame)
        cv2.imshow("preview", previewMessage.getCvFrame())
        key = cv2.waitKey(1)
        if key == ord("s"):
            controlQueue.send(dai.Buffer())
        if key == ord("q"):
            break
```

#### C++

```cpp
#include <atomic>
#include <csignal>
#include <iostream>
#include <memory>
#include <opencv2/opencv.hpp>
#include <vector>

#include "depthai/depthai.hpp"

// Global flag for graceful shutdown
std::atomic<bool> quitEvent(false);

// Signal handler
void signalHandler(int signum) {
    quitEvent = true;
}

int main() {
    // Set up signal handlers
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    try {
        // Create device and pipeline
        std::shared_ptr<dai::Device> device = std::make_shared<dai::Device>();
        dai::Pipeline pipeline(device);

        // Get connected cameras and create camera nodes
        std::vector<std::shared_ptr<dai::node::Camera>> cameras;
        std::vector<std::string> inputKeys;

        for(const auto& socket : device->getConnectedCameras()) {
            auto camera = pipeline.create<dai::node::Camera>();
            camera->build(socket);
            cameras.push_back(camera);
            inputKeys.push_back(std::to_string(cameras.size() - 1));
        }

        // Create script node
        auto script = pipeline.create<dai::node::Script>();

        // Link cameras to script inputs
        for(size_t i = 0; i < cameras.size(); i++) {
            std::string inputName = std::to_string(i);
            cameras[i]->requestFullResolutionOutput()->link(script->inputs[inputName]);
            script->inputs[inputName].setBlocking(false);
            script->inputs[inputName].setMaxSize(1);
        }

        // Create control and preview queues
        auto controlQueue = script->inputs["control"].createInputQueue();
        auto preview = script->outputs["out"].createOutputQueue();

        // Set the script content
        std::string scriptContent = R"(
            inputToStream = 0
            maxID = )" + std::to_string(inputKeys.size() - 1)
                                    + R"(
            while True:
                controlMessage = node.inputs["control"].tryGet()
                if controlMessage is not None:
                    if(inputToStream < maxID):
                        inputToStream += 1
                    else:
                        inputToStream = 0
                frame = node.inputs[str(inputToStream)].get()
                node.outputs["out"].send(frame)
        )";
        script->setScript(scriptContent);

        // Start pipeline
        pipeline.start();
        std::cout << "To switch between streams, press 's'" << std::endl;

        // Main loop
        while(pipeline.isRunning() && !quitEvent) {
            auto previewMessage = preview->get<dai::ImgFrame>();
            cv::Mat frame = previewMessage->getCvFrame();
            cv::imshow("preview", frame);

            int key = cv::waitKey(1);
            if(key == 's') {
                auto controlMessage = std::make_shared<dai::Buffer>();
                controlQueue->send(controlMessage);
            } else if(key == 'q') {
                break;
            }
        }

        // Cleanup
        pipeline.stop();
        pipeline.wait();

    } catch(const std::exception& e) {
        std::cerr << "Error: " << e.what() << std::endl;
        return 1;
    }

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.