# Parameters

> **Pipeline AutoCalibration**
> Since ROS driver version `3.2.1`, pipeline [AutoCalibration](https://docs.luxonis.com/software-v3/depthai/depthai-components/host_nodes/auto_calibration.md) is enabled by default. To disable it, set `driver.i_pipeline_auto_calibration_mode` to `OFF`.

The driver can be configured by a large number of parameters. Description of all parameters for each node can be found below, most
of them mirror DepthAI C++/Python API. Parameters that begin with `r_` can be freely modified during runtime, for example with
rqt.

Parameters that begin with `i_` are set when camera is initializing, to change them you have to call `stop` and `start` services.
This can be used to hot swap NNs during runtime, changing resolutions, etc.

## Driver

 * `driver.i_publish_tf_from_calibration: true` <bool> - setting this to true launches TFPublisher
 * `driver.i_tf_device_name: [NODE_NAME]` <string> - if not set, defaults to the node name
 * `driver.i_tf_device_model: ''` <string> - if not set, it will be automatically detected. If the node is unable to detect STL
   file for the device it is set to `OAK-D-S2`. To explicitly set it in `driver.launch.py`, set `override_cam_model:=true`
 * `driver.i_tf_base_frame: oak` <string> - Frame that is used as an the root for camera frames, usually in the same place as
   CAM_A (center sensor for OAK-D lineup)
 * `driver.i_tf_parent_frame: oak_parent_frame` <string> - Set to the frame that you want to connect the camera to (for example
   robot end effector)
 * `driver.i_tf_cam_pos_x: '0.0'` <string> - Position of base frame w.r.t parent frame
 * `driver.i_tf_cam_pos_y: '0.0'` <string> - Position of base frame w.r.t parent frame
 * `driver.i_tf_cam_pos_z: '0.0'` <string> - Position of base frame w.r.t parent frame
 * `driver.i_tf_cam_roll: '0.0'` <string> - Orientation of base frame w.r.t parent frame
 * `driver.i_tf_cam_pitch: '0.0'` <string> - Orientation of base frame w.r.t parent frame
 * `driver.i_tf_cam_yaw: '0.0'` <string> - Orientation of base frame w.r.t parent frame Outside of TF-publishing related
   parameters `driver` has additional parameters

 * `i_usb_speed: SUPER` <string> - USB speed set for using current interface, it is automatically deduced but can be overridden,
   for example to use SUPER_PLUS explicitly available options: * LOW
    * FULL
    * HIGH (USB2)
    * SUPER (USB3)
    * SUPER_PLUS - for connecting with a high speed interface (like Thunderbolt), can be unstable in certain scenarios
 * `i_device_id: ""` <string> - Used to connect to a device with a specific ID
 * `i_ip ""` <string> - Used to connect to a device with specific IP
 * `i_usb_port_id: ""` <string> - Used to connect to devices on specific USB port
 * `i_pipeline_dump: false` <bool> - Whether to dump created pipeline to a JSON file (used for debugging)
 * `i_calibration_dump: false` <bool> - Whether to dump calibration to a JSON file
 * `i_external_calibration_path: ""` <string> - Used to override device calibration
 * `i_pipeline_auto_calibration_mode: ""` <string or bool> - Pipeline auto-calibration mode. Empty leaves the DepthAI pipeline
   default unchanged. Set to `OFF` to disable auto-calibration. Valid string values are `OFF`, `ON_START`, and `CONTINUOUS`.
   Boolean values are also accepted for backwards-compatible configuration: `true` maps to `ON_START`, and `false` maps to `OFF`.
 * `i_enable_ir : true` <bool> - Whether to enable IR projector
 * `i_restart_on_diagnostics_error: false` <bool> - If diagnostics publishing is enabled in the pipeline and it reports an error,
   driver will be restarted
 * `i_rs_compat: false` <bool> - Turn on Realsense compatibility. Topic, frame names and param names will be changed to reflect RS
   cameras.
 * `r_laser_dot_intensity: 0.6` <float> <0.0-1.0> - Sets laser dot projector intensity. Additional power might be required via
   Y-adapter in USB cameras
 * `r_floodlight_intensity: 0.6` <float> <0.0-1.0> - Sets floodlight projector intensity. Additional power might be required via
   Y-adapter in USB cameras

## Pipeline generation

Parameters start with name `pipeline_gen`

 * `i_pipeline_type` can be either * `RGB` - only publishes RGB stream , NN available
    * `RGBD` - Publishes RGB + Depth streams (set `i_publish_topic` for left and right cameras to enable them), NN & Spatial NN
      available
    * `Stereo` - Publishes streams from left and right sensors, NN can be set for each sensor separately
    * `RGBStereo` - Publishes RGB + Left + Right streams, NN can be set for each sensor separately
    * `Depth` - Publishes only depth stream, NN can be set on stereo node via parameter
    * `CamArray` - Publishes streams for all detected sensors, NN can be set for each sensor separately
    * `Tof` - Publishes only TOF stream, no NN available
    * `DepthTof` - Publishes Depth + TOF streams, specific to OAK-D-SR-POE, NN can be set on stereo node via parameter
    * `StereoToF` - Publishes Stereo + TOF streams, specific to OAK-D-SR-POE, NN can be set on stereo node via parameter
    * `RGBToF` - Publishes RGB + TOF streams, specific to OAK-D-SR-POE, NN can be set on stereo node via parameter
    * `Thermal` - Targeted towards OAK-T cameras, publishes RGB + Thermal stream.
 * `i_nn_type: spatial` <string> - Type of NN to be created with pipelines
 * `i_enable_imu: true` <bool> - Whether to enable IMU node in certain pipelines
 * `i_enable_diagnostics: false` <bool> - Whether to enable diagnostics node
 * `i_enable_rgbd: false` <bool> - Whether to enable RGBD node in certain pipelines

## Image sensors

Sensor parameters begin with `sensor_name.[PARAMETER_NAME]`, for example `rgb.i_width`

### Initial parameters

 * `i_board_socket_id` <int> - Socket ID of the sensor, used mostly for alignment, calibration and deducing frame names,
   automatically detected for each sensor but can be overridden
 * `i_enable_feature_tracker: false` <bool> - Enables FeatureTracker node for this particular sensor
 * `i_enable_nn: false` <bool> - Enables NeuralNetwork for this particular sensor
 * `i_max_q_size: 8` <int> - Sets DAI queue size
 * `i_low_bandwidth: false` <bool> - When set to true, enables VideoEncoder for this particular sensor to improve latency between
   camera and host. By default DAI Encoded frames (only in case of MJPEG Encoder, for H264 enable `i_publish_compressed`
   parameter) are decoded to ROS Image messages on host.
 * `i_low_bandwidth_profile: 4` <int> - Type of encoder used. Following types are available: * H264_BASELINE,
    * H264_HIGH,
    * H264_MAIN,
    * H265_MAIN,
    * MJPEG (default)
 * `i_low_bandwidth_frame_freq: 30` <int> - Frame frequency of the Encoder, used in H26X types
 * `i_low_bandwidth_bitrate: 0` <int> - Bitrate of the Encoder, used in H26X types
 * `i_low_bandwidth_quality: 50` <int> - Quality of the MJPEG Encoder
 * `i_publish_compressed: false` <bool> - Instead of converting DAI Encoded frames to ROS Image messages publish them in
   respective compressed image formats (CompressedImage for MJPEG and FFMPEGMsgs::FFMPPEGPacket for H26X types)
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_calibration_file: ""` <string> - Used to override DAI calibration with ROS calibration
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_enable_lazy_publisher: true` <bool> - Whether to publish data only in the case where a subscription is detected on an
   image/camera_info topic
 * `i_add_exposure_offset: false` <bool> - Whether to add exposure offset to ROS timestamp
 * `i_exposure_offset: 0` <int> - Exposure offset type: * START
    * MIDDLE
    * END
 * `i_reverse_stereo_socket_order: false` <bool> - See `Stereo socket order` section below for more information
 * `i_synced: :false` <bool> - Whether to add the output to the synced outputs group, all publishers synced will publish images
   with the same timestamps
 * `i_publish_topic: true/false` <bool> - Whether to publish on ROS topic, by default true on sensors on CAM_A socket, false
   otherwise
 * `i_publish_full_resolution: false` <bool> - Whether to publish full resolution image
 * `i_use_max_resolution_possible: false` <bool> - Whether to use maximum resolution possible
 * `i_width: 640` <int> - Width of the image
 * `i_height: 400` <int> - Height of the image
 * `i_fps: 30.0` <float> - Sensor FPS
 * `i_undistorted: true` <bool> - Whether to undistort the image
 * `i_resize_mode: "CROP"` <string> - Type of resize used when undistorting the image, refer to DAI Camera node for more
   information, can be: * CROP
    * LETTERBOX
    * STRETCH
 * `i_fsync_continuous: false` <bool> - Whether to set Frame Sync mode. If enabled, `i_fsync_mode` parameter is used for the mode
 * `i_fsync_mode: "INPUT` <string> - Type of FSync mode, can be: * OFF
    * OUTPUT
    * INPUT
 * `i_fsync_trigger: false` <bool> - Whether to use external trigger for image capturing
 * `i_num_frames_burst: 1` <int> - How many frames in triggered burst
 * `i_num_frames_discard: 0` <int> - How many frames to discard in an initial burst (they may have worse quality)

### Runtime parameters

 * `r_iso: 800` <int> <100-1600> - ISO setting when setting manual exposure, set `r_set_man_exposure` to use
 * `r_exposure: 1000` <int> <1-33000> - Exposure setting when setting manual exposure, set `r_set_man_exposure` to use
 * `r_set_man_exposure: false` <bool> - Whether to set manual exposure
 * `r_set_autoexposure_limit: false` <bool> - Whether to limit the auto exposure
 * `r_auto_exposure_limit: 1000` <int> - Auto exposure limit
 * `r_set_man_focus: false` <bool> - Whether to set manual focus
 * `r_focus: 1` <int> <1-255> - Focus value
 * `r_set_man_whitebalance: false` <bool> - Whether to set manual whitebalance
 * `r_whitebalance: 3000` <int> <1000-12000> - Manual whitebalance
 * `r_set_sharpness: false` <bool> - Whether to set sharpness manually
 * `r_sharpness: 1` <int> <1-4> - Sharpness level
 * `r_set_chroma_denoise: false` - Whether to set chroma denoise manually
 * `r_chroma_denoise: 1` <int> <1-4> - Chroma denoise level
 * `r_set_luma_denoise: false` - Whether to set luma denoise manually
 * `r_luma_denoise: 1` <int> <1-4> - Luma denoise level
 * `r_set_auto_exp_region: false` <bool> - Whether to use part of image for controlling exposure
 * `r_auto_exp_region_start_x: 0` <int> - Start point for rectangle used for autoexposure (in image coordinates, i.e X right, Y
   down)
 * `r_auto_exp_region_start_y: 0` <int> - Start point for rectangle used for autoexposure (in image coordinates, i.e X right, Y
   down)
 * `r_auto_exp_region_width: 0` <int> - Width of the autoexposure region
 * `r_auto_exp_region_height: 0` <int> - Height of the autoexposure region

## Stereo parameters

### Depth alignment

When setting `stereo.aligned: true`, stereo output is aligned to board socket specified by `stereo.i_board_socket_id` parameter
(by default 0/CAM_A)

You can enable rectified Stereo streams by setting, for example in the case of right stream `i_publish_right_rect: true`.

### Stereo socket order

By default, right camera is treated as first when used for stereo computation, which is reflected in CameraInfo messages. If you
want to reverse that logic, set `stereo.i_reverse_stereo_socket_order: true` (this can be also set for individual sensors).

### Custom Sensor sockets

Configuration of which sensors are used for computing stereo pair can be done either programmatically, by specifying them in a
constructor of a Stereo node (for example when building a custom pipeline), or via parameters -
`stereo.i_left_socket_id`/`stereo.i_right_socket_id`. Please note that currently if you want to use rgb/center socket instead of
one of the given pairs you will need to build a custom pipeline for that.

### Parameters

For more information on filters, visit [Configuring Stereo
Depth](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/stereo_depth.md)

 * `i_max_q_size: 30` <int> - Sets DAI queue size
 * `i_fps: 30.0` <float> - Stereo FPS
 * `i_low_bandwidth: false` <bool> - Refer to the parameter description in `Sensor` node. NOTE This parameter is incompatible with
   `i_subpixel` parameter.
 * `i_low_bandwidth_profile: 4` <int> - Type of encoder used. Following types are available:
    * H264_BASELINE,
    * H264_HIGH,
    * H264_MAIN,
    * H265_MAIN,
    * MJPEG (default)
 * `i_low_bandwidth_frame_freq: 30` <int> - Frame frequency of the Encoder, used in H26X types
 * `i_low_bandwidth_bitrate: 0` <int> - Bitrate of the Encoder, used in H26X types
 * `i_low_bandwidth_quality: 50` <int> - Quality of the MJPEG Encoder
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_calibration_file: ""` <string> - Used to override DAI calibration with ROS calibration
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_enable_lazy_publisher: true` <bool> - Whether to publish data only in the case where a subscription is detected on an
   image/camera_info topic
 * `i_add_exposure_offset: false` <bool> - Whether to add exposure offset to ROS timestamp
 * `i_exposure_offset: 0` <int> - Exposure offset type:
    * START
    * MIDDLE
    * END
 * `i_reverse_stereo_socket_order: false` <bool> - See `Stereo socket order` section below for more information
 * `i_synced: :false` <bool> - Whether to add the output to the synced outputs group, all publishers synced will publish images
   with the same timestamps
 * `i_publish_topic: true/false` <bool> - Whether to publish on ROS topic, by default true on sensors on CAM_A socket, false
   otherwise
 * `i_output_disparity: false` <bool> - Whether to output disparity instead of depth
 * `i_enable_left_spatial_nn: false` <bool> - Whether to create spatial NN with left sensor as RGB source
 * `i_enable_right_spatial_nn: false` <bool> - Whether to create spatial NN with right sensor as RGB source
 * `i_enable_left_rgbd: false` <bool> - Whether to create RGBD node with left sensor as RGB source
 * `i_enable_right_rgbd: false` <bool> - Whether to create RGBD node with right sensor as RGB source
 * `i_aligned: true` <bool> - Whether to align stereo node to `i_board_socket_id`
 * `i_run_align_on_host: true` <bool> - Whether to run align node on host (this is only in case of RVC4)
 * `i_depth_preset: FAST_ACCURACY` <string> - What kind of default depth preset to apply. WARNING In case of types other than
   FAST_ACCURACY, other stereo filtering parameters might be overridden. Additionally, in some cases decimation filter is applied
   resulting in lower final image size and increased processing might reduce available resources that are shared with, for example
   Neural Networks on RVC2 devices. Following settings are exposed:
    * FAST_ACCURACY
    * DEFAULT
    * FACE
    * HIGH_DETAIL
    * ROBOTICS
 * `i_enable_distortion_correction: true` <bool> - Toggling distortion correction on output stream
 * `i_set_disparity_to_depth_use_spec_translation: false` <bool> - Whether to use baseline from CAD data, not the calibration data
 * `i_bilateral_sigma: 0` <int> <0-65535> - Value for bilateral sigma filter. Large values of this parameter means that farther
   colors within pixel neighbourhood will be mixed together, resulting in large areas of semi-equal color.
 * `i_lrc_threshold: 10` <int> <0-255> - Threshold for left-right, right-left disparity map combine.
 * `i_stereo_conf_threshold: 15` <int> <0-255> - Confidence threshold for disparity calculation. High value means more depth
   values are discarded
 * `i_subpixel: true` <bool> - Compute disparity with sub-pixel interpolation (3 fractional bits by default. Suitable for long
   range. Currently incompatible with extended disparity and low_bandwidth mode. Setting subpixel results in more depth values
   being output (less visible "steps" in pointclouds at the cost of more bandwidth and resources being used. Automatically enabled
   on some depth presets.
 * `i_subpixel_fractional_bits: 3` <int> <3-5> - Defines the number of fractional disparities: 2^x
 * `i_rectify_edge_fill_color: 0` <int> <-1-255> - Fill color for missing data at the edges. 0-255 for grayscale or -1 to
   replicate pixels
 * `i_enable_alpha_scaling: false` <bool> - Enable alpha scaling.
 * `i_alpha_scaling: 0.0` <float> - Alpha scaling parameter. It is a free scaling parameter between 0, (where all pixels in the
   undistorted image are valid) and 1 (where all the source image pixels are retained in the undistorted image). On some high
   distortion lenses, and/or due to rectification (image rotated) invalid areas may appear even with alpha=0, in these cases alpha
   < 0.0 helps removing invalid areas.
 * `i_disparity_width: DISPARITY_96` <string> - Disparity search range. Values:
    * DISPARITY_64
    * DISPARITY_96
 * `i_extended_disp: false` <bool> - Disparity range increased from 0-95 to 0-190, combined with full resolution and downscaled
   images. Suitable for short range objects. Currently incompatible with sub-pixel disparity.
 * `i_enable_companding: false` <bool> - Enable disparity companding using sparse matching. Matching pixel by pixel for N
   disparities. Matching every 2nd pixel for M disparities. Matching every 4th pixel for T disparities. In case of 96 disparities:
   N=48, M=32, T=16. This way the search range is extended to 176 disparities, by sparse matching. Note, when enabling this flag
   only depth map will be affected, disparity map will not
 * `i_enable_temporal_filter: false` <bool> - Enable temporal filter.
 * `i_temporal_filter_alpha: 0.4` <float> <0.0-1.0> - The alpha factor in an exponential moving average with Alpha=1 - no filter.
   Alpha=0 - infinite filter. Determines the extent of the temporal history that should be averaged.
 * `i_temporal_filter_delta: 20` <int> - Step-size boundary. Establishes the threshold used to preserve "edges". If the disparity
   value between neighboring pixels exceed the disparity threshold set by this delta parameter, then filtering will be temporarily
   disabled. Default value 0 means auto: 3 disparity integer levels. In case of subpixel mode it's 3*number of subpixel levels.
 * `i_temporal_filter_persistency: VALID_2_IN_LAST_4` <string> - Persistency mode. If the current disparity/depth value is
   invalid, it will be replaced by an older value, based on persistency mode. Valid values:
    * PERSISTENCY_OFF
    * VALID_8_OUT_OF_8
    * VALID_2_IN_LAST_3
    * VALID_2_IN_LAST_4
    * VALID_2_OUT_OF_8
    * VALID_1_IN_LAST_2
    * VALID_1_IN_LAST_5
    * VALID_1_IN_LAST_8
    * PERSISTENCY_INDEFINITELY
 * `i_enable_speckle_filter: false` <bool> - Enable speckle filter.
 * `i_speckle_filter_speckle_range: 50` <int> - Speckle search range.
 * `i_enable_disparity_shift: false` <bool> - Shift input frame by a number of pixels to increase minimum depth. For example
   shifting by 48 will change effective disparity search range from (0,95] to [48,143]. An alternative approach to reducing the
   minZ. We normally only recommend doing this when it is known that there will be no objects farther away than MaxZ, such as
   having a depth camera mounted above a table pointing down at the table surface.
 * `i_disparity_shift: 0` <int> - Disparity shift value.
 * `i_enable_spatial_filter: false` <bool> - Enable spatial filter.
 * `i_spatial_filter_hole_filling_radius: 2` <int> - An in-place heuristic symmetric hole-filling mode applied horizontally during
   the filter passes. Intended to rectify minor artefacts with minimal performance impact. Search radius for hole filling.
 * `i_spatial_filter_alpha: 0.5` <float> - The Alpha factor in an exponential moving average with Alpha=1 - no filter. Alpha = 0 -
   infinite filter. Determines the amount of smoothing.
 * `i_spatial_filter_delta: 20` <int> - Similar to delta in temporal filter.
 * `i_spatial_filter_num_iterations: 1` <int> - Number of iterations over the image in both horizontal and vertical direction.
 * `i_enable_threshold_filter: false` <bool> - Enable threshold filter
 * `i_threshold_filter_min_range: 400` <int> - Minimum range in depth units(mm). Depth values under this value are invalidated.
 * `i_threshold_filter_max_range: 15000` <int> - Maximum range in depth units. Depth values over this value are invalidated.
 * `i_enable_brightness_filter: false` <bool> - Enable brightness filter
 * `i_brightness_filter_min_brightness: 0` <int> - Minimum pixel brightness. If input pixel is less or equal than this value the
   depth value is invalidated.
 * `i_brightness_filter_max_brightness: 255` <int> - Maximum pixel brightness. If input pixel is more or equal than this value the
   depth value is invalidated.
 * `i_enable_decimation_filter: false` <bool> - Enable decimation filter. Affects final image size.
 * `i_decimation_filter_decimation_mode: PIXEL_SKIPPING` <string> - Decimation algorithm type. Available values:
    * PIXEL_SKIPPING
    * NON_ZERO_MEDIAN
    * NON_ZERO_MEAN
 * `i_decimation_filter_decimation_factor: 1` <int> <1-4> - Valid values are 1,2,3,4. Disparity/depth map x/y resolution will be
   decimated with this value.
 * `i_use_neural_depth: false` <bool>- Whether to use Neural Depth instead of regular Stereo (available only on RVC4)
 * `i_neural_depth_model: NEURAL_DEPTH_SMALL` <string> - Type of Neural Depth. Following types are available
    * NEURAL_DEPTH_LARGE
    * NEURAL_DEPTH_MEDIUM
    * NEURAL_DEPTH_SMALL
    * NEURAL_DEPTH_NANO
 * `r_edge_threshold: 10` <int> - Edge threshold for Neural Depth
 * `r_confidence_threshold: 125` <int> - Confidence threshold for Neural Depth
 * Following parameters are for the same for left and right rectified streams, below are parameters for left for the sake of
   brevity
    * `i_publish_left_rect: false` <bool> - Whether to publish rectified left stream
    * `i_left_rect_low_bandwidth: false` <bool> - Left rect low bandwidth provile
    * `i_left_rect_low_bandwidth_profile: 4` <int> - Left Rect LB profile
    * `i_left_rect_low_bandwidth_frame_freq: 30` <int> - Left Rect LB frame frequency
    * `i_left_rect_low_bandwidth_bitrate: 0` <int> - Left Rect LB bitrate
    * `i_left_rect_low_bandwidth_quality: 50` <int> - Left Rect LB quality
    * `i_left_rect_publish_compressed: false` <bool> - Whether to publish compressed images for left rect
    * `i_left_rect_add_exposure_offset: false` <bool> - Left Rect add exposure offset
    * `i_left_rect_exposure_offset: 0` <int> - Left Rect exposure offset setting
    * `i_left_rect_enable_feature_tracker: false` <bool> - Whether to add feature tracker for rectified left
    * `i_left_rect_synced: false` <bool> - Whether to sync left rect with other streams

## Feature Tracker

Each sensor node (and rectified streams from Stereo node) has the option to add FeatureTracker node, which publishes
`depthai_ros_msgs/msg/TrackedFeatures` messages. To enable features on, for example rgb node, set `rgb: i_enable_feature_tracker:
true`. To enable publishing on rectified streams, set for example `stereo: i_left_rect_enable_feature_tracker`

### Parameters

 * `i_motion_estimation_type: LUKAS_KANADE_OPTICAL_FLOW` <string> - Motion estimator type, can be: * LUKAS_KANADE_OPTICAL_FLOW
    * HW_MOTION_ESTIMATION
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)

## IMU

### Parameters:

 * `i_max_q_size: 8` <int> - Sets DAI queue size
 * `i_acc_freq: 480` <int> - Accelerometer sensor frequency
 * `i_acc_cov: 0.0` <float> - Accelerometer covariance
 * `i_batch_report_threshold: 5` <int> - Batch report size
 * `i_enable_rotation: false` <bool> - Whether to enable rotation vector & magnetometer data (available when using IMU_WITH_MAGN/
   IMU_WITH_MAGN_SPLIT message type and BNO086 sensor)
 * `i_gyro_cov: 0.0` <float> - Gyroscope covariance
 * `i_gyro_freq: 400` <int> - Gyroscope frequency
 * `i_mag_cov: 0.0` <float> - Magnetometer covariance
 * `i_mag_freq: 100` <int> - Magnetometer frequency
 * `i_max_batch_reports: 10` <int> - Max reports per batch
 * `i_message_type: IMU` <string> - ROS publisher type: * `IMU` - sensor_msgs/Imu
    * `IMU_WITH_MAG` - depthai_ros_msgs/ImuWithMagneticField
    * `IMU_WITH_MAG_SPLIT` - two publishers - sensor_msgs/Imu & sensor_msgs/MagneticField
 * `i_rot_cov: -1.0` <float> - Rotation covariance
 * `i_rot_freq: 400` <int> - Rotation frequency
 * `i_sync_method: COPY` <string> - sync method. Available options (WARNING RVC4 Devices only support COPY for now): * `COPY`
    * `LINEAR_INTERPOLATE_GYRO`
    * `LINEAR_INTERPOLATE_ACCEL`
 * `i_rotation_vector_type` <string> - type of rotation vector, for more information, refer to [this
   link](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/imu.md). Available options: * `ROTATION_VECTOR`
    * `GAME_ROTATION_VECTOR`
    * `GEOMAGNETIC_ROTATION_VECTOR`
    * `ARVR_STABILIZED_ROTATION_VECTOR`
    * `ARVR_STABILIZED_GAME_ROTATION_VECTOR`
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)

## Neural networks

In most of the pipeline types there is an option to easily turn enable Neural Networks.

 * `camera.i_nn_type` can be either `none` (no NN), `rgb` or `spatial`. This is responsible for whether the NN that we load should
   also take depth information (and for example provide detections in 3D format). Default set to `spatial`

### Parameters

 * `i_nn_family: detection` <string> - sets what kind of NN we want to have. Currently available options are: *`detection` *
   `segmentation` (for now only on RVC2)
 * `i_nn_model: yolov6-nano` <string> - Which model we want to load, models are downloaded from the web automatically when the
   driver is started, similarly to DepthAI C++/Python examples.
 * `i_nn_confidence_threshold: 0.5` <float> - Confidence threshold for NN
 * `i_nn_depth_lower_threshold: 100` <int> - (Spatial only) lower depth threshold for detections (in mm)
 * `i_nn_depth_upper_threshold: 10000` <int> - (Spatial only) upper depth threshold for detections (in mm)
 * `i_enable_passthrough: false` <bool> - Whether to publish RGB passthrough image
 * `i_enable_passthrough_depth: false` <bool> - Whether to publish depth passthrough image
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_bounding_box_scale_factor: 0.5` <float> <0.0-1.0> - Bounding box scale factor for detections
 * `i_max_q_size: 8` <int> - Sets DAI queue size

You can also choose to run NN on a specific sensor by setting `sensor_name.i_enable_nn` to `true`. After that, you can similarly
set `sensor_name_nn.i_nn_model` to a path to a config file. You can also set up spatial NN for Stereo node and use one of its
left/right streams as rgb input. This can be enabled in cameras with RGB side sensors such as OAK-D-SR and OAK-D-LR. Setting up is
also similar:

 * `stereo.i_enable_left_spatial_nn` - set to true to enable spatial NN with left sensor as input

## Sync

Currently you can sync any number of image topics with a sync node wrapper. To create a sync node, set `pipeline_gen:
i_enable_sync: true`, and, for example `rgb.i_synced: true` and `stereo.i_synced: true`. This example configuration is applied
when running `driver.launch.py` with `pointcloud.enable:=true` argument.

### Parameters

 * `i_sync_threshold: 10` <int> - Set maximal interval between messages in a group in milliseconds.
 * `i_sync_attempts: 10` <int> - Number of attempts for syncing

## ToF

ToF node is available on ToF, RgbTof, StereoToF and DepthTof pipelines. Its parameters are similar to regular camera node

### Parameters

 * `i_publish_topic: true` <bool> - Whether to publish topic
 * `i_max_q_size: 8` <int> - Sets DAI queue size
 * `i_low_bandwidth: false` <bool> - Refer to the parameter description in `Sensor` node. NOTE This parameter is incompatible with
   `i_subpixel` parameter.
 * `i_low_bandwidth_profile: 4` <int> - Type of encoder used. Following types are available: * H264_BASELINE,
    * H264_HIGH,
    * H264_MAIN,
    * H265_MAIN,
    * MJPEG (default)
 * `i_low_bandwidth_frame_freq: 30` <int> - Frame frequency of the Encoder, used in H26X types
 * `i_low_bandwidth_bitrate: 0` <int> - Bitrate of the Encoder, used in H26X types
 * `i_low_bandwidth_quality: 50` <int> - Quality of the MJPEG Encoder
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_calibration_file: ""` <string> - Used to override DAI calibration with ROS calibration
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_enable_lazy_publisher: true` <bool> - Whether to publish data only in the case where a subscription is detected on an
   image/camera_info topic
 * `i_publish_compressed: false` <bool> - Whether to publish compressed images
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_add_exposure_offset: false` <bool> - Whether to add exposure offset to ROS timestamp
 * `i_exposure_offset: 0` <int> - Exposure offset type: * START
    * MIDDLE
    * END
 * `i_width: 640` <int> - Width of the image
 * `i_height: 400` <int> - Height of the image
 * `i_fps: 30` <int> - FPS of the image
 * `i_aligned :false` <bool> - Whether to align the image to the other sensor
 * `i_aligned_socket_id: ""` <string> - Socket to align the image to
 * `i_run_align_on_host: true` <bool> - Whether to run align node on host (this is only in case of RVC4)
 * `i_synced: :false` <bool> - Whether to add the output to the synced outputs group, all publishers synced will publish images
   with the same timestamps
 * `i_preset_mode: TOF_MID_RANGE` <string> - Preset mode for image filtering

## Thermal

Thermal camera similarly operates as camera node with the option to set some additional runtime parameters

### Parameters

 * `i_publish_topic: true` <bool> - Whether to publish topic
 * `i_max_q_size: 8` <int> - Sets DAI queue size
 * `i_low_bandwidth: false` <bool> - Refer to the parameter description in `Sensor` node. NOTE This parameter is incompatible with
   `i_subpixel` parameter.
 * `i_low_bandwidth_profile: 4` <int> - Type of encoder used. Following types are available: * H264_BASELINE,
    * H264_HIGH,
    * H264_MAIN,
    * H265_MAIN,
    * MJPEG (default)
 * `i_low_bandwidth_frame_freq: 30` <int> - Frame frequency of the Encoder, used in H26X types
 * `i_low_bandwidth_bitrate: 0` <int> - Bitrate of the Encoder, used in H26X types
 * `i_low_bandwidth_quality: 50` <int> - Quality of the MJPEG Encoder
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_calibration_file: ""` <string> - Used to override DAI calibration with ROS calibration
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_enable_lazy_publisher: true` <bool> - Whether to publish data only in the case where a subscription is detected on an
   image/camera_info topic
 * `i_publish_compressed: false` <bool> - Whether to publish compressed images
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_add_exposure_offset: false` <bool> - Whether to add exposure offset to ROS timestamp
 * `i_exposure_offset: 0` <int> - Exposure offset type: * START
    * MIDDLE
    * END
 * `i_width: 640` <int> - Width of the image
 * `i_height: 400` <int> - Height of the image
 * `i_fps: 30.0` <float> - FPS of the image
 * `i_aligned :false` <bool> - Whether to align the image to the other sensor
 * `i_aligned_socket_id: ""` <string> - Socket to align the image to
 * `i_run_align_on_host: true` <bool> - Whether to run align node on host (this is only in case of RVC4)
 * `i_synced: :false` <bool> - Whether to add the output to the synced outputs group, all publishers synced will publish images
   with the same timestamps
 * `i_orientation: NORMAL` <string> - Orientation of the image. Available options: * NORMAL
    * MIRROR
    * FLIP
    * MIRROR_FLIP
 * `r_auto_ffc: false` <bool> - Auto Flat-Field-Correction. Controls whether the shutter is controlled by the sensor module
   automatically or not.
 * `r_close_manual_shutter: false` <bool> - Set this to True/False to close/open the shutter when autoFFC is disabled.
 * `r_brightness_level: 0` <int> <0-255> - Image brightness level.
 * `r_time_noise_filter_level: 0` <int> <0-3> - Time noise filter level. Filters out the noise that appears over time.

## RGBD

RGBD node can be turned on in some pipelines by turning on `pipeline_gen.i_enable_rgbd` parameter or by setting
`i_enable_left/right_rgbd` in Stereo node.

### Parameters

 * `i_publish_topic: true` <bool> - Whether to publish topic
 * `i_max_q_size: 2` <int> - Sets DAI queue size
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_num_threads: 1` <int> - Number of threads used for RGBD node
 * `i_run_sync_on_host: true` <bool> - Whether to sync messages on host
 * `i_run_align_on_host: true` <bool> - Whether to run align node on host (this is only in case of RVC4)

## VIO

VIO node can be turned on in some pipelines by turning on `pipeline_gen.i_enable_vio` parameter.

### Parameters

 * `i_publish_topic: true` <bool> - Whether to publish topic
 * `i_max_q_size: 2` <int> - Sets DAI queue size
 * `i_update_ros_base_time_on_ros_msg: false` <bool> - Enable if you experience timeshifts in your system (for example in the case
   where system clock is externally controlled
 * `i_get_base_device_timestamp: false` <bool> - Controls whether DAI timestamps obtained for data are synchronized to host
   (Timestamps themselves are still aligned to ROS time)
 * `i_run_sync_on_host: true` <bool> - Whether to sync messages on host
 * `i_imu_update_rate: 400` <int> - Rate of updating the imu messages
 * `i_width: 640` <int> - Width of the images
 * `i_height: 400` <int> - Height of the images
 * `i_fps: 60.0` <float> - FPS of the images
 * `i_config_path: 'depthai_ros_driver_default.json'` <string> - Full path to config.json used, when default value is used, config
   from depthai_ros_driver/config/custom is used
 * `i_override_local_transform: false` <bool> - Whether to override local transform, when enabled, following parameters can be set
   * `i_local_transform_x: 0.0` <float> - X position
    * `i_local_transform_y: 0.0` <float> - Y position
    * `i_local_transform_z: 0.0` <float> - Z position
    * `i_local_transform_qx: 0.0` <float> - X component of quaternion
    * `i_local_transform_qy: 0.0` <float> - Y component of quaternion
    * `i_local_transform_qz: 0.0` <float> - Z component of quaternion
    * `i_local_transform_qw: 0.0` <float> - w component of quaternion
 * `i_override_imu_extrinsics: false` <bool> - Whether to override IMU extrinsics with other values * `i_imu_extr_x: 0.0` <float>
   - X position
    * `i_imu_extr_y: 0.0` <float> - Y position
    * `i_imu_extr_z: 0.0` <float> - Z position
    * `i_imu_extr_qx: 0.0` <float> - X component of quaternion
    * `i_imu_extr_qy: 0.0` <float> - Y component of quaternion
    * `i_imu_extr_qz: 0.0` <float> - Z component of quaternion
    * `i_imu_extr_qw: 0.0` <float> - w component of quaternion
 * `i_set_acc_bias: false` <bool> - Override default accelerometer bias
 * `i_accel_bias: 9x0.0` <vector<double>> - Accelerometer bias
 * `i_set_acc_noise_std: false` <bool> - Override standard noise for accelerometer
 * `i_acc_noise_std: 3x0.0` <vector<double>> - Accelerometer standard noise
 * `i_set_gyro_bias: false` <bool> - Override default gyroscope bias
 * `i_gyro_bias: 9x0.0` <vector<double>> - Gyroscope bias
 * `i_set_gyro_noise_std: false` <bool> - Override standard noise for gyroscope
 * `i_gyro_noise_std: 3x0.0` <vector<double>> - Gyroscope standard noise
 * `i_publish_tf: true` <bool> - Whether to publish TF frame as well
 * `i_frame_id: odom` <string> - Frame ID of the messages
 * `i_child_frame_id: oak_parent_frame` <string> - Child frame ID
 * `i_covariance: 36x0.0` <vector<double>> - Covariance for the messages