Manual Conversion with OpenVino (RVC2 & RVC3)
Manual Conversion with OpenVino (RVC2 & RVC3)
Overview
Command Line
1pip install modelconvCommand Line
1modelconverter shell <platform>platform stands for the target platform you aim to convert for, so either rvc2 or rvc3.This is equivalent to starting a new Docker container from the luxonis/modelconverter-<platform>:latest image and running it as an interactive terminal session (-it) with the --rm flag to ensure the container is automatically removed once the session is exited:Command Line
1docker run --rm -it \
2 -v $(pwd)/shared_with_container:/app/shared_with_container/ \
3 luxonis/modelconverter-<platform>:latestCommand Line
1pip install openvino-dev==2022.3Simplify model (Optional)
.onnx model, you can run the simplification as:Command Line
1pip install onnxsim
2onnxsim <path to .onnx model> <path to simplified .onnx model>Compile OpenVINO IR
.xml file), and storing the model's weights and biases (.bin file). OpenVINO Model Optimizer (v2022.3.0) is used for this conversion job and the following source model formats are supported:- ONNX
- TensorFlow
- PyTorch
- PaddlePaddle
- MXNet
- Kaldi
- Caffe
Command Line
1mo --input_model <path to the (un-)simplified source model> --compress_to_fp16--compress_to_fp16 parameter to obtain optimal performance on our devices. You can find additional details here.Consult the
mo --help for the full list of conversion options.If planning to use your model in Luxonis ecosystem, we propose you set the flags so that the model expects un-normalized BGR input.Therefore, be sure to set the --reverse_input_channels, --mean_values, and --scale_values flags if the model expects RGB input or normalization.Quantize (RVC3 only)
Compile BLOB
Command Line
1compile_tool -d MYRIAD -m <path to .xml model (make sure that .bin is at the same root)>.../tools/compile_tool directory of your OpenVINO installation. You can run it as:Command Line
1cd .../tools/compile_tool
2./compile_tool -d MYRIAD -m ...Consult the
compile_tool -h for the full list of conversion options.Advanced
Model Optimizer
Mean and Scale Values
--mean_values and --scale_values. By default, frames from Camera node are in U8 data type, ranging from [0,255].However, models are typically trained with normalized frames within the range of [-1,1] or [0,1]. To ensure accurate inference results, frames need to be normalized beforehand.Although creating a custom model that normalizes frames before inference is an option (example here), it is more efficient to include this normalization directly within the model itself using the flags during model optimizer step.Here are some common normalization options (assuming that the initial input is in the range of [0,255]):- For required input with values between 0 and 1, use mean=0 and scale=255, computed as
([0,255] - 0) / 255 = [0,1]. - For required input with values between -1 and 1, use mean=127.5 and scale=127.5, computed as
([0,255] - 127.5) / 127.5 = [-1,1]. - For required input with values between -0.5 and 0.5, use mean=127.5 and scale=255, computed as
([0,255] - 127.5) / 255 = [-0.5,0.5].
Model Layout
--layout parameter. For example:Command Line
1--layout NCHW- N - batch size
- C - channels
- H - height
- W - width
[NeuralNetwork(0)] [warning] Input image (416x416) does not match NN (3x416)You have the option to switch between Interleaved / HWC and Planar / CHW layout through the API when requesting the output:Python
1import depthai as dai
2pipeline = dai.Pipeline()
3cam = pipeline.create(dai.node.Camera).build()
4output = cam.requestOutput(
5 size=SIZE, type=dai.ImgFrame.Type.BGR888i # or BGR888p (i stands for interleaved, and p stands for planar)
6)Color Order
Camera node, by default, outputs frames in BGR format. Mismatching the color order between input frames and the trained model can lead to inaccurate predictions. To address this, the --reverse_input_channels flag is utilized.Moreover, there is an option to switch the camera output to RGB via the API, eliminating the need for the flag:Python
1import depthai as dai
2pipeline = dai.Pipeline()
3cam = pipeline.create(dai.node.Camera).build()
4output = cam.requestOutput(
5 size=SIZE, type=dai.ImgFrame.Type.RGB888p
6)Compile Tool
Input Layer Precision
-ip U8 will incorporate a conversion layer U8->FP16 on all input layers of the model, which is typically the desired configuration. However, in specific scenarios, such as when working with data other than frames, using FP16 precision directly is necessary. In such cases, you can opt for -ip FP16