Encoding Max Limit
Similar samples:
Demo
Source code
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4
5# Create pipeline
6pipeline = dai.Pipeline()
7
8# Define sources and outputs
9camRgb = pipeline.create(dai.node.ColorCamera)
10monoLeft = pipeline.create(dai.node.MonoCamera)
11monoRight = pipeline.create(dai.node.MonoCamera)
12ve1 = pipeline.create(dai.node.VideoEncoder)
13ve2 = pipeline.create(dai.node.VideoEncoder)
14ve3 = pipeline.create(dai.node.VideoEncoder)
15
16ve1Out = pipeline.create(dai.node.XLinkOut)
17ve2Out = pipeline.create(dai.node.XLinkOut)
18ve3Out = pipeline.create(dai.node.XLinkOut)
19
20ve1Out.setStreamName('ve1Out')
21ve2Out.setStreamName('ve2Out')
22ve3Out.setStreamName('ve3Out')
23
24# Properties
25camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
26camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)
27monoLeft.setCamera("left")
28monoRight.setCamera("right")
29
30# Setting to 26fps will trigger error
31ve1.setDefaultProfilePreset(25, dai.VideoEncoderProperties.Profile.H264_MAIN)
32ve2.setDefaultProfilePreset(25, dai.VideoEncoderProperties.Profile.H265_MAIN)
33ve3.setDefaultProfilePreset(25, dai.VideoEncoderProperties.Profile.H264_MAIN)
34
35# Linking
36monoLeft.out.link(ve1.input)
37camRgb.video.link(ve2.input)
38monoRight.out.link(ve3.input)
39
40ve1.bitstream.link(ve1Out.input)
41ve2.bitstream.link(ve2Out.input)
42ve3.bitstream.link(ve3Out.input)
43
44# Connect to device and start pipeline
45with dai.Device(pipeline) as dev:
46
47 # Output queues will be used to get the encoded data from the output defined above
48 outQ1 = dev.getOutputQueue('ve1Out', maxSize=30, blocking=True)
49 outQ2 = dev.getOutputQueue('ve2Out', maxSize=30, blocking=True)
50 outQ3 = dev.getOutputQueue('ve3Out', maxSize=30, blocking=True)
51
52 # Processing loop
53 with open('mono1.h264', 'wb') as fileMono1H264, open('color.h265', 'wb') as fileColorH265, open('mono2.h264', 'wb') as fileMono2H264:
54 print("Press Ctrl+C to stop encoding...")
55 while True:
56 try:
57 # Empty each queue
58 while outQ1.has():
59 outQ1.get().getData().tofile(fileMono1H264)
60
61 while outQ2.has():
62 outQ2.get().getData().tofile(fileColorH265)
63
64 while outQ3.has():
65 outQ3.get().getData().tofile(fileMono2H264)
66 except KeyboardInterrupt:
67 break
68
69 print("To view the encoded data, convert the stream file (.h264/.h265) into a video file (.mp4), using commands below:")
70 cmd = "ffmpeg -framerate 25 -i {} -c copy {}"
71 print(cmd.format("mono1.h264", "mono1.mp4"))
72 print(cmd.format("mono2.h264", "mono2.mp4"))
73 print(cmd.format("color.h265", "color.mp4"))Pipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。