单目预览
类似示例:
演示
源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6# Create pipeline
7pipeline = dai.Pipeline()
8
9# Define sources and outputs
10monoLeft = pipeline.create(dai.node.MonoCamera)
11monoRight = pipeline.create(dai.node.MonoCamera)
12xoutLeft = pipeline.create(dai.node.XLinkOut)
13xoutRight = pipeline.create(dai.node.XLinkOut)
14
15xoutLeft.setStreamName('left')
16xoutRight.setStreamName('right')
17
18# Properties
19monoLeft.setCamera("left")
20monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
21monoRight.setCamera("right")
22monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
23
24# Linking
25monoRight.out.link(xoutRight.input)
26monoLeft.out.link(xoutLeft.input)
27
28# Connect to device and start pipeline
29with dai.Device(pipeline) as device:
30
31 # Output queues will be used to get the grayscale frames from the outputs defined above
32 qLeft = device.getOutputQueue(name="left", maxSize=4, blocking=False)
33 qRight = device.getOutputQueue(name="right", maxSize=4, blocking=False)
34
35 while True:
36 # Instead of get (blocking), we use tryGet (non-blocking) which will return the available data or None otherwise
37 inLeft = qLeft.tryGet()
38 inRight = qRight.tryGet()
39
40 if inLeft is not None:
41 cv2.imshow("left", inLeft.getCvFrame())
42
43 if inRight is not None:
44 cv2.imshow("right", inRight.getCvFrame())
45
46 if cv2.waitKey(1) == ord('q'):
47 break管道
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。