Script NNData 示例
演示
Command Line
1~/depthai-python/examples/Script$ python3 script_nndata_datatype.py
2层名称: ['fp16', 'uint8']
3NNData 大小: 13
4FP16 值: [1.0, 1.2001953125, 3.900390625, 5.5]
5UINT8 值: [6, 9, 4, 2, 0]源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2import depthai as dai
3import time
4
5# Start defining a pipeline
6pipeline = dai.Pipeline()
7
8# Script node
9script = pipeline.create(dai.node.Script)
10script.setScript("""
11 buf = NNData(150)
12 buf.setLayer("fp16", [1.0, 1.2, 3.9, 5.5])
13 buf.setLayer("uint8", [6, 9, 4, 2, 0])
14 node.warn("Names of layers: " + str(buf.getAllLayerNames()))
15 node.io['host'].send(buf)
16""")
17
18# XLinkOut
19xout = pipeline.create(dai.node.XLinkOut)
20xout.setStreamName('host')
21script.outputs['host'].link(xout.input)
22
23# Connect to device with pipeline
24with dai.Device(pipeline) as device:
25 device.setLogLevel(dai.LogLevel.WARN)
26 device.setLogOutputLevel(dai.LogLevel.WARN)
27
28 nndata = device.getOutputQueue("host").get()
29 time.sleep(0.5)
30
31 print(f"NNData size: {len(nndata.getData())}")
32 print("FP16 values:", nndata.getLayerFp16("fp16"))
33 print("UINT8 values:",nndata.getLayerUInt8("uint8"))Pipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。