RGB-热力对齐
演示

源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3"""
4Due to an issue with our calibration, you might receive the following error when running this script on early release OAK Thermal devices:
5```bash
6[ImageAlign(4)] [error] Failed to get calibration data: Extrinsic connection between the requested cameraId's doesn't exist. Please recalibrate or modify your calibration data
7```
8If this happens, please download the calibration data + script from https://drive.google.com/drive/folders/1Q_MZMqWMKDC1eOqVHGPeDO-NJgFmnY5U,
9place them into the same folder, connect the camera to the computer and run the script. This will update the
10calibration and add required extrinsics between the camera sensors.
11"""
12
13import cv2
14import depthai as dai
15import numpy as np
16import time
17from datetime import timedelta
18
19FPS = 25.0
20
21RGB_SOCKET = dai.CameraBoardSocket.CAM_A
22COLOR_RESOLUTION = dai.ColorCameraProperties.SensorResolution.THE_1080_P
23
24class FPSCounter:
25 def __init__(self):
26 self.frameTimes = []
27
28 def tick(self):
29 now = time.time()
30 self.frameTimes.append(now)
31 self.frameTimes = self.frameTimes[-100:]
32
33 def getFps(self):
34 if len(self.frameTimes) <= 1:
35 return 0
36 # Calculate the FPS
37 return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])
38
39device = dai.Device()
40
41thermalWidth, thermalHeight = -1, -1
42thermalFound = False
43for features in device.getConnectedCameraFeatures():
44 if dai.CameraSensorType.THERMAL in features.supportedTypes:
45 thermalFound = True
46 thermalSocket = features.socket
47 thermalWidth, thermalHeight = features.width, features.height
48 break
49if not thermalFound:
50 raise RuntimeError("No thermal camera found!")
51
52
53ISP_SCALE = 3
54
55calibrationHandler = device.readCalibration()
56rgbDistortion = calibrationHandler.getDistortionCoefficients(RGB_SOCKET)
57distortionModel = calibrationHandler.getDistortionModel(RGB_SOCKET)
58if distortionModel != dai.CameraModel.Perspective:
59 raise RuntimeError("Unsupported distortion model for RGB camera. This example supports only Perspective model.")
60
61pipeline = dai.Pipeline()
62
63# Define sources and outputs
64camRgb = pipeline.create(dai.node.ColorCamera)
65thermalCam = pipeline.create(dai.node.Camera)
66thermalCam.setBoardSocket(thermalSocket)
67thermalCam.setFps(FPS)
68
69sync = pipeline.create(dai.node.Sync)
70out = pipeline.create(dai.node.XLinkOut)
71align = pipeline.create(dai.node.ImageAlign)
72cfgIn = pipeline.create(dai.node.XLinkIn)
73
74
75camRgb.setBoardSocket(RGB_SOCKET)
76camRgb.setResolution(COLOR_RESOLUTION)
77camRgb.setFps(FPS)
78camRgb.setIspScale(1,ISP_SCALE)
79
80out.setStreamName("out")
81
82sync.setSyncThreshold(timedelta(seconds=0.5 / FPS))
83
84cfgIn.setStreamName("config")
85
86cfg = align.initialConfig.get()
87staticDepthPlane = cfg.staticDepthPlane
88
89# Linking
90align.outputAligned.link(sync.inputs["aligned"])
91camRgb.isp.link(sync.inputs["rgb"])
92camRgb.isp.link(align.inputAlignTo)
93thermalCam.raw.link(align.input)
94sync.out.link(out.input)
95cfgIn.out.link(align.inputConfig)
96
97
98rgbWeight = 0.4
99thermalWeight = 0.6
100
101
102def updateBlendWeights(percentRgb):
103 """
104 Update the rgb and depth weights used to blend depth/rgb image
105 @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
106 """
107 global thermalWeight
108 global rgbWeight
109 rgbWeight = float(percentRgb) / 100.0
110 thermalWeight = 1.0 - rgbWeight
111
112def updateDepthPlane(depth):
113 global staticDepthPlane
114 staticDepthPlane = depth
115
116# Connect to device and start pipeline
117with device:
118 device.startPipeline(pipeline)
119 queue = device.getOutputQueue("out", 8, False)
120 cfgQ = device.getInputQueue("config")
121
122 # Configure windows; trackbar adjusts blending ratio of rgb/depth
123 windowName = "rgb-thermal"
124
125 # Set the window to be resizable and the initial size
126 cv2.namedWindow(windowName, cv2.WINDOW_NORMAL)
127 cv2.resizeWindow(windowName, 1280, 720)
128 cv2.createTrackbar(
129 "RGB Weight %",
130 windowName,
131 int(rgbWeight * 100),
132 100,
133 updateBlendWeights,
134 )
135 cv2.createTrackbar(
136 "Static Depth Plane [mm]",
137 windowName,
138 0,
139 2000,
140 updateDepthPlane,
141 )
142 fpsCounter = FPSCounter()
143 while True:
144 messageGroup = queue.get()
145 assert isinstance(messageGroup, dai.MessageGroup)
146 frameRgb = messageGroup["rgb"]
147 assert isinstance(frameRgb, dai.ImgFrame)
148 thermalAligned = messageGroup["aligned"]
149 assert isinstance(thermalAligned, dai.ImgFrame)
150 frameRgbCv = frameRgb.getCvFrame()
151 fpsCounter.tick()
152
153 rgbIntrinsics = calibrationHandler.getCameraIntrinsics(RGB_SOCKET, int(frameRgbCv.shape[1]), int(frameRgbCv.shape[0]))
154
155 cvFrameUndistorted = cv2.undistort(
156 frameRgbCv,
157 np.array(rgbIntrinsics),
158 np.array(rgbDistortion),
159 )
160
161 # Colorize the aligned depth
162 thermalFrame = thermalAligned.getCvFrame().astype(np.float32)
163 # Create a mask for nan values
164 mask = np.isnan(thermalFrame)
165 # Replace nan values with a mean for visualization
166 thermalFrame[mask] = np.nanmean(thermalFrame)
167 thermalFrame = cv2.normalize(thermalFrame, None, 0, 255, cv2.NORM_MINMAX, cv2.CV_8U)
168 colormappedFrame = cv2.applyColorMap(thermalFrame, cv2.COLORMAP_MAGMA)
169 # Apply the mask back with black pixels (0)
170 colormappedFrame[mask] = 0
171
172 blended = cv2.addWeighted(cvFrameUndistorted, rgbWeight, colormappedFrame, thermalWeight, 0)
173
174 cv2.putText(
175 blended,
176 f"FPS: {fpsCounter.getFps():.2f}",
177 (10, 30),
178 cv2.FONT_HERSHEY_SIMPLEX,
179 1,
180 (255, 255, 255),
181 2,
182 )
183
184 cv2.imshow(windowName, blended)
185
186 key = cv2.waitKey(1)
187 if key == ord("q"):
188 break
189
190 cfg.staticDepthPlane = staticDepthPlane
191 cfgQ.send(cfg)管道
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。