ON THIS PAGE

  • Updating OS
  • Update from host (keep data)
  • Update from device (keep data)
  • Full OS Flash (wipe data)
  • Update OS with Recovery (last resort)
  • Enabling SSH
  • pip
  • Changelog
  • 1.33.0
  • 1.32.1
  • 1.31.2
  • 1.30.1
  • 1.29.2
  • 1.27.1
  • 1.25.3
  • 1.24.0
  • 1.23.1
  • 1.23.0
  • 1.21.1
  • 1.20.5
  • 1.18.3
  • 1.15.0
  • 1.14.1
  • 1.13.1
  • 1.11.0
  • 1.8.0
  • 1.6
  • 1.5
  • 1.4.1
  • 1.4
  • 1.3
  • 1.2
  • 1.1
  • 1.0
  • 0.26
  • 0.25
  • 0.24
  • 0.23
  • 0.22
  • 0.21
  • 0.20

Luxonis OS

Luxonis OS is a custom Linux distribution based on Yocto. It is custom-designed for the cameras built around the RVC4 chip, as the chip has 6core ARM CPU. The OS is pre-installed on all OAK4 cameras and can be updated for latest features.We assume you already know how to connect to your device using SSH or ADB as this is required for transferring files and sending some update commands.First check your OS version by connecting to the device either through SSH or ADB and run the following command on the device:
Command Line
1cat /etc/os-release

Updating OS

Your device offers multiple update methods so you can update it from different parts of the system, maintain compatibility across OS versions, and have a reliable fallback if one method fails. We suggest reading through all the steps and warnings before executing the commands.Jump to method:

Update from host (keep data)

You can update your device from host (eg. your PC) using oakctl host command line tool. This allows you to:
  • update and preserve data - does not delete user data on the device
  • update from host directly - you don't need to connect to device using SSH or ADB

Steps

  1. Download and install the oakctl tool.
  2. Make sure you have the latest oakctl version installed.
Command Line
1oakctl self-update
Then run the following command to update the device OS:
Command Line
1oakctl device update
Wait for the update to complete. The device will reboot automatically after the update.

Example output

Command Line
1$ oakctl device update
2> Do you want to update to the latest firmware? Yes
3✔ Starting firmware update...          
4✔ Update processed                                                                                                                                                                
5✔ Device is offline, should be back online soon.
6✔ Device is back online.
7✔ Device updated successfully!
8Device Info:
9  OS:   Luxonis OS RVC4 1.33.0
10  Architecture:  linux/arm64
11  Model:  Luxonis, Inc. KalamaP OAK4-D R2
12	Platform:  rvc4

Update from device (keep data)

You can update your device by using SSH or ADB to login and then using agentconfd command line tool. This enables you to:
  • update and preserve data - does not delete user data on the device
  • update without installing anything on the host machine
  • update using URL (easy, single command update, but camera needs to have internet access)
  • update using a locally downloaded OTA file (multi command update, but camera doesn't need internet access)

Option 1: Update using URL

Command Line
1# ADB/SSH into the device first, then on device run:
2agentconfd update https://luxonisos-rvc4.fra1.digitaloceanspaces.com/OTA/full_update_luxonis_ext4-1.33.0.zip
3reboot  # reboot device after update

Option 2: Update using a downloaded OTA update file

  1. Download the OTA update file for the latest 1.33.0 version (other versions available in Changelog).
  2. Copy the downloaded full_update_luxonis_ext4-1.33.0.zip image (via scp or adb push) to the device - see Direct access to the device.
  3. SSH or ADB into the camera and run the following commands on the device:
Command Line
1# ADB/SSH into the device first, then on device run:
2agentconfd update /data/full_update_luxonis_ext4-1.33.0.zip
3reboot  # reboot device after update

Full OS Flash (wipe data)

You can flash a new OS onto your device form host using oakctl command line tool. This allows you to:
  • update the OS, completely wiping all user data in the process
  • update device running any OS version (even the OS 1.x and older)
  • flash the device through USB3

Preparation

  1. Download and install the oakctl tool.
  2. Connect the camera with both PoE M12 cable (for power) and USB3 cable to PC (for flashing).
  3. Then follow one of two options:

Option 1: Flash using URL

Command Line
1oakctl device flash https://luxonisos-rvc4.fra1.digitaloceanspaces.com/PRODUCTION/luxonis_os_rvc4-1.33.0.tar.xz

Option 2: Flash using a downloaded file

  1. First, download the full-flash .tar.xz image (latest 1.33.0, other versions available in Changelog) and extract it (e.g. with 7-Zip/WinRAR/tar).
  2. Perform the full OS flash using oakctl and the path to the downloaded file.
Command Line
1oakctl device flash <path-to-downloaded-image>

If you're getting errors when doing a Full OS Flash

It might be because the USB is sometimes unreliable in EDL mode. Make sure:
  • the USB cable and port are USB3 capable
  • you use a high quality USB3 cable
  • you try out all possible USB-C cable orientations (with power cycles in between)
  • to try different USB ports on your PC

Update OS with Recovery (last resort)

  1. Download the OTA update file for the latest version (other versions available in Changelog).
  2. Copy the downloaded full_update_luxonis_ext4-1.33.0.zip image (via scp or adb push) to the device - see Direct access to the device.
  3. SSH or ADB into the camera and run the following commands on the device:
Command Line
1# ADB/SSH into the device first, then on device run:
2recovery --wipe_cache --update_package=/data/full_update_luxonis_ext4-1.33.0.zip
3reboot

Enabling SSH

In some newer OS versions SSH is disabled by default (OS versions 1.18 and later). To enable it, you first need to connect to the device via ADB and enable the SSH.
  • Download the sshd_config file - right-click and save as sshd_config.
  • Open terminal and push the downloaded file to the device by running
Command Line
1oakctl adb root && oakctl adb push sshd_config /etc/ssh/sshd_config
  • Reboot the device
  • [Optional] Now you can connect to the device via SSH (default password oelinux123). If you wish to disable password, run passwd -d root when connected to the device (either via ADB or SSH).

pip

By default, pip isn't installed on the OS, so user has to install it manually:
Command Line
1python3 -m ensurepip

Changelog

1.33.0

(5 June 2026) - OTA update, Full OS Flash
  • Boot in powersave mode if limited input power (less than 25W) available
  • Add temperature measurement feature for dot projector in STM32 firmware
  • Enable/add custom UVC extensions (XUs) in kernel
  • Implement max ISO for auto exposure
  • Bump agentconfd to v1.12.0:
    • Support power profiles for limited power mode
  • Bump oak-agent to v0.22.1:
    • Fixes for container filling up disk space
  • Remove/fix frame duration override for PTP when exposure is at maximum
  • Fix long boot time if no USB-C cable plugged in:
    • Regression introduced in 1.32.0 with USB ETH feature
    • Fix color rendering for OV9782 sensor

1.32.1

(19 May 2026) - OTA update, Full OS Flash
  • Add basic support for iToF VD55H1 for OAK4-Lite
  • Add UVC still image capture support
  • Add USB Ethernet (NCM) support
  • Power profiles:
    • Introduce power profiles for +50 °C, +25 °C and -25 °C for OAK4-Lite PoE variant
    • Persist last user-selected power profiles during reboot
    • Board-specific USB power limits in bootloader (blink red LED if not enough input power, but have minimum required setting power for each board individually)
  • Bump oakctl version to v0.20.0, oak-agent to v0.20.0 and agentconfd to v1.11.0
  • For developers:
    • Expose CCI I2C as a normal I2C device (for easier development purposes)
  • Stop logging logcat file to persistent storage as it fills up disk space too quickly
    • Regression introduced in 1.28.0
  • Split/refactor OAK4-Lite device into two variants: USB and PoE
  • Fix OV9782 sensor driver on OAK4-D

1.31.2

(7 May 2026) - OTA update, Full OS Flash
  • Update agentconfd daemon to v1.10.1
    • Added M8 detect support for OAK4-LITE
    • Added basic power profiles to limit peak power draw to 15 W for OAK4-LITE
  • Update oak-agent to v0.19.1 and oakctl to v0.20.0
    • Added support for new flags on oakctl device update (--url, --path, --local)
  • Fix cropping in HFR mode on the IMX586 sensor
  • Fix IMU orientations and unify them across all devices
  • Fix persistent logs filling up disk space indefinitely
    • Regression introduced in 1.28.0
  • Add USB PD power querying and contracting support in the bootloader
    • The red LED now blinks when the power source cannot supply at least 25 W

1.30.1

(10 Apr 2026) - OTA update, Full OS Flash
  • Added basic support for new board type: OAK4-LITE
  • Added IMX586 4K@60 FPS support
  • Update NN models to 1.2.2410
  • Add M8 WiFi dongle support (Ezurio)
  • Update agentconfd to v1.9.1:
    • Add WiFi support
  • Fixed blooming issue on some OV9282 CCMs
  • Propagate DNS updates to running containers without the need for restart (by moving DNS ownership to systemd-resolved)
  • For developers:
    • Exposed sensor mode HDR, HFR, FOV to DepthAI
    • Correctly working DepthAI image transformations for non full FOV sensor modes
    • Correctly working sensor images alignment in non full FOV modes

1.29.2

(8 Apr 2026) - OTA update, Full OS Flash
  • Enable required Linux kernel features (cgroups, namespaces, netfilter, IPVS) to improve container support for Docker and K3s
  • Exposed negotiated USB PD (Power Delivery) voltage and current through sysfs
  • Implemented persistent logging with compression and rotation (kernel, logcat, systemd journal)
  • Updated agentconfd daemon to v1.8.1, cli to v1.6.0, and messages to v1.6.0
  • Updated oak-agent to v0.18.6 and oakctl to v0.18.6
  • Added INA700 measurement_target parameter in device tree for easier use with agentconfd
  • Fixed busybox wget to correctly use CA certificates
  • Standardized kernel versioning (clean version string without custom suffixes)

1.27.1

(3 Mar 2026) - OTA update, Full OS Flash
  • Add support for the OG05B1B sensor over 2 MIPI lanes on OAK4-D
    • 2592x1944 @ 45 FPS
    • 1920x1080 @ 90 FPS
  • Enable stereo microphone support with PulseAudio configuration:
    • regular0 - PAL_STREAM_DEEP_BUFFER (post-processing with echo cancellation enabled)
    • regular1 - PAL_STREAM_RAW
    • regular2 - PAL_STREAM_LOW_LATENCY
  • Update OG05B10 tuning profiles
  • Update depthai-gate with DAI USB support
  • Fix USB enumeration when connected to USB-PD. Properly enumerates as USB3 instead of USB2
    • Configure TPS to work on interrupt
    • Improve TPS driver logic by better interrupt handling
    • Improve TPS start sequence when connected on USB-PD
  • Fix non-working WinUSB descriptor.
  • Improve OG05B10 driver to match FSYNC value from STM signal generator

1.25.3

(19 Feb 2026) - OTA update, Full OS Flash
  • Add Camera PTP feature to synchronize camera frames
    • Update Ethernet driver to custom rtl8125 with PTP support
  • Enable 12 MHz camera clock
  • Add TLS support in wget using OpenSSL
  • Update SNPE library to v2.41
  • Add USB burst mode on Luxons USB descriptor interfaces
  • Update oak-agent to v0.18.3
  • Update oak-ctl to v0.18.2
  • Update agentconfd to v1.7.1:
    • Add configurable oak-agent paths in SetupParameters (conf_dir, conf_file, and apps conf dir)
  • Fix occasional two-stream camera crash
  • Simplify CAMX camera pipeline by removing redundant use-cases

1.24.0

(2 Feb 2026) - OTA update, Full OS Flash
  • Add OG05B10 sensor tuning for PZ029 CCM used on the OAK4-D device
  • Update depthai-gate to 0.0.26
  • Improve camera synchronization logic using FSYNC over STM
    • Allow loading custom firmware for debugging purposes
    • Improve error handling
    • Remove GPIO control
    • Remove kernel loading and unloading on startup
    • Unload the kernel only on unrecoverable failure
    • Dynamically detect STM bus and address
    • Add a command to show dynamically detected I2C bus and address
    • Detect the device in bootloader mode
    • Add missing STM FSYNC pin
    • Add external I/O FSYNC pin data
    • Rename STM LED limit fields
    • Add shutdown hooks
    • Add closest frequency query
    • Add ioctl: set camera data with fixed-point decimal FPS
    • Rename LED limit variables
    • Update STM firmware
    • Fix: automatic downgrading to match STM firmware with the kernel driver
    • Fix: retry flashing if STM gets stuck in bootloader mode
    • Fix: force reflashing if STM firmware is broken
  • Update agentconfd daemon from v1.6.2 to v1.6.5, with the following changes:
    • Added M8 detect line on the dev kit
    • Fix static IP rollback after 3 minutes
    • Fix a potential bug where the /etc/agentconfd/.update_status.json file could be temporarily empty
    • Fix agentconfd update --status
    • Fix OTA update status to enter the Error state on boot after abrupt power loss during an OTA update
  • Fix: Make OTA robust against power cycles during OTA updates, which was not applied correctly in the 1.19.0 release

1.23.1

(8 Jan 2026) – OTA update, Full OS Flash
  • OG05B10 tuning apply fix

1.23.0

(25 Dec 2025) – OTA update, Full OS Flash
  • OG05B10 sensor:
    • Move to 4 lane DPHY MIPI
      • 2592x1944@60
      • 1920x1080@90 central crop
    • Add tuned chromatix profile
    • Enable sensor for OAK4-D device
  • Add luxonis .dlc model: SMv4_3XL_input_780x1248_output_780x1248_v9_snpe_2320
  • Introduce DEV-KIT R6 version
  • Route USB2 lines to USBC connector by default for OAK4-S R9 HW version. This fixes USB2 for OAK4-S R9.
  • Add back CONFIG_RTNICPG used by RTL MAC address programming.

1.21.1

(1 Dec 2025) – OTA update, Full OS Flash
  • Updated frame timestamp handling to remove the qtime_to_boottime calculation, fixing frame timestamp generation for DAI
  • Added Luxonis USB interfaces
    • Interface 3: Luxonis DepthAI Gate
    • Interface 4: Luxonis DepthAI Device
  • Integrated UVC driver updates, enabling the OAK UVC application to run on mainline OS
  • Enabled data journaling on the filesystem to prevent data corruption during power cuts

1.20.5

(27 Oct 2025) – OTA update, Full OS Flash
  • Introduce a feature to limit the maximum exposure time
  • Expose HDR control parameters: Exposure Ratio & Tone Weight
  • Add IMX586 sensor native resolutions: 2K@119, 1080p@240 and 720p@480
  • Provide OG05B10 production configuration for 2 lane dphy
    • 2592x1944@45. Reduced from 53 for more stability
    • 1920x1080@90. Central crop instead of end crop
    • Adjust image orientation to match mounted sensor on the OAK4S-CS device
  • Update depthai_gate to 0.0.25. Migration to direct HAL camera control, dropping qmmf & gstreamer dependencies
  • Rename Ethernet interface to eth0 for simplicity
  • Add support for IPv4LL
  • Add support for dynamic tuning profile changes
  • Add Luxonis tuning profiles for OV9282 wide FOV and NFOV
  • Update agentconfd to v1.6.2 & oak-agent to 0.17.0
    • agetnconfd: Release notes:
    • Factory reset button monitor: Fixed a race condition where start-setup could incorrectly execute during a 10-second factory reset button hold
    • fix: /etc/resolv.conf sometimes empty after agentconfd setup or configure
    • fix: setup without internet failure and long timeout
    • fix: agentconfd update OTA package download failures on unstable networks
    • fix: agentconfd update wouldn't be killed properly upon CTRL+C during recovery stage. The CLI would hang, but the actual update would be terminated
    • feat: Added optional --checksum to UpdateParameters feat: Implemented checksum check on downloaded OTA package
  • Update default app (viewer) to v1.4.51
  • Reduce IR dot and flood current limits. Ensures the system remains within the 25 W power budget.
    • Extended STM tool to support LED current control
    • Fix IPv4LL to avoid clearing the local address if DHCP is not found after a timeout
  • Limit USB speed to SuperSpeed (5 Gbps) to avoid issues observed on some devices
  • Improve LuxonisSideChannel shutdown handling during camx exit
  • Focus improvement:
    • Improve the autofocus algorithm with proper actuator step size and range.
    • Refine initial startup code to align with the selected tuning profile.
    • Enable actuator support on DEVKIT R2 and R3 revisions.
  • Fix IO settings to match expected nominal electrical values
  • Make OTA robust against power cycles during OTA updates
  • Limit BOB power rail to prevent voltage spikes above 3.6V

1.18.3

(4 Sep 2025) – OTA update, Full OS Flash
  • Fix missing ethernet phy on devkit R3
  • Disable fastboot via factory reset button on OAK4-S
  • Use sysMonApp version 10.0.29
  • Fix oak4-s R9 fsync stm reset pin. The pin was configured as active low even though it's active high. This caused the stm to not work on the new design
  • Add support for OAK4-S R9 revision
  • Add support for OAK4-D R9 revision
  • Add support for DEV-KIT R3 revision
  • Add support for INA power measurement device
  • Camera optimisation: Do not select 8k resolution if not required since it occupies 2 IFEs
  • IMX586 improvements:
    • Improve HDR with introducing HDR3
  • Add OG05B1B support over 2 lane DPHY:
    • 2592x1944@53
    • 1920x1080@90
    • AEC control
  • Improve OG051B0
    • Tune configuration for more stable and less noise outputs
    • Improve dynamic res/fps detection
    • Introduce 2 lane DPHY as default setting
  • Add OG01A1B: not enabled by default
    • 1280x1024@120
    • AEC control
  • Update default-app to 1.4.7
    • Fix Hub setup with opening default app
    • Fix Yolo World model caching and configuration form
    • Fix actions buttons on Point Cloud panel.
    • Support for mouse over measurements on Depth Stream
  • Update oak-agent to v0.14.0:
    • Larger queues for handling mqtt events, leading to less probability of some messages being dropped
    • Increase number of WebRTC connection retries
    • Improved the handling of mqtt events by not forwarding them to the library if there is no active broker connection
    • Fixed deadlock in mqtt handler
    • Hotfixed a possible mqtt recovery issue after loosing internet connection which would leave the device in offline mode on hub
    • Expose network configuration via mqtt
    • Monitor ssl certs for expiry and renew them if close to expiry.
    • mqtt connection exponential backoff
    • Interactive app exec (docker run -it equivilent.)
  • Update agentconfd to v1.5.2
    • factory-reset-button: Fix bug where if the button was released while the led was still blinking, factory-reset wouldn't be performed
    • misc: Bump rust toolchain and edition to be able to use some of the latest features - specifically: if let &&
      • meta-rust-bin: Update to latest main
    • Remove cargo and rust: 1.81.0
    • Add cargo and rust: 1.89.0, reason being that agentconfd requires 1.89.0 now
    • The new default device state is setup completed
    • Upon 5s factory-reset button hold a special factory reset will be performed which will result in the setup app starting upon next boot
    • ssh is configured with prohibit-password by default. It can be re-configured to allow ssh pass login via setup
    • Fix network configuration persistency on when re-configuring multiple times
    • Fix layer build: Invalidate & remove all files from all layers above first layer that differs in hash
    • Changed the factory-reset pin on devkit from GPIO34 to GPIO43. (factory-reset through GPIO didn't work on devkit before)
    • Added R9 HW revisions

1.15.0

(8 Jul 2025) – OTA update, Full OS Flash
  • Introduce OAK4-LR device with R1 revision support
  • Fix stm-fsync driver to not produce lib/list_debug.c:24 crash
  • Update: agentconfd, oakctl & oak-agent to 0.12
    • agentconfd
    • OTA: Reset status LED on recovery failure.
    • Networking: Use auto DNS by default instead of setting DNS=GW.

1.14.1

(24 Jun 2025) – OTA update, Full OS Flash
  • og05b10 sensor: optimize driver for OAK4S custom setup
    • The sensor is powered and clocked from a custom CBA board
    • Do not turn on VIO/VANA/VDIO power
    • Do not set MCLK
    • Add longer delays on reset line since it goes through level shifter 1v8 -> 3v3
    • Optimize timings
  • Update STM Firmware with M8 external frame sync support
  • Fix -25C spine-net-run test Bump VDD_CX voltage from NOMINAL_L1 to TURBO_L1 for 3.2GHz and 3.6GHz
  • Revert: "Fix overlay corruption on powerloss" which produces corrupted filesystem on factory-reset

1.13.1

(20 Jun 2025)
  • Fix sporadic reboot issue causing device to enter Sahara mode
  • Introduce og05b10 colour global‑shutter sensor
    • 2592 × 1944 @ 50 FPS
    • 1920 × 1080 @ 90 FPS (end‑crop)
    • Free‑running & slave configuration
    • AEC control
  • Make IMX586 more robust on stream start (2nd iteration)
  • Apply correct accelerometer & gyro orientation for OAK4S & OAK4D
  • Fix overlay corruption on power‑loss
  • Remove unused packages: Qualcomm data packages for modem & TFTP server
  • Add fsync-stm-output notation in DTS
  • Update default oak‑app to 1.1.5
  • Update oak‑agent & oakctl to 0.11.0
  • Update agentconfd with M8 support
  • Expose baseboard EEPROM with fix for reads bigger than page‑size
  • Enable STM for SOM‑based devices, OAK4S & OAK4SR
  • Simplify actuator probe on camera discovery
  • Improve STM start‑up sequence by removing redundant firmware update
  • Make IMX586 more robust on start stream (first iteration)
  • Update agentconfd to 1.4.2
    • OTA: added status LED behaviour
    • OTA: utilise /data dir to avoid full OS in RAM
    • Provide DEVKIT default configuration

1.11.0

(22nd of May) - OTA update, Full OS Flash
  • New Features:
    • Expose eeproms to device agnostic paths for calibration and baseboard eeproms at /sys/bus/nvmem/devices/calibration-eeprom/nvmem and /sys/bus/nvmem/devices/baseboard-eeprom/nvmem
    • Add dynamic actuator functionality with actuator detection support
      • If actuator device is not functional, mark as actuator not present
      • Corner case: actuator IC present but lens mechanics not detected from OS (DAI should read eeprom)
    • Add mechanism for loading custom overlay DTBs & driver modules at runtime
    • Update setup-app to work for OAK4S R5 & OAK4D R7
    • Add support for MIRA220 sensor (1600x1400@30fps):
      • Master and slave (fsync) modes
      • Add 1280x1120 MIRA220 4/5 scale ISP output
      • Fix real gain to "artificial" digital gain conversion to avoid noise from ISPDigital gain
    • Add r8125 Realtek custom driver & linuxptp 4.4 targeting r8125 driver (currently disabled)
    • Add network development tools: iperf3 and ethtool
    • Enable direct devmem access for IO runtime configuration
    • Introduce public SDK for 3rd party development
    • Update SNPE to 2.32 version
    • Update DepthAI Gate to v0.23
    • Update oak apps:
      • oakctl v0.9.0
      • oak-agent v0.9.0
      • default-app v0.11.17
  • Fixes and Improvements:
    • Improve handling for runtime storage with tmp directory cleanup
    • Hotfix for IMU perf drop on ICM: Revert changes and use LSM IMU instead of ICM
    • Improve camera discovery: do not fail when one of the specified sensor driver is not present
    • OAK4S fix: perform USB_SEL change only for R2 revision

1.8.0

(9th of Apr)
  • Introduced OAK4D R7 version to match hardware revisions in production (no functional change).
  • Introduced OAK4S R5 version to match hardware revisions in production (no functional change).
  • Extended UEFI bootloader to use FORCE_USB_BOOT for factory reset with active high logic.
  • Added OS power profiles.

1.6

(12 Mar 2025) – OTA update, Full OS Flash
  • Added support for 48 MP resolution (IMX586) on OAK4 cameras (max 18 FPS).
  • Updated dot‑projector settings for improved safety.

1.5

(27 Feb 2025) – OTA update, Full OS Flash
  • Updated oakctl, oak‑agent and depthai‑gate versions.
  • Added RTW88 driver for RLT8811CU Wi‑Fi chip.
  • Moved to ICM4x IMU sensor as default accelerometer & gyroscope.
  • Fixed factory‑reset process.
  • Corrected flood‑light pins on OAK4D R2.
Below versions contain both OTA and Full‑flash updates in a single .tar.xz. To get the OTA (.zip) file, extract the archive.

1.4.1

(14 Feb 2025) – Download
  • Fixed IMU/Mic not working without USB connected.
  • Reduced power‑consumption.
  • Fixed I2C‑bus and FSYNC issues.

1.4

(11 Feb 2025) – Download

1.3

(29 Jan 2025) – Download
  • Enabled performance optimizations → faster boot‑up & improved CPU performance.
  • Improved Ethernet‐driver stability.
  • Added support for IMX586 QBC HDR mode.

1.2

(10 Jan 2025) – Download
  • /home is now read/write and persists across OTA updates.
  • Fixed CDAF autofocus.
  • Added manual‑focus actuator control.
  • Updated oak‑agent and bundled default apps.
  • Tested with DepthAI v3 – 3.0.0a11.

1.1

(17 Dec 2024) – Issue with DepthAI v3 compatibility
  • Improved factory‑mode without overlaying /etc.
  • Fixed camera‑sensor enumerations from 1.0 release.
  • Fixed Luxonis OUI MAC assignment when NIC unprogrammed.

1.0

(9 Dec 2024) – Issue with DepthAI v3 compatibility
  • Increased system (rootfs) & user‑data storage to 5 GB and 76 GB respectively.
  • Kept system rootfs read‑only.
  • Unified ID for EDL and ADB based on SoC ID.
  • Added low‑power detection on POE (note: when powered by sufficient USB‑PD, device may still report low‑power until boot‑complete).
  • Extended OTA update to include UEFI‑bootloader binary.

0.26

(4 Dec 2024) – Download
  • Fixed automatic USB‑role detection on boot.
  • Upgraded SNPE to v2.23.
  • Updated depthai‑gate to v0.21.
  • Disabled factory‑mode by default.
  • Added support for OAK4‑S R2 and OAK4‑D R2.

0.25

(19 Nov 2024) – Download
  • Requires DepthAI 3.0.0a8.
  • Added multiple SNPE versions.
  • Added USB support for Mediatek MT7601U Wi‑Fi chip.
  • Fixed communication with Windows host (USB‑peripheral mode).
  • Fixed status LED behaviour.
  • Assigned MAC on Ethernet if not already flashed.
  • Fixed R8169 driver (Realtek NIC).

0.24

(20 Oct 2024) – Download
  • Integrated oak‑agent into the OS.
  • Introduced factory‑mode.

0.23

(4 Oct 2024) – Download
  • Improved IR‑LED driving logic for FSYNC STM on OAK4‑D.
  • Enhanced image‑quality on OV9282 sensors (driver improvements).

0.22

(23 Sep 2024) – Download
  • Added support for AK0991x magnetometer.
  • Implemented sensor‑fusion for rotv & game_rv algorithms.
  • Added FSYNC support using STM co‑processor.
  • Added EEPROM driver to enable calibration EEPROM.

0.21

(8 Sep 2024) – Download
  • Fixed colour‑sensor on OAK4‑D.
  • Fixed USB2 communication on OAK4‑S.
  • Added factory‑reset button (USB_BOOT) support on OAK4‑S & OAK4‑D.
  • Added IMU support on OAK4 cameras.
  • Fixed IMX582 sensor support.

0.20

(2 Aug 2024) – Download
  • Added board‑identification support.
  • Added hardware‑in‑loop tests.
  • Updated depthai‑gate to v0.0.20.
  • Updated system libraries.