HubAI is the AI-focused layer of Luxonis Hub, built for managing models across our ecosystem. It provides an integrated interface for converting and adapting custom models, along with a growing collection of pre-trained models prepared for deployment across Luxonis devices. From rapid experimentation to scalable production workflows, HubAI enables fast testing, iteration, and deployment — all from a single platform.
When you need the fastest path from a raw model file to a deployable Luxonis format, the Quick Conversion interface is the most direct option. It enables rapid, one-off conversions without creating a model entry or maintaining version history. Just upload your model, convert it immediately, and download a variant optimized for your Luxonis device.
For long-term workflows, collaboration, or managing model variants, the Model Registry serves as the core of HubAI. Here, you can browse a curated collection of public models categorized by task and ready for deployment, or upload your own models to maintain versions, share them with your team or the community, and keep track of updates over time.Unlike Quick Conversion — which focuses on speed and simplicity — the Model Registry includes a more robust workflow for conversion called Detailed Conversion. This workflow offers advanced configuration, supports multiple variants of a model, and fits naturally into versioned model management — making it ideal for production-ready and collaborative development.