Camera¶
Camera node is a source of image frames. You can control in at runtime with the InputControl
and InputConfig
.
It aims to unify the ColorCamera and MonoCamera into one node.
Compared to ColorCamera node, Camera node:
Supports cam.setSize(), which replaces both
cam.setResolution()
andcam.setIspScale()
. Camera node will automatically find resolution that fits best, and apply correct scaling to achieve user-selected sizeSupports cam.setCalibrationAlpha(), example here: Undistort camera stream
Supports cam.loadMeshData() and cam.setMeshStep(), which can be used for custom image warping (undistortion, perspective correction, etc.)
Automatically undistorts camera stream if HFOV of the camera is greater than 85°. You can disable this with:
cam.setMeshSource(dai.CameraProperties.WarpMeshSource.NONE)
.
Besides points above, compared to MonoCamera node, Camera node:
Doesn’t have
out
output, as it has the same outputs as ColorCamera (raw
,isp
,still
,preview
,video
). This means thatpreview
will output 3 planes of the same grayscale frame (3x overhead), andisp
/video
/still
will output luma (useful grayscale information) + chroma (all values are 128), which will result in 1.5x bandwidth overhead
How to place it¶
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.Camera)
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::Camera>();
Inputs and Outputs¶
Camera node
┌──────────────────────────────┐
│ ┌─────────────┐ │
│ │ Image │ raw │ raw
│ │ Sensor │---┬--------├────────►
│ └────▲────────┘ | │
│ │ ┌--------┘ │
│ ┌─┴───▼─┐ │ isp
inputControl │ │ │-------┬-------├────────►
──────────────►│------│ ISP │ ┌─────▼────┐ │ video
│ │ │ | |--├────────►
│ └───────┘ │ Image │ │ still
inputConfig │ │ Post- │--├────────►
──────────────►│----------------|Processing│ │ preview
│ │ │--├────────►
│ └──────────┘ │
└──────────────────────────────┘
Message types
inputConfig
- ImageManipConfiginputControl
- CameraControlraw
- ImgFrame - RAW10 bayer data. Demo code for unpacking hereisp
- ImgFrame - YUV420 planar (same as YU12/IYUV/I420)still
- ImgFrame - NV12, suitable for bigger size frames. The image gets created when a capture event is sent to the Camera, so it’s like taking a photopreview
- ImgFrame - RGB (or BGR planar/interleaved if configured), mostly suited for small size previews and to feed the image into NeuralNetworkvideo
- ImgFrame - NV12, suitable for bigger size frames
ISP (image signal processor) is used for bayer transformation, demosaicing, noise reduction, and other image enhancements. It interacts with the 3A algorithms: auto-focus, auto-exposure, and auto-white-balance, which are handling image sensor adjustments such as exposure time, sensitivity (ISO), and lens position (if the camera module has a motorized lens) at runtime. Click here for more information.
Image Post-Processing converts YUV420 planar frames from the ISP into video
/preview
/still
frames.
still
(when a capture is triggered) and isp
work at the max camera resolution, while video
and preview
are
limited to max 4K (3840 x 2160) resolution, which is cropped from isp
.
For IMX378 (12MP), the post-processing works like this:
┌─────┐ Cropping to ┌─────────┐ Downscaling ┌──────────┐
│ ISP ├────────────────►│ video ├───────────────►│ preview │
└─────┘ max 3840x2160 └─────────┘ and cropping └──────────┘
The image above is the isp
output from the Camera (12MP resolution from IMX378). If you aren’t downscaling ISP,
the video
output is cropped to 4k (max 3840x2160 due to the limitation of the video
output) as represented by
the blue rectangle. The Yellow rectangle represents a cropped preview
output when the preview size is set to a 1:1 aspect
ratio (eg. when using a 300x300 preview size for the MobileNet-SSD NN model) because the preview
output is derived from
the video
output.
Usage¶
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.Camera)
cam.setPreviewSize(300, 300)
cam.setBoardSocket(dai.CameraBoardSocket.CAM_A)
# Instead of setting the resolution, user can specify size, which will set
# sensor resolution to best fit, and also apply scaling
cam.setSize(1280, 720)
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::Camera>();
cam->setPreviewSize(300, 300);
cam->setBoardSocket(dai::CameraBoardSocket::CAM_A);
// Instead of setting the resolution, user can specify size, which will set
// sensor resolution to best fit, and also apply scaling
cam->setSize(1280, 720);
Limitations¶
Here are known camera limitations for the RVC2:
ISP can process about 600 MP/s, and about 500 MP/s when the pipeline is also running NNs and video encoder in parallel
3A algorithms can process about 200..250 FPS overall (for all camera streams). This is a current limitation of our implementation, and we have plans for a workaround to run 3A algorithms on every Xth frame, no ETA yet
Examples of functionality¶
Reference¶
-
class
depthai.node.
Camera
Camera node. Experimental node, for both mono and color types of sensors
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.CameraProperties
-
property
frameEvent
Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getBoardSocket
(self: depthai.node.Camera) → depthai.CameraBoardSocket Retrieves which board socket to use
- Returns
Board socket to use
-
getCalibrationAlpha
(self: depthai.node.Camera) → Optional[float] Get calibration alpha parameter that determines FOV of undistorted frames
-
getCamera
(self: depthai.node.Camera) → str Retrieves which camera to use by name
- Returns
Name of the camera to use
-
getFps
(self: depthai.node.Camera) → float Get rate at which camera should produce frames
- Returns
Rate in frames per second
-
getHeight
(self: depthai.node.Camera) → int Get sensor resolution height
-
getImageOrientation
(self: depthai.node.Camera) → depthai.CameraImageOrientation Get camera image orientation
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getMeshSource
(self: depthai.node.Camera) → depthai.CameraProperties.WarpMeshSource Gets the source of the warp mesh
-
getMeshStep
(self: depthai.node.Camera) → Tuple[int, int] Gets the distance between mesh points
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
getPreviewHeight
(self: depthai.node.Camera) → int Get preview height
-
getPreviewSize
(self: depthai.node.Camera) → Tuple[int, int] Get preview size as tuple
-
getPreviewWidth
(self: depthai.node.Camera) → int Get preview width
-
getSize
(self: depthai.node.Camera) → Tuple[int, int] Get sensor resolution as size
-
getStillHeight
(self: depthai.node.Camera) → int Get still height
-
getStillSize
(self: depthai.node.Camera) → Tuple[int, int] Get still size as tuple
-
getStillWidth
(self: depthai.node.Camera) → int Get still width
-
getVideoHeight
(self: depthai.node.Camera) → int Get video height
-
getVideoSize
(self: depthai.node.Camera) → Tuple[int, int] Get video size as tuple
-
getVideoWidth
(self: depthai.node.Camera) → int Get video width
-
getWidth
(self: depthai.node.Camera) → int Get sensor resolution width
-
property
id
Id of node
-
property
initialControl
Initial control options to apply to sensor
-
property
inputConfig
Input for ImageManipConfig message, which can modify crop parameters in runtime
Default queue is non-blocking with size 8
-
property
inputControl
Input for CameraControl message, which can modify camera parameters in runtime
Default queue is blocking with size 8
-
property
isp
Outputs ImgFrame message that carries YUV420 planar (I420/IYUV) frame data.
Generated by the ISP engine, and the source for the ‘video’, ‘preview’ and ‘still’ outputs
-
loadMeshData
(self: depthai.node.Camera, warpMesh: buffer) → None Specify mesh calibration data for undistortion See loadMeshFiles for the expected data format
-
loadMeshFile
(self: depthai.node.Camera, warpMesh: Path) → None Specify local filesystem paths to the undistort mesh calibration files.
When a mesh calibration is set, it overrides the camera intrinsics/extrinsics matrices. Overrides useHomographyRectification behavior. Mesh format: a sequence of (y,x) points as ‘float’ with coordinates from the input image to be mapped in the output. The mesh can be subsampled, configured by setMeshStep.
With a 1280x800 resolution and the default (16,16) step, the required mesh size is:
width: 1280 / 16 + 1 = 81
height: 800 / 16 + 1 = 51
-
property
preview
Outputs ImgFrame message that carries BGR/RGB planar/interleaved encoded frame data.
Suitable for use with NeuralNetwork node
-
property
raw
Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor, and the source for the ‘isp’ output.
-
setBoardSocket
(self: depthai.node.Camera, boardSocket: depthai.CameraBoardSocket) → None Specify which board socket to use
- Parameter
boardSocket
: Board socket to use
- Parameter
-
setCalibrationAlpha
(self: depthai.node.Camera, alpha: float) → None Set calibration alpha parameter that determines FOV of undistorted frames
-
setCamera
(self: depthai.node.Camera, name: str) → None Specify which camera to use by name
- Parameter
name
: Name of the camera to use
- Parameter
-
setFps
(self: depthai.node.Camera, fps: float) → None Set rate at which camera should produce frames
- Parameter
fps
: Rate in frames per second
- Parameter
-
setImageOrientation
(self: depthai.node.Camera, imageOrientation: depthai.CameraImageOrientation) → None Set camera image orientation
-
setIsp3aFps
(self: depthai.node.Camera, arg0: int) → None Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
setMeshSource
(self: depthai.node.Camera, source: depthai.CameraProperties.WarpMeshSource) → None Set the source of the warp mesh or disable
-
setMeshStep
(self: depthai.node.Camera, width: int, height: int) → None Set the distance between mesh points. Default: (32, 32)
-
setPreviewSize
(*args, **kwargs) Overloaded function.
setPreviewSize(self: depthai.node.Camera, width: int, height: int) -> None
Set preview output size
setPreviewSize(self: depthai.node.Camera, size: Tuple[int, int]) -> None
Set preview output size, as a tuple <width, height>
-
setRawOutputPacked
(self: depthai.node.Camera, packed: bool) → None Configures whether the camera raw frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
-
setSize
(*args, **kwargs) Overloaded function.
setSize(self: depthai.node.Camera, width: int, height: int) -> None
Set desired resolution. Sets sensor size to best fit
setSize(self: depthai.node.Camera, size: Tuple[int, int]) -> None
Set desired resolution. Sets sensor size to best fit
-
setStillSize
(*args, **kwargs) Overloaded function.
setStillSize(self: depthai.node.Camera, width: int, height: int) -> None
Set still output size
setStillSize(self: depthai.node.Camera, size: Tuple[int, int]) -> None
Set still output size, as a tuple <width, height>
-
setVideoSize
(*args, **kwargs) Overloaded function.
setVideoSize(self: depthai.node.Camera, width: int, height: int) -> None
Set video output size
setVideoSize(self: depthai.node.Camera, size: Tuple[int, int]) -> None
Set video output size, as a tuple <width, height>
-
property
still
Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
The message is sent only when a CameraControl message arrives to inputControl with captureStill command set.
-
property
video
Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
Suitable for use with VideoEncoder node
-
class
-
class
dai::node
::
Camera
: public dai::NodeCRTP<Node, Camera, CameraProperties>¶ Camera node. Experimental node, for both mono and color types of sensors.
Public Functions
Constructs Camera node.
-
void
setBoardSocket
(CameraBoardSocket boardSocket)¶ Specify which board socket to use
- Parameters
boardSocket
: Board socket to use
-
CameraBoardSocket
getBoardSocket
() const¶ Retrieves which board socket to use
- Return
Board socket to use
-
void
setCamera
(std::string name)¶ Specify which camera to use by name
- Parameters
name
: Name of the camera to use
-
std::string
getCamera
() const¶ Retrieves which camera to use by name
- Return
Name of the camera to use
-
void
setImageOrientation
(CameraImageOrientation imageOrientation)¶ Set camera image orientation.
-
CameraImageOrientation
getImageOrientation
() const¶ Get camera image orientation.
-
void
setSize
(std::tuple<int, int> size)¶ Set desired resolution. Sets sensor size to best fit.
-
void
setSize
(int width, int height)¶ Set desired resolution. Sets sensor size to best fit.
-
void
setPreviewSize
(int width, int height)¶ Set preview output size.
-
void
setPreviewSize
(std::tuple<int, int> size)¶ Set preview output size, as a tuple <width, height>
-
void
setVideoSize
(int width, int height)¶ Set video output size.
-
void
setVideoSize
(std::tuple<int, int> size)¶ Set video output size, as a tuple <width, height>
-
void
setStillSize
(int width, int height)¶ Set still output size.
-
void
setStillSize
(std::tuple<int, int> size)¶ Set still output size, as a tuple <width, height>
-
void
setFps
(float fps)¶ Set rate at which camera should produce frames
- Parameters
fps
: Rate in frames per second
-
void
setIsp3aFps
(int isp3aFps)¶ Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
float
getFps
() const¶ Get rate at which camera should produce frames
- Return
Rate in frames per second
-
std::tuple<int, int>
getPreviewSize
() const¶ Get preview size as tuple.
-
int
getPreviewWidth
() const¶ Get preview width.
-
int
getPreviewHeight
() const¶ Get preview height.
-
std::tuple<int, int>
getVideoSize
() const¶ Get video size as tuple.
-
int
getVideoWidth
() const¶ Get video width.
-
int
getVideoHeight
() const¶ Get video height.
-
std::tuple<int, int>
getStillSize
() const¶ Get still size as tuple.
-
int
getStillWidth
() const¶ Get still width.
-
int
getStillHeight
() const¶ Get still height.
-
std::tuple<int, int>
getSize
() const¶ Get sensor resolution as size.
-
int
getWidth
() const¶ Get sensor resolution width.
-
int
getHeight
() const¶ Get sensor resolution height.
-
void
setMeshSource
(Properties::WarpMeshSource source)¶ Set the source of the warp mesh or disable.
-
Properties::WarpMeshSource
getMeshSource
() const¶ Gets the source of the warp mesh.
-
void
loadMeshFile
(const dai::Path &warpMesh)¶ Specify local filesystem paths to the undistort mesh calibration files.
When a mesh calibration is set, it overrides the camera intrinsics/extrinsics matrices. Overrides useHomographyRectification behavior. Mesh format: a sequence of (y,x) points as ‘float’ with coordinates from the input image to be mapped in the output. The mesh can be subsampled, configured by
setMeshStep
.With a 1280x800 resolution and the default (16,16) step, the required mesh size is:
width: 1280 / 16 + 1 = 81
height: 800 / 16 + 1 = 51
-
void
loadMeshData
(span<const std::uint8_t> warpMesh)¶ Specify mesh calibration data for undistortion See
loadMeshFiles
for the expected data format
-
void
setMeshStep
(int width, int height)¶ Set the distance between mesh points. Default: (32, 32)
-
std::tuple<int, int>
getMeshStep
() const¶ Gets the distance between mesh points.
-
void
setCalibrationAlpha
(float alpha)¶ Set calibration alpha parameter that determines FOV of undistorted frames.
-
tl::optional<float>
getCalibrationAlpha
() const¶ Get calibration alpha parameter that determines FOV of undistorted frames.
-
void
setRawOutputPacked
(bool packed)¶ Configures whether the camera
raw
frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false
), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
Public Members
-
CameraControl
initialControl
¶ Initial control options to apply to sensor
-
Input
inputConfig
= {*this, "inputConfig", Input::Type::SReceiver, false, 8, {{DatatypeEnum::ImageManipConfig, false}}}¶ Input for ImageManipConfig message, which can modify crop parameters in runtime
Default queue is non-blocking with size 8
-
Input
inputControl
= {*this, "inputControl", Input::Type::SReceiver, true, 8, {{DatatypeEnum::CameraControl, false}}}¶ Input for CameraControl message, which can modify camera parameters in runtime
Default queue is blocking with size 8
-
Output
video
= {*this, "video", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
Suitable for use with VideoEncoder node
-
Output
preview
= {*this, "preview", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries BGR/RGB planar/interleaved encoded frame data.
Suitable for use with NeuralNetwork node
-
Output
still
= {*this, "still", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
The message is sent only when a CameraControl message arrives to inputControl with captureStill command set.
-
Output
isp
= {*this, "isp", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries YUV420 planar (I420/IYUV) frame data.
Generated by the ISP engine, and the source for the ‘video’, ‘preview’ and ‘still’ outputs
-
Output
raw
= {*this, "raw", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor, and the source for the ‘isp’ output.
-
Output
frameEvent
= {*this, "frameEvent", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
Public Static Functions
-
int
getScaledSize
(int input, int num, int denom)¶ Computes the scaled size given numerator and denominator
Public Static Attributes
-
static constexpr const char *
NAME
= "Camera"¶
Private Members
-
std::shared_ptr<RawCameraControl>
rawControl
¶