UVC¶
The DepthAI UVC (USB Video Class) node allows OAK devices to function as standard webcams. This feature is particularly useful for integrating OAK devices into applications that require video input, such as video conferencing tools or custom video processing applications.
What is UVC?¶
UVC refers to the USB Video Class standard, which is a USB device class that describes devices capable of streaming video. This standard allows video devices to interface with computers and other devices without needing specific drivers, making them immediately compatible with a wide range of systems and software.
How Does the UVC Node Work?¶
The UVC node in DepthAI leverages this standard to stream video from OAK devices. When the UVC node is enabled, the OAK device is recognized as a standard webcam by the host system. This allows the device to be used in any application that supports webcam input, such as Zoom, Skype, or custom video processing software.
The UVC node streams video data over a USB connection. It is important to use a USB3 cable for this purpose, as USB2 may not provide the necessary bandwidth for stable video streaming.
Note
The UVC node can currently handle NV12 video streams from OAK devices. For streams in other formats, conversion to NV12 is necessary, which can be achieved using the ImageManip node. It’s important to note that streams incompatible with NV12 conversion, like depth streams, are not supported by the UVC node.
Examples of UVC Node Usage¶
DepthAI Demo Script: The DepthAI demo script includes a UVC application that can be run to enable the UVC node on an OAK device.
python3 depthai_demo.py --app uvc
Custom Python Script: A custom Python script can be written to enable the UVC node and configure the video stream parameters. Here are some pre-written examples:
OBS Forwarding: For applications where direct UVC node usage is not possible, OBS Studio can be used to forward the UVC stream.
Reference¶
-
class
depthai.node.
UVC
UVC (USB Video Class) node
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.UVCProperties
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
property
id
Id of node
-
property
input
Input for image frames to be streamed over UVC
Default queue is blocking with size 8
-
setGpiosOnInit
(self: depthai.node.UVC, list: Dict[int, int]) → None Set GPIO list <gpio_number, value> for GPIOs to set (on/off) at init
-
setGpiosOnStreamOff
(self: depthai.node.UVC, list: Dict[int, int]) → None Set GPIO list <gpio_number, value> for GPIOs to set when streaming is disabled
-
setGpiosOnStreamOn
(self: depthai.node.UVC, list: Dict[int, int]) → None Set GPIO list <gpio_number, value> for GPIOs to set when streaming is enabled
-
class
-
class
dai::node
::
UVC
: public dai::NodeCRTP<Node, UVC, UVCProperties>¶ UVC (USB Video Class) node.
Public Functions
-
void
setGpiosOnInit
(std::unordered_map<int, int> list)¶ Set GPIO list <gpio_number, value> for GPIOs to set (on/off) at init.
-
void
setGpiosOnStreamOn
(std::unordered_map<int, int> list)¶ Set GPIO list <gpio_number, value> for GPIOs to set when streaming is enabled.
-
void
setGpiosOnStreamOff
(std::unordered_map<int, int> list)¶ Set GPIO list <gpio_number, value> for GPIOs to set when streaming is disabled.
Public Members
-
Input
input
= {*this, "in", Input::Type::SReceiver, true, 8, true, {{DatatypeEnum::Buffer, true}}}¶ Input for image frames to be streamed over UVC
Default queue is blocking with size 8
Public Static Attributes
-
static constexpr const char *
NAME
= "UVC"¶
-
void