# ObjectTrackerConfig

`ObjectTrackerConfig` stores the parameters that drive the
[`ObjectTracker`](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/object_tracker.md) node. It lets you
configure tracker types (zero-term / short-term), association thresholds, maximum number of simultaneously tracked objects, and
ROI re-acquisition behavior when detections are temporarily lost.

Set `ObjectTracker.initialConfig` to establish defaults and send live updates through `inputTrackerConfig` when you need to adapt
the pipeline—for example, to increase the IOU threshold in crowded scenes or to switch from median-flow to kernelized correlation
tracking. The node will apply the new configuration without requiring a pipeline rebuild.

## Reference

### dai::ObjectTrackerConfig

Kind: class

ObjectTrackerConfig message. Carries ROI (region of interest) and threshold for depth calculation

#### std::vector< int32_t > trackletIdsToRemove

Kind: variable

Tracklet IDs to remove from tracking. Tracklet will transition to REMOVED state.

#### ObjectTrackerConfig()

Kind: function

Construct ObjectTrackerConfig message.

#### ~ObjectTrackerConfig()

Kind: function

#### ObjectTrackerConfig & forceRemoveID(int32_t id)

Kind: function

Force remove a tracklet with specified ID.

#### ObjectTrackerConfig & forceRemoveIDs(std::vector< int32_t > ids)

Kind: function

Force remove tracklets with specified IDs.

#### void serialize(std::vector< std::uint8_t > & metadata, DatatypeEnum & datatype)

Kind: function

#### DatatypeEnum getDatatype()

Kind: function

Get the datatype of this specific message.

return: DatatypeEnum

#### DEPTHAI_SERIALIZE(ObjectTrackerConfig, Buffer::sequenceNum, Buffer::ts, Buffer::tsDevice, Buffer::tsSystem, trackletIdsToRemove)

Kind: function

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.