Sample - Bare minimum code to access DepthAI camera

Demo

Source code

import cv2
import depthai

device = depthai.Device('', False)

p = device.create_pipeline(config={
    "streams": ["metaout", "previewout"],
    "ai": {
        "blob_file": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.blob",
        "blob_file_config": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.json"
    }
})

if p is None:
    raise RuntimeError("Error initializing pipelne")

entries_prev = []

while True:
    nnet_packets, data_packets = p.get_available_nnet_and_data_packets()

    for nnet_packet in nnet_packets:
        entries_prev = []
        for e in nnet_packet.entries():
            if e[0]['id'] == -1.0 or e[0]['confidence'] == 0.0:
                break
            if e[0]['confidence'] > 0.5:
                entries_prev.append(e[0])

    for packet in data_packets:
        if packet.stream_name == 'previewout':
            data = packet.getData()
            data0 = data[0, :, :]
            data1 = data[1, :, :]
            data2 = data[2, :, :]
            frame = cv2.merge([data0, data1, data2])

            img_h = frame.shape[0]
            img_w = frame.shape[1]

            for e in entries_prev:
                pt1 = int(e['left'] * img_w), int(e['top'] * img_h)
                pt2 = int(e['right'] * img_w), int(e['bottom'] * img_h)

                cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

            cv2.imshow('previewout', frame)

    if cv2.waitKey(1) == ord('q'):
        break

del p
del device

Explanation

The code is divided into three phases: initialization, processing results and deinitialization.

Initialization is done here, as it’s initializing the device and making sure that the pipeline is created

device = depthai.Device('', False)

p = device.create_pipeline(config={
    "streams": ["metaout", "previewout"],
    "ai": {
        "blob_file": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.blob",
        "blob_file_config": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.json"
    }
})

if p is None:
    raise RuntimeError("Error initializing pipelne")

Deinitialization is basically only two lines of code, and whereas it’s not necessary to include it, it’s definitely recommended

del p
del device

Now, the results processing consists of two phases - parsing nnet results and displaying the frames.

Parsing neural network results

Below, you’ll se the part that’s parsing the results from neural network

entries_prev = []

while True:
    nnet_packets, data_packets = p.get_available_nnet_and_data_packets()

    for nnet_packet in nnet_packets:
        entries_prev = []
        for e in nnet_packet.entries():
            if e[0]['id'] == -1.0 or e[0]['confidence'] == 0.0:
                break
            if e[0]['confidence'] > 0.5:
                entries_prev.append(e[0])

Here, we’re using a little trick. Notice, that entries_prev is populated with only the correct entries, and is reset (set to []) only when we receive a new nnet packet, because it’s a first instruction in the for loop of nnet_packets.

This way, if there are no new results from neural network, we keep the old ones and therefore the bounding boxes don’t flick.

Also, having this approach, we’re sure that only one output of the neural network is displayed (if nnet_packets would contain two of them).

Conditions e[0]['id'] == -1.0 or e[0]['confidence'] == 0.0 eleminate the background noise that can be produced

Condition e[0]['confidence'] > 0.5 is our confidence threshold. You can modify 0.5 according to your needs and use case.

The result of this processing step is populated (or empty) array entries_prev

Displaying the frames

for packet in data_packets:
    if packet.stream_name == 'previewout':
        data = packet.getData()
        data0 = data[0, :, :]
        data1 = data[1, :, :]
        data2 = data[2, :, :]
        frame = cv2.merge([data0, data1, data2])

        img_h = frame.shape[0]
        img_w = frame.shape[1]

        for e in entries_prev:
            pt1 = int(e['left'] * img_w), int(e['top'] * img_h)
            pt2 = int(e['right'] * img_w), int(e['bottom'] * img_h)

            cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

        cv2.imshow('previewout', frame)

if cv2.waitKey(1) == ord('q'):
    break

This stage is also divided into three phases - preparing the frame, augumenting the frame and adding control signals

Preparing the frame basically means that we’re transforming the frame to OpenCV-usable form.

First, we need to assure we’re operating on packet from previewout stream, so it’s a frame from 4K color camera.

Next, we get the data from the packet and transform it from CHW (Channel, Height, Width) form used by DepthAI to HWC (Height, Width, Channel) that is used by OpenCV.

for packet in data_packets:
    if packet.stream_name == 'previewout':
        data = packet.getData()  # e.x. shape (3, 300, 300)
        data0 = data[0, :, :]
        data1 = data[1, :, :]
        data2 = data[2, :, :]
        frame = cv2.merge([data0, data1, data2])  # e.x. shape (300, 300, 3)

Augumenting the frame means any process that changes what is being displayed. In this example, I’m adding red rectangles around detected items. You can also add here text displays, latency info - basically whatever your business logic requires.

Since the position of the bounding boxes are returned from neural network as floats in range (0, 1), which specify position of the point relative to it’s width/height, we need to transform it into the actual point on the image (which you can see as we’re doing e.x. int(e['left'] * img_w)).

Next, using cv2.rectangle, we’re printing the actual rectangle on the frame. Finally, when the frame is ready, we display it using cv2.imshow function.

img_h = frame.shape[0]
img_w = frame.shape[1]

for e in entries_prev:
    pt1 = int(e['left'] * img_w), int(e['top'] * img_h)
    pt2 = int(e['right'] * img_w), int(e['bottom'] * img_h)

    cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

cv2.imshow('previewout', frame)

Adding control signals is the last part, where you can add interactivity to the displayed image. We’re adding just one command - to terminate the program - when you press the q button.

if cv2.waitKey(1) == ord('q'):
    break

Do you have any questions/suggestions? Feel free to get in touch and let us know!