Installation¶
Note
Refer to DepthAI installer documentation to install full DepthAI demo and its dependencies and requirements.
Follow the steps below to just install depthai api library dependencies for your platform.
Execute the script below to install macOS dependencies:
curl -fL https://docs.luxonis.com/install_dependencies.sh | bash
Please refer to documentation below if any issues occur.
Windows 10/11 users can either install DepthAI dependencies via Windows Installer, or follow instructions below.
Execute the script below to install Linux dependencies:
sudo wget -qO- https://docs.luxonis.com/install_dependencies.sh | bash
Please refer to Supported Platforms if any issues occur.
Once installed, you can install the DepthAI library from PyPI.
Supported Platforms¶
See documentation below for other platforms or additional information.
Platform |
Instructions |
---|---|
Windows 10/11 |
|
macOS |
|
Ubuntu |
|
Raspberry Pi OS |
|
Jetson Nano/Xavier |
|
ROS |
Follow tutorial at depthai-ros |
Windows 7 |
|
Docker |
|
Kernel Virtual Machine |
|
VMware |
|
Virtual Box |
|
WSL2 |
If you do not see a particular platform or package format listed below please reach out to us on Discord or on Github.
macOS¶
bash -c "$(curl -fL https://docs.luxonis.com/install_depthai.sh)"
Close and re-open the terminal window after this command.
The script also works on M1 Macs, Homebrew being installed under Rosetta 2, as some Python packages are still missing native M1 support. In case you already have Homebrew installed natively and things don’t work, see here for some additional troubleshooting steps.
Note that if the video streaming window does not appear consider running the following:
python3 -m pip install opencv-python --force-reinstall --no-cache-dir
See the Video preview window fails to appear on macOS thread on our forum for more information.
We provide Mac M1 prebuilt Python wheels for depthai since the version 2.17.3.1
.
Ubuntu¶
sudo wget -qO- https://docs.luxonis.com/install_dependencies.sh | bash
Note! If opencv fails with illegal instruction after installing from PyPi, add:
echo "export OPENBLAS_CORETYPE=ARMV8" >> ~/.bashrc
source ~/.bashrc
Raspberry Pi OS¶
sudo curl -fL https://docs.luxonis.com/install_dependencies.sh | bash
We have also prepared pre-configured RPi images so you can get up & running faster.
Jetson¶
To install DepthAI on Jetson Nano or Jetson Xavier, perform the following steps, after completing a fresh install and setup. On the first log in, do not immediately run updates.
This first step is optional: go to the Software (App Store) and delete the apps or software that you probably will not use.
Open a terminal window and run the following commands:
sudo apt update && sudo apt upgrade sudo reboot now
Change the size of your SWAP. These instructions come from the Getting Started with AI on Jetson from Nvidia:
# Disable ZRAM: sudo systemctl disable nvzramconfig # Create 4GB swap file sudo fallocate -l 4G /mnt/4GB.swap sudo chmod 600 /mnt/4GB.swap sudo mkswap /mnt/4GB.swap
If you have an issue with the final command, you can try the following:
sudo vi /etc/fstab # Add this line at the bottom of the file /mnt/4GB.swap swap swap defaults 0 0 # Reboot sudo reboot now
The next step is to install pip
and python3
:
sudo -H apt install -y python3-pip
After that, install and set up virtual environment:
sudo -H pip3 install virtualenv virtualenvwrapper
Add following lines to the bash script:
sudo vi ~/.bashrc # Virtual Env Wrapper Configuration export WORKON_HOME=$HOME/.virtualenvs export VIRTUALENVWRAPPER_PYTHON=/usr/bin/python3 source /usr/local/bin/virtualenvwrapper.sh
Save and reload the script by running the command source ~/.bashrc
. Then create a virtual environment (in this example it’s called depthAI
).
mkvirtualenv depthAI -p python3
Note! Before installing depthai
, make sure you’re in the virtual environment.
#Download and install the dependency package sudo wget -qO- https://docs.luxonis.com/install_dependencies.sh | bash #Clone github repository git clone https://github.com/luxonis/depthai-python.git cd depthai-python
Last step is to edit .bashrc
with the line:
echo "export OPENBLAS_CORETYPE=ARMV8" >> ~/.bashrc
Navigate to the folder with depthai
examples folder, run python install_requirements.py
and then run python rgb_preview.py
.
openSUSE¶
For openSUSE, available in this official article how to install the OAK device on the openSUSE platform.
Windows 10¶
For Windows 10/11, we recommend using the Chocolatey package manager to install DepthAI’s dependencies on Windows. Chocolatey is very similar to Homebrew for macOS.
To install Chocolatey and use it to install DepthAI’s dependencies do the following:
Right click on Start
Choose Windows PowerShell (Admin) and run the following:
Set-ExecutionPolicy Bypass -Scope Process -Force; [System.Net.ServicePointManager]::SecurityProtocol = [System.Net.ServicePointManager]::SecurityProtocol -bor 3072; iex ((New-Object System.Net.WebClient).DownloadString('https://chocolatey.org/install.ps1'))
Close the PowerShell and then re-open another PowerShell (Admin) by repeating the first two steps.
Install Python and PyCharm
choco install cmake git python pycharm-community -y
Windows 7¶
Although we do not officially support Windows 7, members of the community have
had success manually installing WinUSB using Zadig. After connecting your DepthAI device look for a
device with USB ID: 03E7 2485
and install the WinUSB driver by
selecting WinUSB(v6.1.7600.16385) and then Install WCID Driver.
WSL 2¶
Steps below were performed on WSL 2 running Ubuntu 20.04, while host machine was running Win10 20H2 (OS build 19042.1586). Original tutorial written here by SputTheBot.
To get an OAK running on WSL 2, you first need to attach USB device to WSL 2. We have used usbipd-win (2.3.0) for that. Inside WSL 2 you also need to install depthai dependencies and USB/IP client tool (2 commands).
To attach the OAK camera to WSL 2, we have prepared a Python script below that you need to execute on the host computer (in Admin mode).
import time
import os
while True:
output = os.popen('usbipd wsl list').read() # List all USB devices
rows = output.split('\n')
for row in rows:
if ('Movidius MyriadX' in row or 'Luxonis Device' in row) and 'Not attached' in row: # Check for OAK cameras that aren't attached
busid = row.split(' ')[0]
out = os.popen(f'usbipd wsl attach --busid {busid}').read() # Attach an OAK camera
print(out)
print(f'Usbipd attached Myriad X on bus {busid}') # Log
time.sleep(.5)
After that, you can check lsusb
command inside the WLS 2 and you should be able to see Movidius MyriadX
.
Note
Examples that don’t show any frames (eg. IMU example) should work. We haven’t spent enough time to get OpenCV display frames inside WSL 2, but you could try it out yourself, some ideas here.
Docker¶
We maintain a Docker image containing DepthAI, it’s dependencies and helpful tools in the luxonis/depthai-library repository on Docker Hub. It builds upon the luxonis/depthai-base image.
Run the rgb_preview.py
example inside a Docker container on a Linux host
(with the X11 windowing system):
docker pull luxonis/depthai-library
docker run --rm \
--privileged \
-v /dev/bus/usb:/dev/bus/usb \
--device-cgroup-rule='c 189:* rmw' \
-e DISPLAY=$DISPLAY \
-v /tmp/.X11-unix:/tmp/.X11-unix \
luxonis/depthai-library:latest \
python3 /depthai-python/examples/ColorCamera/rgb_preview.py
To allow the container to update X11 you may need to run xhost local:root
on the host.
Note: If you are using OAK POE device on Linux host machine, you should add --network=host
argument to your docker command, so depthai inside docker will be able to communicate with the OAK POE.
Kernel Virtual Machine¶
To access the OAK-D camera in the Kernel Virtual Machine, there is a need to attach and detach USB devices on the fly when the host machine detects changes in the USB bus.
OAK-D camera changes the USB device type when it is used by DepthAI API. This happens in background when the camera is used natively. But when the camera is used in a virtual environment the situation is different.
On your host machine, use the following code:
SUBSYSTEM=="usb", ACTION=="bind", ENV{ID_VENDOR_ID}=="03e7", MODE="0666", RUN+="/usr/local/bin/movidius_usb_hotplug.sh depthai-vm"
SUBSYSTEM=="usb", ACTION=="remove", ENV{PRODUCT}=="3e7/2485/1", ENV{DEVTYPE}=="usb_device", MODE="0666", RUN+="/usr/local/bin/movidius_usb_hotplug.sh depthai-vm"
SUBSYSTEM=="usb", ACTION=="remove", ENV{PRODUCT}=="3e7/f63b/100", ENV{DEVTYPE}=="usb_device", MODE="0666", RUN+="/usr/local/bin/movidius_usb_hotplug.sh depthai-vm"
The script that the udev rule is calling (movidius_usb_hotplug.sh) should then attach/detach the USB device to the virtual machine.
In this case we need to call virsh
command. For example, the script could do the following:
#!/bin/bash
# Abort script execution on errors
set -e
if [ "${ACTION}" == 'bind' ]; then
COMMAND='attach-device'
elif [ "${ACTION}" == 'remove' ]; then
COMMAND='detach-device'
if [ "${PRODUCT}" == '3e7/2485/1' ]; then
ID_VENDOR_ID=03e7
ID_MODEL_ID=2485
fi
if [ "${PRODUCT}" == '3e7/f63b/100' ]; then
ID_VENDOR_ID=03e7
ID_MODEL_ID=f63b
fi
else
echo "Invalid udev ACTION: ${ACTION}" >&2
exit 1
fi
echo "Running virsh ${COMMAND} ${DOMAIN} for ${ID_VENDOR}." >&2
virsh "${COMMAND}" "${DOMAIN}" /dev/stdin <<END
<hostdev mode='subsystem' type='usb'>
<source>
<vendor id='0x${ID_VENDOR_ID}'/>
<product id='0x${ID_MODEL_ID}'/>
</source>
</hostdev>
END
exit 0
Note that when the device is disconnected from the USB bus, some udev environmental variables are not available (ID_VENDOR_ID
or ID_MODEL_ID
),
that is why you need to use PRODUCT
environmental variable to identify which device has been disconnected.
The virtual machine where DepthAI API application is running should have defined a udev rules that identify the OAK-D camera. The udev rule is described here
Solution provided by Manuel Segarra-Abad
VMware¶
Using the OAK-D device in a VMware requires some extra one-time settings that need to be set up for it to work.
First of all, make sure the USB controller is switched from USB2 to USB3. Go to Virtual Machine Settings -> USB Controller -> USB compatibility
and change
to USB 3.1 (or USB 3.0 for older VMware versions, as available).
Depending on what state the device is, there could be two devices showing up, and both need to be routed to the VM.
Those could be visible at Player -> Removable Devices
:
Intel Movidius MyriadX
Intel VSC Loopback Device or Intel Luxonis Device
In Linux OS, run these commands to give USB permissions for the regular user:
echo 'SUBSYSTEM=="usb", ATTRS{idVendor}=="03e7", MODE="0666"' | sudo tee /etc/udev/rules.d/80-movidius.rules
sudo udevadm control --reload-rules && sudo udevadm trigger
If Virtual Machine doesn’t detect the device, try the following: find and select option like Forget connection rule (for both devices), then try running the DepthAI example again inside the VM. Choose to route to VM and select to not ask again (this is important, as there is a timeout, and the device watchdog could get triggered if the host doesn’t start communication in few seconds). You may need to repeat running the script a few times, until all gets set properly for VMware.
Virtual Box¶
If you want to use VirtualBox to run the DepthAI source code, please make sure that you allow the VM to access the USB devices. Also, be aware that by default, it supports only USB 1.1 devices, and DepthAI operates in two stages:
For showing up when plugged in. We use this endpoint to load the firmware onto the device, which is a usb-boot technique. This device is USB2.
For running the actual code. This shows up after USB booting and is USB3.
In order to support the DepthAI modes, you need to download and install Oracle VM VirtualBox Extension Pack. Once this is installed, enable USB3 (xHCI) Controller in the USB settings.
Once this is done, you’ll need to route the Myriad as USB device from Host to the VBox. This is the filter for depthai before it has booted, which is at that point a USB2 device:
The last step is to add the USB Intel Loopback device. The depthai device boots its firmware over USB, and after it has booted, it shows up as a new device.
This device shows just up when the depthai/OAK is trying to reconnect (during runntime, so right after running a pipeline on depthai, such as :bash: python3 depthai_demo.py).
It might take a few tries to get this loopback device shown up and added, as you need to do this while depthai is trying to connect after a pipeline has been built (and so it has at that point now booted its internal firmware over USB2).
For enabling it only once, you can see the loopback device here (after the pipeline has been started):
And then for permanently enabling this pass-through to virtual box, enable this in setting below:
And then for each additional depthai/OAK device you would like to pass through, repeat just this last loopback settings step for each unit (as each unit will have its own unique ID).
Install from PyPI¶
After installing depthai dependencies, you can either refer to depthai-core for C++ development, or download the depthai Python library via PyPi:
python3 -m pip install depthai
For other installation options, see other installation options.
Test installation¶
We have a set of examples that should help you verify if your setup was correct.
First, clone the depthai-python repository and change directory into this repo:
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python
Next install the requirements for this repository. Note that we recommend installing the dependencies in a virtual environment, so that they don’t interfere with other Python tools/environments on your system.
For development machines like Mac/Windows/Ubuntu/etc., we recommend the PyCharm IDE, as it automatically makes/manages virtual environments for you, along with a bunch of other benefits. Alternatively,
conda
,pipenv
, orvirtualenv
could be used directly (and/or with your preferred IDE).For installations on resource-constrained systems, such as the Raspberry Pi or other small Linux systems, we recommend
conda
,pipenv
, orvirtualenv
. To set up a virtual environment withvirtualenv
, runvirtualenv venv && source venv/bin/activate
.
Using a virtual environment (or system-wide, if you prefer), run the following to install the requirements for this example repository:
cd examples
python3 install_requirements.py
Now, run the rgb_preview.py
script from within examples
directory to make sure everything is working:
python3 ColorCamera/rgb_preview.py
If all goes well a small window video display should appear. And example is shown below:
Run Other Examples¶
After you have run this example, you can run other examples to learn about DepthAI possibilities. You can also proceed to:
Our tutorials, starting with a Hello World tutorial explaining the API usage step by step (here)
Our experiments, containing implementations of various user use cases on DepthAI (here)
You can also proceed below to learn how to convert your own neural network to run on DepthAI.
And we also have online model training below, which shows you how to train and convert models for DepthAI:
Online ML Training and model Conversion: HERE
Other installation methods¶
To get the latest and yet unreleased features from our source code, you can go ahead and compile depthai package manually.
Dependencies to build from source
CMake > 3.2.0
Generation tool (Ninja, make, …)
C/C++ compiler
libusb1 development package
On Debian based systems (Raspberry Pi OS, Ubuntu, …) these can be acquired by running:
sudo apt-get -y install cmake libusb-1.0-0-dev build-essential
Assuming a stock Mac OS X install, depthai-python library needs following dependencies
Homebrew (If it’s not installed already)
/bin/bash -c "$(curl -fsSL https://raw.githubusercontent.com/Homebrew/install/master/install.sh)"
Python,
libusb
, CMake,wget
brew install coreutils python3 cmake libusb wget
And now you’re ready to clone the depthai-python from Github and build it for Mac OS X.
Pip allows users to install the packages from specific commits, even if they are not yet released on PyPi.
To do so, use the command below - and be sure to replace the <commit_sha>
with the correct commit hash from here
python3 -m pip install git+https://github.com/luxonis/depthai-python.git@<commit_sha>
From time to time, it may be of interest to use a specific branch. This may occur, for example,
because we have listened to your feature request and implemented a quick implementation in a branch.
Or it could be to get early access to a feature that is soaking in our develop
for stability purposes before being merged into main
(develop
is the branch we use to soak new features before merging them into main
):
So when working in the depthai-python repository, using a branch can be accomplished with the following commands.
Prior to running the following, you can either clone the repository independently
(for not over-writing any of your local changes) or simply do a git pull
first.
git checkout <branch>
git submodule update --init --recursive
python3 setup.py develop
If desired, you can also install the package from the source code itself - it will allow you to make the changes to the API and see them live in action.
To do so, first download the repository and then add the package to your python interpreter in development mode
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python
git submodule update --init --recursive
python3 setup.py develop # you may need to add sudo if using system interpreter instead of virtual environment
If you want to use other branch (e.g. develop
) than default (main
), you can do so by typing
git checkout develop # replace the "develop" with a desired branch name
git submodule update --recursive
python3 setup.py develop
Or, if you want to checkout a specific commit, type
git checkout <commit_sha>
git submodule update --recursive
python3 setup.py develop