YoloDetectionNetwork¶
Yolo detection network node is very similar to NeuralNetwork (in fact it extends it). The only difference is that this node
is specifically for the (tiny) Yolo V3/V4 NN and it decodes the result of the NN on device. This means that Out
of this node is not a
NNData (a byte array) but a ImgDetections that can easily be used in your code.
How to place it¶
pipeline = dai.Pipeline()
yoloDet = pipeline.create(dai.node.YoloDetectionNetwork)
dai::Pipeline pipeline;
auto yoloDet = pipeline.create<dai::node::YoloDetectionNetwork>();
Inputs and Outputs¶
┌───────────────────┐
│ │ out
│ ├───────────►
│ Yolo │
│ Detection │
input │ Network │ passthrough
───────────►│-------------------├───────────►
│ │
└───────────────────┘
Message types
input
- ImgFrameout
- ImgDetectionspassthrough
- ImgFrame
Usage¶
pipeline = dai.Pipeline()
yoloDet = pipeline.create(dai.node.YoloDetectionNetwork)
yoloDet.setBlobPath(nnBlobPath)
# Yolo specific parameters
yoloDet.setConfidenceThreshold(0.5)
yoloDet.setNumClasses(80)
yoloDet.setCoordinateSize(4)
yoloDet.setAnchors([10,14, 23,27, 37,58, 81,82, 135,169, 344,319])
yoloDet.setAnchorMasks({"side26": [1, 2, 3], "side13": [3, 4, 5]})
yoloDet.setIouThreshold(0.5)
dai::Pipeline pipeline;
auto yoloDet = pipeline.create<dai::node::YoloDetectionNetwork>();
yoloDet->setBlobPath(nnBlobPath);
// yolo specific parameters
yoloDet->setConfidenceThreshold(0.5f);
yoloDet->setNumClasses(80);
yoloDet->setCoordinateSize(4);
yoloDet->setAnchors({10, 14, 23, 27, 37, 58, 81, 82, 135, 169, 344, 319});
yoloDet->setAnchorMasks({{"side13", {3, 4, 5}}, {"side26", {1, 2, 3}}});
yoloDet->setIouThreshold(0.5f);
Examples of functionality¶
Reference¶
-
class
depthai.node.
YoloDetectionNetwork
YoloDetectionNetwork node. Parses Yolo results
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.DetectionNetworkProperties
-
getAnchorMasks
(self: depthai.node.YoloDetectionNetwork) → Dict[str, List[int]] Get anchor masks
-
getAnchors
(self: depthai.node.YoloDetectionNetwork) → List[float] Get anchors
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getConfidenceThreshold
(self: depthai.node.DetectionNetwork) → float Retrieves threshold at which to filter the rest of the detections.
- Returns
Detection confidence
-
getCoordinateSize
(self: depthai.node.YoloDetectionNetwork) → int Get coordianate size
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getIouThreshold
(self: depthai.node.YoloDetectionNetwork) → float Get Iou threshold
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getNumClasses
(self: depthai.node.YoloDetectionNetwork) → int Get num classes
-
getNumInferenceThreads
(self: depthai.node.NeuralNetwork) → int How many inference threads will be used to run the network
- Returns
Number of threads, 0, 1 or 2. Zero means AUTO
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
property
id
Id of node
-
property
input
Input message with data to be inferred upon Default queue is blocking with size 5
-
property
inputs
Inputs mapped to network inputs. Useful for inferring from separate data sources Default input is non-blocking with queue size 1 and waits for messages
-
property
out
Outputs ImgDetections message that carries parsed detection results. Overrides NeuralNetwork ‘out’ with ImgDetections output message type.
-
property
passthrough
Passthrough message on which the inference was performed.
Suitable for when input queue is set to non-blocking behavior.
-
property
passthroughs
Passthroughs which correspond to specified input
-
setAnchorMasks
(self: depthai.node.YoloDetectionNetwork, anchorMasks: Dict[str, List[int]]) → None Set anchor masks
-
setAnchors
(self: depthai.node.YoloDetectionNetwork, anchors: List[float]) → None Set anchors
-
setBlobPath
(self: depthai.node.NeuralNetwork, path: object) → None Load network blob into assets and use once pipeline is started.
- Throws:
Error if file doesn’t exist or isn’t a valid network blob.
- Parameter
path
: Path to network blob
-
setConfidenceThreshold
(self: depthai.node.DetectionNetwork, thresh: float) → None Specifies confidence threshold at which to filter the rest of the detections.
- Parameter
thresh
: Detection confidence must be greater than specified threshold to be added to the list
- Parameter
-
setCoordinateSize
(self: depthai.node.YoloDetectionNetwork, coordinates: int) → None Set coordianate size
-
setIouThreshold
(self: depthai.node.YoloDetectionNetwork, thresh: float) → None Set Iou threshold
-
setNumClasses
(self: depthai.node.YoloDetectionNetwork, numClasses: int) → None Set num classes
-
setNumInferenceThreads
(self: depthai.node.NeuralNetwork, numThreads: int) → None How many threads should the node use to run the network.
- Parameter
numThreads
: Number of threads to dedicate to this node
- Parameter
-
setNumNCEPerInferenceThread
(self: depthai.node.NeuralNetwork, numNCEPerThread: int) → None How many Neural Compute Engines should a single thread use for inference
- Parameter
numNCEPerThread
: Number of NCE per thread
- Parameter
-
setNumPoolFrames
(self: depthai.node.NeuralNetwork, numFrames: int) → None Specifies how many frames will be available in the pool
- Parameter
numFrames
: How many frames will pool have
- Parameter
-
class
-
class
dai::node
::
YoloDetectionNetwork
: public dai::NodeCRTP<DetectionNetwork, YoloDetectionNetwork, DetectionNetworkProperties>¶ YoloDetectionNetwork node. Parses Yolo results.
Public Functions
-
void
setNumClasses
(int numClasses)¶ Set num classes.
-
void
setCoordinateSize
(int coordinates)¶ Set coordianate size.
-
void
setAnchors
(std::vector<float> anchors)¶ Set anchors.
-
void
setAnchorMasks
(std::map<std::string, std::vector<int>> anchorMasks)¶ Set anchor masks.
-
void
setIouThreshold
(float thresh)¶ Set Iou threshold.
-
int
getNumClasses
() const¶ Get num classes.
-
int
getCoordinateSize
() const¶ Get coordianate size.
-
std::vector<float>
getAnchors
() const¶ Get anchors.
-
std::map<std::string, std::vector<int>>
getAnchorMasks
() const¶ Get anchor masks.
-
float
getIouThreshold
() const¶ Get Iou threshold.
-
void
Got questions?
We’re always happy to help with code or other questions you might have.