Frame syncing on OAK¶
This example showcases how you can use Script node to perform Message syncing of multiple streams. Example uses ImgFrame’s timestamps to achieve syncing precision.
Similar syncing demo scripts (python) can be found at our depthai-experiments repository in gen2-syncing folder.
Demo¶
Terminal log after about 13 minutes. Color and disparity streams are perfectly in-sync.
[1662574807.8811488] Stream rgb, timestamp: 7:26:21.601595, sequence number: 21852 [1662574807.8821492] Stream disp, timestamp: 7:26:21.601401, sequence number: 21852
[1662574807.913144] Stream rgb, timestamp: 7:26:21.634982, sequence number: 21853 [1662574807.9141443] Stream disp, timestamp: 7:26:21.634730, sequence number: 21853
[1662574807.9451444] Stream rgb, timestamp: 7:26:21.668243, sequence number: 21854 [1662574807.946151] Stream disp, timestamp: 7:26:21.668057, sequence number: 21854
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
This example script requires external file(s) to run. If you are using:
depthai-python, run
python3 examples/install_requirements.py
to download required file(s)dephtai-core, required file(s) will get downloaded automatically when building the example
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 | import depthai as dai import time FPS = 30 pipeline = dai.Pipeline() # Define a source - color camera camRgb = pipeline.create(dai.node.ColorCamera) # Since we are saving RGB frames in Script node we need to make the # video pool size larger, otherwise the pipeline will freeze because # the ColorCamera won't be able to produce new video frames. camRgb.setVideoNumFramesPool(10) camRgb.setFps(FPS) left = pipeline.create(dai.node.MonoCamera) left.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) left.setBoardSocket(dai.CameraBoardSocket.LEFT) left.setFps(FPS) right = pipeline.create(dai.node.MonoCamera) right.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) right.setBoardSocket(dai.CameraBoardSocket.RIGHT) right.setFps(FPS) stereo = pipeline.createStereoDepth() stereo.initialConfig.setMedianFilter(dai.MedianFilter.KERNEL_7x7) stereo.setLeftRightCheck(True) stereo.setExtendedDisparity(False) stereo.setSubpixel(False) left.out.link(stereo.left) right.out.link(stereo.right) # Script node will sync high-res frames script = pipeline.create(dai.node.Script) # Send both streams to the Script node so we can sync them stereo.disparity.link(script.inputs["disp_in"]) camRgb.video.link(script.inputs["rgb_in"]) script.setScript(""" FPS=30 import time from datetime import timedelta import math # Timestamp threshold (in miliseconds) under which frames will be considered synced. # Lower number means frames will have less delay between them, which can potentially # lead to dropped frames. MS_THRESHOL=math.ceil(500 / FPS) def check_sync(queues, timestamp): matching_frames = [] for name, list in queues.items(): # Go through each available stream # node.warn(f"List {name}, len {str(len(list))}") for i, msg in enumerate(list): # Go through each frame of this stream time_diff = abs(msg.getTimestamp() - timestamp) if time_diff <= timedelta(milliseconds=MS_THRESHOL): # If time diff is below threshold, this frame is considered in-sync matching_frames.append(i) # Append the position of the synced frame, so we can later remove all older frames break if len(matching_frames) == len(queues): # We have all frames synced. Remove the excess ones i = 0 for name, list in queues.items(): queues[name] = queues[name][matching_frames[i]:] # Remove older (excess) frames i+=1 return True else: return False # We don't have synced frames yet names = ['disp', 'rgb'] frames = dict() # Dict where we store all received frames for name in names: frames[name] = [] while True: for name in names: f = node.io[name+"_in"].tryGet() if f is not None: frames[name].append(f) # Save received frame if check_sync(frames, f.getTimestamp()): # Check if we have any synced frames # Frames synced! node.info(f"Synced frame!") # node.warn(f"Queue size. Disp: {len(frames['disp'])}, rgb: {len(frames['rgb'])}") for name, list in frames.items(): syncedF = list.pop(0) # We have removed older (excess) frames, so at positions 0 in dict we have synced frames node.info(f"{name}, ts: {str(syncedF.getTimestamp())}, seq {str(syncedF.getSequenceNum())}") node.io[name+'_out'].send(syncedF) # Send synced frames to the host time.sleep(0.001) # Avoid lazy looping """) script_out = ['disp', 'rgb'] for name in script_out: # Create XLinkOut for disp/rgb streams xout = pipeline.create(dai.node.XLinkOut) xout.setStreamName(name) script.outputs[name+'_out'].link(xout.input) with dai.Device(pipeline) as device: device.setLogLevel(dai.LogLevel.INFO) device.setLogOutputLevel(dai.LogLevel.INFO) names = ['rgb', 'disp'] queues = [device.getOutputQueue(name) for name in names] while True: for q in queues: img: dai.ImgFrame = q.get() # Display timestamp/sequence number of two synced frames print(f"Time: {time.time()}. Stream {q.getName()}, timestamp: {img.getTimestamp()}, sequence number: {img.getSequenceNum()}") |
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 | #include <chrono> #include <iostream> // Includes common necessary includes for development using depthai library #include "depthai/depthai.hpp" static constexpr auto FPS = 30; int main() { dai::Pipeline pipeline; // Define a source - color camera auto camRgb = pipeline.create<dai::node::ColorCamera>(); // Since we are saving RGB frames in Script node we need to make the // video pool size larger, otherwise the pipeline will freeze because // the ColorCamera won't be able to produce new video frames. camRgb->setVideoNumFramesPool(10); camRgb->setFps(FPS); auto left = pipeline.create<dai::node::MonoCamera>(); left->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); left->setBoardSocket(dai::CameraBoardSocket::LEFT); left->setFps(FPS); auto right = pipeline.create<dai::node::MonoCamera>(); right->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); right->setBoardSocket(dai::CameraBoardSocket::RIGHT); right->setFps(FPS); auto stereo = pipeline.create<dai::node::StereoDepth>(); stereo->initialConfig.setMedianFilter(dai::MedianFilter::KERNEL_7x7); stereo->setLeftRightCheck(true); stereo->setExtendedDisparity(false); stereo->setSubpixel(false); stereo->setDepthAlign(dai::CameraBoardSocket::RGB); left->out.link(stereo->left); right->out.link(stereo->right); // Script node will sync high-res frames auto script = pipeline.create<dai::node::Script>(); // Send both streams to the Script node so we can sync them stereo->disparity.link(script->inputs["disp_in"]); camRgb->video.link(script->inputs["rgb_in"]); script->setScript(R"( FPS=30 import time from datetime import timedelta import math # Timestamp threshold (in miliseconds) under which frames will be considered synced. # Lower number means frames will have less delay between them, which can potentially # lead to dropped frames. MS_THRESHOL=math.ceil(500 / FPS) def check_sync(queues, timestamp): matching_frames = [] for name, list in queues.items(): # Go through each available stream # node.warn(f"List {name}, len {str(len(list))}") for i, msg in enumerate(list): # Go through each frame of this stream time_diff = abs(msg.getTimestamp() - timestamp) if time_diff <= timedelta(milliseconds=MS_THRESHOL): # If time diff is below threshold, this frame is considered in-sync matching_frames.append(i) # Append the position of the synced frame, so we can later remove all older frames break if len(matching_frames) == len(queues): # We have all frames synced. Remove the excess ones i = 0 for name, list in queues.items(): queues[name] = queues[name][matching_frames[i]:] # Remove older (excess) frames i+=1 return True else: return False # We don't have synced frames yet names = ['disp', 'rgb'] frames = dict() # Dict where we store all received frames for name in names: frames[name] = [] while True: for name in names: f = node.io[name+"_in"].tryGet() if f is not None: frames[name].append(f) # Save received frame if check_sync(frames, f.getTimestamp()): # Check if we have any synced frames # Frames synced! node.info(f"Synced frame!") for name, list in frames.items(): syncedF = list.pop(0) # We have removed older (excess) frames, so at positions 0 in dict we have synced frames node.info(f"{name}, ts: {str(syncedF.getTimestamp())}, seq {str(syncedF.getSequenceNum())}") node.io[name+'_out'].send(syncedF) # Send synced frames to the host time.sleep(0.001) # Avoid lazy looping )"); std::vector<std::string> scriptOut{"disp", "rgb"}; // Create XLinkOut for disp/rgb streams for(auto& name : scriptOut) { auto xout = pipeline.create<dai::node::XLinkOut>(); xout->setStreamName(name); script->outputs[name + "_out"].link(xout->input); } dai::Device device(pipeline); device.setLogOutputLevel(dai::LogLevel::INFO); device.setLogLevel(dai::LogLevel::INFO); std::vector<std::string> names{"rgb", "disp"}; std::map<std::string, std::shared_ptr<dai::DataOutputQueue>> streams; for(auto& name : names) { streams[name] = device.getOutputQueue(name); } while(true) { for(auto& iter : streams) { auto name = iter.first; auto queue = iter.second; auto img = queue->get<dai::ImgFrame>(); // Display timestamp/sequence number of two synced frames std::cout << "Stream " << name << ", timestamp: " << img->getTimestamp().time_since_epoch().count() << ", sequence number: " << img->getSequenceNum() << std::endl; } } } |
Got questions?
We’re always happy to help with code or other questions you might have.