- (Recommended) Online via HubAI
- Offline via ModelConverter - HubAI uses the same tool, but it's more user-friendly
Demo
Command Line
1Received NN data: (1, 9, 16, 85)
2Received NN data: (1, 9, 16, 85)
3Received NN data: (1, 9, 16, 85)
4Received NN data: (1, 9, 16, 85)
5Received NN data: (1, 9, 16, 85)
6Received NN data: (1, 9, 16, 85)- Batch size 1, as it runs inference on every (single) frame
- 9x16 grid, as YOLO divides the input image into a grid of size 9x16 cells
- 85 (prediction) values per grid, 4 for bounding box, 1 for confidence score, and 80 for class probabilities (as it was trained on 80-class dataset - COCO)
Deploying custom model
.dlc, you can deploy it to OAK4 by editing NeuralNetwork example with the following snippet:Python
1nn = pipeline.create(dai.node.NeuralNetwork)
2nn.setModelPath('my_model.dlc')
3nn.setBackend("snpe") # Specify SNPE NN backend. This usually gets set under the hood
4# Specify SNPE (RVC4) specific settings, like DSP runtime and NN performance profile
5nn.setBackendProperties({"runtime": "dsp", "performance_profile": "default"})archive.tar.xz, you can edit that example with this snippet:Python
1cam = pipeline.create(dai.node.Camera).build(socket)
2# If your nn model requires 640x640 input size (BGR):
3cam_out = cam.requestOutput((640, 640), dai.ImgFrame.Type.BGR888p)
4
5nn_archive = dai.NNArchive('./my_nn_archive.tar.xz')
6nn = pipeline.create(dai.node.NeuralNetwork).build(cam_out, nn_archive)Pipeline
Source code
Python
PythonGitHub
1#!/usr/bin/env python3
2import cv2
3import depthai as dai
4import numpy as np
5import time
6
7# Create pipeline
8with dai.Pipeline() as pipeline:
9 cameraNode = pipeline.create(dai.node.Camera).build()
10 # Longer form - useful in case of a local NNArchive
11 # modelDescription = dai.NNModelDescription("yolov6-nano", platform=pipeline.getDefaultDevice().getPlatformAsString())
12 # archive = dai.NNArchive(dai.getModelFromZoo(modelDescription))
13 # neuralNetwork = pipeline.create(dai.node.NeuralNetwork).build(cameraNode, archive)
14 neuralNetwork = pipeline.create(dai.node.NeuralNetwork).build(cameraNode, dai.NNModelDescription("yolov6-nano"))
15
16 qNNData = neuralNetwork.out.createOutputQueue()
17
18 pipeline.start()
19
20
21 while pipeline.isRunning():
22 inNNData: dai.NNData = qNNData.get()
23 tensor = inNNData.getFirstTensor()
24 assert(isinstance(tensor, np.ndarray))
25 print(f"Received NN data: {tensor.shape}")Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.