# DataDreamer®

![DataDreamer examples](https://raw.githubusercontent.com/luxonis/datadreamer/main/images/grid_image_3x2_generated_dataset.jpg)

## Quickstart

[DataDreamer](https://github.com/luxonis/datadreamer) enables you to create annotated datasets from scratch using Generative AI
and foundational Computer Vision models. This allows you to train your own models for edge AI applications, such as object
detection, without the need for real-world data.

To generate your dataset with custom classes, you need to execute only two commands:

```bash
pip install datadreamer
datadreamer --class_names person moon robot
```

 * Google Colab notebook with instructions on how to generate a dataset, train a model, and export it to for RVC2/RVC3:
   [DataDreamer
   Quickstart](https://colab.research.google.com/github/luxonis/datadreamer/blob/main/examples/generate_dataset_and_train_yolo.ipynb)
 * Helmet detection example: [Helmet detection](https://github.com/luxonis/datadreamer/blob/main/examples/helmet_detection.ipynb)
 * More info in the [DataDreamer GitHub repository](https://github.com/luxonis/datadreamer)

## Overview

![DataDreamer scheme](https://raw.githubusercontent.com/luxonis/datadreamer/main/images/datadreamer_scheme.gif)

`DataDreamer` is an advanced toolkit engineered to facilitate the development of edge AI models, irrespective of initial data
availability. Distinctive features of DataDreamer include:

 * Synthetic Data Generation: Eliminate the dependency on extensive datasets for AI training. DataDreamer empowers users to
   generate synthetic datasets from the ground up, utilizing advanced AI algorithms capable of producing high-quality, diverse
   images.
 * Knowledge Extraction from Foundational Models: `DataDreamer` leverages the latent knowledge embedded within sophisticated,
   pre-trained AI models. This capability allows for the transfer of expansive understanding from these "Foundation models" to
   smaller, custom-built models, enhancing their capabilities significantly.
 * Efficient and Potent Models: The primary objective of `DataDreamer` is to enable the creation of compact models that are both
   size-efficient for integration into any device and robust in performance for specialized tasks.

## Features

 * Prompt Generation: Automate the creation of image prompts using powerful language models.
   Provided class names: ["horse", "robot"]
   Generated prompt: "A photo of a horse and a robot coexisting peacefully in the midst of a serene pasture."
 * Image Generation: Generate synthetic datasets with state-of-the-art generative models.

![generated image](https://raw.githubusercontent.com/luxonis/datadreamer/main/images/generated_image.jpg)

 * Dataset Annotation: Leverage foundation models to label datasets automatically.

![annotated image](https://raw.githubusercontent.com/luxonis/datadreamer/main/images/annotated_image.jpg)

 * Edge Model Training: Train efficient small-scale neural networks for edge deployment. (not part of this library)

## Installation

You can either [download it](https://pypi.org/project/datadreamer/#files) or install it using pip:

```bash
pip install datadreamer
```

## Available models

| Model Category | Model Names | Description/Notes |
| --- | --- | --- |
| Prompt Generation | [Mistral-7B-Instruct-v0.1](https://huggingface.co/mistralai/Mistral-7B-Instruct-v0.1) | Semantically rich
prompts |
|  | [TinyLlama-1.1B-Chat-v1.0](https://huggingface.co/TinyLlama/TinyLlama-1.1B-Chat-v1.0) | Tiny LM |
|  | Simple random generator | Joins randomly chosen object names |
| Image Generation | [SDXL-1.0](https://huggingface.co/stabilityai/stable-diffusion-xl-base-1.0) | Slow and accurate (1024x1024
images) |
|  | [SDXL-Turbo](https://huggingface.co/stabilityai/sdxl-turbo) | Fast and less accurate (512x512 images) |
|  | [SDXL-Lightning](https://huggingface.co/ByteDance/SDXL-Lightning) | Fast and accurate (1024x1024 images) |
| Image Annotation | [OWLv2](https://huggingface.co/google/owlv2-base-patch16-ensemble) | Open-Vocabulary object detector |

## Example

```bash
datadreamer --save_dir path/to/save_directory --class_names person moon robot --prompts_number 20 --prompt_generator simple --num_objects_range 1 3 --image_generator sdxl-turbo
```

This command generates images for the specified objects, saving them and their annotations in the given directory. The script
allows customization of the generation process through various parameters, adapting to different needs and hardware
configurations.

## Useful tips

 * Batched generation: To speed up the generation process, consider increasing the batch size with `--batch_size_prompt`,
   `--batch_size_image` and `--batch_size_annotation` parameters. If you are running out of memory, try reducing the batch size.
 * Better image quality: For better image quality, consider tuning the following parameters: * `--image_generator`: Choose a model
   with higher image quality. SDXL-Turbo -> SDXL-Lightning -> SDXL (from fastest to slowest, and from lowest to highest quality).
    * `--use_image_tester` and `--image_tester_patience`: Enable iterative image generation and use the CLIP model to select the
      best images. Consider increasing the patience to get better results.
 * Number of objects per image: To generate images with a different number of objects, use the `--num_objects_range` parameter.
   For example, `--num_objects_range 1 3` generates images with 1, 2, or 3 objects. Values higher than 3 are not recommended due
   to the limited ability of the current models to generate complex scenes.
 * Prompt generation: To generate more diverse prompts consider using the `--prompt_generator tiny` generator which uses a small
   language model to generate prompts.