# Camera

Camera node is a source of [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md). You can control
in at runtime with the `InputControl` and `InputConfig`

It aims to unify the [Color Camera](https://docs.luxonis.com/software/depthai-components/nodes/color_camera.md) and
[MonoCamera](https://docs.luxonis.com/software/depthai-components/nodes/mono_camera.md) into one node.

Compared to [Color Camera](https://docs.luxonis.com/software/depthai-components/nodes/color_camera.md) node, Camera node:

 * Supports cam.setSize(), which replaces both `cam.setResolution()` and `cam.setIspScale()`. Camera node will automatically find
   resolution that fits best, and apply correct scaling to achieve user-selected size
 * Supports cam.setCalibrationAlpha(), example here: [Undistort camera
   stream](https://docs.luxonis.com/software/depthai/examples/camera_undistort.md)
 * Supports cam.loadMeshData() and cam.setMeshStep(), which can be used for custom image warping (undistortion, perspective
   correction, etc.)
 * Automatically undistorts camera stream if HFOV of the camera is greater than 85°. You can disable this with:
   `cam.setMeshSource(dai.CameraProperties.WarpMeshSource.NONE)`.

Besides points above, compared to [MonoCamera](https://docs.luxonis.com/software/depthai-components/nodes/mono_camera.md) node,
Camera node:

 * Doesn't have `out` output, as it has the same outputs as
   [ColorCamera](https://docs.luxonis.com/software/depthai-components/nodes/color_camera.md) (`raw`, `isp`, `still`, `preview`,
   `video`). This means that `preview` will output 3 planes of the same grayscale frame (3x overhead), and `isp` / `video` /
   `still` will output luma (useful grayscale information) + chroma (all values are 128), which will result in 1.5x bandwidth
   overhead

## How to place it

#### Python

```python
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.Camera)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::Camera>();
```

## Inputs and Outputs

Message types

 * `inputConfig` - [ImageManipConfig](https://docs.luxonis.com/software/depthai-components/messages/image_manip_config.md)
 * `inputControl` - [CameraControl](https://docs.luxonis.com/software/depthai-components/messages/camera_control.md)
 * `raw` - [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md) - RAW10 bayer data. Demo code
   for unpacking [here](https://github.com/luxonis/oak-examples/blob/3f1b2b2/gen2-color-isp-raw/main.py#L13-L32)
 * `isp` - [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md) - YUV420 planar (same as
   YU12/IYUV/I420)
 * `still` - [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md) - NV12, suitable for bigger
   size frames. The image gets created when a capture event is sent to the Camera, so it's like taking a photo
 * `preview` - [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md) - RGB (or BGR
   planar/interleaved if configured), mostly suited for small size previews and to feed the image into
   [NeuralNetwork](https://docs.luxonis.com/software/depthai-components/nodes/neural_network.md)
 * `video` - [ImgFrame](https://docs.luxonis.com/software/depthai-components/messages/img_frame.md) - NV12, suitable for bigger
   size frames

ISP (image signal processor) is used for bayer transformation, demosaicing, noise reduction, and other image enhancements. It
interacts with the 3A algorithms: auto-focus, auto-exposure, and auto-white-balance, which are handling image sensor adjustments
such as exposure time, sensitivity (ISO), and lens position (if the camera module has a motorized lens) at runtime. Click
[here](https://en.wikipedia.org/wiki/Image_processor) for more information.

Image Post-Processing converts YUV420 planar frames from the ISP into `video`/`preview`/`still` frames.

`still` (when a capture is triggered) and `isp` work at the max camera resolution, while `video` and `preview` are limited to max
4K (3840 x 2160) resolution, which is cropped from `isp`. For IMX378 (12MP), the post-processing works like this:

The image above is the `isp` output from the Camera (12MP resolution from IMX378). If you aren't downscaling ISP, the `video`
output is cropped to 4k (max 3840x2160 due to the limitation of the `video` output) as represented by the blue rectangle. The
Yellow rectangle represents a cropped `preview` output when the preview size is set to a 1:1 aspect ratio (eg. when using a
300x300 preview size for the MobileNet-SSD NN model) because the `preview` output is derived from the `video` output.

## Usage

#### Python

```python
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.Camera)
cam.setPreviewSize(300, 300)
cam.setBoardSocket(dai.CameraBoardSocket.CAM_A)
# Instead of setting the resolution, user can specify size, which will set
# sensor resolution to best fit, and also apply scaling
cam.setSize(1280, 720)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::Camera>();
cam->setPreviewSize(300, 300);
cam->setBoardSocket(dai::CameraBoardSocket::CAM_A);
// Instead of setting the resolution, user can specify size, which will set
// sensor resolution to best fit, and also apply scaling
cam->setSize(1280, 720);
```

## 3A Algorithms

The 3A - Auto-Exposure (AE), Auto-White Balance (AWB), and Auto-Focus (AF) - algorithms are used to optimize image quality and run
directly on RVC. By default, these settings are in AUTO mode, with limits (e.g., min/max exposure) specific to each sensor (see
[supported sensors](https://docs.luxonis.com/hardware/platform/sensors/sensors.md) for details).

You can manually control these settings either by following the steps in [RGB camera control
example](https://docs.luxonis.com/software/depthai/examples/rgb_camera_control.md) or by using the [cam_test.py
script](https://github.com/luxonis/depthai-python/blob/main/utilities/cam_test.py).

 * Stereo Cameras: Sensors share the same I2C bus, ensuring synchronized 3A settings automatically (AWB, AE).
 * Independent Sensors: On setups like OAK FFC or OAK-D-LR, where each sensor has its own I2C, the `3a-follow` feature can be used
   to synchronize 3A settings from one sensor to others.

Example Usage

```python
cam['cam_b'].initialControl.setMisc("3a-follow", dai.CameraBoardSocket.CAM_A)
cam['cam_c'].initialControl.setMisc("3a-follow", dai.CameraBoardSocket.CAM_A)
```

The `3a-follow` feature copies the 3A settings (exposure, ISO, and white balance) from a primary camera (e.g., CAM_A) to other
cameras in the setup (e.g., CAM_B and CAM_C).

## Limitations

Here are known camera limitations for the [RVC2](https://docs.luxonis.com/hardware/platform/rvc/rvc2.md):

 * ISP can process about 600 MP/s, and about 500 MP/s when the pipeline is also running NNs and video encoder in parallel
 * 3A algorithms can process about 200..250 FPS overall (for all camera streams). This is a current limitation of our
   implementation, and we have plans for a workaround to run 3A algorithms on every Xth frame, no ETA yet

## Examples of functionality

 * [Undistort camera stream](https://docs.luxonis.com/software/depthai/examples/script_camera_control.md)

## Reference

### depthai.node.Camera(depthai.Node)

Kind: Class

Camera node. Experimental node, for both mono and color types of sensors

#### getBoardSocket(self) -> depthai.CameraBoardSocket: depthai.CameraBoardSocket

Kind: Method

Retrieves which board socket to use

Returns:
    Board socket to use

#### getCalibrationAlpha(self) -> float|None: float|None

Kind: Method

Get calibration alpha parameter that determines FOV of undistorted frames

#### getCamera(self) -> str: str

Kind: Method

Retrieves which camera to use by name

Returns:
    Name of the camera to use

#### getFps(self) -> float: float

Kind: Method

Get rate at which camera should produce frames

Returns:
    Rate in frames per second

#### getHeight(self) -> int: int

Kind: Method

Get sensor resolution height

#### getImageOrientation(self) -> depthai.CameraImageOrientation: depthai.CameraImageOrientation

Kind: Method

Get camera image orientation

#### getMeshSource(self) -> depthai.CameraProperties.WarpMeshSource: depthai.CameraProperties.WarpMeshSource

Kind: Method

Gets the source of the warp mesh

#### getMeshStep(self) -> tuple [ int, int ]: tuple [ int, int ]

Kind: Method

Gets the distance between mesh points

#### getPreviewHeight(self) -> int: int

Kind: Method

Get preview height

#### getPreviewSize(self) -> tuple [ int, int ]: tuple [ int, int ]

Kind: Method

Get preview size as tuple

#### getPreviewWidth(self) -> int: int

Kind: Method

Get preview width

#### getSize(self) -> tuple [ int, int ]: tuple [ int, int ]

Kind: Method

Get sensor resolution as size

#### getStillHeight(self) -> int: int

Kind: Method

Get still height

#### getStillSize(self) -> tuple [ int, int ]: tuple [ int, int ]

Kind: Method

Get still size as tuple

#### getStillWidth(self) -> int: int

Kind: Method

Get still width

#### getVideoHeight(self) -> int: int

Kind: Method

Get video height

#### getVideoSize(self) -> tuple [ int, int ]: tuple [ int, int ]

Kind: Method

Get video size as tuple

#### getVideoWidth(self) -> int: int

Kind: Method

Get video width

#### getWidth(self) -> int: int

Kind: Method

Get sensor resolution width

#### loadMeshData(self, warpMesh: typing_extensions.Buffer)

Kind: Method

Specify mesh calibration data for undistortion See `loadMeshFiles` for the
expected data format

#### loadMeshFile(self, warpMesh: Path)

Kind: Method

Specify local filesystem paths to the undistort mesh calibration files.

When a mesh calibration is set, it overrides the camera intrinsics/extrinsics
matrices. Overrides useHomographyRectification behavior. Mesh format: a sequence
of (y,x) points as 'float' with coordinates from the input image to be mapped in
the output. The mesh can be subsampled, configured by `setMeshStep`.

With a 1280x800 resolution and the default (16,16) step, the required mesh size
is:

width: 1280 / 16 + 1 = 81

height: 800 / 16 + 1 = 51

#### setBoardSocket(self, boardSocket: depthai.CameraBoardSocket)

Kind: Method

Specify which board socket to use

Parameter ``boardSocket``:
    Board socket to use

#### setCalibrationAlpha(self, alpha: typing.SupportsFloat)

Kind: Method

Set calibration alpha parameter that determines FOV of undistorted frames

#### setCamera(self, name: str)

Kind: Method

Specify which camera to use by name

Parameter ``name``:
    Name of the camera to use

#### setFps(self, fps: typing.SupportsFloat)

Kind: Method

Set rate at which camera should produce frames

Parameter ``fps``:
    Rate in frames per second

#### setImageOrientation(self, imageOrientation: depthai.CameraImageOrientation)

Kind: Method

Set camera image orientation

#### setIsp3aFps(self, isp3aFps: typing.SupportsInt)

Kind: Method

Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls
etc.). Default (0) matches the camera FPS, meaning that 3A is running on each
frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases
the convergence rate of 3A. Note that camera controls will be processed at this
rate. E.g. if camera is running at 30 fps, and camera control is sent at every
frame, but 3A fps is set to 15, the camera control messages will be processed at
15 fps rate, which will lead to queueing.

#### setMeshSource(self, source: depthai.CameraProperties.WarpMeshSource)

Kind: Method

Set the source of the warp mesh or disable

#### setMeshStep(self, width: typing.SupportsInt, height: typing.SupportsInt)

Kind: Method

Set the distance between mesh points. Default: (32, 32)

#### setPreviewSize()

Kind: Method

#### setRawOutputPacked(self, packed: bool)

Kind: Method

Configures whether the camera `raw` frames are saved as MIPI-packed to memory.
The packed format is more efficient, consuming less memory on device, and less
data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on
3 bytes. When packing is disabled (`false`), data is saved lsb-aligned, e.g. a
RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000'00pp'pppp'pppp.
Default is auto: enabled for standard color/monochrome cameras where ISP can
work with both packed/unpacked, but disabled for other cameras like ToF.

#### setSize()

Kind: Method

#### setStillSize()

Kind: Method

#### setVideoSize()

Kind: Method

#### frameEvent

Kind: Property

Outputs metadata-only ImgFrame message as an early indicator of an incoming
frame.

It's sent on the MIPI SoF (start-of-frame) event, just after the exposure of the
current frame has finished and before the exposure for next frame starts. Could
be used to synchronize various processes with camera capture. Fields populated:
camera id, sequence number, timestamp

#### initialControl

Kind: Property

Initial control options to apply to sensor

#### inputConfig

Kind: Property

Input for ImageManipConfig message, which can modify crop parameters in runtime

Default queue is non-blocking with size 8

#### inputControl

Kind: Property

Input for CameraControl message, which can modify camera parameters in runtime

Default queue is blocking with size 8

#### isp

Kind: Property

Outputs ImgFrame message that carries YUV420 planar (I420/IYUV) frame data.

Generated by the ISP engine, and the source for the 'video', 'preview' and
'still' outputs

#### preview

Kind: Property

Outputs ImgFrame message that carries BGR/RGB planar/interleaved encoded frame
data.

Suitable for use with NeuralNetwork node

#### raw

Kind: Property

Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame
data.

Captured directly from the camera sensor, and the source for the 'isp' output.

#### still

Kind: Property

Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane
interleaved) frame data.

The message is sent only when a CameraControl message arrives to inputControl
with captureStill command set.

#### video

Kind: Property

Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane
interleaved) frame data.

Suitable for use with VideoEncoder node

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.