# ToF

ToF node is used for converting the raw data from the ToF sensor into a depth map. Currently, these 2 products contain a ToF
sensor:

 * [OAK-D ToF](https://shop.luxonis.com/products/oak-d-sr-poe) - integrated 33D ToF sensor, together with a stereo camera pair
 * [OAK-FFC ToF 33D](https://shop.luxonis.com/products/oak-ffc-tof-33d) - standalone FFC module with a 33D ToF sensor

ToF's `depth` output can be used instead of
[StereoDepth](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md)'s - so you can link `ToF.depth` to
[MobileNetSpatialDetectionNetwork](https://docs.luxonis.com/software/depthai-components/nodes/mobilenet_spatial_detection_network.md)/[YoloSpatialDetectionNetwork](https://docs.luxonis.com/software/depthai-components/nodes/yolo_spatial_detection_network.md)
or [SpatialLocationCalculator](https://docs.luxonis.com/software/depthai-components/nodes/spatial_location_calculator.md)
directly.

ToF's depth accuracy is, in general, more accurate compared to Stereo depth. You can see [ToF depth accuracy
here](https://docs.luxonis.com/hardware/platform/depth/depth-accuracy.md).

ToF pointcloud demo video, showcasing the depth accuracy:

[Video: OAK ToF Demo pointcloud](https://www.youtube.com/watch?v=scPFNsCXQtc)

## How to place it

#### Python

```python
pipeline = dai.Pipeline()
tof = pipeline.create(dai.node.ToF)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto tof = pipeline.create<dai::node::ToF>();
```

## Inputs and Outputs

## ToF Settings

In [ToF depth](https://docs.luxonis.com/software/depthai/examples/tof_depth.md) example we allow users to quickly configure ToF
settings.

Here are the most important settings:

 * Optical Correction: It's a process that corrects the optical effect. When enabled, the ToF returns depth map (represented by
   Green Line on graph below) instead of distance, so it matches
   [StereoDepth](https://docs.luxonis.com/software/depthai-components/nodes/stereo_depth.md) depth reporting. It does
   rectification and distance to depth conversion (Z-map).
 * Undistortion: `depth` and `amplitude` frames are undistorted by default.
 * Phase Unwrapping - Process that corrects the phase wrapping effect of the ToF sensor. You can set it to [0..5 are optimized].
   The higher the number, the longer the ToF range, but it also increases the noise. Approximate max distance (for exact value,
   see [Max distance](#Max%20distance) below):
    * `0` - Disabled, up to ~1.87 meters (utilizing 80MHz modulation frequency)
    * `1` - Up to ~3 meters
    * `2` - Up to ~4.5 meters
    * `3` - Up to ~6 meters
    * `4` - Up to ~7.5 meters
 * Burst mode: When enabled, ToF node won't reuse frames, as shown on the graph below. It's related to post-processing of the ToF
   frames, not the actual sensor/projector. It's disabled by default.
 * Phase shuffle Temporal filter: Averages shuffled and non-shuffled frames of the same modulation frequency to reduce noise. It's
   enabled by default. You can disable it to reduce [ToF motion blur](#ToF%20motion%20blur) and system load.

![ToF diagram: distance reported along the ray to a pixel vs optically corrected distance](https://docs.luxonis.com/static/images/software/depthai/nodes/tof-optical-correction.excalidraw.png)

Here's the time diagram which showcases how ToF decoding gets done based on the settings.

![ToF capture timing at 100 FPS: decoded depth frames for each shuffle filter and burst mode setting](https://docs.luxonis.com/static/images/software/depthai/nodes/tof-diagram.webp)

## Phase unwrapping

If the time it takes for the light to travel from ToF sensor and back exceeds the period of the emitted wave (1.5m or 1.87m), the
resulting measurement will "wrap" back to a lower value. This is called phase wrapping. It's similar to how a clock resets after
12 hours. Phase unwrapping is possible as our ToF has two different modulation frequencies (80Mhz and 100MHz).

Phase unwrapping aims to correct this by allowing the sensor to interpret longer distances without confusion. It uses algorithms
to keep track of how many cycles (round trips of the wave) have occurred, thus correcting the "wrapped" phases. The downside is
that the more cycles the sensor has to keep track of, the more noise it introduces into the measurement.

## ToF motion blur

To reduce motion blur, we recommend these settings:

 * Increase camera FPS. It goes up to 160 FPS, which causes frame capture to be the fastest (6.25ms between frames). This will
   reduce motion blur as ToF combines multiple frames to get the depth. Note that 160FPS will increase system load significantly
   (see [Debugging](https://docs.luxonis.com/software/depthai/debugging.md) DepthAI pipeline). Note also that higher FPS -> lower
   exposure times, which can increase noise.
 * Disable phase shuffle temporal filter. This will introduce more noise.
 * Disable phase unwrapping. This will reduce max distance to 1.87 meters (utilizing 80MHz modulation frequency), so about 1 cubic
   meter of space will be visible (very limited use-cases).
 * Enable burst mode. This is irrelevant if shuffle filter and phase unwrapping are disabled (see diagram above). When enabled,
   ToF node won't reuse frames (lower FPS).

In the diagram above, the less frames are combined (bottom of the diagram), the less motion blur there is. The more frames are
combined (top of the diagram), there's more filtering (better accuracy) but it results in more motion blur.

## Max distance

Maximum ToF distance depends on the modulation frequency and the phase unwrapping level. If phase unwrapping is enabled, max
distance is the shorter of both modulation frequencies (so max distance at 100MHz). Here's the formula:

```math
c = 299792458.0 # speed of light in m/s

MAX_80MHZ_M = c / (80000000 * 2) = 1.873 m
MAX_100MHZ_M = c / (100000000 * 2) = 1.498 m

MAX_DIST_80MHZ_M = (phaseUnwrappingLevel + 1) * 1.873 + (phaseUnwrapErrorThreshold / 2)
MAX_DIST_100MHZ_M = (phaseUnwrappingLevel + 1) * 1.498 + (phaseUnwrapErrorThreshold / 2)

MAX_DIST_PHASE_UNWRAPPING_M = MAX_DIST_100MHZ_M
```

## ToF FPS

Sensor/emitter can go up to 160 FPS, which will translte to depth output at either 40 FPS (burst mode enabled) or 80 FPS (burst
mode disabled). This is due to different modulation frequencies (80MHz and 100MHz) and the need to combine shuffled/non-shuffled
frames to reduce noise.

## Usage

#### Python

```python

pipeline = dai.Pipeline()

tof_cam = pipeline.create(dai.node.Camera)
tof_cam.setFps(30)
# We assume the ToF camera sensor is on port CAM_A
tof_cam.setBoardSocket(dai.CameraBoardSocket.CAM_A)

tof = pipeline.create(dai.node.ToF)

# Higher number => faster processing. 1 shave core can do 30FPS.
tof.setNumShaves(1)

# Median filter, kernel size 5x5
tof.initialConfig.setMedianFilter(dai.MedianFilter.KERNEL_5x5)

tofConfig = tof.initialConfig.get()
# Temporal filter averages shuffle/non-shuffle frequencies
tofConfig.enablePhaseShuffleTemporalFilter = True
# Phase unwrapping, for longer range.
tofConfig.phaseUnwrappingLevel = 4 # Up to 7.5 meters
tofConfig.phaseUnwrapErrorThreshold = 300
tof.initialConfig.set(tofConfig)

# ToF node converts raw sensor frames into depth
tof_cam.raw.link(tof.input)

# Send ToF depth output to the host, or perhaps to SLC / Spatial Detection Network
tof.depth.link(xout.input)
```

#### C++

```cpp

dai::Pipeline pipeline;

auto tofCam = pipeline.create<dai::node::MonoCamera>();
// We assume the ToF camera sensor is on port CAM_A
tofCam->setBoardSocket(dai::CameraBoardSocket::AUTO);

auto tof = pipeline.create<dai::node::ToF>();
// ToF node converts raw sensor frames into depth
tofCam->raw.link(tof->input);

auto xout = pipeline.create<dai::node::XLinkOut>();
xout->setStreamName("depth");
// Send ToF depth output to the host
tof->depth.link(xout->input);
```

## Examples of functionality

 * [ToF depth](https://docs.luxonis.com/software/depthai/examples/tof_depth.md) - Example of getting ToF depth
 * [RGB-ToF Alignment](https://docs.luxonis.com/software/depthai/examples/tof_align.md) - Align tof depth to color stream

## Reference

### depthai.node.ToF(depthai.Node)

Kind: Class

ToF node

#### setNumFramesPool(self, arg0: typing.SupportsInt) -> ToF: ToF

Kind: Method

Specify number of frames in output pool

Parameter ``numFramesPool``:
    Number of frames in output pool

#### setNumShaves(self, arg0: typing.SupportsInt) -> ToF: ToF

Kind: Method

Specify number of shaves reserved for ToF decoding.

#### amplitude

Kind: Property

Outputs ImgFrame message that carries amplitude image.

#### depth

Kind: Property

Outputs ImgFrame message that carries decoded depth image.

#### initialConfig

Kind: Property

Initial config to use for depth calculation.

#### input

Kind: Property

Input raw ToF data. Default queue is blocking with size 8.

#### inputConfig

Kind: Property

Input ToF message with ability to modify parameters in runtime. Default queue is
non-blocking with size 4.

#### intensity

Kind: Property

Outputs ImgFrame message that carries intensity image.

#### phase

Kind: Property

Outputs ImgFrame message that carries phase image, useful for debugging. float32
type.

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.