IMU
IMU (inertial measurement unit) node can be used to receive data from the IMU chip on the device. Our OAK devices use either:- BNO085 (datasheet here) 9-axis sensor, combining accelerometer, gyroscope, and magnetometer. It also does sensor fusion on the (IMU) chip itself. We have efficiently integrated this driver into the DepthAI.
- BMI270 6-axis sensor, combining accelerometer and gyroscope.
How to place it
Python
C++
Python
Python
1pipeline = dai.Pipeline()
2imu = pipeline.create(dai.node.IMU)Inputs and Outputs
Limitations
- For BNO086, gyroscope frequency above 400Hz can produce some jitter from time to time due to sensor HW limitation.
Please take note that all OAK-D-Lite cameras from Kickstarter do not have an IMU on board.
IMU sensor frequencies
Below are the discrete stable frequencies available for each (raw) IMU sensor. Some maximum IMU frequencies are higher, eg. for BNO086, maximum frequency for gyroscope is 1000Hz, but up to 400Hz is stable (due to driver limitation).BNO086:Note that BNO IMU "rounds up" the input frequency to the next available frequency. For example, if you set the frequency to 101 it will round it to 200Hz.- Accelerometer: 15Hz, 31Hz, 62Hz, 125Hz, 250Hz 500Hz
- Gyroscope: 25Hz, 33Hz, 50Hz, 100Hz, 200Hz, 400Hz
- Magnetometer: 100Hz
| BNO086 Sensor | Max Frequency |
|---|---|
| ACCELEROMETER_RAW | 512 Hz |
| ACCELEROMETER | 512 Hz |
| LINEAR_ACCELERATION | 400 Hz |
| GRAVITY | 400 Hz |
| GYROSCOPE_RAW | 1000 Hz |
| GYROSCOPE_CALIBRATED / GYROSCOPE_UNCALIBRATED | 100 Hz |
| MAGNETOMETER_RAW | 100 Hz |
| MAGNETOMETER_CALIBRATED / MAGNETOMETER_UNCALIBRATED | 100 Hz |
| ROTATION_VECTOR | 400 Hz |
| GAME_ROTATION_VECTOR | 400 Hz |
| GEOMAGNETIC_ROTATION_VECTOR | 100 Hz |
| ARVR_STABILIZED_ROTATION_VECTOR | 100 Hz |
| ARVR_STABILIZED_GAME_ROTATION_VECTOR | 100 Hz |
- Accelerometer: 25Hz, 50Hz, 100Hz, 200Hz, 250Hz
- Gyroscope: 25Hz, 50Hz, 100Hz, 200Hz, 250Hz
Usage
Python
C++
Python
Python
1pipeline = dai.Pipeline()
2imu = pipeline.create(dai.node.IMU)
3
4# enable ACCELEROMETER_RAW and GYROSCOPE_RAW at 100 hz rate
5imu.enableIMUSensor([dai.IMUSensor.ACCELEROMETER_RAW, dai.IMUSensor.GYROSCOPE_RAW], 100)
6# above this threshold packets will be sent in batch of X, if the host is not blocked and USB bandwidth is available
7imu.setBatchReportThreshold(1)
8# maximum number of IMU packets in a batch, if it's reached device will block sending until host can receive it
9# if lower or equal to batchReportThreshold then the sending is always blocking on device
10# useful to reduce device's CPU load and number of lost packets, if CPU load is high on device side due to multiple nodes
11imu.setMaxBatchReports(10)IMU sensors
When enabling the IMU sensors (imu.enableIMUSensor()), you can select between the following sensors:ACCELEROMETER_RAWACCELEROMETERLINEAR_ACCELERATIONGRAVITYGYROSCOPE_RAWGYROSCOPE_CALIBRATEDGYROSCOPE_UNCALIBRATEDMAGNETOMETER_RAWMAGNETOMETER_CALIBRATEDMAGNETOMETER_UNCALIBRATEDROTATION_VECTORGAME_ROTATION_VECTORGEOMAGNETIC_ROTATION_VECTORARVR_STABILIZED_ROTATION_VECTORARVR_STABILIZED_GAME_ROTATION_VECTOR
class
depthai.IMUSensor
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
method
method
method
method
method
method
method
method
method
method
property
property
Examples of functionality
Reference
class
depthai.node.IMU(depthai.Node)
method
method
method
getBatchReportThreshold(self) -> int: intAbove this packet threshold data will be sent to host, if queue is not blocked
method
getMaxBatchReports(self) -> int: intMaximum number of IMU packets in a batch report
method
setBatchReportThreshold(self, batchReportThreshold: int)Above this packet threshold data will be sent to host, if queue is not blocked
method
setMaxBatchReports(self, maxBatchReports: int)Maximum number of IMU packets in a batch report
property
out
Outputs IMUData message that carries IMU packets.
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.