DepthAI v2 has been superseded by DepthAI v3. You are viewing legacy documentation.

ON THIS PAGE

  • StereoDepth
  • How to place it
  • Inputs and Outputs
  • Internal block diagram of StereoDepth node
  • Currently configurable blocks
  • Limitations
  • Changing camera calibration during runtime
  • Depth Presets
  • Depth Presets
  • Stereo depth FPS
  • Usage
  • Examples of functionality
  • Reference
  • Disparity
  • Calculate depth using disparity map
  • Min stereo depth distance
  • Disparity shift to lower min depth perception
  • Max stereo depth distance
  • Depth perception accuracy
  • Limitation
  • Measuring real-world object dimensions

StereoDepth

StereoDepth node calculates the disparity and/or depth from the stereo camera pair (2x MonoCamera/ColorCamera). We suggest following Configuring Stereo Depth tutorial to achieve the best depth results.

How to place it

Python
C++

Python

Python
1pipeline = dai.Pipeline()
2stereo = pipeline.create(dai.node.StereoDepth)

Inputs and Outputs

There are also debug outputs (all are ImgFrame): debugDispLrCheckIt1, debugDispLrCheckIt2, debugExtDispLrCheckIt1, debugExtDispLrCheckIt2, debugDispCostDump and confidenceMap.

Internal block diagram of StereoDepth node

On the diagram, red rectangle are firmware settings that are configurable via the API. Gray rectangles are settings that that are not yet exposed to the API. We plan on exposing as much configurability as possible, but please inform us if you would like to see these settings configurable sooner.If you click on the image, you will be redirected to the webapp. Some blocks have notes that provide additional technical information.

Currently configurable blocks

  • Stereo Mode:
    • Left-Right Check:
      • Left-Right Check or LR-Check is used to remove incorrectly calculated disparity pixels due to occlusions at object borders (Left and Right camera views are slightly different).
        1. Computes disparity by matching in R->L direction.
        2. Computes disparity by matching in L->R direction.
        3. Combines results from steps 1 and 2, running on Shave: each pixel d = disparity_LR(x,y) is compared with disparity_RL(x-d,y). If the difference is above a threshold, the pixel at (x,y) in the final disparity map is invalidated.
      • You can use debugDispLrCheckIt1 and debugDispLrCheckIt2 debug outputs for debugging/fine-tuning purposes.
    • Extended Disparity:
      • Extended disparity mode allows detecting closer distance objects for the given baseline. This increases the maximum disparity search from 96 to 191, meaning the range is now: [0..190].
        1. Computes disparity on the original size images (e.g. 1280x720).
        2. Computes disparity on 2x downscaled images (e.g. 640x360).
        3. Combines the two level disparities on Shave, effectively covering a total disparity range of 191 pixels (in relation to the original resolution).
      • You can use debugExtDispLrCheckIt1 and debugExtDispLrCheckIt2 debug outputs for debugging/fine-tuning purposes.
    • Subpixel Disparity:
      • Subpixel mode improves the precision and is especially useful for long-range measurements. It also helps for better estimating surface normals.
      • In this mode, stereo cameras perform: 94 depth steps * 8 subpixel depth steps + 2 (min/max values) = 754 depth steps.
      • For comparison of normal disparity vs. subpixel disparity images, click here.
  • Depth Filters:
    • Depth Filtering / Depth Post-Processing is performed at the end of the depth pipeline. It helps with noise reduction and overall depth quality.
  • Mesh files:
    • Mesh files (homography matrix) are generated using the camera intrinsics, distortion coeffs, and rectification rotations. These files help in overcoming the distortions in the camera increasing the accuracy and also help in when wide FOV lens are used.
    • Currently, mesh files are generated only for stereo cameras on the host during calibration. The generated mesh files are stored in depthai/resources which users can load to the device. This process will be moved to on device in the upcoming releases.
  • Confidence Threshold:
    • Confidence threshold: Stereo depth algorithm searches for the matching feature from the right camera point to the left image (along the 96 disparity levels). During this process, it computes the cost for each disparity level and chooses the minimal cost between two disparities and uses it to compute the confidence at each pixel. Stereo node will output disparity/depth pixels only where depth confidence is below the confidence threshold (lower the confidence value means better depth accuracy).
    • LR check threshold: Disparity is considered for the output when the difference between LR and RL disparities is smaller than the LR check threshold.

Limitations

  • Median filtering is disabled when subpixel mode is set to 4 or 5 bits.
  • For RGB-depth alignment the RGB camera has to be placed on the same horizontal line as the stereo camera pair.
  • RGB-depth alignment doesn't work when using disparity shift.

Changing camera calibration during runtime

Since the depthai-2.29.0 release, changing the camera calibration during runtime is possible. The calibration can be changed using the device.setCalibration() method and can be used if device stereo quality degrades over time due to environmental factors. The same data can be obtained using the device.getCalibration().

Depth Presets

We have made a few depth presets that can be used to quickly set up the StereoDepth node for different scenarios, without having to manually set all the parameters listed under Configutring stereo depth.

Depth Presets

FeatureDefaultFaceHigh DetailRobotics
Base ProfileHIGH_DENSITYHIGH_DENSITYHIGH_ACCURACYHIGH_DENSITY
Median Filter7x7 kernelOffOff7x7 kernel
Subpixel Precision3-bit5-bit5-bit3-bit
Extended DisparityNoYesYesNo
Range0-15m3cm-3m0-15m0-10m
Temporal FilterEnabledEnabledEnabledDisabled
Use CaseGeneral purposeFace tracking, biometrics3D scanning, object detailsNavigation, obstacle detection
All presets include:
  • Left-right consistency check
  • 2x decimation with pixel skipping
  • Speckle filtering (range: 200, threshold: 2)
  • 3 hardware resources for post-processing

Stereo depth FPS

StereoDepth handles quite a few complex operations across multiple hardware blocks, and the FPS depends on the setting of this node. So instead of FPS, let's look at the latency of each operation.First in the pipeline (see Internal block diagram) is rectification, which runs on warp engine. Because wide FOV frames requires a more complex mesh to get rectified, it takes a bit longer to process.
Process \ Resolution400P [ms]720P [ms]800P [ms]
Rectification1.556
Wide FOV rectification2.589
Then we have actual stereo disparity matching, which runs on it's own stereo engine. This is usually the most time-consuming part (unless we have heavy post-processing filters), which means it's likely the bottleneck in the pipeline. First the glossary:
  • LR: Left-Right check (stereo.setLeftRightCheck()). It requires 2 stereo matching operations (L->R and R->L direction) and then a combines results
  • Ext: Extended disparity mode (stereo.setExtendedDisparity()). It requires 2 stereo matching operations (original and downscaled) and then combines results
  • Sub: Subpixel matching (stereo.setSubpixel()). For each pixel you get 96 bytes for cost map (one byte for each disparity level), so for 800P frame about 98MB of data needs to get moved to CMX memory (used by SHAVEs) for subpixel calculation. So bottleneck in this case is memory bandwidth (~4.1GB/sec). Number of subpixel bits doesn't affect latency
Process \ Resolution400P [ms]720P [ms]800P [ms]
No LR, No Ext, No Sub3.47.48.1
No LR, No Ext, Sub6.221.723.9
No LR, Ext, No Sub8.521.523.5
No LR, Ext, Sub1132.736.7
LR, No Ext, No Sub7.41819.8
LR, No Ext, Sub10.127.630.5
LR, Ext, No Sub16.743.748.3
LR, Ext, Sub20.45662
As this step is likely the bottleneck, we can calculate the FPS from it. So if you enable LR, Ext and Sub at 800P, you'll get around (1 sec/62 ms =) 16 FPS.At the end we have filtering - like median filtering (running on median hardware block), which is a simple operation and doesn't add much latency. Kernel type (3x3, 5x5, 7x7) doesn't affect the latency:
Process \ Resolution400P [ms]720P [ms]800P [ms]
Median filtering (3x3 / 5x5 / 7x7)0.81.81.8
There are also other post-processing filters which can take significant compute/latency, but we haven't done extensive measurements for them yet.

Usage

Python
C++

Python

Python
1pipeline = dai.Pipeline()
2stereo = pipeline.create(dai.node.StereoDepth)
3
4# Better handling for occlusions:
5stereo.setLeftRightCheck(False)
6# Closer-in minimum depth, disparity range is doubled:
7stereo.setExtendedDisparity(False)
8# Better accuracy for longer distance, fractional disparity 32-levels:
9stereo.setSubpixel(False)
10
11# Define and configure MonoCamera nodes beforehand
12left.out.link(stereo.left)
13right.out.link(stereo.right)

Examples of functionality

Reference

class

depthai.node.StereoDepth(depthai.Node)

class
PresetMode
Preset modes for stereo depth.  Members:    HIGH_ACCURACY : **Deprecated:** Will be removed in future releases and replaced with DEFAULT    HIGH_DENSITY : **Deprecated:** Will be removed in future releases and replaced with DEFAULT    DEFAULT    FACE    HIGH_DETAIL    ROBOTICS
method
enableDistortionCorrection(self, arg0: bool)
Equivalent to useHomographyRectification(!enableDistortionCorrection)
method
getMaxDisparity(self) -> float: float
Useful for normalization of the disparity map.  Returns:     Maximum disparity value that the node can return
method
loadMeshData(self, dataLeft: list [ int ], dataRight: list [ int ])
Specify mesh calibration data for 'left' and 'right' inputs, as vectors of bytes. Overrides useHomographyRectification behavior. See `loadMeshFiles` for the expected data format
method
loadMeshFiles(self, pathLeft: Path, pathRight: Path)
Specify local filesystem paths to the mesh calibration files for 'left' and 'right' inputs.  When a mesh calibration is set, it overrides the camera intrinsics/extrinsics matrices. Overrides useHomographyRectification behavior. Mesh format: a sequence of (y,x) points as 'float' with coordinates from the input image to be mapped in the output. The mesh can be subsampled, configured by `setMeshStep`.  With a 1280x800 resolution and the default (16,16) step, the required mesh size is:  width: 1280 / 16 + 1 = 81  height: 800 / 16 + 1 = 51
method
setAlphaScaling(self, arg0: float)
Free scaling parameter between 0 (when all the pixels in the undistorted image are valid) and 1 (when all the source image pixels are retained in the undistorted image). On some high distortion lenses, and/or due to rectification (image rotated) invalid areas may appear even with alpha=0, in these cases alpha < 0.0 helps removing invalid areas. See getOptimalNewCameraMatrix from opencv for more details.
method
setBaseline(self, arg0: float)
Override baseline from calibration. Used only in disparity to depth conversion. Units are centimeters.
method
setConfidenceThreshold(self, arg0: int)
Confidence threshold for disparity calculation  Parameter ``confThr``:     Confidence threshold value 0..255
method
setDefaultProfilePreset(self, arg0: StereoDepth.PresetMode)
Sets a default preset based on specified option.  Parameter ``mode``:     Stereo depth preset mode
method
method
setDepthAlignmentUseSpecTranslation(self, arg0: bool)
Use baseline information for depth alignment from specs (design data) or from calibration. Default: true
method
setDisparityToDepthUseSpecTranslation(self, arg0: bool)
Use baseline information for disparity to depth conversion from specs (design data) or from calibration. Default: true
method
setEmptyCalibration(self)
Specify that a passthrough/dummy calibration should be used, when input frames are already rectified (e.g. sourced from recordings on the host)
method
setExtendedDisparity(self, enable: bool)
Disparity range increased from 0-95 to 0-190, combined from full resolution and downscaled images.  Suitable for short range objects. Currently incompatible with sub-pixel disparity
method
setFocalLength(self, arg0: float)
Override focal length from calibration. Used only in disparity to depth conversion. Units are pixels.
method
setFocalLengthFromCalibration(self, arg0: bool)
Whether to use focal length from calibration intrinsics or calculate based on calibration FOV. Default value is true.
method
method
setLeftRightCheck(self, enable: bool)
Computes and combines disparities in both L-R and R-L directions, and combine them.  For better occlusion handling, discarding invalid disparity values
method
setMedianFilter(self, arg0: depthai.MedianFilter)
Parameter ``median``:     Set kernel size for disparity/depth median filtering, or disable
method
setMeshStep(self, width: int, height: int)
Set the distance between mesh points. Default: (16, 16)
method
setNumFramesPool(self, arg0: int)
Specify number of frames in pool.  Parameter ``numFramesPool``:     How many frames should the pool have
method
method
setOutputKeepAspectRatio(self, keep: bool)
Specifies whether the frames resized by `setOutputSize` should preserve aspect ratio, with potential cropping when enabled. Default `true`
method
method
setOutputSize(self, width: int, height: int)
Specify disparity/depth output resolution size, implemented by scaling.  Currently only applicable when aligning to RGB camera
method
setPostProcessingHardwareResources(self, arg0: int, arg1: int)
Specify allocated hardware resources for stereo depth. Suitable only to increase post processing runtime.  Parameter ``numShaves``:     Number of shaves.  Parameter ``numMemorySlices``:     Number of memory slices.
method
setRectification(self, enable: bool)
Rectify input images or not.
method
setRectificationUseSpecTranslation(self, arg0: bool)
Obtain rectification matrices using spec translation (design data) or from calibration in calculations. Should be used only for debugging. Default: false
method
setRectifyEdgeFillColor(self, color: int)
Fill color for missing data at frame edges  Parameter ``color``:     Grayscale 0..255, or -1 to replicate pixels
method
setRectifyMirrorFrame(self, arg0: bool)
DEPRECATED function. It was removed, since rectified images are not flipped anymore. Mirror rectified frames, only when LR-check mode is disabled. Default `true`. The mirroring is required to have a normal non-mirrored disparity/depth output.  A side effect of this option is disparity alignment to the perspective of left or right input: `false`: mapped to left and mirrored, `true`: mapped to right. With LR-check enabled, this option is ignored, none of the outputs are mirrored, and disparity is mapped to right.  Parameter ``enable``:     True for normal disparity/depth, otherwise mirrored
method
setRuntimeModeSwitch(self, arg0: bool)
Enable runtime stereo mode switch, e.g. from standard to LR-check. Note: when enabled resources allocated for worst case to enable switching to any mode.
method
setSubpixel(self, enable: bool)
Computes disparity with sub-pixel interpolation (3 fractional bits by default).  Suitable for long range. Currently incompatible with extended disparity
method
setSubpixelFractionalBits(self, subpixelFractionalBits: int)
Number of fractional bits for subpixel mode. Default value: 3. Valid values: 3,4,5. Defines the number of fractional disparities: 2^x. Median filter postprocessing is supported only for 3 fractional bits.
method
useHomographyRectification(self, arg0: bool)
Use 3x3 homography matrix for stereo rectification instead of sparse mesh generated on device. Default behaviour is AUTO, for lenses with FOV over 85 degrees sparse mesh is used, otherwise 3x3 homography. If custom mesh data is provided through loadMeshData or loadMeshFiles this option is ignored.  Parameter ``useHomographyRectification``:     true: 3x3 homography matrix generated from calibration data is used for     stereo rectification, can't correct lens distortion. false: sparse mesh is     generated on-device from calibration data with mesh step specified with     setMeshStep (Default: (16, 16)), can correct lens distortion. Implementation     for generating the mesh is same as opencv's initUndistortRectifyMap     function. Only the first 8 distortion coefficients are used from calibration     data.
property
confidenceMap
Outputs ImgFrame message that carries RAW8 confidence map. Lower values means higher confidence of the calculated disparity value. RGB alignment, left-right check or any postproccessing (e.g. median filter) is not performed on confidence map.
property
debugDispCostDump
Outputs ImgFrame message that carries cost dump of disparity map. Useful for debugging/fine tuning.
property
debugDispLrCheckIt1
Outputs ImgFrame message that carries left-right check first iteration (before combining with second iteration) disparity map. Useful for debugging/fine tuning.
property
debugDispLrCheckIt2
Outputs ImgFrame message that carries left-right check second iteration (before combining with first iteration) disparity map. Useful for debugging/fine tuning.
property
debugExtDispLrCheckIt1
Outputs ImgFrame message that carries extended left-right check first iteration (downscaled frame, before combining with second iteration) disparity map. Useful for debugging/fine tuning.
property
debugExtDispLrCheckIt2
Outputs ImgFrame message that carries extended left-right check second iteration (downscaled frame, before combining with first iteration) disparity map. Useful for debugging/fine tuning.
property
depth
Outputs ImgFrame message that carries RAW16 encoded (0..65535) depth data in depth units (millimeter by default).  Non-determined / invalid depth values are set to 0
property
disparity
Outputs ImgFrame message that carries RAW8 / RAW16 encoded disparity data: RAW8 encoded (0..95) for standard mode; RAW8 encoded (0..190) for extended disparity mode; RAW16 encoded for subpixel disparity mode: - 0..760 for 3 fractional bits (by default) - 0..1520 for 4 fractional bits - 0..3040 for 5 fractional bits
property
initialConfig
Initial config to use for StereoDepth.
property
inputConfig
Input StereoDepthConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
property
left
Input for left ImgFrame of left-right pair  Default queue is non-blocking with size 8
property
outConfig
Outputs StereoDepthConfig message that contains current stereo configuration.
property
rectifiedLeft
Outputs ImgFrame message that carries RAW8 encoded (grayscale) rectified frame data.
property
rectifiedRight
Outputs ImgFrame message that carries RAW8 encoded (grayscale) rectified frame data.
property
right
Input for right ImgFrame of left-right pair  Default queue is non-blocking with size 8
property
syncedLeft
Passthrough ImgFrame message from 'left' Input.
property
syncedRight
Passthrough ImgFrame message from 'right' Input.

Disparity

Disparity refers to the distance between two corresponding points in the left and right image of a stereo pair.When calculating the disparity, each pixel in the disparity map gets assigned a confidence value 0..255 by the stereo matching algorithm, as:
  • 0 - maximum confidence that it holds a valid value
  • 255 - minimum confidence, so there is more chance that the value is incorrect
(this confidence score is kind-of inverted, if say comparing with NN)For the final disparity map, a filtering is applied based on the confidence threshold value: the pixels that have their confidence score larger than the threshold get invalidated, i.e. their disparity value is set to zero. You can set the confidence threshold with stereo.initialConfig.setConfidenceThreshold().

Calculate depth using disparity map

Disparity and depth are inversely related. As disparity decreases, depth increases exponentially depending on baseline and focal length. Meaning, if the disparity value is close to zero, then a small change in disparity generates a large change in depth. Similarly, if the disparity value is big, then large changes in disparity do not lead to a large change in depth.By considering this fact, depth can be calculated using this formula:
Python
1depth = focal_length_in_pixels * baseline / disparity_in_pixels
Where baseline is the distance between two mono cameras. Note the unit used for baseline and depth is the same.To get focal length in pixels, you can Calibration Reader, as focal length in pixels is written in camera intrinsics (intrinsics[0][0]):
Python
1import depthai as dai
2
3with dai.Device() as device:
4  calibData = device.readCalibration()
5  intrinsics = calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_C)
6  print('Right mono camera focal length in pixels:', intrinsics[0][0])
Here's theoretical calculation of the focal length in pixels:
Python
1focal_length_in_pixels = image_width_in_pixels * 0.5 / tan(HFOV * 0.5 * PI/180)
2
3# With 400P mono camera resolution where HFOV=71.9 degrees
4focal_length_in_pixels = 640 * 0.5 / tan(71.9 * 0.5 * PI / 180) = 441.25
5
6# With 800P mono camera resolution where HFOV=71.9 degrees
7focal_length_in_pixels = 1280 * 0.5 / tan(71.9 * 0.5 * PI / 180) = 882.5
Examples for calculating the depth value, using the OAK-D (7.5cm baseline):
Python
1# For OAK-D @ 400P mono cameras and disparity of eg. 50 pixels
2depth = 441.25 * 7.5 / 50 = 66.19 # cm
3
4# For OAK-D @ 800P mono cameras and disparity of eg. 10 pixels
5depth = 882.5 * 7.5 / 10 = 661.88 # cm
Note the value of disparity depth data is stored in uint16, where 0 is a special value, meaning that distance is unknown.

Min stereo depth distance

If the depth results for close-in objects look weird, this is likely because they are below the minimum depth-perception distance of the device.To calculate this minimum distance, use the Calculate depth using disparity map and choose the maximum value for disparity_in_pixels parameter (keep in mind it is inveresly related, so maximum value will yield the smallest result).For example OAK-D has a baseline of 7.5cm, focal_length_in_pixels of 882.5 pixels and the default maximum value for disparity_in_pixels is 95. By using the Calculate depth using disparity map we get:
Python
1min_distance = focal_length_in_pixels * baseline / disparity_in_pixels = 882.5 * 7.5cm / 95 = 69.67cm
or roughly 70cm.However this distance can be cut in 1/2 (to around 35cm for the OAK-D) with the following options:
  1. Changing the resolution to 640x400, instead of the standard 1280x800.
  2. Enabling Extended Disparity.
Extended Disparity mode increases the levels of disparity to 191 from the standard 96 pixels, thereby 1/2-ing the minimum depth. It does so by computing the 96-pixel disparities on the original 1280x720 and on the downscaled 640x360 image, which are then merged to a 191-level disparity. For more information see the Extended Disparity tab in Currently configurable blocks.Using the previous OAK-D example, disparity_in_pixels now becomes 190 and the minimum distance is:
Python
1min_distance = focal_length_in_pixels * baseline / disparity_in_pixels = 882.5 * 7.5cm / 190 = 34.84cm
or roughly 35cm.See these examples for how to enable Extended Disparity.

Disparity shift to lower min depth perception

Another option to perceive closer depth range is to use disparity shift. Disparity shift will shift the starting point of the disparity search, which will significantly decrease max depth (MazZ) perception, but it will also decrease min depth (MinZ) perception. Disparity shift can be combined with extended/subpixel/LR-check modes.Left graph shows min and max disparity and depth for OAK-D (7.5cm baseline, 800P resolution, ~70° HFOV) by default (disparity shift=0). See Calculate depth using disparity map. Since hardware (stereo block) has a fixed 95 pixel disparity search, DepthAI will search from 0 pixels (depth=INF) to 95 pixels (depth=71cm).Right graph shows the same, but at disparity shift set to 30 pixels. This means that disparity search will be from 30 pixels (depth=2.2m) to 125 pixels (depth=50cm). This also means that depth will be very accurate at the short range (theoretically below 5mm depth error).Limitations:
  • Because of the inverse relationship between disparity and depth, MaxZ will decrease much faster than MinZ as the disparity shift is increased. Therefore, it is advised not to use a larger than necessary disparity shift.
  • Tradeoff in reducing the MinZ this way is that objects at distances farther away than MaxZ will not be seen.
  • Because of the point above, we only recommend using disparity shift when MaxZ is known, such as having a depth camera mounted above a table pointing down at the table surface.
  • Output disparity map is not expanded, only the depth map. So if disparity shift is set to 50, and disparity value obtained is 90, the real disparity is 140.
Compared to Extended disparity, disparity shift:
  • (+) Is faster, as it doesn't require an extra computation, which means there's also no extra latency
  • (-) Reduces the MaxZ (significantly), while extended disparity only reduces MinZ.
Disparity shift can be combined with extended disparity.
method

depthai.StereoDepthConfig.setDisparityShift

Max stereo depth distance

The maximum depth perception distance depends on the (Depth perception accuracy). The formula used to calculate this distance is an approximation, but is as follows:
Python
1Dm = (baseline/2) * tan((90 - HFOV / HPixels)*pi/180)
So using this formula for existing models the theoretical max distance is:
Python
1# For OAK-D (7.5cm baseline)
2Dm = (7.5/2) * tan((90 - 71.9/1280)*pi/180) = 3825.03cm = 38.25 meters
3
4# For OAK-D-CM4 (9cm baseline)
5Dm = (9/2) * tan((90 - 71.9/1280)*pi/180) = 4590.04cm = 45.9 meters
If greater precision for long range measurements is required, consider enabling Subpixel Disparity or using a larger baseline distance between mono cameras. For a custom baseline, you could consider using OAK-FFC device or design your own baseboard PCB with required baseline. For more information see Subpixel Disparity under the Stereo Mode tab in Currently configurable blocks.

Depth perception accuracy

Disparity depth works by matching features from one image to the other and its accuracy is based on multiple parameters:Texture of objects / backgroundsBackgrounds may interfere with the object detection, since backgrounds are objects too, which will make depth perception less accurate. So disparity depth works very well outdoors as there are very rarely perfectly-clean/blank surfaces there - but these are relatively commonplace indoors (in clean buildings at least).LightingIf the illumination is low, the diparity map will be of low confidence, which will result in a noisy depth map.Baseline / distance to objectsLower baseline enables us to detect the depth at a closer distance as long as the object is visible in both the frames. However, this reduces the accuracy for large distances due to less pixels representing the object and disparity decreasing towards 0 much faster. So the common norm is to adjust the baseline according to how far/close we want to be able to detect objects.

Limitation

Since depth is calculated from disparity, which requires the pixels to overlap, there is inherently a vertical band on the left side of the left mono camera and on the right side of the right mono camera, where depth cannot be calculated, since it is seen by only 1 camera. That band is marked with B on the following picture.Meaning of variables on the picture:
  • BL [cm] - Baseline of stereo cameras.
  • Dv [cm] - Minimum distace where both cameras see an object (thus where depth can be calculated).
  • B [pixels] - Width of the band where depth cannot be calculated.
  • W [pixels] - Width of mono in pixels camera or amount of horizontal pixels, also noted as HPixels in other formulas.
  • D [cm] - Distance from the camera plane to an object (see image Measuring real-world object dimensions).
  • F [cm] - Width of image at the distance D.
With the use of the tan function, the following formulas can be obtained:
  • F = 2 * D * tan(HFOV/2)
  • Dv = (BL/2) * tan(90 - HFOV/2)
In order to obtain B, we can use tan function again (same as for F), but this time we must also multiply it by the ratio between W and F in order to convert units to pixels. That gives the following formula:
Python
1B = 2 * Dv * tan(HFOV/2) * W / F
2B = 2 * Dv * tan(HFOV/2) * W / (2 * D * tan(HFOV/2))
3B = W * Dv / D  # pixels
Example: If we are using OAK-D, which has a HFOV of 72°, a baseline (BL) of 7.5 cm and 640x400 (400P) resolution is used, therefore W = 640 and an object is D = 100 cm away, we can calculate B in the following way:
Command Line
1Dv = 7.5 / 2 * tan(90 - 72/2) = 3.75 * tan(54°) = 5.16 cm
2B = 640 * 5.16 / 100 = 33 # pixels
Credit for calculations and images goes to our community member gregflurry, which he made on this forum post.

Measuring real-world object dimensions

Because the depth map contains the Z distance, objects in parallel with the camera are measured accurately standard. For objects not in parallel, the Euclidean distance calculation can be used. Please refer to the below:When running eg. the RGB & MobilenetSSD with spatial data example, you could calculate the distance to the detected object from XYZ coordinates (SpatialImgDetections) using the code below (after code line 143 of the example):
Python
1distance = math.sqrt(detection.spatialCoordinates.x ** 2 + detection.spatialCoordinates.y ** 2 + detection.spatialCoordinates.z ** 2) # mm

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.