# IMU

IMU ([inertial measurement unit](https://en.wikipedia.org/wiki/Inertial_measurement_unit)) node can be used to receive data from
the IMU chip on the device.

Luxonis devices use different IMU stacks depending on platform generation:

 * RVC2 devices use either [BNO08X](https://docs.luxonis.com/hardware/platform/sensors/imu/bno08x.md) or
   [BMI270](https://docs.luxonis.com/hardware/platform/sensors/imu/bmi270.md)
 * RVC4 devices use [LSM6DSV](https://docs.luxonis.com/hardware/platform/sensors/imu/lsm6dsv.md) together with an
   [AK09919](https://docs.luxonis.com/hardware/platform/sensors/imu/ak09919.md) magnetometer.

The IMU chip is connected to the [RVC](https://docs.luxonis.com/hardware/platform/rvc/rvc2.md) over SPI. See [OAK Hardware
documentation](https://docs.luxonis.com/hardware.md) to check whether your OAK camera has IMU integrated.

> **Looking for the conceptual docs?**
> For sensor families, output semantics, reference frames, factory calibration, and noise characterization, see the [IMU hardware reference](https://docs.luxonis.com/hardware/platform/sensors/imu.md). For practical usage, see the IMU examples below.

## How to place it

#### Python

```python

pipeline = dai.Pipeline()
imu = pipeline.create(dai.node.IMU)
```

#### C++

```cpp

dai::Pipeline pipeline;
auto imu = pipeline.create<dai::node::IMU>();
```

## Inputs and Outputs

## Pipeline flow

The usual IMU node flow is:

 1. Create `dai::node::IMU`
 2. Enable one or more `IMUSensor` reports at a requested rate
 3. Configure batching with `setBatchReportThreshold()` and `setMaxBatchReports()`
 4. Consume `IMUData` packets from the host output queue

## Limitations

 * On RVC2 devices with BNO08X, gyroscope frequencies above 400 Hz can produce occasional jitter due to sensor hardware
   limitations.

## Requested report rate

`imu.enableIMUSensor(..., reportRate)` accepts a requested report rate in Hz.

Actual runtime behavior depends on the IMU and platform:

 * On RVC2 devices using BNO08X, requested rates round up to the next supported rate.
 * On RVC2 devices using BMI270, requested rates round down to the next supported rate. Requests above 400 Hz currently top out
   around 250 Hz.
 * On RVC4 devices using LSM6DSV + AK09919, treat validated runtime rates as platform-specific rather than assuming the silicon
   max ODR maps directly to the host stream rate.

For detailed per-sensor runtime behavior and hardware characteristics, see the [IMU hardware
reference](https://docs.luxonis.com/hardware/platform/sensors/imu.md).

### High-rate raw streaming used in examples

The current `depthai-core` IMU examples and tests use the following raw-stream rates for high-rate capture:

 * `ACCELEROMETER_RAW` at `480 Hz`
 * `GYROSCOPE_RAW` at `400 Hz`

## Batching

The IMU node batches packets before sending them to the host.

 * `setBatchReportThreshold(N)` sets the minimum number of IMU packets that should be ready before the device is allowed to send a
   batch
 * `setMaxBatchReports(M)` sets the maximum number of packets included in one batch

Higher batching can reduce host overhead and help when USB bandwidth or host scheduling becomes the bottleneck.

## Packet fields and report semantics

Each `IMUData` message contains one or more `IMUPacket` entries. Each packet only carries the fields for the reports that were
enabled in the node configuration.

Typical fields include:

 * `acceleroMeter`
 * `gyroscope`
 * `magneticField`
 * `rotationVector`

Use the report families like this:

 * `*_RAW`: direct sensor output in the sensor-native frame
 * `*_UNCALIBRATED`: rotated into the Luxonis RDF frame using `imuExtrinsics`, without IMU calibration parameters applied
 * `*_CALIBRATED`: rotated into the Luxonis RDF frame and corrected using IMU calibration parameters
 * fused outputs such as `ROTATION_VECTOR` and `GAME_ROTATION_VECTOR`: forwarded from the sensor's internal processing path

## Usage

#### Python

```python

pipeline = dai.Pipeline()
imu = pipeline.create(dai.node.IMU)

# enable ACCELEROMETER_RAW and GYROSCOPE_RAW at 100 hz rate
imu.enableIMUSensor([dai.IMUSensor.ACCELEROMETER_RAW, dai.IMUSensor.GYROSCOPE_RAW], 100)
# above this threshold packets will be sent in batch of X, if the host is not blocked and USB bandwidth is available
imu.setBatchReportThreshold(1)
# maximum number of IMU packets in a batch, if it's reached device will block sending until host can receive it
# if lower or equal to batchReportThreshold then the sending is always blocking on device
# useful to reduce device's CPU load  and number of lost packets, if CPU load is high on device side due to multiple nodes
imu.setMaxBatchReports(10)
```

#### C++

```cpp

dai::Pipeline pipeline;
auto imu = pipeline.create<dai::node::IMU>();

// enable ACCELEROMETER_RAW and GYROSCOPE_RAW at 100 hz rate
imu->enableIMUSensor({dai::IMUSensor::ACCELEROMETER_RAW, dai::IMUSensor::GYROSCOPE_RAW}, 100);
// above this threshold packets will be sent in batch of X, if the host is not blocked and USB bandwidth is available
imu->setBatchReportThreshold(1);
// maximum number of IMU packets in a batch, if it's reached device will block sending until host can receive it
// if lower or equal to batchReportThreshold then the sending is always blocking on device
// useful to reduce device's CPU load  and number of lost packets, if CPU load is high on device side due to multiple nodes
imu->setMaxBatchReports(10);
```

## Report availability by hardware

> **Current public API scope**
> The current `depthai-core` IMU enum and docstrings are still BNO08X-oriented. In the bindings, the node is still documented as `IMU node for BNO08X`, so fused and processed report coverage should be read together with the hardware docs and validated on the target device when the sensor path is not BNO08X.

| Report family | `IMUSensor` values | BNO08X | BMI270 | LSM6DSV | AK09919 | Notes |
| --- | --- | --- | --- | --- | --- | --- |
| Raw acceleration | `ACCELEROMETER_RAW` | Yes | Yes | Yes | No | Raw accelerometer stream |
| Accelerometer in Luxonis frame, without IMU calibration parameters | `ACCELEROMETER_UNCALIBRATED` | Yes | Yes | Yes | No | `RAW
-> UNCALIBRATED` applies `imuExtrinsics`. This is the unified IMU-frame accelerometer path. |
| Accelerometer in Luxonis frame, with IMU calibration parameters | `ACCELEROMETER_CALIBRATED` | Yes | Yes | Yes | No | Requires
IMU calibration parameters to be present in the runtime calibration payload. |
| Raw angular velocity | `GYROSCOPE_RAW` | Yes | Yes | Yes | No | Raw gyroscope stream |
| Gyroscope in Luxonis frame, without IMU calibration parameters | `GYROSCOPE_UNCALIBRATED` | Yes | Yes | Yes | No | `RAW ->
UNCALIBRATED` applies `imuExtrinsics`. On older devices this is expected to work out of the box. |
| Gyroscope in Luxonis frame, with IMU calibration parameters | `GYROSCOPE_CALIBRATED` | Yes | Yes | Yes | No | Requires IMU
calibration parameters to be present in the runtime calibration payload. |
| Raw magnetic field | `MAGNETOMETER_RAW` | Yes | No | No | Yes | On RVC4, raw magnetometer data comes from the AK09919 companion
sensor. |
| Processed magnetic field | `MAGNETOMETER_CALIBRATED`, `MAGNETOMETER_UNCALIBRATED` | Yes | No | No | Validate on target hardware
| Public enum/docstrings are still BNO08X-shaped for processed magnetometer outputs. |
| Derived acceleration outputs | `LINEAR_ACCELERATION`, `GRAVITY` | Yes | No | Validate on target hardware | No | BNO08X exposes
these directly. For non-BNO paths, validate availability on the target device and branch. |
| Fused orientation outputs | `ROTATION_VECTOR`, `GAME_ROTATION_VECTOR`, `GEOMAGNETIC_ROTATION_VECTOR`,
`ARVR_STABILIZED_ROTATION_VECTOR`, `ARVR_STABILIZED_GAME_ROTATION_VECTOR` | Yes | No | Validate on target hardware | No standalone
| These are sensor-fusion outputs, not host-side fusion done by the IMU node. |

## Calibration and extrinsics

Use `device.readCalibration()` to read the factory calibration payload from the device. Use `device.getCalibration()` and
`device.setCalibration()` when working with runtime calibration overrides.

For the processed inertial outputs, use this model:

 * `RAW -> UNCALIBRATED`: align the sensor-native frame into the Luxonis RDF frame using `imuExtrinsics`
 * `UNCALIBRATED -> CALIBRATED`: apply the accelerometer or gyroscope calibration set in the IMU calibration parameters
 * `ACCELEROMETER_UNCALIBRATED` and `GYROSCOPE_UNCALIBRATED` therefore share the unified IMU-frame path
 * `ACCELEROMETER_CALIBRATED` and `GYROSCOPE_CALIBRATED` add the runtime calibration correction on top of that

### Processed output transforms

#### RAW -> UNCALIBRATED

```python
import depthai as dai
import numpy as np

with dai.Pipeline() as pipeline:
    imu = pipeline.create(dai.node.IMU)
    imu.enableIMUSensor(dai.IMUSensor.ACCELEROMETER_RAW, 100)
    imu_q = imu.out.createOutputQueue(maxSize=10, blocking=False)

    device = pipeline.getDefaultDevice()
    calib = device.readCalibration()
    imu_to_cam = np.array(calib.getImuToCameraExtrinsics(dai.CameraBoardSocket.CAM_A, False))
    R_imu_to_cam = imu_to_cam[:3, :3]

    pipeline.start()
    pkt = imu_q.get().packets[0]
    raw = np.array([pkt.acceleroMeter.x, pkt.acceleroMeter.y, pkt.acceleroMeter.z])
    uncalibrated = R_imu_to_cam @ raw
```

#### UNCALIBRATED -> CALIBRATED

```python
import depthai as dai
import numpy as np

imu_calibration = [
    [1.0, 0.0, 0.0, 0.125],
    [0.0, 1.0, 0.0, 0.000],
    [0.0, 0.0, 1.0, 0.000],
]

with dai.Pipeline() as pipeline:
    imu = pipeline.create(dai.node.IMU)
    imu.enableIMUSensor(dai.IMUSensor.ACCELEROMETER_UNCALIBRATED, 100)
    imu_q = imu.out.createOutputQueue(maxSize=10, blocking=False)

    pipeline.start()
    pkt = imu_q.get().packets[0]
    uncalibrated = np.array([pkt.acceleroMeter.x, pkt.acceleroMeter.y, pkt.acceleroMeter.z])

    calibration = np.array(imu_calibration)
    calibrated = calibration[:, :3] @ uncalibrated + calibration[:, 3]
```

## Reading multiple IMU streams

If the target hardware exposes the selected reports, you can enable multiple IMU report families and read only the fields that
were requested.

#### Python

```python
import depthai as dai

with dai.Pipeline() as pipeline:
    imu = pipeline.create(dai.node.IMU)

    imu.enableIMUSensor(dai.IMUSensor.ACCELEROMETER_RAW, 100)
    imu.enableIMUSensor(dai.IMUSensor.GYROSCOPE_RAW, 100)
    imu.enableIMUSensor(dai.IMUSensor.MAGNETOMETER_RAW, 100)

    imu.setBatchReportThreshold(1)
    imu.setMaxBatchReports(10)

    imu_q = imu.out.createOutputQueue(maxSize=50, blocking=False)

    pipeline.start()
    while pipeline.isRunning():
        imu_data = imu_q.get()
        for pkt in imu_data.packets:
            a = pkt.acceleroMeter
            g = pkt.gyroscope
            m = pkt.magneticField
```

#### C++

```cpp
#include "depthai/depthai.hpp"

int main() {
    dai::Pipeline pipeline;
    auto imu = pipeline.create<dai::node::IMU>();

    imu->enableIMUSensor(dai::IMUSensor::ACCELEROMETER_RAW, 100);
    imu->enableIMUSensor(dai::IMUSensor::GYROSCOPE_RAW, 100);
    imu->enableIMUSensor(dai::IMUSensor::MAGNETOMETER_RAW, 100);

    imu->setBatchReportThreshold(1);
    imu->setMaxBatchReports(10);

    auto imuQ = imu->out.createOutputQueue(50, false);

    pipeline.start();
    while(pipeline.isRunning()) {
        auto data = imuQ->get<dai::IMUData>();
        for(const auto& pkt : data->packets) {
            const auto& a = pkt.acceleroMeter;
            const auto& g = pkt.gyroscope;
            const auto& m = pkt.magneticField;
        }
    }
}
```

## Examples of functionality

 * [IMU Accelerometer & Gyroscope](https://docs.luxonis.com/software-v3/depthai/examples/imu/imu_accelerometer_gyroscope.md)
 * [IMU Rotation Vector](article://software-v3.depthai.examples.imu_rotation_vector)
 * [IMU and Video Sync](article://software-v3.depthai.examples.imu_video_sync)

## Reference

### dai::node::IMU

Kind: class

IMU node for BNO08X.

#### Output out

Kind: variable

Outputs IMUData message that carries IMU packets.

#### Input mockIn

Kind: variable

Mock IMU data for replaying recorded data

#### void enableIMUSensor(IMUSensorConfig sensorConfig)

Kind: function

Enable a new IMU sensor with explicit configuration

#### void enableIMUSensor(const std::vector< IMUSensorConfig > & sensorConfigs)

Kind: function

Enable a list of IMU sensors with explicit configuration

#### void enableIMUSensor(IMUSensor sensor, uint32_t reportRate)

Kind: function

Enable a new IMU sensor with default configuration

#### void enableIMUSensor(const std::vector< IMUSensor > & sensors, uint32_t reportRate)

Kind: function

Enable a list of IMU sensors with default configuration

#### void setBatchReportThreshold(std::int32_t batchReportThreshold)

Kind: function

Above this packet threshold data will be sent to host, if queue is not blocked

#### std::int32_t getBatchReportThreshold()

Kind: function

Above this packet threshold data will be sent to host, if queue is not blocked

#### void setMaxBatchReports(std::int32_t maxBatchReports)

Kind: function

Maximum number of IMU packets in a batch report

#### std::int32_t getMaxBatchReports()

Kind: function

Maximum number of IMU packets in a batch report

#### void enableFirmwareUpdate(bool enable)

Kind: function

Whether to perform firmware update or not. Default value: false.

#### DeviceNodeCRTP()

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)

Kind: function

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.