DepthAI v2 has been superseded by DepthAI v3. You are viewing legacy documentation.

ON THIS PAGE

  • ImgFrame
  • Examples of functionality
  • Reference

ImgFrame

These are all the images (regardless of their encoding/format), as well as the depth/disparity "image". ColorCamera and MonoCamera are the source of the image frame messages.

Examples of functionality

Reference

class

depthai.ImgFrame(depthai.Buffer)

class
class
Type
Members:    YUV422i    YUV444p    YUV420p    YUV422p    YUV400p    RGBA8888    RGB161616    RGB888p    BGR888p    RGB888i    BGR888i    RGBF16F16F16p    BGRF16F16F16p    RGBF16F16F16i    BGRF16F16F16i    GRAY8    GRAYF16    LUT2    LUT4    LUT16    RAW16    RAW14    RAW12    RAW10    RAW8    PACK10    PACK12    YUV444i    NV12    NV21    BITSTREAM    HDR    NONE
method
method
getCategory(self) -> int: int
Retrieves image category
method
getColorTemperature(self) -> int: int
Retrieves white-balance color temperature of the light source, in kelvins
method
getCvFrame(self) -> typing.Any: typing.Any
Returns BGR or grayscale frame compatible with use in other opencv functions
method
method
getFrame(self, copy: bool = False) -> numpy.ndarray: numpy.ndarray
Returns numpy array with shape as specified by width, height and type
method
getHeight(self) -> int: int
Retrieves image height in pixels
method
getInstanceNum(self) -> int: int
Retrieves instance number
method
getLensPosition(self) -> int: int
Retrieves lens position, range 0..255. Returns -1 if not available
method
getLensPositionRaw(self) -> float: float
Retrieves lens position, range 0.0f..1.0f. Returns -1 if not available
method
getSensitivity(self) -> int: int
Retrieves sensitivity, as an ISO value
method
getSequenceNum(self) -> int: int
Retrieves sequence number
method
method
method
method
getWidth(self) -> int: int
Retrieves image width in pixels
method
setCategory(self, category: int) -> ImgFrame: ImgFrame
Parameter ``category``:     Image category
method
setFrame(self, array: numpy.ndarray)
Copies array bytes to ImgFrame buffer
method
setHeight(self, height: int) -> ImgFrame: ImgFrame
Specifies frame height  Parameter ``height``:     frame height
method
setInstanceNum(self, instance: int) -> ImgFrame: ImgFrame
Instance number relates to the origin of the frame (which camera)  Parameter ``instance``:     Instance number
method
setSequenceNum(self, seq: int) -> ImgFrame: ImgFrame
Specifies sequence number  Parameter ``seq``:     Sequence number
method
method
setTimestamp(self, timestamp: datetime.timedelta) -> ImgFrame: ImgFrame
Retrieves image timestamp related to dai::Clock::now()
method
setTimestampDevice(self, arg0: datetime.timedelta) -> ImgFrame: ImgFrame
Sets image timestamp related to dai::Clock::now()
method
setType(self, type: RawImgFrame.Type) -> ImgFrame: ImgFrame
Specifies frame type, RGB, BGR, ...  Parameter ``type``:     Type of image
method
setWidth(self, width: int) -> ImgFrame: ImgFrame
Specifies frame width  Parameter ``width``:     frame width
class

depthai.ImgFrame.Specs

class

depthai.ImgFrame.Type

variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
method
method
method
method
method
method
method
method
method
method
property
property

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.