StereoDepthConfig¶
This message is used to configure the StereoDepth node. With this message you can set filters, confidences, thresholds and mode of the StereoDepth node.
Examples of functionality¶
Reference¶
-
class
depthai.
StereoDepthConfig
StereoDepthConfig message.
-
class
CensusTransform
The basic cost function used by the Stereo Accelerator for matching the left and right images is the Census Transform. It works on a block of pixels and computes a bit vector which represents the structure of the image in that block. There are two types of Census Transform based on how the middle pixel is used: Classic Approach and Modified Census. The comparisons that are made between pixels can be or not thresholded. In some cases a mask can be applied to filter out only specific bits from the entire bit stream. All these approaches are: Classic Approach: Uses middle pixel to compare against all its neighbors over a defined window. Each comparison results in a new bit, that is 0 if central pixel is smaller, or 1 if is it bigger than its neighbor. Modified Census Transform: same as classic Census Transform, but instead of comparing central pixel with its neighbors, the window mean will be compared with each pixel over the window. Thresholding Census Transform: same as classic Census Transform, but it is not enough that a neighbor pixel to be bigger than the central pixel, it must be significant bigger (based on a threshold). Census Transform with Mask: same as classic Census Transform, but in this case not all of the pixel from the support window are part of the binary descriptor. We use a ma sk “M” to define which pixels are part of the binary descriptor (1), and which pixels should be skipped (0).
-
class
KernelSize
Census transform kernel size possible values.
Members:
AUTO :
KERNEL_5x5 :
KERNEL_7x7 :
KERNEL_7x9 :
-
property
name
-
property
-
property
enableMeanMode
If enabled, each pixel in the window is compared with the mean window value instead of the central pixel.
-
property
kernelMask
Census transform mask, default - auto, mask is set based on resolution and kernel size. Disabled for 400p input resolution. Enabled for 720p. 0XA82415 for 5x5 census transform kernel. 0XAA02A8154055 for 7x7 census transform kernel. 0X2AA00AA805540155 for 7x9 census transform kernel. Empirical values.
-
property
kernelSize
Census transform kernel size.
-
property
threshold
Census transform comparison threshold value.
-
class
-
class
CostAggregation
Cost Aggregation is based on Semi Global Block Matching (SGBM). This algorithm uses a semi global technique to aggregate the cost map. Ultimately the idea is to build inertia into the stereo algorithm. If a pixel has very little texture information, then odds are the correct disparity for this pixel is close to that of the previous pixel considered. This means that we get improved results in areas with low texture.
-
property
divisionFactor
Cost calculation linear equation parameters.
-
property
horizontalPenaltyCostP1
Horizontal P1 penalty cost parameter.
-
property
horizontalPenaltyCostP2
Horizontal P2 penalty cost parameter.
-
property
verticalPenaltyCostP1
Vertical P1 penalty cost parameter.
-
property
verticalPenaltyCostP2
Vertical P2 penalty cost parameter.
-
property
-
class
CostMatching
The matching cost is way of measuring the similarity of image locations in stereo correspondence algorithm. Based on the configuration parameters and based on the descriptor type, a linear equation is applied to computing the cost for each candidate disparity at each pixel.
-
class
DisparityWidth
Disparity search range: 64 or 96 pixels are supported by the HW.
Members:
DISPARITY_64 :
DISPARITY_96 :
-
property
name
-
property
-
class
LinearEquationParameters
The linear equation applied for computing the cost is: COMB_COST = α*AD + β*(CTC<<3). CLAMP(COMB_COST >> 5, threshold). Where AD is the Absolute Difference between 2 pixels values. CTC is the Census Transform Cost between 2 pixels, based on Hamming distance (xor). The α and β parameters are subject to fine tuning by the user.
-
property
confidenceThreshold
Disparities with confidence value under this threshold are accepted. Higher confidence threshold means disparities with less confidence are accepted too.
-
property
disparityWidth
Disparity search range, default 96 pixels.
-
property
enableCompanding
Disparity companding using sparse matching. Matching pixel by pixel for N disparities. Matching every 2nd pixel for M disparitites. Matching every 4th pixel for T disparities. In case of 96 disparities: N=48, M=32, T=16. This way the search range is extended to 176 disparities, by sparse matching. Note: when enabling this flag only depth map will be affected, disparity map is not.
-
property
invalidDisparityValue
Used only for debug purposes, SW postprocessing handled only invalid value of 0 properly.
-
property
linearEquationParameters
Cost calculation linear equation parameters.
-
class
-
class
MedianFilter
Median filter config for disparity post-processing
Members:
MEDIAN_OFF
KERNEL_3x3
KERNEL_5x5
KERNEL_7x7
-
property
name
-
property
-
class
PostProcessing
Post-processing filters, all the filters are applied in disparity domain.
-
class
DecimationFilter
Decimation filter. Reduces the depth scene complexity. The filter runs on kernel sizes [2x2] to [8x8] pixels.
-
class
DecimationMode
Decimation algorithm type.
Members:
PIXEL_SKIPPING :
NON_ZERO_MEDIAN :
NON_ZERO_MEAN :
-
property
name
-
property
-
property
decimationFactor
Decimation factor. Valid values are 1,2,3,4. Disparity/depth map x/y resolution will be decimated with this value.
-
property
decimationMode
Decimation algorithm type.
-
class
-
class
SpatialFilter
1D edge-preserving spatial filter using high-order domain transform.
-
property
alpha
The Alpha factor in an exponential moving average with Alpha=1 - no filter. Alpha = 0 - infinite filter. Determines the amount of smoothing.
-
property
delta
Step-size boundary. Establishes the threshold used to preserve “edges”. If the disparity value between neighboring pixels exceed the disparity threshold set by this delta parameter, then filtering will be temporarily disabled. Default value 0 means auto: 3 disparity integer levels. In case of subpixel mode it’s 3*number of subpixel levels.
-
property
enable
Whether to enable or disable the filter.
-
property
holeFillingRadius
An in-place heuristic symmetric hole-filling mode applied horizontally during the filter passes. Intended to rectify minor artefacts with minimal performance impact. Search radius for hole filling.
-
property
numIterations
Nubmer of iterations over the image in both horizontal and vertical direction.
-
property
-
class
SpeckleFilter
Speckle filtering. Removes speckle noise.
-
property
enable
Whether to enable or disable the filter.
-
property
speckleRange
Speckle search range.
-
property
-
class
TemporalFilter
Temporal filtering with optional persistence.
-
class
PersistencyMode
Persistency algorithm type.
Members:
PERSISTENCY_OFF :
VALID_8_OUT_OF_8 :
VALID_2_IN_LAST_3 :
VALID_2_IN_LAST_4 :
VALID_2_OUT_OF_8 :
VALID_1_IN_LAST_2 :
VALID_1_IN_LAST_5 :
VALID_1_IN_LAST_8 :
PERSISTENCY_INDEFINITELY :
-
property
name
-
property
-
property
alpha
The Alpha factor in an exponential moving average with Alpha=1 - no filter. Alpha = 0 - infinite filter. Determines the extent of the temporal history that should be averaged.
-
property
delta
Step-size boundary. Establishes the threshold used to preserve surfaces (edges). If the disparity value between neighboring pixels exceed the disparity threshold set by this delta parameter, then filtering will be temporarily disabled. Default value 0 means auto: 3 disparity integer levels. In case of subpixel mode it’s 3*number of subpixel levels.
-
property
enable
Whether to enable or disable the filter.
-
property
persistencyMode
Persistency mode. If the current disparity/depth value is invalid, it will be replaced by an older value, based on persistency mode.
-
class
-
class
ThresholdFilter
Threshold filtering. Filters out distances outside of a given interval.
-
property
maxRange
Maximum range in depth units. Depth values over this value are invalidated.
-
property
minRange
Minimum range in depth units. Depth values under this value are invalidated.
-
property
-
property
bilateralSigmaValue
Sigma value for bilateral filter. 0 means disabled. A larger value of the parameter means that farther colors within the pixel neighborhood will be mixed together.
-
property
decimationFilter
Decimation filter. Reduces disparity/depth map x/y complexity, reducing runtime complexity for other filters.
-
property
median
Set kernel size for disparity/depth median filtering, or disable
-
property
spatialFilter
This type of filter will smooth the depth noise while attempting to preserve edges.
- Type
Edge-preserving filtering
-
property
speckleFilter
Speckle filtering. Removes speckle noise.
-
property
temporalFilter
Temporal filtering with optional persistence.
-
property
thresholdFilter
Threshold filtering. Filters out distances outside of a given interval.
-
class
-
get
(self: depthai.StereoDepthConfig) → depthai.RawStereoDepthConfig Retrieve configuration data for StereoDepth.
- Returns
config for stereo depth algorithm
-
getBilateralFilterSigma
(self: depthai.StereoDepthConfig) → int Get sigma value for 5x5 bilateral filter
-
getConfidenceThreshold
(self: depthai.StereoDepthConfig) → int Get confidence threshold for disparity calculation
-
getData
(self: object) → numpy.ndarray[numpy.uint8] Get non-owning reference to internal buffer
- Returns
Reference to internal buffer
-
getDepthUnit
(self: depthai.StereoDepthConfig) → depthai.RawStereoDepthConfig.AlgorithmControl.DepthUnit Get depth unit of depth map.
-
getLeftRightCheckThreshold
(self: depthai.StereoDepthConfig) → int Get threshold for left-right check combine
-
getMaxDisparity
(self: depthai.StereoDepthConfig) → float Useful for normalization of the disparity map.
- Returns
Maximum disparity value that the node can return
-
getMedianFilter
(self: depthai.StereoDepthConfig) → depthai.MedianFilter Get median filter setting
-
getRaw
(self: depthai.ADatatype) → depthai.RawBuffer
-
set
(self: depthai.StereoDepthConfig, config: depthai.RawStereoDepthConfig) → depthai.StereoDepthConfig Set explicit configuration.
- Parameter
config
: Explicit configuration
- Parameter
-
setBilateralFilterSigma
(self: depthai.StereoDepthConfig, sigma: int) → depthai.StereoDepthConfig A larger value of the parameter means that farther colors within the pixel neighborhood will be mixed together, resulting in larger areas of semi-equal color.
- Parameter
sigma
: Set sigma value for 5x5 bilateral filter. 0..65535
- Parameter
-
setConfidenceThreshold
(self: depthai.StereoDepthConfig, confThr: int) → depthai.StereoDepthConfig Confidence threshold for disparity calculation
- Parameter
confThr
: Confidence threshold value 0..255
- Parameter
-
setData
(*args, **kwargs) Overloaded function.
setData(self: depthai.Buffer, arg0: List[int]) -> None
- Parameter
data
: Copies data to internal buffer
setData(self: depthai.Buffer, arg0: numpy.ndarray[numpy.uint8]) -> None
- Parameter
data
: Copies data to internal buffer
-
setDepthAlign
(self: depthai.StereoDepthConfig, align: depthai.RawStereoDepthConfig.AlgorithmControl.DepthAlign) → depthai.StereoDepthConfig - Parameter
align
: Set the disparity/depth alignment: centered (between the ‘left’ and ‘right’ inputs), or from the perspective of a rectified output stream
- Parameter
-
setDepthUnit
(self: depthai.StereoDepthConfig, arg0: depthai.RawStereoDepthConfig.AlgorithmControl.DepthUnit) → depthai.StereoDepthConfig Set depth unit of depth map.
Meter, centimeter, millimeter, inch, foot or custom unit is available.
-
setExtendedDisparity
(self: depthai.StereoDepthConfig, enable: bool) → depthai.StereoDepthConfig Disparity range increased from 95 to 190, combined from full resolution and downscaled images. Suitable for short range objects
-
setLeftRightCheck
(self: depthai.StereoDepthConfig, enable: bool) → depthai.StereoDepthConfig Computes and combines disparities in both L-R and R-L directions, and combine them.
For better occlusion handling, discarding invalid disparity values
-
setLeftRightCheckThreshold
(self: depthai.StereoDepthConfig, sigma: int) → depthai.StereoDepthConfig - Parameter
threshold
: Set threshold for left-right, right-left disparity map combine, 0..255
- Parameter
-
setMedianFilter
(self: depthai.StereoDepthConfig, median: depthai.MedianFilter) → depthai.StereoDepthConfig - Parameter
median
: Set kernel size for disparity/depth median filtering, or disable
- Parameter
-
setSubpixel
(self: depthai.StereoDepthConfig, enable: bool) → depthai.StereoDepthConfig Computes disparity with sub-pixel interpolation (3 fractional bits by default).
Suitable for long range. Currently incompatible with extended disparity
-
setSubpixelFractionalBits
(self: depthai.StereoDepthConfig, subpixelFractionalBits: int) → depthai.StereoDepthConfig Number of fractional bits for subpixel mode. Default value: 3. Valid values: 3,4,5. Defines the number of fractional disparities: 2^x. Median filter postprocessing is supported only for 3 fractional bits.
-
class
-
class
dai
::
StereoDepthConfig
: public dai::Buffer¶ StereoDepthConfig message.
Public Types
-
using
MedianFilter
= dai::MedianFilter¶
-
using
AlgorithmControl
= RawStereoDepthConfig::AlgorithmControl¶
-
using
PostProcessing
= RawStereoDepthConfig::PostProcessing¶
-
using
CensusTransform
= RawStereoDepthConfig::CensusTransform¶
-
using
CostMatching
= RawStereoDepthConfig::CostMatching¶
-
using
CostAggregation
= RawStereoDepthConfig::CostAggregation¶
Public Functions
-
StereoDepthConfig
()¶ Construct StereoDepthConfig message.
-
~StereoDepthConfig
() = default¶
-
StereoDepthConfig &
setDepthAlign
(AlgorithmControl::DepthAlign align)¶ - Parameters
align
: Set the disparity/depth alignment: centered (between the ‘left’ and ‘right’ inputs), or from the perspective of a rectified output stream
-
StereoDepthConfig &
setConfidenceThreshold
(int confThr)¶ Confidence threshold for disparity calculation
- Parameters
confThr
: Confidence threshold value 0..255
-
int
getConfidenceThreshold
() const¶ Get confidence threshold for disparity calculation
-
StereoDepthConfig &
setMedianFilter
(MedianFilter median)¶ - Parameters
median
: Set kernel size for disparity/depth median filtering, or disable
-
MedianFilter
getMedianFilter
() const¶ Get median filter setting
-
StereoDepthConfig &
setBilateralFilterSigma
(uint16_t sigma)¶ A larger value of the parameter means that farther colors within the pixel neighborhood will be mixed together, resulting in larger areas of semi-equal color.
- Parameters
sigma
: Set sigma value for 5x5 bilateral filter. 0..65535
-
uint16_t
getBilateralFilterSigma
() const¶ Get sigma value for 5x5 bilateral filter
-
StereoDepthConfig &
setLeftRightCheckThreshold
(int threshold)¶ - Parameters
threshold
: Set threshold for left-right, right-left disparity map combine, 0..255
-
int
getLeftRightCheckThreshold
() const¶ Get threshold for left-right check combine
-
StereoDepthConfig &
setLeftRightCheck
(bool enable)¶ Computes and combines disparities in both L-R and R-L directions, and combine them.
For better occlusion handling, discarding invalid disparity values
-
StereoDepthConfig &
setExtendedDisparity
(bool enable)¶ Disparity range increased from 95 to 190, combined from full resolution and downscaled images. Suitable for short range objects
-
StereoDepthConfig &
setSubpixel
(bool enable)¶ Computes disparity with sub-pixel interpolation (3 fractional bits by default).
Suitable for long range. Currently incompatible with extended disparity
-
StereoDepthConfig &
setSubpixelFractionalBits
(int subpixelFractionalBits)¶ Number of fractional bits for subpixel mode. Default value: 3. Valid values: 3,4,5. Defines the number of fractional disparities: 2^x. Median filter postprocessing is supported only for 3 fractional bits.
-
StereoDepthConfig &
setDepthUnit
(AlgorithmControl::DepthUnit depthUnit)¶ Set depth unit of depth map.
Meter, centimeter, millimeter, inch, foot or custom unit is available.
-
AlgorithmControl::DepthUnit
getDepthUnit
()¶ Get depth unit of depth map.
-
float
getMaxDisparity
() const¶ Useful for normalization of the disparity map.
- Return
Maximum disparity value that the node can return
-
StereoDepthConfig &
set
(dai::RawStereoDepthConfig config)¶ Set explicit configuration.
- Parameters
config
: Explicit configuration
-
dai::RawStereoDepthConfig
get
() const¶ Retrieve configuration data for StereoDepth.
- Return
config for stereo depth algorithm
Private Members
-
using
Got questions?
We’re always happy to help with code or other questions you might have.