Camera 高帧率 (HFR)
Supported on:RVC4
3.4.0 中的高帧率 (HFR) 模式在配备 RVC4 平台和 IMX586 传感器的 OAK4 设备上实现了超快速感知。这些管道可以捕获和处理高达 480 FPS 的数据,包括对每一帧进行神经网络推理。预览功能
HFR 模式是 DepthAI
3.4.0 中的早期预览功能。当前模式固定为 1920x1080 @ 240 FPS 和 1280x720 @ 480 FPS。HFR 的重要性
- 以更少的运动模糊捕获快速运动。
- 以全吞吐量对每一帧运行神经网络推理。
- 降低闭环系统的端到端感知延迟。
支持的 HFR 模式
| 分辨率 | 帧率 |
|---|---|
| 1920 x 1080 | 240 FPS |
| 1280 x 720 | 480 FPS |
示例应用
- 具有快速零件移动的工业自动化。
- 需要更快控制循环的机器人工作负载。
- 体育分析和高速运动跟踪。
- 高速视觉检测系统。
包含的示例管道
Object Detection
Run YOLOv6 with HFR input at up to 480 FPS.
Small Live Preview
Display a lightweight preview stream at 240/480 FPS.
Video Encoding
Encode and save high-frame-rate video streams.
源代码
高帧率目标检测 (YOLOv6)
Python
PythonGitHub
1#!/usr/bin/env python3
2import depthai as dai
3import sys
4
5FPS = 480
6
7with dai.Pipeline() as pipeline:
8 device = pipeline.getDefaultDevice()
9 platform = device.getPlatform()
10 if platform != dai.Platform.RVC4:
11 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
12 sys.exit(0)
13
14 # Exit cleanly if the selected HFR mode is not advertised by CAM_A.
15 supportsRequestedFps = False
16 for cameraFeature in device.getConnectedCameraFeatures():
17 if cameraFeature.socket != dai.CameraBoardSocket.CAM_A:
18 continue
19 for config in cameraFeature.configs:
20 if config.width == 1280 and config.height == 720 and config.maxFps >= FPS:
21 supportsRequestedFps = True
22 break
23 break
24 if not supportsRequestedFps:
25 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
26 sys.exit(0)
27
28 # Download the model
29 nnArchivePath = dai.getModelFromZoo(dai.NNModelDescription("yolov6-nano", platform="RVC4"))
30 nnArchive = dai.NNArchive(nnArchivePath)
31 inputSize = nnArchive.getInputSize()
32 cameraNode = pipeline.create(dai.node.Camera).build()
33
34 # Configure the ImageManip as in HFR mode requesting arbitrary outputs is not yet supported
35 cameraOutput = cameraNode.requestOutput((1280, 720), fps=FPS)
36 imageManip = pipeline.create(dai.node.ImageManip)
37 imageManip.initialConfig.setOutputSize(inputSize[0], inputSize[1])
38 imageManip.setMaxOutputFrameSize(int(inputSize[0] * inputSize[1] * 3))
39 imageManip.initialConfig.setFrameType(dai.ImgFrame.Type.BGR888i)
40 imageManip.inputImage.setMaxSize(12)
41 cameraOutput.link(imageManip.inputImage)
42
43 # Configure the DetectionNetwork
44 detectionNetwork = pipeline.create(dai.node.DetectionNetwork)
45 detectionNetwork.setNNArchive(nnArchive)
46 imageManip.out.link(detectionNetwork.input)
47
48 benchmarkIn = pipeline.create(dai.node.BenchmarkIn)
49 benchmarkIn.setRunOnHost(True)
50 benchmarkIn.sendReportEveryNMessages(FPS)
51 detectionNetwork.out.link(benchmarkIn.input)
52
53
54 qDet = detectionNetwork.out.createOutputQueue()
55 pipeline.start()
56
57 while pipeline.isRunning():
58 inDet: dai.ImgDetections = qDet.get()
59 # print(f"Got {len(inDet.detections)} nn detections ")小型实时预览
Python
PythonGitHub
1#!/usr/bin/env python3
2import depthai as dai
3import sys
4import time
5import cv2
6
7SIZE = (1280, 720)
8FPS = 480
9
10# SIZE = (1920, 1080)
11# FPS = 240
12
13with dai.Pipeline() as pipeline:
14 device = pipeline.getDefaultDevice()
15 platform = device.getPlatform()
16 if platform != dai.Platform.RVC4:
17 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
18 sys.exit(0)
19
20 # Exit cleanly if the selected HFR mode is not advertised by CAM_A.
21 supportsRequestedFps = False
22 for cameraFeature in device.getConnectedCameraFeatures():
23 if cameraFeature.socket != dai.CameraBoardSocket.CAM_A:
24 continue
25 for config in cameraFeature.configs:
26 if config.width == SIZE[0] and config.height == SIZE[1] and config.maxFps >= FPS:
27 supportsRequestedFps = True
28 break
29 break
30 if not supportsRequestedFps:
31 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
32 sys.exit(0)
33
34 cam = pipeline.create(dai.node.Camera).build()
35 benchmarkIn = pipeline.create(dai.node.BenchmarkIn)
36 benchmarkIn.setRunOnHost(True)
37 benchmarkIn.sendReportEveryNMessages(FPS)
38
39 imageManip = pipeline.create(dai.node.ImageManip)
40 imageManip.initialConfig.setOutputSize(250, 250)
41 imageManip.setMaxOutputFrameSize(int(250* 250 * 1.6))
42
43 # One of the two modes can be selected
44 # NOTE: Generic resolutions are not yet supported through camera node when using HFR mode
45 output = cam.requestOutput(SIZE, fps=FPS)
46
47 output.link(imageManip.inputImage)
48 imageManip.out.link(benchmarkIn.input)
49
50 outputQueue = imageManip.out.createOutputQueue()
51
52 pipeline.start()
53 while pipeline.isRunning():
54 imgFrame = outputQueue.get()
55 assert isinstance(imgFrame, dai.ImgFrame)
56 cv2.imshow("frame", imgFrame.getCvFrame())
57 cv2.waitKey(1)保存编码流
Python
PythonGitHub
1import depthai as dai
2
3# Capture Ctrl+C and set a flag to stop the loop
4import time
5import cv2
6import threading
7import signal
8import sys
9
10PROFILE = dai.VideoEncoderProperties.Profile.H264_MAIN
11
12quitEvent = threading.Event()
13signal.signal(signal.SIGTERM, lambda *_args: quitEvent.set())
14signal.signal(signal.SIGINT, lambda *_args: quitEvent.set())
15
16SIZE = (1280, 720)
17FPS = 480
18
19# SIZE = (1920, 1080)
20# FPS = 240
21
22class VideoSaver(dai.node.HostNode):
23 def __init__(self, *args, **kwargs):
24 dai.node.HostNode.__init__(self, *args, **kwargs)
25 self.file_handle = open('video_hfr.encoded', 'wb')
26
27 def build(self, *args):
28 self.link_args(*args)
29 return self
30
31 def process(self, frame):
32 frame.getData().tofile(self.file_handle)
33
34with dai.Pipeline() as pipeline:
35 device = pipeline.getDefaultDevice()
36 platform = device.getPlatform()
37 if platform != dai.Platform.RVC4:
38 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
39 sys.exit(0)
40
41 # Exit cleanly if the selected HFR mode is not advertised by CAM_A.
42 supportsRequestedFps = False
43 for cameraFeature in device.getConnectedCameraFeatures():
44 if cameraFeature.socket != dai.CameraBoardSocket.CAM_A:
45 continue
46 for config in cameraFeature.configs:
47 if config.width == SIZE[0] and config.height == SIZE[1] and config.maxFps >= FPS:
48 supportsRequestedFps = True
49 break
50 break
51 if not supportsRequestedFps:
52 print("This example is only supported on IMX586 and Luxonis OS 1.20.5 or higher", file=sys.stderr)
53 sys.exit(0)
54
55 camRgb = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_A)
56 output = camRgb.requestOutput(SIZE, fps=FPS)
57
58 # ImageManip is added to workaround a limitation with VideoEncoder with native resolutions
59 # This limitation will be lifted in the future
60 imageManip = pipeline.create(dai.node.ImageManip)
61 imageManip.initialConfig.setOutputSize(SIZE[0], SIZE[1] + 10) # To avoid a passthrough
62 imageManip.setMaxOutputFrameSize(int(SIZE[0] * (SIZE[1] + 10) * 1.6))
63 imageManip.inputImage.setMaxSize(12)
64 output.link(imageManip.inputImage)
65 output = imageManip.out
66
67 benchmarkIn = pipeline.create(dai.node.BenchmarkIn)
68 benchmarkIn.setRunOnHost(True)
69
70 encoded = pipeline.create(dai.node.VideoEncoder).build(output,
71 frameRate = FPS,
72 profile = PROFILE)
73 encoded.out.link(benchmarkIn.input)
74 saver = pipeline.create(VideoSaver).build(encoded.out)
75
76 pipeline.start()
77 print("Started to save video to video.encoded")
78 print("Press Ctrl+C to stop")
79 timeStart = time.monotonic()
80 while pipeline.isRunning() and not quitEvent.is_set():
81 time.sleep(1)
82 pipeline.stop()
83 pipeline.wait()
84 saver.file_handle.close()
85
86print("To view the encoded data, convert the stream file (.encoded) into a video file (.mp4) using a command below:")
87print(f"ffmpeg -framerate {FPS} -i video_hfr.encoded -c copy video_hfr.mp4")
88
89print("If the FPS is not set correctly, you can ask ffmpeg to generate it with the command below")
90
91print(f"""
92ffmpeg -fflags +genpts -r {FPS} -i video_hfr.encoded \\
93 -vsync cfr -fps_mode cfr \\
94 -video_track_timescale {FPS}00 \\
95 -c:v copy \\
96 video_hfr.mp4
97""")需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。