Buffer¶
Just a good old buffer. All other messages derive from the Buffer
class.
Reference¶
-
class
depthai.
Buffer
Base message - buffer of binary data
-
getData
(self: object) → numpy.ndarray[numpy.uint8] Get non-owning reference to internal buffer
- Returns
Reference to internal buffer
-
getRaw
(self: depthai.ADatatype) → depthai.RawBuffer
-
getSequenceNum
(self: depthai.Buffer) → int Retrieves sequence number
-
getTimestamp
(self: depthai.Buffer) → datetime.timedelta Retrieves timestamp related to dai::Clock::now()
-
getTimestampDevice
(self: depthai.Buffer) → datetime.timedelta Retrieves timestamp directly captured from device’s monotonic clock, not synchronized to host time. Used mostly for debugging
-
setData
(*args, **kwargs) Overloaded function.
setData(self: depthai.Buffer, arg0: List[int]) -> None
- Parameter
data
: Copies data to internal buffer
setData(self: depthai.Buffer, arg0: numpy.ndarray[numpy.uint8]) -> None
- Parameter
data
: Copies data to internal buffer
-
setSequenceNum
(self: depthai.Buffer, arg0: int) → depthai.Buffer Retrieves sequence number
-
setTimestamp
(self: depthai.Buffer, arg0: datetime.timedelta) → depthai.Buffer Sets timestamp related to dai::Clock::now()
-
setTimestampDevice
(self: depthai.Buffer, arg0: datetime.timedelta) → depthai.Buffer Sets timestamp related to dai::Clock::now()
-
-
class
dai
::
Buffer
: public dai::ADatatype¶ Base message - buffer of binary data.
Subclassed by dai::AprilTagConfig, dai::AprilTags, dai::CameraControl, dai::EdgeDetectorConfig, dai::EncodedFrame, dai::FeatureTrackerConfig, dai::ImageManipConfig, dai::ImgDetections, dai::ImgFrame, dai::IMUData, dai::MessageGroup, dai::NNData, dai::PointCloudConfig, dai::PointCloudData, dai::SpatialImgDetections, dai::SpatialLocationCalculatorConfig, dai::SpatialLocationCalculatorData, dai::StereoDepthConfig, dai::SystemInformation, dai::ToFConfig, dai::TrackedFeatures, dai::Tracklets
Public Functions
-
~Buffer
() = default¶
-
std::vector<std::uint8_t> &
getData
() const¶ Get non-owning reference to internal buffer.
- Return
Reference to internal buffer
-
void
setData
(const std::vector<std::uint8_t> &data)¶ - Parameters
data
: Copies data to internal buffer
-
void
setData
(std::vector<std::uint8_t> &&data)¶ - Parameters
data
: Moves data to internal buffer
-
std::chrono::time_point<std::chrono::steady_clock, std::chrono::steady_clock::duration>
getTimestamp
() const¶ Retrieves timestamp related to dai::Clock::now()
-
std::chrono::time_point<std::chrono::steady_clock, std::chrono::steady_clock::duration>
getTimestampDevice
() const¶ Retrieves timestamp directly captured from device’s monotonic clock, not synchronized to host time. Used mostly for debugging
-
int64_t
getSequenceNum
() const¶ Retrieves sequence number
-
Buffer &
setTimestamp
(std::chrono::time_point<std::chrono::steady_clock, std::chrono::steady_clock::duration> timestamp)¶ Sets timestamp related to dai::Clock::now()
-