Device information¶
This example shows how you can query device information.
The first part of the code queries all available devices without actually booting any device. For each found device, it prints the following information:
Device name: Either IP, in case of OAK PoE cameras, or USB path in case of OAK USB cameras
MxId: Unique Mx (chip) identification code
State: State of the device. Note that OAK PoE cameras have bootloader flashed which initializes the network stack
Afterwards, the example boots into the first found device and prints available camera sensors, and reads calibration and eeprom data which stores product and board names.
Demo¶
Searching for all available devices...
Found device '1.3', MxId: '18443010D116631200', State: 'UNBOOTED'
Found device '192.168.33.201', MxId: '184430102163DB0F00', State: 'BOOTLOADER'
Found device '192.168.33.192', MxId: '1844301011F4C51200', State: 'BOOTLOADER'
Booting the first available camera (1.3)...
Available camera sensors: {<CameraBoardSocket.CAM_C: 2>: 'OV9282', <CameraBoardSocket.CAM_A: 0>: 'IMX378', <CameraBoardSocket.CAM_B: 1>: 'OV9282'}
Product name: OAK-D Pro AF, board name DM9098
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 | import depthai as dai from typing import List print('Searching for all available devices...\n') # Query all available devices (USB and POE OAK cameras) infos: List[dai.DeviceInfo] = dai.DeviceBootloader.getAllAvailableDevices() if len(infos) == 0: print("Couldn't find any available devices.") exit(-1) for info in infos: # Converts enum eg. 'XLinkDeviceState.X_LINK_UNBOOTED' to 'UNBOOTED' state = str(info.state).split('X_LINK_')[1] print(f"Found device '{info.name}', MxId: '{info.mxid}', State: '{state}'") # Connect to a specific device. We will just take the first one print(f"\nBooting the first available camera ({infos[0].name})...") with dai.Device(dai.Pipeline(), infos[0], usb2Mode=False) as device: print("Available camera sensors: ", device.getCameraSensorNames()) calib = device.readCalibration() eeprom = calib.getEepromData() print(f"Product name: {eeprom.productName}, board name {eeprom.boardName}") |
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 | #include <iostream> // Includes common necessary includes for development using depthai library #include "depthai/depthai.hpp" int main() { std::cout << "Searching for all available devices...\n\n"; auto infos = dai::Device::getAllAvailableDevices(); if(infos.size() <= 0) { std::cout << "Couldn't find any available devices.\n"; return -1; } for(auto& info : infos) { std::cout << "Found device: " << info.name << " mxid: " << info.mxid << " state: " << info.state << std::endl; } // Connect to device and start pipeline std::cout << "\nBooting the first available camera (" << infos[0].name << ")...\n"; dai::Device device(dai::Pipeline(), infos[0]); std::cout << "Available camera sensors: "; for(auto& sensor : device.getCameraSensorNames()) { std::cout << "Socket: " << sensor.first << " - " << sensor.second << ", "; } std::cout << std::endl; auto eeprom = device.readCalibration2().getEepromData(); std::cout << "Product name: " << eeprom.productName << ", board name: " << eeprom.boardName << std::endl; return 0; } |