MonoCamera¶
MonoCamera node is a source of image frames. You can control in at runtime with the inputControl
. Some DepthAI modules don’t
have mono camera(s). Two mono cameras are used to calculate stereo depth (with StereoDepth node).
How to place it¶
pipeline = dai.Pipeline()
mono = pipeline.create(dai.node.MonoCamera)
dai::Pipeline pipeline;
auto mono = pipeline.create<dai::node::MonoCamera>();
Inputs and Outputs¶
┌─────────────────┐
│ │ out
inputControl │ ├───────────►
──────────────►│ MonoCamera | raw
│ ├───────────►
│ │
└─────────────────┘
Message types
inputControl
- CameraControlout
- ImgFrameraw
- ImgFrame - RAW10 data. Demo code for unpacking here (for ColorCamera)
Usage¶
pipeline = dai.Pipeline()
mono = pipeline.create(dai.node.MonoCamera)
mono.setCamera("right")
mono.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
dai::Pipeline pipeline;
auto mono = pipeline.create<dai::node::MonoCamera>();
mono->setCamera("right");
mono->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
Examples of functionality¶
Reference¶
-
class
depthai.node.
MonoCamera
MonoCamera node. For use with grayscale sensors.
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.MonoCameraProperties
-
property
frameEvent
Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getBoardSocket
(self: depthai.node.MonoCamera) → depthai.CameraBoardSocket Retrieves which board socket to use
- Returns
Board socket to use
-
getCamId
(self: depthai.node.MonoCamera) → int
-
getCamera
(self: depthai.node.MonoCamera) → str Retrieves which camera to use by name
- Returns
Name of the camera to use
-
getFps
(self: depthai.node.MonoCamera) → float Get rate at which camera should produce frames
- Returns
Rate in frames per second
-
getFrameEventFilter
(self: depthai.node.MonoCamera) → List[depthai.FrameEvent]
-
getImageOrientation
(self: depthai.node.MonoCamera) → depthai.CameraImageOrientation Get camera image orientation
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getNumFramesPool
(self: depthai.node.MonoCamera) → int Get number of frames in main (ISP output) pool
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
getRawNumFramesPool
(self: depthai.node.MonoCamera) → int Get number of frames in raw pool
-
getResolution
(self: depthai.node.MonoCamera) → depthai.MonoCameraProperties.SensorResolution Get sensor resolution
-
getResolutionHeight
(self: depthai.node.MonoCamera) → int Get sensor resolution height
-
getResolutionSize
(self: depthai.node.MonoCamera) → Tuple[int, int] Get sensor resolution as size
-
getResolutionWidth
(self: depthai.node.MonoCamera) → int Get sensor resolution width
-
property
id
Id of node
-
property
initialControl
Initial control options to apply to sensor
-
property
inputControl
Input for CameraControl message, which can modify camera parameters in runtime Default queue is blocking with size 8
-
property
out
Outputs ImgFrame message that carries RAW8 encoded (grayscale) frame data.
Suitable for use StereoDepth node. Processed by ISP
-
property
raw
Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor
-
setBoardSocket
(self: depthai.node.MonoCamera, boardSocket: depthai.CameraBoardSocket) → None Specify which board socket to use
- Parameter
boardSocket
: Board socket to use
- Parameter
-
setCamId
(self: depthai.node.MonoCamera, arg0: int) → None
-
setCamera
(self: depthai.node.MonoCamera, name: str) → None Specify which camera to use by name
- Parameter
name
: Name of the camera to use
- Parameter
-
setFps
(self: depthai.node.MonoCamera, fps: float) → None Set rate at which camera should produce frames
- Parameter
fps
: Rate in frames per second
- Parameter
-
setFrameEventFilter
(self: depthai.node.MonoCamera, events: List[depthai.FrameEvent]) → None
-
setImageOrientation
(self: depthai.node.MonoCamera, imageOrientation: depthai.CameraImageOrientation) → None Set camera image orientation
-
setIsp3aFps
(self: depthai.node.MonoCamera, arg0: int) → None Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
setNumFramesPool
(self: depthai.node.MonoCamera, arg0: int) → None Set number of frames in main (ISP output) pool
-
setRawNumFramesPool
(self: depthai.node.MonoCamera, arg0: int) → None Set number of frames in raw pool
-
setRawOutputPacked
(self: depthai.node.MonoCamera, packed: bool) → None Configures whether the camera raw frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
-
setResolution
(self: depthai.node.MonoCamera, resolution: depthai.MonoCameraProperties.SensorResolution) → None Set sensor resolution
-
class
-
class
dai::node
::
MonoCamera
: public dai::NodeCRTP<Node, MonoCamera, MonoCameraProperties>¶ MonoCamera node. For use with grayscale sensors.
Public Functions
-
void
setBoardSocket
(CameraBoardSocket boardSocket)¶ Specify which board socket to use
- Parameters
boardSocket
: Board socket to use
-
CameraBoardSocket
getBoardSocket
() const¶ Retrieves which board socket to use
- Return
Board socket to use
-
void
setCamera
(std::string name)¶ Specify which camera to use by name
- Parameters
name
: Name of the camera to use
-
std::string
getCamera
() const¶ Retrieves which camera to use by name
- Return
Name of the camera to use
-
void
setCamId
(int64_t id)¶
-
int64_t
getCamId
() const¶
-
void
setImageOrientation
(CameraImageOrientation imageOrientation)¶ Set camera image orientation.
-
CameraImageOrientation
getImageOrientation
() const¶ Get camera image orientation.
-
void
setResolution
(Properties::SensorResolution resolution)¶ Set sensor resolution.
-
Properties::SensorResolution
getResolution
() const¶ Get sensor resolution.
-
void
setFrameEventFilter
(const std::vector<dai::FrameEvent> &events)¶
-
std::vector<dai::FrameEvent>
getFrameEventFilter
() const¶
-
void
setFps
(float fps)¶ Set rate at which camera should produce frames
- Parameters
fps
: Rate in frames per second
-
void
setIsp3aFps
(int isp3aFps)¶ Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
float
getFps
() const¶ Get rate at which camera should produce frames
- Return
Rate in frames per second
-
std::tuple<int, int>
getResolutionSize
() const¶ Get sensor resolution as size.
-
int
getResolutionWidth
() const¶ Get sensor resolution width.
-
int
getResolutionHeight
() const¶ Get sensor resolution height.
-
void
setNumFramesPool
(int num)¶ Set number of frames in main (ISP output) pool.
-
void
setRawNumFramesPool
(int num)¶ Set number of frames in raw pool.
-
int
getNumFramesPool
() const¶ Get number of frames in main (ISP output) pool.
-
int
getRawNumFramesPool
() const¶ Get number of frames in raw pool.
-
void
setRawOutputPacked
(bool packed)¶ Configures whether the camera
raw
frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false
), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
Public Members
-
CameraControl
initialControl
¶ Initial control options to apply to sensor
-
Input
inputControl
= {*this, "inputControl", Input::Type::SReceiver, true, 8, {{DatatypeEnum::CameraControl, false}}}¶ Input for CameraControl message, which can modify camera parameters in runtime Default queue is blocking with size 8
-
Output
out
= {*this, "out", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries RAW8 encoded (grayscale) frame data.
Suitable for use StereoDepth node. Processed by ISP
-
Output
raw
= {*this, "raw", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor
-
Output
frameEvent
= {*this, "frameEvent", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
Public Static Attributes
-
static constexpr const char *
NAME
= "MonoCamera"¶
Private Members
-
std::shared_ptr<RawCameraControl>
rawControl
¶
-
void