SPIIn¶
SPIIn node is used for receiving data that was sent from a MCU (via SPI). You can find demos here.
This allows you for example to control eg. ColorCamera or ImageManip from the MCU or send a Buffer of data from the MCU to a Script node.
SPIOut is used for sending data from the VPU to a MCU (via SPI).
How to place it¶
pipeline = dai.Pipeline()
spi = pipeline.create(dai.node.SPIIn)
dai::Pipeline pipeline;
auto spi = pipeline.create<dai::node::SPIIn>();
Inputs and Outputs¶
┌─────────────┐
SPI │ │
(from MCU) | │ out
----------►│ SPIIn ├─────────►
│ │
│ │
└─────────────┘
Message types
out
-Any
Usage¶
pipeline = dai.Pipeline()
spi = pipeline.create(dai.node.SPIIn)
spi.setStreamName("control")
spi.setBusId(0)
dai::Pipeline pipeline;
auto spi = pipeline.create<dai::node::SPIIn>();
spi->setStreamName("control");
spi->setBusId(0);
Examples of functionality¶
Reference¶
-
class
depthai.node.
SPIIn
SPIIn node. Receives messages over SPI.
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.SPIInProperties
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getBusId
(self: depthai.node.SPIIn) → int Get bus id
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getMaxDataSize
(self: depthai.node.SPIIn) → int Get maximum messages size in bytes
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getNumFrames
(self: depthai.node.SPIIn) → int Get number of frames in pool
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
getStreamName
(self: depthai.node.SPIIn) → str Get stream name
-
property
id
Id of node
-
property
out
Outputs message of same type as send from host.
-
setBusId
(self: depthai.node.SPIIn, id: int) → None Specifies SPI Bus number to use
- Parameter
id
: SPI Bus id
- Parameter
-
setMaxDataSize
(self: depthai.node.SPIIn, maxDataSize: int) → None Set maximum message size it can receive
- Parameter
maxDataSize
: Maximum size in bytes
- Parameter
-
setNumFrames
(self: depthai.node.SPIIn, numFrames: int) → None Set number of frames in pool for sending messages forward
- Parameter
numFrames
: Maximum number of frames in pool
- Parameter
-
setStreamName
(self: depthai.node.SPIIn, name: str) → None Specifies stream name over which the node will receive data
- Parameter
name
: Stream name
- Parameter
-
class
-
class
dai::node
::
SPIIn
: public dai::NodeCRTP<Node, SPIIn, SPIInProperties>¶ SPIIn node. Receives messages over SPI.
Public Functions
-
void
setStreamName
(const std::string &name)¶ Specifies stream name over which the node will receive data
- Parameters
name
: Stream name
-
void
setBusId
(int id)¶ Specifies SPI Bus number to use
- Parameters
id
: SPI Bus id
-
void
setMaxDataSize
(std::uint32_t maxDataSize)¶ Set maximum message size it can receive
- Parameters
maxDataSize
: Maximum size in bytes
-
void
setNumFrames
(std::uint32_t numFrames)¶ Set number of frames in pool for sending messages forward
- Parameters
numFrames
: Maximum number of frames in pool
-
std::string
getStreamName
() const¶ Get stream name.
-
int
getBusId
() const¶ Get bus id.
-
std::uint32_t
getMaxDataSize
() const¶ Get maximum messages size in bytes.
-
std::uint32_t
getNumFrames
() const¶ Get number of frames in pool.
Public Members
-
Output
out
= {*this, "out", Output::Type::MSender, {{DatatypeEnum::Buffer, true}}}¶ Outputs message of same type as send from host.
Public Static Attributes
-
static constexpr const char *
NAME
= "SPIIn"¶
-
void