ColorCamera¶
ColorCamera node is a source of image frames. You can control in at runtime with the InputControl
and InputConfig
.
How to place it¶
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.ColorCamera)
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::ColorCamera>();
Inputs and Outputs¶
ColorCamera node
┌──────────────────────────────┐
│ ┌─────────────┐ │
│ │ Image │ raw │ raw
│ │ Sensor │---┬--------├────────►
│ └────▲────────┘ | │
│ │ ┌--------┘ │
│ ┌─┴───▼─┐ │ isp
inputControl │ │ │-------┬-------├────────►
──────────────►│------│ ISP │ ┌─────▼────┐ │ video
│ │ │ | |--├────────►
│ └───────┘ │ Image │ │ still
inputConfig │ │ Post- │--├────────►
──────────────►│----------------|Processing│ │ preview
│ │ │--├────────►
│ └──────────┘ │
└──────────────────────────────┘
Message types
inputConfig
- ImageManipConfiginputControl
- CameraControlraw
- ImgFrame - RAW10 bayer data. Demo code for unpacking hereisp
- ImgFrame - YUV420 planar (same as YU12/IYUV/I420)still
- ImgFrame - NV12, suitable for bigger size frames. The image gets created when a capture event is sent to the ColorCamera, so it’s like taking a photopreview
- ImgFrame - RGB (or BGR planar/interleaved if configured), mostly suited for small size previews and to feed the image into NeuralNetworkvideo
- ImgFrame - NV12, suitable for bigger size frames
ISP (image signal processor) is used for bayer transformation, demosaicing, noise reduction, and other image enhancements. It interacts with the 3A algorithms: auto-focus, auto-exposure, and auto-white-balance, which are handling image sensor adjustments such as exposure time, sensitivity (ISO), and lens position (if the camera module has a motorized lens) at runtime. Click here for more information.
Image Post-Processing converts YUV420 planar frames from the ISP into video
/preview
/still
frames.
still
(when a capture is triggered) and isp
work at the max camera resolution, while video
and preview
are
limited to max 4K (3840 x 2160) resolution, which is cropped from isp
.
For IMX378 (12MP), the post-processing works like this:
┌─────┐ Cropping to ┌─────────┐ Downscaling ┌──────────┐
│ ISP ├────────────────►│ video ├───────────────►│ preview │
└─────┘ max 3840x2160 └─────────┘ and cropping └──────────┘
The image above is the isp
output from the ColorCamera (12MP resolution from IMX378). If you aren’t downscaling ISP,
the video
output is cropped to 4k (max 3840x2160 due to the limitation of the video
output) as represented by
the blue rectangle. The Yellow rectangle represents a cropped preview
output when the preview size is set to a 1:1 aspect
ratio (eg. when using a 300x300 preview size for the MobileNet-SSD NN model) because the preview
output is derived from
the video
output.
Usage¶
pipeline = dai.Pipeline()
cam = pipeline.create(dai.node.ColorCamera)
cam.setPreviewSize(300, 300)
cam.setBoardSocket(dai.CameraBoardSocket.CAM_A)
cam.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
cam.setInterleaved(False)
cam.setColorOrder(dai.ColorCameraProperties.ColorOrder.RGB)
dai::Pipeline pipeline;
auto cam = pipeline.create<dai::node::ColorCamera>();
cam->setPreviewSize(300, 300);
cam->setBoardSocket(dai::CameraBoardSocket::CAM_A);
cam->setResolution(dai::ColorCameraProperties::SensorResolution::THE_1080_P);
cam->setInterleaved(false);
cam->setColorOrder(dai::ColorCameraProperties::ColorOrder::RGB);
Limitations¶
Here are known camera limitations for the RVC2:
ISP can process about 600 MP/s, and about 500 MP/s when the pipeline is also running NNs and video encoder in parallel
3A algorithms can process about 200..250 FPS overall (for all camera streams). This is a current limitation of our implementation, and we have plans for a workaround to run 3A algorithms on every Xth frame, no ETA yet
ISP Scaling numerator value can be 1..16 and denominator value 1..32 for both vertical and horizontal scaling. So you can downscale eg. 12MP (4056x3040) only to resolutions calculated here
Examples of functionality¶
Reference¶
-
class
depthai.node.
ColorCamera
ColorCamera node. For use with color sensors.
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.ColorCameraProperties
-
property
frameEvent
Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getBoardSocket
(self: depthai.node.ColorCamera) → depthai.CameraBoardSocket Retrieves which board socket to use
- Returns
Board socket to use
-
getCamId
(self: depthai.node.ColorCamera) → int
-
getCamera
(self: depthai.node.ColorCamera) → str Retrieves which camera to use by name
- Returns
Name of the camera to use
-
getColorOrder
(self: depthai.node.ColorCamera) → depthai.ColorCameraProperties.ColorOrder Get color order of preview output frames. RGB or BGR
-
getFp16
(self: depthai.node.ColorCamera) → bool Get fp16 (0..255) data of preview output frames
-
getFps
(self: depthai.node.ColorCamera) → float Get rate at which camera should produce frames
- Returns
Rate in frames per second
-
getFrameEventFilter
(self: depthai.node.ColorCamera) → List[depthai.FrameEvent]
-
getImageOrientation
(self: depthai.node.ColorCamera) → depthai.CameraImageOrientation Get camera image orientation
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getInterleaved
(self: depthai.node.ColorCamera) → bool Get planar or interleaved data of preview output frames
-
getIspHeight
(self: depthai.node.ColorCamera) → int Get ‘isp’ output height
-
getIspNumFramesPool
(self: depthai.node.ColorCamera) → int Get number of frames in isp pool
-
getIspSize
(self: depthai.node.ColorCamera) → Tuple[int, int] Get ‘isp’ output resolution as size, after scaling
-
getIspWidth
(self: depthai.node.ColorCamera) → int Get ‘isp’ output width
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
getPreviewHeight
(self: depthai.node.ColorCamera) → int Get preview height
-
getPreviewKeepAspectRatio
(self: depthai.node.ColorCamera) → bool See also
setPreviewKeepAspectRatio
- Returns
Preview keep aspect ratio option
-
getPreviewNumFramesPool
(self: depthai.node.ColorCamera) → int Get number of frames in preview pool
-
getPreviewSize
(self: depthai.node.ColorCamera) → Tuple[int, int] Get preview size as tuple
-
getPreviewWidth
(self: depthai.node.ColorCamera) → int Get preview width
-
getRawNumFramesPool
(self: depthai.node.ColorCamera) → int Get number of frames in raw pool
-
getResolution
(self: depthai.node.ColorCamera) → depthai.ColorCameraProperties.SensorResolution Get sensor resolution
-
getResolutionHeight
(self: depthai.node.ColorCamera) → int Get sensor resolution height
-
getResolutionSize
(self: depthai.node.ColorCamera) → Tuple[int, int] Get sensor resolution as size
-
getResolutionWidth
(self: depthai.node.ColorCamera) → int Get sensor resolution width
-
getSensorCrop
(self: depthai.node.ColorCamera) → Tuple[float, float] - Returns
Sensor top left crop coordinates
-
getSensorCropX
(self: depthai.node.ColorCamera) → float Get sensor top left x crop coordinate
-
getSensorCropY
(self: depthai.node.ColorCamera) → float Get sensor top left y crop coordinate
-
getStillHeight
(self: depthai.node.ColorCamera) → int Get still height
-
getStillNumFramesPool
(self: depthai.node.ColorCamera) → int Get number of frames in still pool
-
getStillSize
(self: depthai.node.ColorCamera) → Tuple[int, int] Get still size as tuple
-
getStillWidth
(self: depthai.node.ColorCamera) → int Get still width
-
getVideoHeight
(self: depthai.node.ColorCamera) → int Get video height
-
getVideoNumFramesPool
(self: depthai.node.ColorCamera) → int Get number of frames in video pool
-
getVideoSize
(self: depthai.node.ColorCamera) → Tuple[int, int] Get video size as tuple
-
getVideoWidth
(self: depthai.node.ColorCamera) → int Get video width
-
getWaitForConfigInput
(self: depthai.node.ColorCamera) → bool See also
setWaitForConfigInput
- Returns
True if wait for inputConfig message, false otherwise
-
property
id
Id of node
-
property
initialControl
Initial control options to apply to sensor
-
property
inputConfig
Input for ImageManipConfig message, which can modify crop parameters in runtime
Default queue is non-blocking with size 8
-
property
inputControl
Input for CameraControl message, which can modify camera parameters in runtime
Default queue is blocking with size 8
-
property
isp
Outputs ImgFrame message that carries YUV420 planar (I420/IYUV) frame data.
Generated by the ISP engine, and the source for the ‘video’, ‘preview’ and ‘still’ outputs
-
property
preview
Outputs ImgFrame message that carries BGR/RGB planar/interleaved encoded frame data.
Suitable for use with NeuralNetwork node
-
property
raw
Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor, and the source for the ‘isp’ output.
-
sensorCenterCrop
(self: depthai.node.ColorCamera) → None Specify sensor center crop. Resolution size / video size
-
setBoardSocket
(self: depthai.node.ColorCamera, boardSocket: depthai.CameraBoardSocket) → None Specify which board socket to use
- Parameter
boardSocket
: Board socket to use
- Parameter
-
setCamId
(self: depthai.node.ColorCamera, arg0: int) → None
-
setCamera
(self: depthai.node.ColorCamera, name: str) → None Specify which camera to use by name
- Parameter
name
: Name of the camera to use
- Parameter
-
setColorOrder
(self: depthai.node.ColorCamera, colorOrder: depthai.ColorCameraProperties.ColorOrder) → None Set color order of preview output images. RGB or BGR
-
setFp16
(self: depthai.node.ColorCamera, fp16: bool) → None Set fp16 (0..255) data type of preview output frames
-
setFps
(self: depthai.node.ColorCamera, fps: float) → None Set rate at which camera should produce frames
- Parameter
fps
: Rate in frames per second
- Parameter
-
setFrameEventFilter
(self: depthai.node.ColorCamera, events: List[depthai.FrameEvent]) → None
-
setImageOrientation
(self: depthai.node.ColorCamera, imageOrientation: depthai.CameraImageOrientation) → None Set camera image orientation
-
setInterleaved
(self: depthai.node.ColorCamera, interleaved: bool) → None Set planar or interleaved data of preview output frames
-
setIsp3aFps
(self: depthai.node.ColorCamera, arg0: int) → None Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
setIspNumFramesPool
(self: depthai.node.ColorCamera, arg0: int) → None Set number of frames in isp pool
-
setIspScale
(*args, **kwargs) Overloaded function.
setIspScale(self: depthai.node.ColorCamera, numerator: int, denominator: int) -> None
Set ‘isp’ output scaling (numerator/denominator), preserving the aspect ratio. The fraction numerator/denominator is simplified first to a irreducible form, then a set of hardware scaler constraints applies: max numerator = 16, max denominator = 63
setIspScale(self: depthai.node.ColorCamera, scale: Tuple[int, int]) -> None
Set ‘isp’ output scaling, as a tuple <numerator, denominator>
setIspScale(self: depthai.node.ColorCamera, horizNum: int, horizDenom: int, vertNum: int, vertDenom: int) -> None
Set ‘isp’ output scaling, per each direction. If the horizontal scaling factor (horizNum/horizDen) is different than the vertical scaling factor (vertNum/vertDen), a distorted (stretched or squished) image is generated
setIspScale(self: depthai.node.ColorCamera, horizScale: Tuple[int, int], vertScale: Tuple[int, int]) -> None
Set ‘isp’ output scaling, per each direction, as <numerator, denominator> tuples
-
setNumFramesPool
(self: depthai.node.ColorCamera, raw: int, isp: int, preview: int, video: int, still: int) → None Set number of frames in all pools
-
setPreviewKeepAspectRatio
(self: depthai.node.ColorCamera, keep: bool) → None Specifies whether preview output should preserve aspect ratio, after downscaling from video size or not.
- Parameter
keep
: If true, a larger crop region will be considered to still be able to create the final image in the specified aspect ratio. Otherwise video size is resized to fit preview size
- Parameter
-
setPreviewNumFramesPool
(self: depthai.node.ColorCamera, arg0: int) → None Set number of frames in preview pool
-
setPreviewSize
(*args, **kwargs) Overloaded function.
setPreviewSize(self: depthai.node.ColorCamera, width: int, height: int) -> None
Set preview output size
setPreviewSize(self: depthai.node.ColorCamera, size: Tuple[int, int]) -> None
Set preview output size, as a tuple <width, height>
-
setRawNumFramesPool
(self: depthai.node.ColorCamera, arg0: int) → None Set number of frames in raw pool
-
setRawOutputPacked
(self: depthai.node.ColorCamera, packed: bool) → None Configures whether the camera raw frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
-
setResolution
(self: depthai.node.ColorCamera, resolution: depthai.ColorCameraProperties.SensorResolution) → None Set sensor resolution
-
setSensorCrop
(self: depthai.node.ColorCamera, x: float, y: float) → None Specifies the cropping that happens when converting ISP to video output. By default, video will be center cropped from the ISP output. Note that this doesn’t actually do on-sensor cropping (and MIPI-stream only that region), but it does postprocessing on the ISP (on RVC).
- Parameter
x
: Top left X coordinate
- Parameter
y
: Top left Y coordinate
- Parameter
-
setStillNumFramesPool
(self: depthai.node.ColorCamera, arg0: int) → None Set number of frames in preview pool
-
setStillSize
(*args, **kwargs) Overloaded function.
setStillSize(self: depthai.node.ColorCamera, width: int, height: int) -> None
Set still output size
setStillSize(self: depthai.node.ColorCamera, size: Tuple[int, int]) -> None
Set still output size, as a tuple <width, height>
-
setVideoNumFramesPool
(self: depthai.node.ColorCamera, arg0: int) → None Set number of frames in preview pool
-
setVideoSize
(*args, **kwargs) Overloaded function.
setVideoSize(self: depthai.node.ColorCamera, width: int, height: int) -> None
Set video output size
setVideoSize(self: depthai.node.ColorCamera, size: Tuple[int, int]) -> None
Set video output size, as a tuple <width, height>
-
setWaitForConfigInput
(self: depthai.node.ColorCamera, wait: bool) → None Specify to wait until inputConfig receives a configuration message, before sending out a frame.
- Parameter
wait
: True to wait for inputConfig message, false otherwise
- Parameter
-
property
still
Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
The message is sent only when a CameraControl message arrives to inputControl with captureStill command set.
-
property
video
Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
Suitable for use with VideoEncoder node
-
class
-
class
dai::node
::
ColorCamera
: public dai::NodeCRTP<Node, ColorCamera, ColorCameraProperties>¶ ColorCamera node. For use with color sensors.
Public Functions
Constructs ColorCamera node.
-
int
getScaledSize
(int input, int num, int denom) const¶ Computes the scaled size given numerator and denominator
-
void
setBoardSocket
(CameraBoardSocket boardSocket)¶ Specify which board socket to use
- Parameters
boardSocket
: Board socket to use
-
CameraBoardSocket
getBoardSocket
() const¶ Retrieves which board socket to use
- Return
Board socket to use
-
void
setCamera
(std::string name)¶ Specify which camera to use by name
- Parameters
name
: Name of the camera to use
-
std::string
getCamera
() const¶ Retrieves which camera to use by name
- Return
Name of the camera to use
-
void
setCamId
(int64_t id)¶ Set which color camera to use.
-
int64_t
getCamId
() const¶ Get which color camera to use.
-
void
setImageOrientation
(CameraImageOrientation imageOrientation)¶ Set camera image orientation.
-
CameraImageOrientation
getImageOrientation
() const¶ Get camera image orientation.
-
void
setColorOrder
(ColorCameraProperties::ColorOrder colorOrder)¶ Set color order of preview output images. RGB or BGR.
-
ColorCameraProperties::ColorOrder
getColorOrder
() const¶ Get color order of preview output frames. RGB or BGR.
-
void
setInterleaved
(bool interleaved)¶ Set planar or interleaved data of preview output frames.
-
bool
getInterleaved
() const¶ Get planar or interleaved data of preview output frames.
-
void
setFp16
(bool fp16)¶ Set fp16 (0..255) data type of preview output frames.
-
bool
getFp16
() const¶ Get fp16 (0..255) data of preview output frames.
-
void
setPreviewSize
(int width, int height)¶ Set preview output size.
-
void
setPreviewSize
(std::tuple<int, int> size)¶ Set preview output size, as a tuple <width, height>
-
void
setPreviewNumFramesPool
(int num)¶ Set number of frames in preview pool.
-
void
setVideoSize
(int width, int height)¶ Set video output size.
-
void
setVideoSize
(std::tuple<int, int> size)¶ Set video output size, as a tuple <width, height>
-
void
setVideoNumFramesPool
(int num)¶ Set number of frames in preview pool.
-
void
setStillSize
(int width, int height)¶ Set still output size.
-
void
setStillSize
(std::tuple<int, int> size)¶ Set still output size, as a tuple <width, height>
-
void
setStillNumFramesPool
(int num)¶ Set number of frames in preview pool.
-
void
setResolution
(Properties::SensorResolution resolution)¶ Set sensor resolution.
-
Properties::SensorResolution
getResolution
() const¶ Get sensor resolution.
-
void
setRawNumFramesPool
(int num)¶ Set number of frames in raw pool.
-
void
setIspNumFramesPool
(int num)¶ Set number of frames in isp pool.
-
void
setNumFramesPool
(int raw, int isp, int preview, int video, int still)¶ Set number of frames in all pools.
-
void
setIspScale
(int numerator, int denominator)¶ Set ‘isp’ output scaling (numerator/denominator), preserving the aspect ratio. The fraction numerator/denominator is simplified first to a irreducible form, then a set of hardware scaler constraints applies: max numerator = 16, max denominator = 63
-
void
setIspScale
(std::tuple<int, int> scale)¶ Set ‘isp’ output scaling, as a tuple <numerator, denominator>
-
void
setIspScale
(int horizNum, int horizDenom, int vertNum, int vertDenom)¶ Set ‘isp’ output scaling, per each direction. If the horizontal scaling factor (horizNum/horizDen) is different than the vertical scaling factor (vertNum/vertDen), a distorted (stretched or squished) image is generated
-
void
setIspScale
(std::tuple<int, int> horizScale, std::tuple<int, int> vertScale)¶ Set ‘isp’ output scaling, per each direction, as <numerator, denominator> tuples.
-
void
setFps
(float fps)¶ Set rate at which camera should produce frames
- Parameters
fps
: Rate in frames per second
-
void
setIsp3aFps
(int isp3aFps)¶ Isp 3A rate (auto focus, auto exposure, auto white balance, camera controls etc.). Default (0) matches the camera FPS, meaning that 3A is running on each frame. Reducing the rate of 3A reduces the CPU usage on CSS, but also increases the convergence rate of 3A. Note that camera controls will be processed at this rate. E.g. if camera is running at 30 fps, and camera control is sent at every frame, but 3A fps is set to 15, the camera control messages will be processed at 15 fps rate, which will lead to queueing.
-
void
setFrameEventFilter
(const std::vector<dai::FrameEvent> &events)¶
-
std::vector<dai::FrameEvent>
getFrameEventFilter
() const¶
-
float
getFps
() const¶ Get rate at which camera should produce frames
- Return
Rate in frames per second
-
std::tuple<int, int>
getPreviewSize
() const¶ Get preview size as tuple.
-
int
getPreviewWidth
() const¶ Get preview width.
-
int
getPreviewHeight
() const¶ Get preview height.
-
std::tuple<int, int>
getVideoSize
() const¶ Get video size as tuple.
-
int
getVideoWidth
() const¶ Get video width.
-
int
getVideoHeight
() const¶ Get video height.
-
std::tuple<int, int>
getStillSize
() const¶ Get still size as tuple.
-
int
getStillWidth
() const¶ Get still width.
-
int
getStillHeight
() const¶ Get still height.
-
std::tuple<int, int>
getResolutionSize
() const¶ Get sensor resolution as size.
-
int
getResolutionWidth
() const¶ Get sensor resolution width.
-
int
getResolutionHeight
() const¶ Get sensor resolution height.
-
std::tuple<int, int>
getIspSize
() const¶ Get ‘isp’ output resolution as size, after scaling.
-
int
getIspWidth
() const¶ Get ‘isp’ output width.
-
int
getIspHeight
() const¶ Get ‘isp’ output height.
-
void
sensorCenterCrop
()¶ Specify sensor center crop. Resolution size / video size
-
void
setSensorCrop
(float x, float y)¶ Specifies the cropping that happens when converting ISP to video output. By default, video will be center cropped from the ISP output. Note that this doesn’t actually do on-sensor cropping (and MIPI-stream only that region), but it does postprocessing on the ISP (on RVC).
- Parameters
x
: Top left X coordinatey
: Top left Y coordinate
-
std::tuple<float, float>
getSensorCrop
() const¶ - Return
Sensor top left crop coordinates
-
float
getSensorCropX
() const¶ Get sensor top left x crop coordinate.
-
float
getSensorCropY
() const¶ Get sensor top left y crop coordinate.
-
void
setWaitForConfigInput
(bool wait)¶ Specify to wait until inputConfig receives a configuration message, before sending out a frame.
- Parameters
wait
: True to wait for inputConfig message, false otherwise
-
bool
getWaitForConfigInput
() const¶ - See
- Return
True if wait for inputConfig message, false otherwise
-
void
setPreviewKeepAspectRatio
(bool keep)¶ Specifies whether preview output should preserve aspect ratio, after downscaling from video size or not.
- Parameters
keep
: If true, a larger crop region will be considered to still be able to create the final image in the specified aspect ratio. Otherwise video size is resized to fit preview size
-
bool
getPreviewKeepAspectRatio
()¶ - See
- Return
Preview keep aspect ratio option
-
int
getPreviewNumFramesPool
()¶ Get number of frames in preview pool.
-
int
getVideoNumFramesPool
()¶ Get number of frames in video pool.
-
int
getStillNumFramesPool
()¶ Get number of frames in still pool.
-
int
getRawNumFramesPool
()¶ Get number of frames in raw pool.
-
int
getIspNumFramesPool
()¶ Get number of frames in isp pool.
-
void
setRawOutputPacked
(bool packed)¶ Configures whether the camera
raw
frames are saved as MIPI-packed to memory. The packed format is more efficient, consuming less memory on device, and less data to send to host: RAW10: 4 pixels saved on 5 bytes, RAW12: 2 pixels saved on 3 bytes. When packing is disabled (false
), data is saved lsb-aligned, e.g. a RAW10 pixel will be stored as uint16, on bits 9..0: 0b0000’00pp’pppp’pppp. Default is auto: enabled for standard color/monochrome cameras where ISP can work with both packed/unpacked, but disabled for other cameras like ToF.
Public Members
-
CameraControl
initialControl
¶ Initial control options to apply to sensor
-
Input
inputConfig
= {*this, "inputConfig", Input::Type::SReceiver, false, 8, {{DatatypeEnum::ImageManipConfig, false}}}¶ Input for ImageManipConfig message, which can modify crop parameters in runtime
Default queue is non-blocking with size 8
-
Input
inputControl
= {*this, "inputControl", Input::Type::SReceiver, true, 8, {{DatatypeEnum::CameraControl, false}}}¶ Input for CameraControl message, which can modify camera parameters in runtime
Default queue is blocking with size 8
-
Output
video
= {*this, "video", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
Suitable for use with VideoEncoder node
-
Output
preview
= {*this, "preview", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries BGR/RGB planar/interleaved encoded frame data.
Suitable for use with NeuralNetwork node
-
Output
still
= {*this, "still", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries NV12 encoded (YUV420, UV plane interleaved) frame data.
The message is sent only when a CameraControl message arrives to inputControl with captureStill command set.
-
Output
isp
= {*this, "isp", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries YUV420 planar (I420/IYUV) frame data.
Generated by the ISP engine, and the source for the ‘video’, ‘preview’ and ‘still’ outputs
-
Output
raw
= {*this, "raw", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs ImgFrame message that carries RAW10-packed (MIPI CSI-2 format) frame data.
Captured directly from the camera sensor, and the source for the ‘isp’ output.
-
Output
frameEvent
= {*this, "frameEvent", Output::Type::MSender, {{DatatypeEnum::ImgFrame, false}}}¶ Outputs metadata-only ImgFrame message as an early indicator of an incoming frame.
It’s sent on the MIPI SoF (start-of-frame) event, just after the exposure of the current frame has finished and before the exposure for next frame starts. Could be used to synchronize various processes with camera capture. Fields populated: camera id, sequence number, timestamp
Public Static Attributes
-
static constexpr const char *
NAME
= "ColorCamera"¶
Private Members
-
std::shared_ptr<RawCameraControl>
rawControl
¶