Calibration Flash¶
This example shows how to flash calibration data of version 6 (gen2 calibration data) to the device.
Similar samples:
Demo¶
Example script output
~/depthai-python/examples$ python3 Calibration/calibration_flash.py
Calibration Data on the device is backed up at:
/home/erik/Luxonis/depthai-python/examples/Calibration/depthai_calib_backup.json
Calibration Flash Successful
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 | #!/usr/bin/env python3 from pathlib import Path import depthai as dai import argparse calibJsonFile = str((Path(__file__).parent / Path('../models/depthai_calib.json')).resolve().absolute()) calibBackUpFile = str((Path(__file__).parent / Path('depthai_calib_backup.json')).resolve().absolute()) parser = argparse.ArgumentParser() parser.add_argument('calibJsonFile', nargs='?', help="Path to calibration file in json", default=calibJsonFile) args = parser.parse_args() # Connect device with dai.Device(dai.OpenVINO.VERSION_UNIVERSAL, dai.UsbSpeed.HIGH) as device: deviceCalib = device.readCalibration() deviceCalib.eepromToJsonFile(calibBackUpFile) print("Calibration Data on the device is backed up at:") print(calibBackUpFile) calibData = dai.CalibrationHandler(args.calibJsonFile) try: device.flashCalibration2(calibData) print('Successfully flashed calibration') except Exception as ex: print(f'Failed flashing calibration: {ex}') |
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 | #include <cstdio> #include <iostream> #include <string> // Includes common necessary includes for development using depthai library #include "depthai/depthai.hpp" int main(int argc, char** argv) { std::string calibJsonFile(CALIB_PATH); std::string calibBackUpFile("depthai_calib_backup.json"); if(argc > 1) { calibJsonFile = std::string(argv[1]); } // Connect device dai::Device device(dai::OpenVINO::VERSION_UNIVERSAL, dai::UsbSpeed::HIGH); dai::CalibrationHandler deviceCalib = device.readCalibration(); deviceCalib.eepromToJsonFile(calibBackUpFile); std::cout << "Calibration Data on the device is backed up at:" << calibBackUpFile << std::endl; dai::CalibrationHandler calibData(calibJsonFile); try { device.flashCalibration2(calibData); std::cout << "Successfully flashed calibration" << std::endl; } catch(const std::exception& ex) { std::cout << "Failed flashing calibration: " << ex.what() << std::endl; } return 0; } |