Pipeline¶
Pipeline is a collection of nodes and links between them. This flow provides an extensive flexibility that users get for their OAK device. When pipeline object is passed to the Device object, pipeline gets serialized to JSON and sent to the OAK device via XLink.
Pipeline first steps¶
To get DepthAI up and running, you have to create a pipeline, populate it with nodes, configure the nodes and link them together. After that, the pipeline can be loaded onto the Device and be started.
pipeline = depthai.Pipeline()
# If required, specify OpenVINO version
pipeline.setOpenVINOVersion(depthai.OpenVINO.Version.VERSION_2021_4)
# Create nodes, configure them and link them together
# Upload the pipeline to the device
with depthai.Device(pipeline) as device:
# Set input/output queues to configure device/host communication through the XLink...
Specifying OpenVINO version¶
When using a NN blob that was not compiled with the latest OpenVINO (that DepthAI supports), you have to specify the OpenVINO version of the pipeline. The reason behind this is that OpenVINO doesn’t provide version inside the blob.
pipeline = depthai.Pipeline()
# Set the correct version:
pipeline.setOpenVINOVersion(depthai.OpenVINO.Version.VERSION_2021_4)
Using multiple devices¶
If user has multiple DepthAI devices, each device can run a different pipeline or the same pipeline (demo here). To use different pipeline for each device, you can create multiple pipelines and pass the desired pipeline to the desired device on initialization.
How to place it¶
pipeline = dai.Pipeline()
dai::Pipeline pipeline;
Reference¶
-
class
depthai.
Pipeline
-
create
(self: depthai.Pipeline, arg0: object) → depthai.Node
-
createAprilTag
(self: depthai.Pipeline) → depthai.node.AprilTag
-
createCamera
(self: depthai.Pipeline) → depthai.node.Camera
-
createColorCamera
(self: depthai.Pipeline) → depthai.node.ColorCamera
-
createDetectionParser
(self: depthai.Pipeline) → depthai.node.DetectionParser
-
createEdgeDetector
(self: depthai.Pipeline) → depthai.node.EdgeDetector
-
createFeatureTracker
(self: depthai.Pipeline) → depthai.node.FeatureTracker
-
createIMU
(self: depthai.Pipeline) → depthai.node.IMU
-
createImageManip
(self: depthai.Pipeline) → depthai.node.ImageManip
-
createMobileNetDetectionNetwork
(self: depthai.Pipeline) → depthai.node.MobileNetDetectionNetwork
-
createMobileNetSpatialDetectionNetwork
(self: depthai.Pipeline) → depthai.node.MobileNetSpatialDetectionNetwork
-
createMonoCamera
(self: depthai.Pipeline) → depthai.node.MonoCamera
-
createNeuralNetwork
(self: depthai.Pipeline) → depthai.node.NeuralNetwork
-
createObjectTracker
(self: depthai.Pipeline) → depthai.node.ObjectTracker
-
createSPIIn
(self: depthai.Pipeline) → depthai.node.SPIIn
-
createSPIOut
(self: depthai.Pipeline) → depthai.node.SPIOut
-
createScript
(self: depthai.Pipeline) → depthai.node.Script
-
createSpatialLocationCalculator
(self: depthai.Pipeline) → depthai.node.SpatialLocationCalculator
-
createStereoDepth
(self: depthai.Pipeline) → depthai.node.StereoDepth
-
createSystemLogger
(self: depthai.Pipeline) → depthai.node.SystemLogger
-
createUVC
(self: depthai.Pipeline) → depthai.node.UVC
-
createVideoEncoder
(self: depthai.Pipeline) → depthai.node.VideoEncoder
-
createWarp
(self: depthai.Pipeline) → depthai.node.Warp
-
createXLinkIn
(self: depthai.Pipeline) → depthai.node.XLinkIn
-
createXLinkOut
(self: depthai.Pipeline) → depthai.node.XLinkOut
-
createYoloDetectionNetwork
(self: depthai.Pipeline) → depthai.node.YoloDetectionNetwork
-
createYoloSpatialDetectionNetwork
(self: depthai.Pipeline) → depthai.node.YoloSpatialDetectionNetwork
-
getAllNodes
(*args, **kwargs) Overloaded function.
getAllNodes(self: depthai.Pipeline) -> List[depthai.Node]
Get a vector of all nodes
getAllNodes(self: depthai.Pipeline) -> List[depthai.Node]
Get a vector of all nodes
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Pipeline) -> depthai.AssetManager
Get pipelines AssetManager as reference
getAssetManager(self: depthai.Pipeline) -> depthai.AssetManager
Get pipelines AssetManager as reference
-
getBoardConfig
(self: depthai.Pipeline) → depthai.BoardConfig Gets board configuration
-
getCalibrationData
(self: depthai.Pipeline) → depthai.CalibrationHandler gets the calibration data which is set through pipeline
- Returns
the calibrationHandler with calib data in the pipeline
-
getConnectionMap
(self: depthai.Pipeline) → Dict[int, Set[depthai.Node.Connection]] Get a reference to internal connection representation
-
getConnections
(self: depthai.Pipeline) → List[depthai.Node.Connection] Get all connections
-
getDeviceConfig
(self: depthai.Pipeline) → depthai.Device.Config Get device configuration needed for this pipeline
-
getGlobalProperties
(self: depthai.Pipeline) → depthai.GlobalProperties - Returns
Global properties of current pipeline
-
getNode
(*args, **kwargs) Overloaded function.
getNode(self: depthai.Pipeline, arg0: int) -> depthai.Node
Get node with id if it exists, nullptr otherwise
getNode(self: depthai.Pipeline, arg0: int) -> depthai.Node
Get node with id if it exists, nullptr otherwise
-
getNodeMap
(self: depthai.Pipeline) → Dict[int, depthai.Node] Get a reference to internal node map
-
getOpenVINOVersion
(self: depthai.Pipeline) → depthai.OpenVINO.Version Get possible OpenVINO version to run this pipeline
-
getRequiredOpenVINOVersion
(self: depthai.Pipeline) → Optional[depthai.OpenVINO.Version] Get required OpenVINO version to run this pipeline. Can be none
-
link
(self: depthai.Pipeline, arg0: depthai.Node.Output, arg1: depthai.Node.Input) → None Link output to an input. Both nodes must be on the same pipeline
Throws an error if they aren’t or cannot be connected
- Parameter
out
: Nodes output to connect from
- Parameter
in
: Nodes input to connect to
- Parameter
-
remove
(self: depthai.Pipeline, node: depthai.Node) → None Removes a node from pipeline
-
serializeToJson
(self: depthai.Pipeline) → json Returns whole pipeline represented as JSON
-
setBoardConfig
(self: depthai.Pipeline, arg0: depthai.BoardConfig) → None Sets board configuration
-
setCalibrationData
(self: depthai.Pipeline, calibrationDataHandler: depthai.CalibrationHandler) → None Sets the calibration in pipeline which overrides the calibration data in eeprom
- Parameter
calibrationDataHandler
: CalibrationHandler object which is loaded with calibration information.
- Parameter
-
setCameraTuningBlobPath
(self: depthai.Pipeline, path: Path) → None Set a camera IQ (Image Quality) tuning blob, used for all cameras
-
setOpenVINOVersion
(self: depthai.Pipeline, version: depthai.OpenVINO.Version) → None Set a specific OpenVINO version to use with this pipeline
-
setSippBufferSize
(self: depthai.Pipeline, sizeBytes: int) → None SIPP (Signal Image Processing Pipeline) internal memory pool. SIPP is a framework used to schedule HW filters, e.g. ISP, Warp, Median filter etc. Changing the size of this pool is meant for advanced use cases, pushing the limits of the HW. By default memory is allocated in high speed CMX memory. Setting to 0 will allocate in DDR 256 kilobytes. Units are bytes.
-
setSippDmaBufferSize
(self: depthai.Pipeline, sizeBytes: int) → None SIPP (Signal Image Processing Pipeline) internal DMA memory pool. SIPP is a framework used to schedule HW filters, e.g. ISP, Warp, Median filter etc. Changing the size of this pool is meant for advanced use cases, pushing the limits of the HW. Memory is allocated in high speed CMX memory Units are bytes.
-
setXLinkChunkSize
(self: depthai.Pipeline, sizeBytes: int) → None Set chunk size for splitting device-sent XLink packets, in bytes. A larger value could increase performance, with 0 disabling chunking. A negative value won’t modify the device defaults - configured per protocol, currently 64*1024 for both USB and Ethernet.
-
unlink
(self: depthai.Pipeline, arg0: depthai.Node.Output, arg1: depthai.Node.Input) → None Unlink output from an input.
Throws an error if link doesn’t exists
- Parameter
out
: Nodes output to unlink from
- Parameter
in
: Nodes input to unlink to
- Parameter
-
-
class
dai
::
Pipeline
¶ Represents the pipeline, set of nodes and connections between them.
Public Types
-
using
NodeConnectionMap
= PipelineImpl::NodeConnectionMap¶
-
using
NodeMap
= PipelineImpl::NodeMap¶
Public Functions
-
Pipeline
()¶ Constructs a new pipeline
-
GlobalProperties
getGlobalProperties
() const¶ - Return
Global properties of current pipeline
-
PipelineSchema
getPipelineSchema
(SerializationType type = DEFAULT_SERIALIZATION_TYPE) const¶ - Return
Pipeline schema
-
void
serialize
(PipelineSchema &schema, Assets &assets, std::vector<std::uint8_t> &assetStorage) const¶
-
nlohmann::json
serializeToJson
() const¶ Returns whole pipeline represented as JSON.
Adds a node to pipeline.
Node is specified by template argument N
Removes a node from pipeline.
-
std::shared_ptr<const Node>
getNode
(Node::Id id) const¶ Get node with id if it exists, nullptr otherwise.
-
std::vector<Node::Connection>
getConnections
() const¶ Get all connections.
-
const NodeConnectionMap &
getConnectionMap
() const¶ Get a reference to internal connection representation.
-
void
link
(const Node::Output &out, const Node::Input &in)¶ Link output to an input. Both nodes must be on the same pipeline
Throws an error if they aren’t or cannot be connected
- Parameters
out
: Nodes output to connect fromin
: Nodes input to connect to
-
void
unlink
(const Node::Output &out, const Node::Input &in)¶ Unlink output from an input.
Throws an error if link doesn’t exists
- Parameters
out
: Nodes output to unlink fromin
: Nodes input to unlink to
-
const AssetManager &
getAssetManager
() const¶ Get pipelines AssetManager as reference.
-
AssetManager &
getAssetManager
()¶ Get pipelines AssetManager as reference.
-
void
setOpenVINOVersion
(OpenVINO::Version version)¶ Set a specific OpenVINO version to use with this pipeline.
-
void
setCalibrationData
(CalibrationHandler calibrationDataHandler)¶ Sets the calibration in pipeline which overrides the calibration data in eeprom
- Parameters
calibrationDataHandler
: CalibrationHandler object which is loaded with calibration information.
-
CalibrationHandler
getCalibrationData
() const¶ gets the calibration data which is set through pipeline
- Return
the calibrationHandler with calib data in the pipeline
-
tl::optional<OpenVINO::Version>
getRequiredOpenVINOVersion
() const¶ Get required OpenVINO version to run this pipeline. Can be none.
-
void
setCameraTuningBlobPath
(const dai::Path &path)¶ Set a camera IQ (Image Quality) tuning blob, used for all cameras.
-
void
setXLinkChunkSize
(int sizeBytes)¶ Set chunk size for splitting device-sent XLink packets, in bytes. A larger value could increase performance, with 0 disabling chunking. A negative value won’t modify the device defaults - configured per protocol, currently 64*1024 for both USB and Ethernet.
-
void
setSippBufferSize
(int sizeBytes)¶ SIPP (Signal Image Processing Pipeline) internal memory pool. SIPP is a framework used to schedule HW filters, e.g. ISP, Warp, Median filter etc. Changing the size of this pool is meant for advanced use cases, pushing the limits of the HW. By default memory is allocated in high speed CMX memory. Setting to 0 will allocate in DDR 256 kilobytes. Units are bytes.
-
void
setSippDmaBufferSize
(int sizeBytes)¶ SIPP (Signal Image Processing Pipeline) internal DMA memory pool. SIPP is a framework used to schedule HW filters, e.g. ISP, Warp, Median filter etc. Changing the size of this pool is meant for advanced use cases, pushing the limits of the HW. Memory is allocated in high speed CMX memory Units are bytes.
-
bool
isOpenVINOVersionCompatible
(OpenVINO::Version version) const¶ Checks whether a given OpenVINO version is compatible with the pipeline.
-
void
setBoardConfig
(BoardConfig board)¶ Sets board configuration.
-
BoardConfig
getBoardConfig
() const¶ Gets board configuration.
Private Members
-
std::shared_ptr<PipelineImpl>
pimpl
¶
-
using