MessageDemux¶
The MessageDemux (Demultiplexer) node is used to separate a MessageGroup into individual outputs. It currently serves as way to demultiplex the output of Sync node.
How to Place It¶
pipeline = dai.Pipeline()
demux = pipeline.create(dai.node.MessageDemux)
dai::Pipeline pipeline;
auto demux = pipeline.create<dai::node::MessageDemux>();
Inputs and Outputs¶
┌───────────────────┐
input │ │
──────────────►│ │
│ MessageDemux │ output1
│ ├───────────►
│ │ output2
│ ├───────────►
│ │ ...
└───────────────────┘
Message types
input
- MessageGroupoutput1
,output2
, … - Individual output messages
Usage¶
The MessageDemux node is particularly useful for handling different types of data coming from a single source. For example, when the Sync node is used to synchronize the outputs of multiple nodes, the output of the Sync node is a MessageGroup containing all the messages from the synchronized nodes. The Demux node can be used to separate the messages into individual streams.
# Create sync node and set sync threshold
sync = pipeline.create(dai.node.Sync)
sync.setSyncThresholdMs(timedelta(milliseconds=100))
# Create demux node
demux = pipeline.create(dai.node.MessageDemux)
# Sync the outputs of multiple nodes
rgb.preview.link(sync.inputs["rgb"])
stereo.depth.link(sync.inputs["depth"])
script.outputs["out"].link(sync.inputs["script"])
sync.out.link(demux.input) # Sync output is a MessageGroup containing all the messages from the synchronized nodes
# Demux the MessageGroup into individual messages
demux.outputs["rgb"].link(xout1.input)
demux.outputs["depth"].link(xout2.input)
demux.outputs["script"].link(xout3.input)
// Create sync node and set sync threshold
auto sync = pipeline.create<dai::node::Sync>();
sync->setSyncThreshold(std::chrono::milliseconds(100));
// Create demux node
auto demux = pipeline.create<dai::node::MessageDemux>();
// Sync the outputs of multiple nodes
rgb.preview.link(sync->input["rgb"]);
stereo.depth.link(sync->input["depth"]);
script.outputs["out"].link(sync->input["script"]);
sync->out.link(demux->input); // Sync output is a MessageGroup containing all the messages from the synchronized nodes
// Demux the MessageGroup into individual messages
demux->outputs["rgb"].link(xout1.input);
demux->outputs["depth"].link(xout2.input);
demux->outputs["script"].link(xout3.input);
Examples of Functionality¶
Reference¶
-
class
depthai.node.
MessageDemux
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.MessageDemuxProperties
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
property
id
Id of node
-
property
input
Input message of type MessageGroup
-
property
outputs
A map of outputs, where keys are same as in the input MessageGroup
-
class
-
class
dai::node
::
MessageDemux
: public dai::NodeCRTP<Node, MessageDemux, MessageDemuxProperties>¶ Public Functions
Public Members
-
Input
input
= {*this, "input", Input::Type::SReceiver, {{DatatypeEnum::MessageGroup, false}}}¶ Input message of type MessageGroup
-
OutputMap
outputs
¶ A map of outputs, where keys are same as in the input MessageGroup
Public Static Attributes
-
static constexpr const char *
NAME
= "MessageDemux"¶
-
Input