UVC & Mono Camera¶
This example demonstrates how to use a mono camera on your OAK device to function as a webcam. The UVC feature allows you to use your OAK device as a regular webcam in applications like OpenCV’s cv2.VideoCapture()
, native camera apps, and more.
How It Works:
The MonoCamera node outputs image data in the GRAY8 format. However, the UVC node expects the data in NV12 format. To bridge this gap, an intermediary ImageManip node is used to convert the GRAY8 output from the MonoCamera node to NV12 format, which is then passed to the UVC node for streaming.
Similar samples:
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
Code used for testing¶
import cv2
# Initialize the VideoCapture object to use the default camera (camera index 0 is webcam)
cap = cv2.VideoCapture(1)
# Check if the camera opened successfully
if not cap.isOpened():
print("Error: Could not open camera.")
exit()
# Loop to continuously get frames from the camera
while True:
ret, frame = cap.read()
if not ret:
print("Error: Could not read frame.")
break
cv2.imshow('Video Feed', frame)
if cv2.waitKey(1) & 0xFF == ord('q'):
break
cap.release()
cv2.destroyAllWindows()
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 | #!/usr/bin/env python3 import time import depthai as dai pipeline = dai.Pipeline() # Define a source - left mono (grayscale) camera mono_left = pipeline.createMonoCamera() mono_left.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P) mono_left.setBoardSocket(dai.CameraBoardSocket.CAM_B) # Create an UVC (USB Video Class) output node uvc = pipeline.createUVC() # Manip for frame type conversion manip = pipeline.createImageManip() manip.initialConfig.setResize(1280, 720) manip.initialConfig.setFrameType(dai.RawImgFrame.Type.NV12) manip.setMaxOutputFrameSize(int(1280*720*1.5)) # Linking manip.out.link(uvc.input) mono_left.out.link(manip.inputImage) # Note: if the pipeline is sent later to device (using startPipeline()), # it is important to pass the device config separately when creating the device config = dai.Device.Config() config.board.uvc = dai.BoardConfig.UVC(1280, 720) config.board.uvc.frameType = dai.ImgFrame.Type.NV12 # config.board.uvc.cameraName = "My Custom Cam" pipeline.setBoardConfig(config.board) # Standard UVC load with depthai with dai.Device(pipeline) as device: # Dot projector device.setIrLaserDotProjectorBrightness(765) print("\nDevice started, please keep this process running") print("and open an UVC viewer to check the camera stream.") print("\nTo close: Ctrl+C") # Doing nothing here, just keeping the host feeding the watchdog while True: try: time.sleep(0.1) except KeyboardInterrupt: break |