XLinkOut¶
XLinkOut node is used to send data from the device to the host via XLink.
How to place it¶
pipeline = dai.Pipeline()
xlinkOut = pipeline.create(dai.node.XLinkOut)
dai::Pipeline pipeline;
auto xlinkOut = pipeline.create<dai::node::XLinkOut>();
Inputs and Outputs¶
┌──────────────┐
│ │
input │ │ (to host)
─────────►│ XLinkOut ├------------►
│ │
│ │
└──────────────┘
Message types
input
-Any
Usage¶
pipeline = dai.Pipeline()
xOut = pipeline.create(dai.node.XLinkOut)
xOut.setStreamName("camOut")
# Here we will send camera preview (ImgFrame) to the host via XLink.
# Host can then display the frame to the user
cam.preview.link(xOut.input)
dai::Pipeline pipeline;
auto xOut = pipeline.create<dai::node::XLinkOut>();
xOut->setStreamName("camOut");
// Here we will send camera preview (ImgFrame) to the host via XLink.
// Host can then display the frame to the user
cam->preview.link(xOut->input);
Examples of functionality¶
Reference¶
-
class
depthai.node.
XLinkOut
XLinkOut node. Sends messages over XLink.
-
class
Connection
Connection between an Input and Output
-
class
Id
Node identificator. Unique for every node on a single Pipeline
-
Properties
alias of
depthai.XLinkOutProperties
-
getAssetManager
(*args, **kwargs) Overloaded function.
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
getAssetManager(self: depthai.Node) -> depthai.AssetManager
Get node AssetManager as a const reference
-
getFpsLimit
(self: depthai.node.XLinkOut) → float Get rate limit in messages per second
-
getInputRefs
(*args, **kwargs) Overloaded function.
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
getInputRefs(self: depthai.Node) -> List[depthai.Node.Input]
Retrieves reference to node inputs
-
getInputs
(self: depthai.Node) → List[depthai.Node.Input] Retrieves all nodes inputs
-
getMetadataOnly
(self: depthai.node.XLinkOut) → bool Get whether to transfer only messages attributes and not buffer data
-
getName
(self: depthai.Node) → str Retrieves nodes name
-
getOutputRefs
(*args, **kwargs) Overloaded function.
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
getOutputRefs(self: depthai.Node) -> List[depthai.Node.Output]
Retrieves reference to node outputs
-
getOutputs
(self: depthai.Node) → List[depthai.Node.Output] Retrieves all nodes outputs
-
getParentPipeline
(*args, **kwargs) Overloaded function.
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
getParentPipeline(self: depthai.Node) -> depthai.Pipeline
-
getStreamName
(self: depthai.node.XLinkOut) → str Get stream name
-
property
id
Id of node
-
property
input
Input for any type of messages to be transferred over XLink stream
Default queue is blocking with size 8
-
setFpsLimit
(self: depthai.node.XLinkOut, fpsLimit: float) → None Specifies a message sending limit. It’s approximated from specified rate.
- Parameter
fps
: Approximate rate limit in messages per second
- Parameter
-
setMetadataOnly
(self: depthai.node.XLinkOut, arg0: bool) → None Specify whether to transfer only messages attributes and not buffer data
-
setStreamName
(self: depthai.node.XLinkOut, streamName: str) → None Specifies XLink stream name to use.
The name should not start with double underscores ‘__’, as those are reserved for internal use.
- Parameter
name
: Stream name
- Parameter
-
class
-
class
dai::node
::
XLinkOut
: public dai::NodeCRTP<Node, XLinkOut, XLinkOutProperties>¶ XLinkOut node. Sends messages over XLink.
Public Functions
-
void
setStreamName
(const std::string &name)¶ Specifies XLink stream name to use.
The name should not start with double underscores ‘__’, as those are reserved for internal use.
- Parameters
name
: Stream name
-
void
setFpsLimit
(float fps)¶ Specifies a message sending limit. It’s approximated from specified rate.
- Parameters
fps
: Approximate rate limit in messages per second
-
void
setMetadataOnly
(bool metadataOnly)¶ Specify whether to transfer only messages attributes and not buffer data
-
std::string
getStreamName
() const¶ Get stream name.
-
float
getFpsLimit
() const¶ Get rate limit in messages per second.
-
bool
getMetadataOnly
() const¶ Get whether to transfer only messages attributes and not buffer data.
Public Members
-
Input
input
= {*this, "in", Input::Type::SReceiver, true, 8, true, {{DatatypeEnum::Buffer, true}}}¶ Input for any type of messages to be transferred over XLink stream
Default queue is blocking with size 8
Public Static Attributes
-
static constexpr const char *
NAME
= "XLinkOut"¶
-
void