系统信息
Supported on:RVC2
演示
Command Line
1Ddr used / total - 0.13 / 414.80 MiB
2 Cmx used / total - 2.24 / 2.50 MiB
3 LeonCss heap used / total - 4.17 / 46.41 MiB
4 LeonMss heap used / total - 2.87 / 27.58 MiB
5 Chip temperature - average: 38.59, css: 39.81, mss: 37.71, upa: 38.65, dss: 38.18
6 Cpu usage - Leon CSS: 7.08%, Leon MSS: 1.48 %
7 ----------------------------------------
8 Ddr used / total - 0.13 / 414.80 MiB
9 Cmx used / total - 2.24 / 2.50 MiB
10 LeonCss heap used / total - 4.17 / 46.41 MiB
11 LeonMss heap used / total - 2.87 / 27.58 MiB
12 Chip temperature - average: 38.59, css: 39.58, mss: 37.94, upa: 38.18, dss: 38.65
13 Cpu usage - Leon CSS: 1.55%, Leon MSS: 0.30 %
14 ----------------------------------------
15 Ddr used / total - 0.13 / 414.80 MiB
16 Cmx used / total - 2.24 / 2.50 MiB
17 LeonCss heap used / total - 4.17 / 46.41 MiB
18 LeonMss heap used / total - 2.87 / 27.58 MiB
19 Chip temperature - average: 38.94, css: 40.04, mss: 38.18, upa: 39.35, dss: 38.18
20 Cpu usage - Leon CSS: 0.56%, Leon MSS: 0.06 %
21 ----------------------------------------
22 Ddr used / total - 0.13 / 414.80 MiB
23 Cmx used / total - 2.24 / 2.50 MiB
24 LeonCss heap used / total - 4.17 / 46.41 MiB
25 LeonMss heap used / total - 2.87 / 27.58 MiB
26 Chip temperature - average: 39.46, css: 40.28, mss: 38.88, upa: 39.81, dss: 38.88
27 Cpu usage - Leon CSS: 0.51%, Leon MSS: 0.06 %
28 ----------------------------------------upa代表 SHAVE 块的温度dss代表 DDR 子系统的温度
源代码
Python
Python
1#!/usr/bin/env python3
2
3import depthai as dai
4
5def printSystemInformation(info: dai.SystemInformation):
6 m = 1024 * 1024 # MiB
7 print(f"Ddr used / total - {info.ddrMemoryUsage.used / m:.2f} / {info.ddrMemoryUsage.total / m:.2f} MiB")
8 print(f"Cmx used / total - {info.cmxMemoryUsage.used / m:.2f} / {info.cmxMemoryUsage.total / m:.2f} MiB")
9 print(f"LeonCss heap used / total - {info.leonCssMemoryUsage.used / m:.2f} / {info.leonCssMemoryUsage.total / m:.2f} MiB")
10 print(f"LeonMss heap used / total - {info.leonMssMemoryUsage.used / m:.2f} / {info.leonMssMemoryUsage.total / m:.2f} MiB")
11 t = info.chipTemperature
12 print(f"Chip temperature - average: {t.average:.2f}, css: {t.css:.2f}, mss: {t.mss:.2f}, upa: {t.upa:.2f}, dss: {t.dss:.2f}")
13 print(f"Cpu usage - Leon CSS: {info.leonCssCpuUsage.average * 100:.2f}%, Leon MSS: {info.leonMssCpuUsage.average * 100:.2f} %")
14 print("----------------------------------------")
15
16# Create pipeline
17pipeline = dai.Pipeline()
18
19# Create system logger node
20sysLog = pipeline.create(dai.node.SystemLogger)
21sysLog.setRate(1) # 1 Hz
22
23# Create output
24sysLogQueue = sysLog.out.createOutputQueue(maxSize=4, blocking=False)
25
26# Start pipeline
27pipeline.start()
28while pipeline.isRunning():
29 sysInfo = sysLogQueue.get() # Blocking call, will wait until a new data has arrived
30 printSystemInformation(sysInfo)Pipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。