此页面由 AI 自动翻译。查看英文原版
DepthAI
  • DepthAI 组件
    • AprilTags
    • 基准测试
    • Camera
    • 校准
    • DetectionNetwork
    • Events
    • FeatureTracker
    • Gate
    • HostNodes
    • ImageAlign
    • ImageManip
    • IMU
    • 杂项
    • 模型动物园
    • NeuralDepth
    • NeuralNetwork
    • ObjectTracker
    • 点云
    • RecordReplay
    • RGBD
    • Script
    • SpatialDetectionNetwork
    • SpatialLocationCalculator
    • StereoDepth
    • Sync
    • VideoEncoder
    • Visualizer
    • VSLAM
    • Warp
    • RVC2-specific
  • 高级教程
  • API 参考
  • 工具
软件栈

本页目录

  • Pipeline
  • Source code

Script Simple

Supported on:RVC2RVC4
This example showcases how to setup the Script node.此示例需要 DepthAI v3 API,请参阅 安装说明

Pipeline

Source code

Python

Python
GitHub
1import depthai as dai
2import time
3
4# Create pipeline
5pipeline = dai.Pipeline()
6script = pipeline.create(dai.node.Script)
7inputQueue = script.inputs["in"].createInputQueue()
8outputQueue = script.outputs["out"].createOutputQueue()
9
10
11script.setScript(
12    """
13    while True:
14        message = node.inputs["in"].get()
15        # Or alternatively:
16        # message = node.io["in"].get()
17        node.warn("I received a message!")
18        node.outputs["out"].send(message)
19        # Or alternatively:
20        # node.io["out"].send(message)
21"""
22)
23
24pipeline.start()
25with pipeline:
26    while pipeline.isRunning():
27        message = dai.ImgFrame()
28        print("Sending a message")
29        inputQueue.send(message)
30        output = outputQueue.get()
31        print("Received a message")
32        time.sleep(1)

C++

1#include <atomic>
2#include <chrono>
3#include <csignal>
4#include <iostream>
5#include <memory>
6#include <thread>
7
8#include "depthai/depthai.hpp"
9
10// Global flag for graceful shutdown
11std::atomic<bool> quitEvent(false);
12
13// Signal handler
14void signalHandler(int signum) {
15    quitEvent = true;
16}
17
18int main() {
19    // Set up signal handlers
20    signal(SIGTERM, signalHandler);
21    signal(SIGINT, signalHandler);
22
23    try {
24        // Create pipeline
25        dai::Pipeline pipeline;
26
27        // Create script node
28        auto script = pipeline.create<dai::node::Script>();
29
30        // Set the script content
31        script->setScript(R"(
32            while True:
33                message = node.inputs["in"].get()
34                # Or alternatively:
35                # message = node.io["in"].get()
36                node.warn("I received a message!")
37                node.outputs["out"].send(message)
38                # Or alternatively:
39                # node.io["out"].send(message)
40        )");
41
42        // Create input and output queues
43        auto inputQueue = script->inputs["in"].createInputQueue();
44        auto outputQueue = script->outputs["out"].createOutputQueue();
45
46        // Start pipeline
47        pipeline.start();
48
49        // Main loop
50        while(pipeline.isRunning() && !quitEvent) {
51            // Create and send a message
52            auto message = std::make_shared<dai::ImgFrame>();
53            std::cout << "Sending a message" << std::endl;
54            inputQueue->send(message);
55
56            // Receive the message
57            auto output = outputQueue->get<dai::ImgFrame>();
58            std::cout << "Received a message" << std::endl;
59
60            // Sleep for 1 second
61            std::this_thread::sleep_for(std::chrono::seconds(1));
62        }
63
64        // Cleanup
65        pipeline.stop();
66        pipeline.wait();
67
68    } catch(const std::exception& e) {
69        std::cerr << "Error: " << e.what() << std::endl;
70        return 1;
71    }
72
73    return 0;
74}

需要帮助?

请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。